This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Overview
The following figure (from CSA) illustrates a general network topology and the different device types.
Matter network topology |
---|
A Matter fabric platform is composed of different equipment types:
- Matter end device
- Matter bridge
- Simple Controller
- Simple Thread Border Router
- Combined Controller and Border Router
The STM end devices have been demonstrated with the following platforms:
- STM OTBR
- Raspberry Pi (RPi)
- Google ecosystem (Google Nest Hub 2nd-gen)
- Apple ecosystem (Apple HomePod Mini)
- Samsung ecosystem (…)
The demonstration procedure is described below for each of those platforms
The STM32WB5MM-DK end device platform with lighting up application has been tested/demonstrated with the STM32MP1 border router and ecosystem of a couple of major Matter players. The operation mode for each ecosystem is presented in the following section.
For all ecosystems, the Matter network will be composed of the following elements:
- 1 x STM32WB5MM-DK board as end device that has been flashed with relevant firmware binaries
- 1 x OpenThread border router
- 1 x Smartphone with the ecosystem associated application installed as a Matter commissioner/controller device
- 1 x Wi-Fi access point
2. STM ecosystem
3. Raspberry Pi ecosystem
4. Google ecosystem
5. Apple ecosystem
6. Samsung ecosystem
7. Multi-fabric
[[Category:Matter|30]]