This article shows how to run FP-AI-VISION1 function pack projects on STM32H747I-DISCO kits by using the People Counting demo as an example. For STM32H747I-DISCO kits shipped with MB1166-A09 LCD daughterboards, an additional step to update drivers is also described. Further, if you only get static on the LCD as shown below, this article may be helpful.
1. Prerequisites
1.1. Hardware
- A Micro-USB to USB cable
- B-CAMS-OMV
- STM32H747I-DISCO board with LCD daughterboard
1.2. Software
- STM32Cube IDE v1.13.1 or higher
- FP-AI-VISION1 function pack v3.1.0
2. Hardware Setup
Connect B-CAMS-OMV camera to STM32H747I-DISCO using the Flexible Flat Cable (FFC). Ensure that the FFC is securely attached to both the ZIF connectors, and that the orientation is as shown in the image below (highlighted in yellow).
Next, attach the USB cable to the USB port labelled as "STLINK-V3E", as shown in the image below (highlighted in blue).
3. Import Project
If the goal is to run the project on STM32H747I-DISCO without any modifications, you can simply drag-and-drop the file "..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\PeopleCounting\Binary\STM32H747I-DISCO_PeopleCounting_Quant8_IntFps_IntFlash_V310.bin"
on to the STM32H747I-DISCO mass storage device, which shows up on connecting the UBS cable to the STLINKV3 USB port, as shown in the hardware setup above.
3.1. Process
The project can be imported into STM32CubeIDE by simply opening the .project file located at ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\PeopleCounting\STM32CubeIDE\.project
by following the steps below:
- Double click the .project file
- STM32CubeIDE will prompt for workspace directory, as shown below. Select an appropriate location and press Launch.
STM32CubeIDE will prompt once the project has been successfully imported. Press OK to proceed. - You will now see the project under the Project Explorer.
3.2. Directory Overview
This project is being deployed on the STM32H747XI MCU which is a dual-core Arm® Cortex®-M7 and Cortex®-M4 MCU. In this project, we only use the M7 core and therefore we will only be working with the CM7 directory. This directory contains the source code specific to the People Counting project. Detailed information about the organization of this directory is available in Section 3.2 of UM2611: Artificial Intelligence (AI) and computer vision function pack for STM32H7 microcontrollers.
4. Update Drivers (Required only if using MB1166-A09)
Drivers for LCD daughterboard MB1166-A09 (pictured below) are currently not included in the FP-AI-VISION1 function pack. In order to deploy the project on STM32H747I-DISCO kits with MB1166-A09 LCD, follow the steps below to install the drivers.
- Download drivers from the (1) STM32CubeH7 GitHub repo by clicking on (2) "Code", and then (3)"Download ZIP", as shown in the image below.
- Extract the contents of
STM32CubeH7-master.zip
to a local directory. - Copy directory
..\STM32CubeH7-master\Drivers\BSP\Components\nt35510
to..\FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\
- Copy files
..\STM32CubeH7-master\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.c
and..\STM32CubeH7-master\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.h
, and paste both files into..\FP-AI-VISION1_V3.1.0\Drivers\BSP\STM32H747I-Discovery\
directory - Use a text editor to open
..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\Common\CM7\Inc\stm32h747i_discovery_conf.h
. On line 34, add a #define for NT35510, and change the OTM8009A #define to 0, as follows:/* LCD controllers defines */ #define USE_LCD_CTRL_NT35510 1U #define USE_LCD_CTRL_OTM8009A 0U #define USE_LCD_CTRL_ADV7533 0U
- From the
FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\nt35510
directory, select the four source files as shown in the image below, and drag and drop the selected files to the components directory in STM32CubeIDE.
- Then in the pop-up window, keep “Link to files” and click OK.
- Drivers should now be indexed into the project
- Then in the pop-up window, keep “Link to files” and click OK.
5. Build & Flash
Right click the project, then (1) Clean and (2) Build the project. The project should build without errors. Now you can click the (3) Run icon to flash and execute the project.
Once execution starts, the screen will display a live output from the camera along with the number of people detected in the frame, as shown below.
6. References
Vision Pack Video Application Notes
UM2611: Artificial Intelligence (AI) and computer vision function pack for STM32H7 microcontrollers