This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
![]() |
Coming soon |
1. Introduction
The STM32CubeWBA firmware provides Real Time debug capabilities. The RTDebug module is GPIO based for a minimal impact on real time timings. The module is present, by default, into the application framework.
While enabling the RTDebug module in the application, the user can choose among a various list of signals the ones it wants to monitor and what GPIO is assigned to each activated debug signal.
2. Concepts
2.1. RTDebug general overview
The main objectives of the RTDebug system module is to provide a GPIO probing solution:
- with accurate timings.
- that is not disturbing real time nor modifying critical executions.
- easy to configure (debug signal selection and GPIO assignation).
- with low footprint, both memory and execution time.
Regarding these objectives, the RTDebug module is configured at compile time. Only the necessary code is compiled, according to the user configuration.
2.2. Debug tables mechanism
2.3. RTDebug module configuration
2.4. Default GPIO assignation
3. Interfaces
TBD.
4. How to
TBD.