How to perform people counting using FP-AI-VISION1 and STM32H747XI

Revision as of 23:10, 7 November 2023 by Registered User

This article shows how to run FP-AI-VISION1 function pack projects on STM32H747I-DISCO kits by using the People Counting demo as an example. For STM32H747I-DISCO kits shipped with MB1166-A09 LCD daughterboards, an additional step to update drivers is also described. Further, if you only get static on the LCD as shown below, this article may be helpful.

1. Prerequisites

1.1. Hardware

1.2. Software


2. Hardware Setup

Connect B-CAMS-OMV camera to STM32H747I-DISCO using the Flexible Flat Cable (FFC). Ensure that the FFC is securely attached to both the ZIF connectors, and that the orientation is as shown in the image below (highlighted in yellow).

Next, attach the USB cable to the USB port labelled as "STLINK-V3E", as shown in the image below (highlighted in blue).


3. Import Project

3.1. Process

The project can be imported into STM32CubeIDE by simply opening the .project file located at ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\PeopleCounting\STM32CubeIDE\.project by following the steps below:

  1. Double click the .project file
  2. STM32CubeIDE will prompt for workspace directory, as shown below. Select an appropriate location and press Launch. STM32CubeIDE will prompt once the project has been successfully imported. Press OK to proceed.
  3. You will now see the project under the Project Explorer.

3.2. Directory Overview

Since this project is being deployed on the STM32H747XI MCU which has an Arm® Cortex®-M7 core, we will only be working with the CM7 directory. This directory contains the source code specific to the People Counting project. Detailed information about the organization of this directory is available in Section 3.2 of UM2611: Artificial Intelligence (AI) and computer vision function pack for STM32H7 microcontrollers.


4. Update Drivers (Required only if using MB1166-A09)

If the LCD daughterboard is the MB1166-A09 revision, as shown below, then follow these steps to update the drivers.

  1. Download drivers from the (1) STM32CubeH7 GitHub repo by clicking on (2) "Code", and then (3)"Download ZIP", as shown in the image below.
  2. Extract the contents of STM32CubeH7-master.zip to a local directory.
  3. Copy ..\STM32CubeH7-master\Drivers\BSP\Components\nt35510 directory to ..\FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\
  4. Copy ..\STM32CubeH7-master\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.c and ..\STM32CubeH7-master\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.h, and paste both into ..\FP-AI-VISION1_V3.1.0\Drivers\BSP\STM32H747I-Discovery\
  5. Use a text editor to open ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\Common\CM7\Inc\stm32h747i_discovery_conf.h. On line 34, add a #define for NT35510, and change the OTM8009A #define to 0, as follows:
    /* LCD controllers defines */ 
    #define USE_LCD_CTRL_NT35510                1U 
    #define USE_LCD_CTRL_OTM8009A               0U 
    #define USE_LCD_CTRL_ADV7533                0U
    
  6. From the FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\nt35510 directory, select the four source files as shown in the image below, and drag and drop the selected files to the components directory in STM32CubeIDE.
    Then in the pop-up window, keep “Link to files” and click OK.
    Drivers should now be indexed into the project

5. Build & Flash

Right click the project, then (1) Clean and (2) Build the project. The project should build without errors. Now you can click the (3) Run icon to flash and execute the project.

Once the execution starts, the screen will display a live output from the camera along with the number of people detected in the frame, as shown below.


6. References

Vision Pack Video Application Notes

UM2611: Artificial Intelligence (AI) and computer vision function pack for STM32H7 microcontrollers