STM32WB-WBA BLE security - OOB via NFC

Under construction.png Coming soon

1. Bluetooth® Low Energy Security - Out of Band Pairing method

The Out of Band (OOB) [1] mechanism is used to both discover the devices as well as to exchange or transfer cryptographic numbers used in the pairing process. It needs to be effective from a security point of view and should be resistant to Man In The Middle (MITM) attacks.

For LE Secure Connection Pairing, if Out Of Band pairing method is used, the public keys, nonce and confirmation values are all exchanged via a different technology than Bluetooth® Low Energy such as NFC or UART.

For LE Legacy Pairing, if Out Of Band pairing method is used, the TK is exchanged using a different wireless technology such as NFC or UART. The main advantage to this method is that a very large TK can be used, up to 128 bits.

Two commands are specific to OOB method , to get and set the OOB data:

  • ACI_GAP_SET_OOB_DATA which allow to generate OOB data or to set OOB data from peer device received via OOB communication. To generate the OOB data, all the parameters need to be set to zero
ACI_GAP_SET_OOB_DATA command - Input parameters
Connectivity aci gap set oob data input param.png


ACI_GAP_SET_OOB_DATA command - Output parameters
Connectivity aci gap set oob data output param.png


  • ACI_GAP_GET_OOB_DATA which allow to get the (i.e. to extract from the Stack) the OOB data generated by the Stack itself.
ACI_GAP_GET_OOB_DATA command - Input parameters
Connectivity aci gap get oob data input param.png


ACI_GAP_GET_OOB_DATA command - Output parameters
Connectivity aci gap get oob data output param.png


During the phase 1 of pairing procedure, e.g Pairing Feature Exchange, the devices exchange their capabilities using pairing request/response. The frame of these messages contain one field of 1 byte named "OOB Data Flag" which indicate if OOB Authentication data are present or not.
For the definition of “OOB Data Flag”, refer to the table below:

OOB Data Flag Description
Connectivity OOB Data Flag.png


2. OOB in LE Secure Connection Pairing

In the following description, it is considered the case where a smartphone connects a STM32WB-WBA and STM32WB-WBA provides OOB data

2.1. Commands sequence for pairing initialization, public key generation, generation and recovery of OOB data on WB-WBA

Sequence to be done in Ble_Hci_Gap_Gatt_Init function (in app_ble.c)

/* Initialize IO capability */
aci_gap_set_io_capability(0x00-display only)

/* Initialize authentication */
aci_gap_set_authentication_requirement(0x01- bonding, 0x00-no MITM, SC_Support=0x01, 0x00-fixed pin, 0x00000000-fixed pin value)

/* Sequence to force the regeneration of the EDCH_public key on OOB source device */
uint8_t ALL_EVENTS[8]={0xDF,0x18,0x03,0x00,0x00,0x00,0x00,0x00};
hci_le_set_event_mask(ALL_EVENTS);

/* generation of a new P-256 public key */
Hci_le_read_local_p256_public_key()

/* Reception of META EVENT */
HCI_LE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_EVENT

/* OOB data generation */
Aci_gap_set_oob_data(device_type=0x00, Address_type=0x00, address=0x00, oob_data_type=0, oob_data_len=0, oob_data=0)

/* OOB data recovery */
Aci_gap_get_oob_data(oob_data_type=0x01-random)
Aci_gap_get_oob_data(oob_data_type=0x02-confirm)

Each part of the previous sequence is detailed in the following section.

2.2. Pairing initialization commands on peripheral side

Pre-requisite before pairing request: initialization of pairing conditions with 2 commands:

aci_gap_set_io_capability(0x00-display only)
aci_gap_set_authentication_requirement(0x01- bonding, 0x00-no MITM, SC_Support=0x01, 0x00-fixed pin, 0x00000000-fixed pin value)

2.3. Public Key generation

The peripheral is the device where the OOB data will be extracted. The central is the device where OOB data will be set.

Following sequence is done before the connection:

On peripheral side:
Sequence to force the regeneration of the EDCH_public key on source device
First action: set LE Event Mask to require which LE events are generated by the HCI for the host.

hci_le_set_event_mask command is used to control which LE events are generated by the HCI for the Host.
Default value of this event mask is 0x000000000003185F. Refer to hci_le_set_event_mask command description.
To receive LE Read Local P-256 Public Key Complete Event, bitmask 0x80 is needed.
The new mask value is 0x00000000000318DF.

uint8_t ALL_EVENTS[8]={0xDF,0x18,0x03,0x00,0x00,0x00,0x00,0x00};
hci_le_set_event_mask(ALL_EVENTS);

Second action: generation of a new P-256 public key (first action necessary to receive the event)

Hci_le_read_local_p256_public_key()

HCI_LE_META_EVENT event received :

HCI_LE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_EVENT

contains Local_P256_Public_Key field.

2.4. OOB data generation

Command used to generate OOB data on device data source:

Aci_gap_set_oob_data(device_type=0x00, Address_type=0x00, address=0x00, oob_data_type=0, oob_data_len=0, oob_data=0)

Previous command is sent with all data equal to zero.

2.5. OOB data recovery

For SC secure pairing:
Two commands used to recover the generated OOB data on device data source
First command:

Aci_gap_get_oob_data(oob_data_type=0x01-random)

HCI_COMMAND_COMPLETE_EVENT event received, contains following fields:
address_type
address
OOB_data_type 0x01 (Random SC)
OOB_data_length
OOB_data : RANDOM_DATA – local pairing data intended to the remote device to be sent via NFC

Second command:

Aci_gap_get_oob_data(oob_data_type=0x02-confirm)

HCI_COMMAND_COMPLETE_EVENT event received, contains following fields:
address_type
address
OOB_data_type 0x02 (Confirm SC)
OOB_data_length
OOB_data : CONFIRM_DATA – local pairing data intended to the remote device to be sent via NFC

RANDOM_DATA and CONFIRM_DATA generated by the BLE stack are written to ST25 (NFC shield).

2.6. OOB data written into NFC shield

Code example

Ndef_Bluetooth_OOB_t NdefBle = { 


                                    .LeOptionalMask = (NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_LE_SECURE_CONNECTIONS_CONFIRMATION_VALUE) |
                                                       NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_LE_SECURE_CONNECTIONS_RANDOM_VALUE)),

                                    .LocalName = "ST25OOB",
                                    .OptionalMask = NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_COMPLETE_LOCAL_NAME),

                                    .Type = NDEF_BLUETOOTH_BLE,
                                    .Role = NDEF_BLE_ROLE_PERIPH_ONLY,
                                    .DeviceAddressType = NDEF_BLE_PUBLIC_ADDRESS_TYPE

                                  };


  for(int i = 5; i >= 0; i --)
    NdefBle.DeviceAddress[i] = bd_addr[5-i];

   status = aci_gap_get_oob_data(1, &at,add,&len, rand);
   status = aci_gap_get_oob_data(2, &at,add,&len, hash);

  for(int i = 5; i >= 0; i --)
    NdefBle.DeviceAddress[i] = add[5-i];
  for(int i = 15; i >= 0; i --)
  {
    NdefBle.SimplePairingRandomizer[i] = rand[15-i];
    NdefBle.SimplePairingHash[i] = hash[15-i];
  }
   NfcTag_SelectProtocol(NFCTAG_TYPE5);

   NFC04A1_NFCTAG_Init(0);
   NDEF_ClearNDEF();
   NDEF_AppendBluetoothOOB(&NdefBle, NULL);

2.7. Transfer of OOB data through NFC

  • RANDOM_DATA = rb
  • CONFIRM_DATA = Cb
Random data and Confirm Data transferred through NFC


3. Bluetooth® Low Energy (BLE) pairing with Secure Connection Encryption

3.1. Example of OOB data transfer in Secure Connection - central generates OOB data

OOB pairing sequence
Connectivity OOB SC.png


Example available under ST github: Client application [2] and Server application [3].

4. OOB in LE Legacy Pairing

In the following description, it is considered the case where two WBs are connected and exchange OOB data via UART.
Both devices MUST set their OOB data flag if they want to use OOB for pairing.
In case of LE Legacy Pairing, only one device generates the TK, the both are using the same TK.


4.1. Commands sequence for pairing initialization, generation and recovery of OOB data on WB/WBA

Sequence to be done in Ble_Hci_Gap_Gatt_Init function (in app_ble.c)

/* Initialize IO capability */
aci_gap_set_io_capability(0x00-display only)

/* Initialize authentication */
aci_gap_set_authentication_requirement(0x01- bonding, 0x00-no MITM, SC_Support=0x01, 0x00-fixed pin, 0x00000000-fixed pin value)

/* OOB data generation */
Aci_gap_set_oob_data(device_type=0x00, Address_type=0x00, address=0x00, oob_data_type=0, oob_data_len=0, oob_data=0)

/* OOB data recovery */
Aci_gap_get_oob_data(oob_data_type=0x00-TK)

4.2. Example of OOB data transfer in Legacy Pairing - central generates OOB data

OOB pairing sequence
Connectivity OOB Legacy.png


Example available under ST github: Client application [4] and Server application [5].

5. ST example : STM32WB55 + NFC04A1 and Android smartphone

ST solution ST25DV-I2C Bluetooth® Low Energy out of band pairing solution[6] is presented on st.com.
A user manual[7] is also available describing the demonstration and a video[8] presents the demonstration.

5.1. References