1. Introduction
The STM32H5 series provides a trusted execution environment security framework: the Secure Manager. It simplifies the security development cycle of embedded applications, by providing ready-to-use security services that are developed according to best practices.
The OEM can choose to develop its application with or without the Secure Manager.
It has an impact on the SFI procedure.
On the STM32H5 series, there are 2 SFI procedures:
2. SFI for STM32H5 series with Secure Manager
This procedure must be used when the OEM wants to install an application that was developed with the Secure Manager. In this case, there are several additional components to prepare, to test and to install.
Here is an overview of the preparation and installation flow:
ST provides the SFI solution to perform the preparation and installation flows.
2.1. Preparation flow
2.1.1. Overview
The purpose of this step is to:
- prepare the encrypted firmware image to install (called SFI image). It is composed of the OEM application and additional components: OEM secrets, Secure Manager and modules.
- provision the OEM key within an HSM or within a global license.
2.1.2. SFI image
2.1.2.1. Overview
Here is an overview of the SFI image creation flow.
2.1.2.2. SFI image generation
Once the OEM application has been developed with the SMAK, the OEM must prepare and test the SFI image to be installed in manufacturing.
For that purpose, the OEM must use the SMAK in production preparation phase. This allows to correctly generate the SFI image (for instance, setting the Secure Manager configuration according to the OEM application) and test it before manufacturing.
The output of the SMAK production preparation phase is the tested SFI image, ready to be installed in manufacturing.
2.1.2.3. Description of the SFI image inputs
The OEM must provide the following inputs:
- the OEM application
- the Secure Manager
- the modules
- the OEM secrets
The sections below provide further details regarding the inputs.
2.1.2.3.1. OEM application
The OEM must provide its application binary, developed with the Secure Manager.
2.1.2.3.2. Secure Manager
The Secure Manager binary is available as an encrypted image from STM32TRUSTEE-SM[1].
2.1.2.3.3. Modules
The Secure Manager offers the possibility to install secure modules.However, the Secure Manager requires these modules to have an specific format. Only SMDK provides this format.
The modules must be developed via the SMDK.
2.1.2.3.4. OEM secrets
The OEM secrets are the OEM data, the OEM keys and also the Secure Manager OEM configuration.
The OEM secrets are described in detail in the Secure Manager configuration.
During the SFI procedure, the OEM must set its secrets and must especially pay attention of the following secrets:
- Factory Internal Trusted Storage (ITS)
- The OEM can change the factory ITS blob default content to include its own keys and data.
- Secure Manager keys
- The OEM must update the default Secure Manager keys and use their own keys.
- Secure Modules configuration
- The OEM must set the license type for each module (no license, global license or chip specific license).
- The OEM must set the licensed modules installation model (same model for all licensed modules).
- The OEM must set the secure SRAM size used by the modules (one secure SRAM area shared between all the modules).
- Option Bytes
- The OEM must set carefully the Product state.
2.1.2.4. SFI image output description
The Trusted Package Creator encrypts the SFI images inputs with the OEM key and generates a SFI image.
The SFI image is then an encrypted image containing the Secure Manager, the OEM application, the OEM secrets and the modules.
2.1.3. OEM key provisioning
The OEM must provide its OEM key to the CM manufacturing in a way the OEM key cannot be read or extracted clearly by the CM manufacturing. Only STM32 can handle the OEM key.
In SFI for STM32H5 with Secure Manager, there are 2 ways to provide the OEM key to the CM manufacturing:
- either the OEM provisions (via the Trusted Package Creator) its OEM key in a HSM, or
- the OEM provisions (via the Trusted Package Creator) its OEM key within a global license file
Then:
- Only STMicroelectronics STM32 microcontrollers can securely install the SFI image.
- Authenticity, integrity, and confidentiality of the SFI image content is ensured
Using HSM allows to count the number of STM32 chips to program.
NOTE: The global license is not available in SFI for STM32H5 without Secure Manager.
2.2. Installation flow
There is one additional input compared to other platforms: the module license information file.
This file indicates if the module to install is licensed or not.
In case the module is licensed, the file either gives the module global license file path or the file indicates the HSM slot ID (HSM card provisioned with the module secret key and initialized with a max counter of licenses), in case of module chip specific license.
The installation procedure is similar to generic SFI installation procedure deployed on other STM32 product when SFI is supported.
2.3. Step by Step SFI procedure
Follow How to start SFI on STM32H5 with Secure Manager to run a SFI procedure on STM32H5 with Secure Manager.
3. SFI for STM32H5 without Secure Manager
This procedure shall be used when the OEM wants to installed its application developed without the Secure Manager.
In this case, the SFI procedure on the STM32H5 series is similar to the SFI procedure applied on other platforms.
Follow SFI Step-by-step on STM32 boards to run an SFI procedure on STM32H5 without Secure Manager.