This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Overview
The package for Matter device over Thread® shows several Matter end device sample applications. These examples are based on Matter and behave as Matter accessories communicating over an 802.15.4 Thread network. Every Matter end device can interact with other devices within the scope of a fabric.
System presentation |
---|
2. Boards needed
- as Matter accessory, P-NUCLEO-WB55 or STM32WB5MM-DK:
- as Thread RCP firmware, P-NUCLEO-WB55 ST radio coprocessor (RCP) if used:
3. Package content
You can download the necessary files from Github.
This Hotspot firmware package includes two application examples, lighting and window covering. Both examples are delivered for P-NUCLEO-WB55 and STM32WB5MM-DK.
For any other question related to the product, the hardware performance or characteristics, the tools, and the environment, you can submit it to the ST Community on the STM32 MCUs related page.