Introduction to Matter

Revision as of 15:23, 18 July 2023 by Registered User

1. Introduction

Matter is a new smart home protocol that allows different devices to work together easily, regardless of the manufacturer. It's designed to simplify the smart home experience and maintaining security and privacy.

One of the favors of Matter is that it's an open standard, which means that any device manufacturer can use it. Matter is an initiative of the Connectivity Standards Alliance (CSA), and developed through collaboration amongst all the leaders of the IoT industry.

2. Device Roles in Matter Network

Smart homes utilize either Wi-Fi or Thread technologies to operate connected devices. Each device has a distinct role within the Matter network.

Matter Nettwork
Connectivity matter overview.png
  • End devices are connected objects serving a final application like thermostats, light bulbs, door locks, and other smart home devices that can be controlled through a smart home platform. .
  • Router/Bridges are devices that serve as intermediaries between end devices and the network's central hub. Routers are devices that connect multiple end devices to the network, allowing them to communicate with each other and with the central hub. Bridges, on the other hand, are devices that enable communication between devices that use different communication protocols. For example, a bridge can enable a device that uses Wi-Fi to communicate with a device that uses Thread.
  • Controllers are devices such as smartphones or tablets used to commission an end device into a Matter network through Bluetooth® Low Energy. Controllers are devices that serve as the central hub for the smart home network.
Matter Stack Overview
Connectivity Matter Stack overview.png

3. References


No categories assignedEdit