1. Introduction
- Debug authentication controls
- Debug opening : Re-open Debug Access on the STM32 in a secured way.
- Regressions : Perform regression to product states OPEN or TZ-CLOSED in a secured way, erasing user data in user Flash, SRAM and OBKeys.
- It can be used
- During development
- During manufacturing
- For field return analysis
- Debug Authentication is only useful when STM32 is no more in product state OPEN
Refer to STM32 Product State Life cycle to learn more about product state lifecycle
- Features
- When TZ disabled: usage of a password (very similar to U5). Only regression possible
- When TZ enabled: usage of cryptography (certificates). Regressions and debug opening
- Debug Authentication principle
- Uses JTAG dedicated access point (ap0) to communicate with the chip
- Secure protocol defined by ARM : ARM PSA ADAC V1.0. (Authenticated Debug Access Control)[1]
2. Debug Authentication for STM32H5 devices
STM32H5 Serie devices have different behaviors that make the use of Debug Authentication special for each of them.
2.1. OBKey area
- STM32H563/573 have OBKey areas that can be use to store keys/ paswords.
- STM32H503 devices don't have OBKey area and use OTP (One Time programming) area to store password. That means that password can't be change anymore once provisioned.
2.2. TrustZone feature
Debug Authentication usage is different depending on the acivation of the TrustZone feature.
- If TrustZone is activated on a device (a code secure and / or non-secure is flashed on the board) a regression/ Debug re-opening from a product state different than "OPEN" can be done using a certificate.
In this case a partial regression (to TZ-CLOSED state) or a full regression (to OPEN state) are possible.
- If TrustZone is not enabled on a device the usage of Debug Authentication can be done only with password.
Only Full regression to OPEN state is possible.
For STM32H503 devices TrustZone can't be activated and password method is always used to perform Debug Authentication.
If you want to learn more about Debug Authentication specific usage for each STM32H5 device, and that you wan't to practice, please refer to [Authentication STM32H5 How to Introduction]