STiROT Overview
STiROT states for Immutable (unchangeable) Root Of Trust and acts as a first boot stage.
This is a ROM code developed by ST, SESIP 3 certified and stored in the STM32 System Flash
The STiROT is embedded in all STM32H57x devices.
Since the STiROT is requiring hardware cryptographic features, it is not supported on STM32H6x and STM32H503 products.
To use STiROT the TrustZone needs to be activated.
The services provided by the STiROT and the different user application use cases will be described in following sections.
STiROT overview article is available at following link
1. STiROT services
The STiROT provides two services
- 1) The Secure Boot (Root of Trust Services):
- It is an immutable code, always executed after a system reset, that activates STM32 runtime protections and verifies the authenticity and integrity of the application code before every execution.
- Integrity: to ensure that a firmware that is going to be executed has not been corrupted or maliciously modified.
- Authenticity: to verify that a firmware is coming from a trusted and known source in order to prevent unauthorized entities to install and execute code.
- Integrity: to ensure that a firmware that is going to be executed has not been corrupted or maliciously modified.
- It is an immutable code, always executed after a system reset, that activates STM32 runtime protections and verifies the authenticity and integrity of the application code before every execution.
- 2) The Secure Firmware Update:
- It is an immutable code that detects if a new firmware image is available, checks its authenticity and verifies the integrity of the code before installing it after decryption.
2. STiROT use cases
There are two possible cases explained below.
- Case 1: The user application is executed after the STiROT (1 boot stage)
- It is the use case explained in the How_to_start_with_ST-iROT article, for a full secure user application.
- The STiROT application is the first application executed after any reset. STiROT application is executed in temporal isolation 1 (HDPL1) (refer to Introduction_to_Silicon_device_life_cycle article)
- The STiROT application is the first application executed after any reset. STiROT application is executed in temporal isolation 1 (HDPL1) (refer to Introduction_to_Silicon_device_life_cycle article)
- The following figure gives an example of the memory mapping when STiROT is activated in a 1 boot stage configuration.
- It shows the user application and data download areas for the different images and the user application location once installed (explained in following sections).
- The entry point after reset is also indicated.
- The following figure gives an example of the memory mapping when STiROT is activated in a 1 boot stage configuration.
- After a successful verification of the user application (integrity and authenticity), the STiROT executes the user application in temporal isolation level 2 (HDPL2) and in secure mode.
- At least the vector table and the reset handler must be in the secure area part.
- After a successful verification of the user application (integrity and authenticity), the STiROT executes the user application in temporal isolation level 2 (HDPL2) and in secure mode.
- To avoid any risk of attack, the MPU is configured to ensure that only the user application is allowed to be executed.
- It is the user application responsibility to update and adapt the MPU configuration to its needs.
- The user application can for instance move to temporal isolation level 3 (HDPL3) and/or switch in non-secure mode.
- The data image management is optional. During the STiROT configuration it can be chosen to activate it or not.
- The data can be for instances used to store keys or any other secret information needed by the user.
- In case there is a verification failure of the user application code, the STiROT will execute the embedded Bootloader (refer to AN2606) to download a new user app code and/or data.
- A verification failure means that the user application code has been altered and is not safe anymore to be executed. For instance, following a hardware attack of the user flash.
- In case there is a verification failure of the user application code, the STiROT will execute the embedded Bootloader (refer to AN2606) to download a new user app code and/or data.
- Case 2: The updatable Root of Trust (uROT) is executed after the STiROT (2 boot stage)
- The uROT is located in the user flash and will act as a second boot stage adapted by the user for his own requirements.
- The following figure shows the entry point after reset and the STiROT controlling the step to uROT.
- The uROT is located in the user flash and will act as a second boot stage adapted by the user for his own requirements.
- The STiROT application is the first application executed after any reset (STiROT application is executed in temporal isolation level 1 (HDPL1) (refer to Introduction_to_Silicon_device_life_cycle article).
- The STiROT application is the first application executed after any reset (STiROT application is executed in temporal isolation level 1 (HDPL1) (refer to Introduction_to_Silicon_device_life_cycle article).
- After a successful verification (integrity and authenticity) of the uRoT, the STiRoT executes the uRoT in temporal isolation level 2 (HDPL2) and in secure mode.
- After a successful verification (integrity and authenticity) of the uRoT, the STiRoT executes the uRoT in temporal isolation level 2 (HDPL2) and in secure mode.
- The uRoT will then execute the secure user application (S-User app) after a successful verification in temporal isolation level 3 (HDPL3) and in secure mode.
- The uRoT will then execute the secure user application (S-User app) after a successful verification in temporal isolation level 3 (HDPL3) and in secure mode.
- In case there is a verification failure of the uROT application, the STiROT will execute the embedded Bootloader (refer to AN2606) in order to download a new uRoT code and/or data.
- A verification failure means that the uROT code has been altered and is not anymore safe to be executed. For instance after a hardware attack of the user flash.
- In case there is a verification failure of the uROT application, the STiROT will execute the embedded Bootloader (refer to AN2606) in order to download a new uRoT code and/or data.
3. STiROT configuration
The possible configuration options are described in the STiROT configuration detailed table.
The STiROT configuration options used by default are listed below. (used in the STM32CUbeFW examples).
- User application images:
- One image: user application code image.
- Two images: one user application code image & one user application data images
- One image: user application code image.
- User application secure and non-secure:
- User application full secure.
- User application secure & user application non-secure.
- User application full secure.
- User application image and execution:
- Flash location and size reserved for code image download.
- Flash location and size reserved for user application installation.
- Flash location and size reserved for code image download.
- User data image:
- Flash location and size reserved for data image download.
- Flash location and size reserved for decrypted user data.
- Flash location and size reserved for data image download.
- Encryption and authentication key location (only ECDSA256 supported)
- Minimal product state:
- STiROT will execute the firmware only if the product state is equal or greater than the "Product state minimal allowed".
- STiROT will execute the firmware only if the product state is equal or greater than the "Product state minimal allowed".
- User application images:
- All the configurations can be chosen by directly editing this STiROT_Config.xml file or graphically using STM32TrustedPackageCreator.
- Default configuration parameters are visible in TrustedPackageCreator.
- Hidden parameters can be made visible by edditing the "Hidden" value in the STiROT_Config.xml file.
- Two keys are provisioned: a key for the authentication and a key for the file encryption.
- Default keys are provided in the STM32Cube_FW but can be regenerated using STM32TrustedPackageCreator. (see How_to_start_with_ST-iROT article).
- All the configurations can be chosen by directly editing this STiROT_Config.xml file or graphically using STM32TrustedPackageCreator.
When the STiROT configuration file (STiROT_Config.xml) is ready, based on this file the STM32TrustedPackageCreator is used to generate the file needed for the device provisioning (STiROT_Config.obk).
A script (Provisioning.bat) provided in the STM32Cube_FW, is guiding the user during the configuration definition and device programming.
The provisioning section describes how the defined STiROT configuration is programmed into the device.
4. Debug Authentication configuration
Explanations about the Debug Authentication (DA) are available in the Introduction_to_Debug_Authentication_for_STM32H5_MCUs article.
The DA configuration is an important step defining the location of the root key, the regression and debug opening permissions for the owner of the root key and root certificate.
These permissions are stored in what is called the SOC_MASK and is programmed into de device during the provisioning step explained in next section.
More explanations and how to practically define the DA configuration is explained in the How_to_start_with_ST-iROT article.
- In summary
- The Debug Authentication is configured using the DA_Config.xml file. (STM32Cube_FW_H5_Vx.x.x\Projects\STM32H573I-DK\ROT_Provisioning\DA\Config)
- This xml file can be directly edited or graphically using STM32TrustedPackageCreator.
- A default root key is provided in the STM32Cube_FW. A new key can be generated using STM32TrustedPackageCreator.
- The permission mask for the debug opening is set using STM32TrustedPackageCreator.
- The DA_Config.obk file is generated using STM32TrustedPackageCreator. This file is used during the device provisioning.
- The Debug Authentication is configured using the DA_Config.xml file. (STM32Cube_FW_H5_Vx.x.x\Projects\STM32H573I-DK\ROT_Provisioning\DA\Config)
- Note: for a commercial product, it is important to regenerate the debug authentication root key (key_1_root.pem), since the key provided in the STM32CubeFW is public.
5. STiROT and DA provisioning
When the STiROT and the DA configurations are defined it will be programmed on the device through the provisioning procedure.
The figure below gives an overview of the provisioning and the needed input files.
- The figure above shows the steps (1 and 2) described in previous sections and the related OBK configuration files generated through STM32TrustedPackageCreator (STiROT_Config.obk and DA_Config.obk)
- The STiROT_Config.obk configuration file is used during the provisioning to store the STiROT configuration in the OB key level1 secure storage of the device.
- The DA_Config.obk configuration file is used during the provisioning to store the Debug Authentication configuration in the OB key secure storage of the device.
- The STiROT_Data.obk file contains some working data, for instance the installed firmware version. For the provisioning it should be initialized with "zero" values. This file is provided in the STM32CubeFW.
- The option bytes defined during the STiROT configuration are programmed during the provisioning.
- Note: option bytes configuration such as SECWM, SRAM2_RST, SRAM2_ECC are extracted from STiROT configuration. Others option bytes such as TZ_EN, SECBOOT_LOCK are configured with a fixed value.
- Note: In order to mitigate the risk of attack, some major information are duplicated between option bytes and Obkeys configuration such as sram2_ecc, sram2_rst, secure watermark, product_state. (see also appendix STiROT_Configuration_detailed_description table)
How to practically perform the provisioning is explained in the How_to_start_with_ST-iROT article.
Using the provisioning script this operation is straightforward (Provisioning.bat, provided in the STM32Cube_FW_H5_Vx.x.x\Projects\STM32H573I-DK\ROT_Provisioning\STiROT).
- This script is performing the following steps:
- Program the option bytes on the device.
- Configure the STiROT and DA on the device.
- And the two steps explained in the next sections.
- Install the code and data images.
- Set the final chosen product state.
- This script is performing the following steps:
6. Firmware code and data images generation
The signed and encrypted user application code image and user data image are generated with STM32TrustedPackageCreator.
The user data image management can be activated or not during the STiROT configuration.
6.1. User application code image generation
The following figure gives an overview of the user application code image generation.
To be installed successfully by the STiROT (see next chapter) this image needs to be encrypted, signed and aligned with the flash memory map config, as described in this section.
The user application code binary file can be generated by any IDE.
With IAR Embedded Workbench IDE the STM32TrustedPackageCreator is launched automatically through the postbuild command (see How_to_start_with_ST-iROT article). In this case the encrypted and signed image creation is done automatically during the user application compilation.
STM32TrustedPackageCreator can be launched separately to generate the encrypted and signed image file using the same encryption and authenticity keys provisioned during the STiROT configuration (see previous figure).
As sown in the figure, STM32TrustedPackageCreator is using a configuration file (STiRoT_Code_Image.xml).
A file example is available in the STM32Cube_FW repository (\STM32Cube_FW_H5\Projects\STM32H573I-DK\ROT_Provisioning\STiROT\Image).
It can be edited directly in the xml file or graphically by using STM32TrustedPackageCreator (see How_to_start_with_ST-iROT article).
A dependency with a user data image version can be added in order to have simultaneous installation of firmware code and data images.
The related version of the data image is defined in the STiRoT_Code_Image.xml and can be updated accordingly.
The next sections will give some details about the mapping configuration and image format requirements for the user application to be compatible with STiROT.
The firmware code download and execution area offsets are chosen (see How_to_start_with_ST-iROT article).
During provisioning process, the stm32h573xx_flash.icf is automatically updated based on mapping information (firmware execution offset and size) provided in the STiROT configuration.
The STM32TrustedPackageCreator generates the stm32h573xx_flash.if file defining a vector table located at: 0x0C000000 + code execution slot offset + 0x400 (header size).
Note: the header is a fixed size of 0x400.
For IAR Embedded Workbench IDE, this file is located in the STiROT_Appli\EWARM directory.
In case of configuration modification, it is mandatory to recompile the user application project to generate the correct binary file.
- The "Magic" is a reserved 16 bytes memory region used to manage the installation
- TLV is a reserved 296 bytes memory region placed at the end of the image. It states for Type Length Value and contains metadata used to manage the images.
On the left of the above figure: the user application code image structure written in a download flash area by the STiROT.
On the right of the above figure: the user application code structure written in the execution flash area by the STiROT.
As described in previous sections, the STiROT decrypts the firmware code before copying it into the execution area.
6.2. User Data Image generation
The following figure gives an overview of the user data image generation.
To be installed successfully by the STiROT (see next chapter) this image needs to be encrypted, signed and aligned with the flash memory map config, as described in this section.
STM32TrustedPackageCreator need to be launched separately to generate the encrypted and signed image file using the same encryption and authenticity keys provisioned during the STiROT configuration. The same keys are also used for the user application code image generation.
As sown in the figure, STM32TrustedPackageCreator is using a configuration file (STiROT_Data_Image.xml).
A file example is available in the STM32Cube_FW (STM32Cube_FW_H5\Projects\STM32H573I-DK\ROT_Provisioning\STiROT\Image).
It can be edited directly in the xml file or graphically by using STM32TrustedPackageCreator (see How_to_start_with_ST-iROT article)
A dependency with a user application firmware image version can be added in order to have simultaneous installation of firmware code and data images.
The related version of the user application firmware image is defined in the STiRoT_Data_Image.xml and can be updated accordingly.
The next paragraph will give some details about the mapping configuration and image format requirements to be compatible with STiROT.
During the STiROT configuration done with STM32TrustedPackageCreator, the user data download and installation area offsets are chosen ([section 5.1)
On the left of the above figure: the user data image structure written in a download flash area by the STiROT.
On the right of the above figure: the user application data structure written in the Obkey store area.
Note that the user data are stored in the Obkey area and not in a user flash area.
For the STM32CubeFW STiROT example (see STM32_STiROT_DA_getting_started), a data.bn file is provided with 64 bytes. These data are just used to be written back during user application execution and have no other meaning.
7. User application firmware and data installation
The following figure summarizes the steps for the user application firmware and data installation.
The download area locations and sizes are defined during the STiROT configuration (See STiROT configuration section).
The execution slot location and size are also defined during the STiROT configuration.
For the CubeFW STiROT example, the user application code and data are in isolation level 2 (HDPL2).
With STM32Cube_FW the provisioning.bat script used during the device provisioning will continue to guide the user during images generation and installation.
- The encrypted user application code is written in the download area
- After authenticity and integrity verifications, the user application code is decrypted and written in the user flash execution area
- The encrypted data are written in the download area
- The data authenticity and integrity are verified. Then the data are decrypted and re-encrypted with the DHUK (Derived Hardware Unique Key) and stored in the secure storage (HDPL2 OB Keys area) (For explanation about the DHUK, please refer to the "Secure storage" wiki article).
A firmware or data update is possible in any product state (except Locked state, see next chapter) through launch of the embedded bootloader.
A practical example is shown in the How_to_start_with_ST-iROT article
- The embedded bootloader is used to copy the encrypted new user application firmware and/or new user data in the user flash download area
- At next hardware reset, the STiROT installs the update(s) after authenticity and integrity verifications
8. Product State setting
Once the user application code and data are flashed into the device, the script is used to set the final state.
This is the last step done through the script.
The following figure shows the possible product state.
(for more details refer to product lifecycle and Debug Authentication wiki articles).
The provided script mentioned previously (Provisioning.bat) is guiding the user also during this phase (see STM32_STiROT_DA_getting_started).
At the end of the provisioning script execution, the product state can be chosen, and the related option byte will be automatically set.
The product state is chosen depending on the user application development phase and the wanted security level.
- Open:
- This state is mainly used during development phase since the device is fully open.
- Debug is fully open.
- The Trust Zone can be disabled or enabled (TZEN option byte programming).
- Embedded Bootloader can be used.
- This state is mainly used during development phase since the device is fully open.
- Provisioning:
- This state is used during the provisioning.
- It is the device state during the provisioning script execution (Provisioning.bat).
- So this state will not be part of the proposed state that can be chosen at the end of the script execution.
- The debug is only available when non secure user application is executed.
- The Trust Zone can be disabled or enabled (TZEN option byte programming).
- Embedded Bootloader can be used.
- Secure Firmware install can be launched in this state (not anymore possible in following states).
- Partial or full regression are possible.
- This state is used during the provisioning.
- Provisioned:
- In this state the STiROT setup is done.
- Debug is available only when non secure user application is executed.
- Debug access for secure application can be available by launching the Debug Authentication (see Debug Authentication setting).
- The STiROT can launch the embedded bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity or missing code)
- Partial or full regression are possible.
- In this state the STiROT setup is done.
- TZ-Closed:
- The Trust Zone closed state is used when the STiROT is provisioned and the secure user application (case 1) or the uROT+Secure user application (case2) (see section 5.1.2).
- For case 2, the uROT is allowing the update of the next isolation level (Code and Data).
- uROT can launch the embedded bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity or missing code).
- uROT can launch the embedded bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity or missing code).
- The debug is only available when non secure user application is executed.
- Debug access for secure application can be available by launching the Debug Authentication (see Debug Authentication setting).
- Partial or full regression are possible.
- The Trust Zone closed state is used when the STiROT is provisioned and the secure user application (case 1) or the uROT+Secure user application (case2) (see section 5.1.2).
- Closed:
- This state is used when the product is fully provisioned.
- The debug is fully closed but can be open by launching the Debug Authentication (see Debug Authentication setting) .
- Partial or full regression are possible.
- This state is used when the product is fully provisioned.
- Locked:
- Locked is final product state that can’t be changed anymore.
- The debug is definitively closed and can’t be reopen through debug authentication.
- No regression is possible anymore
- Locked is final product state that can’t be changed anymore.
- Open:
9. Appendix STiROT
9.1. Application development phase
The most efficient way to develop and debug an application is first to boot directly on user flash in the Open product state by stetting with STM32CubeProgrammer the UBE to 0xB4 and the SECBOOTADD to 0x0C000400 (by default the firmware execution offset is 0x0)
As long as the device is in open state, the user flash can be erased without performing a regression and a debugger can be connected without performing a debug authentication.
Once validated, the secure boot path can be activated :
- DA configuration: important that the Debug Authentication configuration is done correctly (see How_to_start_with_ST-iROT article)
- provisioning the STiROT configuration
- generating the images
- downloading and installing the images
If after provisioning the device is set in another state than open, the Debug Authentication process must be used to open the debugger.
A Firmware update is possible using the embedded bootloader, without opening the debugger, see How_to_start_with_ST-iROT, section 6.5
9.2. STiROT Configuration detailed description
Parameter | Hidden | Description | Additional controls/constraints |
---|---|---|---|
Product state minimal allowed | No | STiROT is executed only if the device is in the chosen minimum life cycle state (Open, Provisioning, Provisioned, TZ-Closed, Closed, Locked). | This information is duplicated from option bytes in order to control that the option bytes is well configured. |
Number of images managed by ST-iRoT | No | 1: Firmware image only. Configuration selected for any application which does not manage secret information. 2: Firmware and data images. As example, in STiROT_OEMuROT bootpath, the data image contains the cryptographic keys of OEMuROT boot. |
Data image slot definition (size and offset) will be available trough STM32TrustedPackageCreator as soon as 2 images configuration is selected. |
High speed clock activation | Yes | 0 : 64 MHz, default configuration 1: 200 MHz, best speed supporting the full range of temperature 2: 250 MHz, max speed clock |
|
Is the firmware full secure | No | Yes : the firmware booted is full secure. As example STiROT_Appli provided in STM32H5 Cube. No : the firmware booted is made of a secure part and non-secure part. As example STiROT_Appli_TrustZone provided in STM32H5 Cube. |
The size of the secure area inside the firmware execution area must be specified as soon as the firmware is not full secure. In this configuration the image generation triggered by the post build command of the non secure project is preceded by an assembly command of the secure and non-secure binaries. |
Firmware execution area offset | No | Offset from begin of the user flash memory.
It must me aligned on a sector start address. |
No overlap allowed between execution areas and download areas.
Firmware execution area cannot be mapped between the 2 download areas. |
Firmware download area offset | No | Offset from begin of the user flash memory.
It must me aligned on a sector start address. |
No overlap allowed between execution areas and download areas.
Firmware execution area cannot be mapped between the 2 download areas. Both firmware and data download areas can overlap. In this case, the installation of a data and firmware image in a single execution using the dependency feature is not possible. |
Firmware area size | No | Size of the firmware.
It must be a multiple of the sector size. |
No overlap allowed between execution areas and download areas.
Firmware slots definition should not exceed the user flash capacity. |
Data area offset in HDPL2 OBkeys | No | Offset from the beginning of HDPL2 Obkeys area (0xFFD0900). | Range allowed from 0xFFD0900 to 0xFFD0BF0 : no overlap with HDPL3 OBKeys.
Parameter disabled for 1 image configuration. |
Data slot size in HDPL2 OBKeys | No | Size of the data area in HDPL2 OBkeys. Maximum is 0x2F0. | Range allowed from 0xFFD0900 to 0xFFD0BF0 : no overlap with HDPL3 OBKeys.
Parameter disabled for the “1 image” configuration. |
Data download area offset | No | Offset from begin of the user flash memory.
It must me aligned on a sector start address. |
Both firmware and data download areas can overlap. In this case, the installation of a data and firmware image in a single execution using the dependency feature is not possible. |
Data download slot size | Yes | Offset from begin of the user flash memory.
It must me aligned on a sector start address. |
Must be 0x2000 for STM32H5 product (parameter hidden). |
Size of the secure area inside the firmware execution area | No | Size of the secure part of the firmware image.
It must be a multiple of the sector size. |
Parameter disabled for the “firmware full secure” configuration.
STiROT will configure the MPU to allow execution only for the secure part of the firmware. Then, it is up to the secure application to update (disable, re-configure) the MPU configuration depending on its needs. |
SRAM2 erasing in case of reset | Yes | Yes (default value) : the SRAM2 is automatically erased by hardware in case of reset. Ensure that all secrets are erased in case of reset.
No : SRAM2 is not erased. Less secure configuration but it can be required when the application has no other possibility to manage persistent information in SRAM2. |
This information is duplicated from option bytes in order to control that the option bytes is well configured. |
SRAM2 ECC management activation | Yes | Yes (default value) : a reset will be generated in case of ECC detection. ECC is a mechanism to prevent mechanisms prevent external attacks.No : ECC not managed. Less secure configuration but it can be selected if hardware attack is not possible. | This information is duplicated from option bytes in order to control that the option bytes is well configured. |
Encryption key | No | Key used to encrypt the firmware and data images | When this key is regenerated, both firmware and data images must be processed with STM32TrustedPackageCreator “Image Gen” tab (STiROT_Code_Image.xml & STiROT_Data_Image.xml) |
Authentication key | No | key used to authenticate the firmware and data images. | When this key is regenerated, both firmware and data images must be processed with STM32TrustedPackageCreator “Image Gen” tab (STiROT_Code_Image.xml & STiROT_Data_Image.xml) |
Output File | No | Name of the output file |
9.3. STiROT Config.obk file format
- Important note: endianness: uint32_t 0x01234567 is represented in obk file as 0xx67452312
Offset | Size | Type | Description |
---|---|---|---|
0 | 4 | uint32_t | sdp command header : destination address |
4 | 4 | uint32_t | sdp command header : data size address |
8 | 4 | uint32_t | sdp command header : encryption enabled/disabled (1/0) |
12 | 32 | array | SHA256 of the following data content (from offset 44 to 268) |
44 | 1 | uint8_t | Number of images managed by ST-iRoT |
45 | 1 | uint8_t | 250 Mhz / 200 Mhz / 64 Mhz : 2 / 1 / 0 |
46 | 1 | uint8_t | Firmware full secure (1/0) |
47 | 1 | uint8_t | Jump into ST bootloader when no valid image(s) |
48 | 4 | uint32_t | Firmware execution area offset |
52 | 4 | uint32_t | Firmware download area offset |
56 | 4 | uint32_t | Firmware area size |
60 | 4 | uint32_t | Data area offset in HDPL2 OBkeys |
64 | 4 | uint32_t | Data slot size in HDPL2 OBKeys |
68 | 4 | uint32_t | Data download area offset |
72 | 4 | uint32_t | Data download slot size |
76 | 4 | uint32_t | Size of the secure area inside the firmware execution area (meaningful only when the firmware is not fully secure. |
80 | 4 | uint32_t | SRAM2 erasing in case of reset |
84 | 4 | uint32_t | SRAM2 ECC management activation |
88 | 4 | uint32_t | Product state minimal allowed (0x0000ED00,Open / 0x00001700,Provisioning / 0x00002E00,Provisioned / 0x0000C600,TZ-Closed / 0x00007200,Closed / 0x00005C00,Locked |
92 | 70 | array | Encryption private key (MCU Boot format) |
162 | 2 | array | Reserved |
164 | 91 | array | Authentication public key (MCU Boot format) |
255 | 13 | array | Reserved (Global alignment of OBKkeys data on 16 bytes) |
9.4. STiROT DA.obk file format
- Important note: endianness: uint32_t 0x01234567 is represented in obk file as 0xx67452312 L
Offset | Size | Type | Description |
---|---|---|---|
0 | 4 | uint32_t | sdp command header : destination address |
4 | 4 | uint32_t | sdp command header : data size address |
8 | 4 | uint32_t | sdp command header : encryption enabled/disabled (1/0) |
12 | 32 | array | SHA256 of the following data content (from offset 44 to 108) |
44 | 32 | array | SHA256 of the DA root authentication public key |
76 | 32 | array | Permissions (cf DA Getting_started for more details) |
9.5. STiROT Data.obk file format
- Important note: endianness: uint32_t 0x01234567 is represented in obk file as 0xx67452312
Offset | Size | Type | Description |
---|---|---|---|
0 | 4 | uint32_t | sdp command header : destination address |
4 | 4 | uint32_t | sdp command header : data size address |
8 | 4 | uint32_t | sdp command header : encryption enabled/disabled (1/0) |
12 | 32 | array | SHA256 of the following data content (from offset 44 to 108) |
44 | 4 | uint32_t | Version n of the firmware image |
48 | 4 | uint32_t | Version n-1 (previous) of the firmware image |
52 | 4 | uint32_t | Version n of the data image |
56 | 4 | uint32_t | Version n-1 (previous) of the data image |
60 | 32 | array | Reserved |
92 | 16 | array | Reserved |