STM32CubeWBA: Memory management

Revision as of 11:52, 9 March 2023 by Registered User (→‎Basic Memory Manager and Heap)
Under construction.png Coming soon

1. Introduction

An enhanced version of dynamic allocation is available with the STM32WBA: the Advanced Memory Manager(AMM). It eases dynamic allocations in a multitask/shared environment without adding much complexity.

The new features provided by AMM are the following:

  • Support several Virtual Memories
  • Minimum size warranty per Virtual Memory (Quality Of Service - QOS)
  • Callback in case of memory allocation failure

2. Features

The Advanced Memory Manager comes on top of a Basic Memory Manager(BMM) - Understand here anything capable of providing basic memory allocation features such as Alloc and Free – and add some new capabilities on top of it.

2.1. Basic Memory Manager and Heap

The Basic Memory Manager (BMM)
Can be anything that is capable to allocate/free memory. For instance, standard malloc() / free() or custom static pool API, etc.
Shall at least support the capability to merge into one single memory two continuous memories that has been freed (coalescence)
Shall be provided by the user before any use of the AMM via the registration function
The Heap
Can either be a dedicated memory provided by the application, or the legacy default Heap provided by most application at link time
Its size shall be at least equal to the sum of all Virtual Memories size

2.2. Virtual Memories and Shared Pool

In a concurrent execution application, dynamic allocation can encounter some issues with heap sharing. For instance, a task may allocate a major part of the available heap leading to allocation failure for all other tasks requesting memory. To avoid that kind of issue, the Advanced Memory Manager introduces the concept of virtual memories and shared pool.

The Virtual memory
Dedicated user memory pool, ie: specific VM IDs.
There to ensure to users the memory amount needed for minimal execution - Heap resource only available for this Virtual Memory ID.
The Shared pool
Mutual memory pool, ie: Can be used by any Virtual Memory ID.
Provide memory for an optimal execution.
Its size corresponds to the BMM pool size minus the space required for the Virtual memories.

For every operations, the user fills his Virtual Memory ID. This helps determine its identity and allow the AMM to identify how much space is remaining in this Virtual Memory.
However, once his Virtual Memory quota is consumed - Sum of all the user allocations = Virtual Memory size -, the user can still pursue with allocation requests. Those requests will take place in the Shared Pool area and are, here, fully dependent of the others users sympathy - Meaning that the request may or may not succeed depending on the availability of resources.

2.3. Retry callback

During program execution, users may encounter some memory allocation failure - Not enough memory available. Instead of setting up a polling mechanism, in an allocation request, the AMM offers the possibility to register a callback.
This callback  inform the requester(in an asynchronous way) that some space has been freed - Either in the shared pool or in its dedicated virtual pool - and a new allocation request can be submitted.
In some cases, the memory can be freed from a different context than the one it has been allocated from. The Callback should not implement any active code and should be used only to set up a new allocation request from the main context.

2.3.1. Single callback case

2.3.2. Multiple callback case

3. Interface

Here comes a list of the available functions for AMM:

AMM_Init

Description

Initialize the Advanced Memory Manager Pool.
Syntax
AMM_Function_Error_t AMM_Init (const AMM_InitParameters_t * const p_InitParams);
Parameters
[in] p_InitParams
Type: const AMM_InitParameters_t * const
Description: Struct of init parameters
Return Value
AMM_Function_Error_t
AMM_DeInit
Description
DeInitialize the Advance Memory Manager Pool
Syntax
AMM_Function_Error_t AMM_DeInit (void);
Parameters
None
Return Value
AMM_Function_Error_t
AMM_Alloc
Description
Allocate a buffer from the Advance Memory Manager Pool.
Syntax
AMM_Function_Error_t AMM_Alloc (const uint8_t VirtualMemoryId,
                                const uint32_t BufferSize,
                                uint32_t ** pp_AllocBuffer,
                                AMM_VirtualMemoryCallbackFunction_t * const p_CallBackFunction);
Parameters
[in] VirtualMemoryId
Type: const uint8_t
Description: Virtual Memory Identifier - AMM_NO_VIRTUAL_ID Can be used.
[in] BufferSize
Type: const uint32_t
Description: Size of the pool with a multiple of 32bits.
ie: BufferSize = 4; TotalSize = BufferSize * 32bits = 4 * 32bits = 128 bits
[out] pp_AllocBuffer
Type: uint32_t **
Description: Pointer onto the allocated buffer
[in] p_CallBackFunction
Type: AMM_VirtualMemoryCallbackFunction_t * const
Description: Pointer onto the Callback to call in case of failure - Can be NULL.
Return Value
AMM_Function_Error_t
AMM_Free
Description
Free the allocated buffer from the Advance Memory Manager Pool
Syntax
AMM_Function_Error_t AMM_Free (uint32_t * const p_BufferAddr);
Parameters
[in] p_BufferAddr
Type: uint32_t * const
Description: Address of the buffer to free
Return Value
AMM_Function_Error_t
AMM_BackgroundProcess
Description
Background routine that aims to call registered callbacks for an allocation retry
Syntax
void AMM_BackgroundProcess (void);
Parameters
None
Return Value
None
AMM_RegisterBasicMemoryManager
Description
Register the Basic Memory Manager functions to use
Syntax
void AMM_RegisterBasicMemoryManager (AMM_BasicMemoryManagerFunctions_t * const p_BasicMemoryManagerFunctions);
Parameters
[in] p_BasicMemoryManagerFunctions
Type: AMM_BasicMemoryManagerFunctions_t * const
Description: Address of the basic memory manager functions
Return Value
None
AMM_ProcessRequest
Description
Request to application for a Background process run
Syntax
void AMM_ProcessRequest (void);
Parameters
None
Return Value
None


Info white.png Information
For more information about the Background process system, please visit this page

4. How to

The following chapters explain "how to" configure and use the Advanced Memory Manager.

4.1. Initialize the AMM

Before any use, AMM needs to be setup and there is few steps to do so.

4.1.1. Basic Memory Manager selection

First things first, you have to determine the Basic Memory Manager you are going to use.
As said above, it can be anything capable of allocation and free. The only mandatory point is coalescence.
In the following examples, the selected BMM will be the Memory manager utility - Already available in the current release under the memory manager folder- UTIL_MM_XXX ().

4.1.2. Basic Memory Manager registration

Once the BMM is identified, you have to register its functions to the AMM. To do so we need to create function wrappers since our BMM will not always fully match the expected function of the AMM register function:

Definition:
static void AMM_WrapperInit (uint32_t * const p_PoolAddr, const uint32_t PoolSize);

static uint32_t * AMM_WrapperAllocate (const uint32_t BufferSize);

static void AMM_WrapperFree (uint32_t * const p_BufferAddr);
Implementation:
static void AMM_WrapperInit (uint32_t * const p_PoolAddr, const uint32_t PoolSize)
{
  UTIL_MM_Init ((uint8_t *)p_PoolAddr, ((size_t)PoolSize * sizeof(uint32_t)));
}

static uint32_t * AMM_WrapperAllocate (const uint32_t BufferSize)
{
  return (uint32_t *)UTIL_MM_GetBuffer (((size_t)BufferSize * sizeof(uint32_t)));
}

static void AMM_WrapperFree (uint32_t * const p_BufferAddr)
{
  UTIL_MM_ReleaseBuffer ((void *)p_BufferAddr);
}
Info white.png Information
Beware that operation with AMM are achieved on a 32bits size reference


Once wrappers are defined, register function is the next function to implement - Definition is already done in the AMM header file. The AMM will call this function at its initialization so we have to provide pointer onto the newly declared wrappers:

Implementation:
void AMM_RegisterBasicMemoryManager (AMM_BasicMemoryManagerFunctions_t * const p_BasicMemoryManagerFunctions)
{
  /* Fulfill the function handle */
  p_BasicMemoryManagerFunctions->Init = AMM_WrapperInit;
  p_BasicMemoryManagerFunctions->Allocate = AMM_WrapperAllocate;
  p_BasicMemoryManagerFunctions->Free = AMM_WrapperFree;
}

With this steps over, the BMM will be linked up with the AMM and fully operational. Next step is the configuration of the AMM.

Info white.png Information
Please give a look to function section for more information on the register function.

4.1.3. Configure and Initialize the AMM

The Advanced memory manager configuration is done at initialization and the parameters are the following:

typedef struct AMM_InitParameters
{
  /* Address of the pool of memory to manage */
  uint32_t * p_PoolAddr;
  /* Size of the pool with a multiple of 32bits.

     ie: PoolSize = 4; TotalSize = PoolSize * 32bits
                                 = 4 * 32bits
                                 = 128 bits */
  uint32_t PoolSize;
  /* Number of Virtual Memory to create */
  uint32_t VirtualMemoryNumber;
  /* List of the Virtual Memory configurations */
  AMM_VirtualMemoryConfig_t a_VirtualMemoryConfigList[];
}AMM_InitParameters_t;

The AMM configuration is a two steps procedure:

  1. Establish the Virtual Memory + Shared pool configurations (How many VMs, What size, etc)
  2. Adapt the pool size and location of the AMM pool according to the configuration firstly determined
4.1.3.1. Virtual Memory and Shared pool configurations
These two are the backbone of the AMM configuration. You will have to determine both and their characteristics to pursue with the AMM initialization.
Virtual Memories configurations
There are 3 characteristics to identify: The number of VMs, the proper size of each VM and their IDs:
The Number of VMs
To determine the number of needed Virtual Memories, you have to identify the number of process that need their own heap for their nominal operating. You shall consider one Virtual Memory for one of these process.
The Size of each VMs
The size of each Virtual Memory will be determined by the process needs. Each Virtual Memory shall be sized to the process nominal heap value. Do not forget that the Virtual Memory size is set on a 32bits basis.
The ID of each VMs
For each VM, you can define an unique ID. This will be used to access the proper Virtual Memory during memory operation.
Those characteristics can afterward be fulfilled in the AMM initialization parameters structure:
For the Number of Virtual Memories:
  /* Number of Virtual Memory to create */
  uint32_t VirtualMemoryNumber;
For the proper configuration of each Virtual Memory, a structure like this shall be instanced:
typedef struct AMM_VirtualMemoryConfig
{
  /* ID of the Virtual Memory */
  uint8_t Id;
  /* Size of the Virtual Memory buffer with a multiple of 32bits.

     ie: BufferSize = 4; TotalSize = BufferSize * 32bits
                                   = 4 * 32bits
                                   = 128 bits */
  uint32_t BufferSize;
}AMM_VirtualMemoryConfig_t;
and provided to the AMM Initialization parameter:
  /* List of the Virtual Memory configurations */
  AMM_VirtualMemoryConfig_t a_VirtualMemoryConfigList[];
Shared Pool configuration
Shared Pool Size
Regarding the Shared Pool size, its size is up to you. The shared pool is designed to allow an optimal execution of each process that need a little bit of heap, once in a while, to perform better.
The Shared Pool configuration is not a proper parameter of AMM initialization. However, it must be defined to determine the whole AMM required pool space. This concept also ease the AMM comprehension and enhance its configuration - This leads to a better optimization of the required space.
4.1.3.2. AMM pool configuration
As seen above, the AMM pool size is mostly dependent of the VM and Shared Pool configurations.
Nonetheless, there is also a management part that need to be considered in the pool size computation.
AMM management part
For operating purposes, the AMM allocates some of the heap provided to it. For each VM, it creates an info element.
Thus user shall consider at the initialization more space for the pool.
Considering all those elements, the AMM pool size representation is as follow:
Pool Size computation
With all the points enounced above, you can compute the adequate Pool Size following this formula:
#define CFG_AMM_POOL_SIZE = (CFG_AMM_NUMBER_OF_VM * AMM_VIRTUAL_INFO_ELEMENT_SIZE) + \
                             CFG_AMM_SHARED_POOL_SIZE + \
                             CFG_AMM_SUM_OF_VMS_SIZE
and afterward fulfill the AMM init parameter, remembering that the size is on a 32bits basis:
  /* Size of the pool with a multiple of 32bits.

     ie: PoolSize = 4; TotalSize = PoolSize * 32bits
                                 = 4 * 32bits
                                 = 128 bits */
  uint32_t PoolSize;
Start Address
The start address can either be a heap located address or a static buffer used as a memory pool.
For instance, use a static allocated buffer:
static uint32_t AMM_Pool[CFG_AMM_POOL_SIZE];
Info white.png Information
Please give a look to function section for more information on the initialization function.

4.2. Allocate memory

The allocation function differs a bit from the standard malloc. It adds:

  • A function error code that informs the user on the state of the operation.
  • The possibility to register a callback function in case of allocation failure.

The function can be called with or without a Virtual Memory ID and with or without the registration of a callback. The following examples will highlight these facts.

Allocation with a Virtual Memory ID and with a callback registration
This is the typical way of calling the allocation function. In this way, the allocation takes places in the Virtual Memory - Or Shared Pool if the first one is full - and the user has his callback registered in case of allocation failure - Due to not enough space available. This one will be invoked once a space liberation occurs.
Here is the example:
uint32_t * p_AllocBuffer = NULL;

uint32_t funcReturn = AMM_ERROR_NOK;

VirtualMemoryId = 0x1;
BufferSize = 0xA;

funcReturn = AMM_Alloc (VirtualMemoryId,
                        BufferSize,
                        &p_AllocBuffer,
                        &CallBackElt);

if (funcReturn == AMM_ERROR_OK)
{
  // Do stuff with the brand new buffer
  ...
}
/*
else if (funcReturn == AMM_XXX)
{
  // Manage the AMM_XXX error
  ...
}
else
{
  ...
}
*/
with the callback parameter looking like this:
static AMM_VirtualMemoryCallbackFunction_t CallBackElt = 
{
  .Header =
  {
    .next = NULL,
    .prev = NULL
  },
  .Callback = Callback
};
and the callback function could be implemented as this:
void Callback (void)
{  
  /* Set event to notify that a new allocation can be requested */
  UTIL_SEQ_SetEvt (1u << AMM_CALLBACK_EVT_BM);
}
Allocation without a Virtual Memory ID and without a callback registration
This is most straight forward way, with no ID and no Callback registration. The allocation will take place in the Shared Pool and in case of failure, the user would need to execute a new request by himself.
Here is the example:
uint32_t * p_AllocBuffer = NULL;

uint32_t funcReturn = AMM_ERROR_NOK;

BufferSize = 0xA;

funcReturn = AMM_Alloc (AMM_NO_VIRTUAL_ID,
                        BufferSize,
                        &p_AllocBuffer,
                        NULL);

if (funcReturn == AMM_ERROR_OK)
{
  // Do stuff with the brand new buffer
  ...
}
/*
else if (funcReturn == AMM_XXX)
{
  // Manage the AMM_XXX error
  ...
}
else
{
  ...
}
*/

4.3. Free memory

The free operation is rather simple, the only difference with the one from the standard lib is that the AMM_Free has a returned error code that can be analyzed.
Here the example:

uint32_t funcReturn = AMM_ERROR_NOK;

funcReturn = AMM_Free (p_AllocatedBuffer);

if (funcReturn == AMM_ERROR_OK)
{
  // Do stuff with the brand new buffer
  ...
}
/*
else if (funcReturn == AMM_XXX)
{
  // Manage the AMM_XXX error
  ...
}
else
{
  ...
}
*/

5. Revisions

Rev. number Description
0.1 First wiki version.