This article describes how to automatize machine learning model code generation and validation through X-CUBE-AI Command Line Interface (CLI). The example is provided for Windows thanks using batch script, however it can be easily adapted to other operating system or through Python. More information on CLI can be found in the embedded documentation.
1. Requirements & installations
- X-CUBE-AI latest version (latest tested v7.2)
- STM32CubeIDE latest version (latest tested v1.10.1)
- STM32CubeProgrammer latest version (latest tested v1.10.1)
- A STM32 evaluation board, for this example: NUCLEO-H723ZG
- A model (Keras .h5, tensorflow lite .tflite or ONNX). For this example we used a MobileNet v1 0.25 quantized with input of image input of 128x128x3.
You can download the model: mobilenet_v1_0.25_128_quantized.tflite.
Once X-CUBE-AI is installed as well as STM32CubeIDE, please note the installation paths, usually by default on Windows (replacing username by your Windows user account name and adapting to your tool version):
- For X-CUBE-AI: C:\Users\username\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\7.2.0
- For STM32CubeIDE: C:\ST\STM32CubeIDE_1.10.1\STM32CubeIDE\
- For arm gcc installed through STM32CubeIDE: C:\ST\STM32CubeIDE_1.10.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\bin
- For STM32CubeProgrammer: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin
2. Validation application generation
In order to generate the initial validation project for the targeted board, we are using the STM32CubeMX with X-CUBE-AI plugin.
2.1. Create a new project
Open STM32CubeMX and start the project using the board selector:
Select the board to use, in our case the NUCLEO-H723ZG, and create a project without initializing all peripherals with their default Mode:
2.2. Add X-CUBE-AI software pack
Select X-CUBE-AI software pack Core and Validation application:
Click on X-CUBE-AI software pack:
If by default the peripherals parameters are not set for the best performance, the system warns you of this. Select 'yes' to make sure that the maximal frequency is used.
X-CUBE-AI configures default parameters to set the best performance as well as configuring the UART used to report performances.
2.3. Generate the validation application
Upload a model, in our example the mobilenet_v1_0.25_128_quantized.tflite.
For our example, we keep the default (from versionv7.2 of X-CUBE-AI) memory options allocate input / output.
You can then generate the corresponding validation application as STM32Cube IDE project in a dedicated directory and then open it
In STM32CubeIDE build the project
To check that the validation application is working as expected, program first the board (either though STM32CubeIDE or STM32CubeProgrammer) then reset the board. Open the validation on target panel and either select the board COM board or leave the automatic detection. Do not select the automatic compilation and download option as the board is already programmed with the right firmware.
Press ok and check that the validation is running correctly.
3. Automatic generation
The below batch script uses ST tools through command line interface to automatically:
- get the full memory footprint of a given model
- get the inference time
- get the validation metrics (validation done on random data)
In below script, the local working directory is "C:\Project" which shall correspond to the directory of the initial validation application project. There is two modes, defined by the variable "mode". The analyze mode, mode=analyze, do only an analyze to get main memory footprint contributors (ie weights and activations buffer). In this mode, it is not needed to generate a validation application (section2 can be skipped) and only X-CUBE-AI needs to be installed. The validation mode, mode=validate (default), do a validation to get full memory footprint (weights, activations and runtime) as well as inference time and validation metrics. In the script a temporary directory "tmp" is generated with two sub directories "stm32ai_ws" and "stm32ai_output". These directories will be used by the X-CUBE-AI stm32ai CLI executable as workspace and output directory. The main outputs and reports are copied from these directories to a result directory, for our example C:\Project\Results\STM32H723\mobilenet_v1_0.25_128_quant.tflite
The total memory footprint for a given model shall consider not only the size of the weights of the model (stored in Flash) and the size of the activations, input, output buffers. The size of the runtime code (Flash and RAM) shall also be considered. The runtime memory footprint can only be measured by building the code with a toolchain. A convenient way to measure the runtime footprint is to generate the code using the relocatable option. A relocatable binary model designates a binary object which can be installed and executed anywhere in a STM32 memory sub-system. It contains a compiled version of the generated NN C-files including the requested forward kernel functions and the weights. The principal objective is to provide a flexible way to upgrade an AI-based application w/o re-generating and flashing the whole end-user firmware. This is the primary element to use for example the FOTA (Firmware Over-The-Air) technology. Please refer to the "Relocatable binary model support" section of the embedded documentation for more information.}} The relocatable binary corresponds to the model runtime code and the related report provide all the needed information to get the full memory footprint. Let's analyze a generate report with relocatable option:
Runtime memory layout (series="stm32h7")
------------------------------------------------------------------
section size (bytes)
------------------------------------------------------------------
header 100*
txt 33,716 network+kernel
rodata 628 network+kernel
data 14,884 network+kernel
bss 384 network+kernel
got 568*
rel 4,172*
weights 478,804 network
------------------------------------------------------------------
FLASH size 528,032 + 4,840* (+0.92%)
RAM size** 15,268 + 568* (+3.72%)
------------------------------------------------------------------
bin size 532,876 binary image
act. size 67,120 activations buffer
------------------------------------------------------------------
(*) extra bytes for relocatable support
(**) Full RAM = RAM + act. + IO if not allocated in activations buffer
The section (*) should not be considered as it is related to specific code of the relocatable feature and not to the runtime code itself. The full Flash size is then composed of the "weights" size, here 478,804 bytes and the sections "txt", "rodata" and "data" so 49,228 bytes for a total of 528,032 bytes. The full RAM size is then composed of the activations (here 67,120 bytes), input and output buffers (if not allocated in activations buffer) and the sections "data" and "bss", so 15,268 bytes, here for a total of 82,388 bytes. Note that to gain RAM space the "Use activation buffer for input buffer" and "Use activation buffer for the output buffer" options are selected in this example and therefore are not adding any memory footprint. Otherwise, they should be added to the total RAM size. Another way would be to build the validation application and analyze the memory map.
To get the inference time, the script generates the code for the given network, replace the needed file in the initial validation application. Then the validation application is rebuild thanks to STM32CubeIDE CLI. The generated firmware .elf is the loaded on the board which shall be connected to the PC through the STLink USB and identified though a COM port. Then the board is reset and the validation application (with random data) is launched. The validation report provides the model inference time as well as the validation error metrics. The script copies the main information in the result.txt file:
STM32H723
mobilenet_v1_0.25_128_quant.tflite
weights (ro) : 478,804 B (467.58 KiB) (1 segment) / -1,391,568(-74.4%) vs float model
weights size : 478804 (1 segments)
activations (rw) : 67,120 B (65.55 KiB) (1 segment) *
activations size : 67120 (1 segments)
ram (total) : 67,120 B (65.55 KiB) = 67,120 + 0 + 0
FLASH size 528,032 + 4,840* (+0.92%)
RAM size** 15,268 + 568* (+3.72%)
(**) Full RAM = RAM + act. + IO if not allocated in activations buffer
duration : 45.774ms
cycles/MACC : 1.85
X-cross #1 n.a. 0.000772025 0.000057365 0.052570902 0.000007414 0.000772028 0.997128242 nl_30_0_conversion, ai_u8, (1,1,1,1001), m_id=[30]
Automatic code generation and validation with X-CUBE-AI CLI script:
@echo off
Rem ******************************************************************************
Rem Copyright (c) 2022 STMicroelectronics. All rights reserved.
Rem ******************************************************************************
Rem This software component is provided to you as part of a software package and
Rem applicable license terms are in the Package_license file. If you received this
Rem software component outside of a package or without applicable license terms,
Rem the terms of the BSD-3-Clause license shall apply.
Rem You may obtain a copy of the BSD-3-Clause at:
Rem https://opensource.org/licenses/BSD-3-Clause
Rem ******************************************************************************
Rem set the different paths to the tools and project location
Rem replace below username by your Windows user account name
set CUBE_FW_DIR=C:\Users\username\STM32Cube\Repository
set X_CUBE_AI_DIR=%CUBE_FW_DIR%\Packs\STMicroelectronics\X-CUBE-AI\7.2.0
set CUBE_IDE_DIR=C:\ST\STM32CubeIDE_1.10.1\STM32CubeIDE\
set ARM_GCC_DIR=C:\ST\STM32CubeIDE_1.10.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\bin
set CUBE_PROG_DIR=C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin
set PATH=%X_CUBE_AI_DIR%\Utilities\windows;%CUBE_IDE_DIR%;%CUBE_PROG_DIR%;%ARM_GCC_DIR%;%PATH%
set locpath=C:\Project
Rem name: to identify the target STM32
set name=STM32H723
Rem STM32 series: stm32
set series=stm32h7
Rem model: model complete file name (including extension)
set model=mobilenet_v1_0.25_128_quant.tflite
Rem prjval: name of the initial X-CUBE-AI validation project
set prjval=STM32H723_project
Rem Com port is optional if only one board is connected to the PC
Rem set cport=COM18
Rem mode: analyze => do only an analyze to get main memory footprint contributors (ie weights and activations buffer)
Rem mode: validate => do a validation to get full memory footprint (weights, activations and runtime) as well as inference time
set mode=validate
Rem create directory
mkdir %locpath%\Results\%name%
mkdir %locpath%\Results\%name%\%model%
mkdir %locpath%\tmp
mkdir %locpath%\tmp\stm32ai_ws
mkdir %locpath%\tmp\stm32ai_output
set result_dir=%locpath%\Results\%name%\%model%
Rem write all result in a specific text file result.txt
del %result_dir%\result.txt
echo %name% >> %result_dir%\result.txt
echo %model% >> %result_dir%\result.txt
if %mode%==analyze (
Rem do only an analyze
@echo on
@echo Analyze %name% %model%
stm32ai analyze -m %locpath%\%model% --allocate-inputs --allocate-outputs -w %locpath%\tmp\stm32ai_ws -o %locpath%\tmp\stm32ai_output
copy /Y %locpath%\tmp\stm32ai_ws\network_report.json %result_dir%
copy /Y %locpath%\tmp\stm32ai_output\network_analyze_report.txt %result_dir%
findstr /b "weights" %result_dir%\network_analyze_report.txt >> %result_dir%\result.txt
findstr /b "activations" %result_dir%\network_analyze_report.txt >> %result_dir%\result.txt
findstr /b "ram" %result_dir%\network_analyze_report.txt >> %result_dir%\result.txt
@echo off
)
if %mode%==validate (
Rem do only a full validation to get full memory footprint (weights, activations and runtime) as well as inference time
@echo on
@echo Get the total memory footprint of the model %model% for %name%
stm32ai generate -m %locpath%\%model% --relocatable --allocate-inputs --allocate-outputs --series %series% -w %locpath%\tmp\stm32ai_ws -o %locpath%\tmp\stm32ai_output
copy /Y %locpath%\tmp\stm32ai_ws\network_report.json %result_dir%
copy /Y %locpath%\tmp\stm32ai_output\network_generate_report.txt %result_dir%\network_generate_relocatable_report.txt
findstr /b "weights" %result_dir%\network_generate_relocatable_report.txt >> %result_dir%\result.txt
findstr /b "activations" %result_dir%\network_generate_relocatable_report.txt >> %result_dir%\result.txt
findstr /b "ram" %result_dir%\network_generate_relocatable_report.txt >> %result_dir%\result.txt
findstr "FLASH" %result_dir%\network_generate_relocatable_report.txt >> %result_dir%\result.txt
findstr "RAM" %result_dir%\network_generate_relocatable_report.txt >> %result_dir%\result.txt
@echo Get the inference time of the model %model% for %name%
@echo Generate %name% %model%
stm32ai generate -m %locpath%\%model% --allocate-inputs --allocate-outputs --lib %X_CUBE_AI_DIR%\Middlewares\ST\AI -w %locpath%\tmp\stm32ai_ws -o %locpath%\tmp\stm32ai_output
copy /Y %locpath%\tmp\stm32ai_output\network*.c %locpath%\%prjval%\X-CUBE-AI\App\
copy /Y %locpath%\tmp\stm32ai_output\network*.h %locpath%\%prjval%\X-CUBE-AI\App\
@echo Building validation project %prjval%.elf
stm32cubeidec.exe --launcher.suppressErrors -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data workspace -import %locpath%\%prjval% -cleanBuild %locpath%\%prjval%\Debug
@echo Programming the board %locpath%\%prjval%\Debug\%prjval%.elf
STM32_Programmer_CLI.exe -c port=SWD mode=UR -w %locpath%\%prjval%\Debug\%prjval%.elf
Rem In case .bin file is preferred the command line needs to be adapted to add the start address
Rem STM32_Programmer_CLI.exe -c port=SWD mode=UR -w %locpath%\%prjval%\Debug\%prjval%.bin 0x08000000
STM32_Programmer_CLI.exe -c port=SWD -hardRst
TIMEOUT 1
@echo Launch the validation application
Rem stm32ai validate -m %locpath%\%model% -q %modelquant% --allocate-inputs --allocate-outputs --mode stm32 -d %cport% -w %locpath%\tmp\stm32ai_ws -o %locpath%\tmp\stm32ai_output
stm32ai validate -m %model% --allocate-inputs --allocate-outputs --mode stm32 -w %locpath%\tmp\stm32ai_ws -o %locpath%\tmp\stm32ai_output
copy /Y %locpath%\tmp\stm32ai_output\network_validate_report.txt %result_dir%
findstr "duration" %result_dir%\network_validate_report.txt >> %result_dir%\result.txt
findstr "cycles/MACC" %result_dir%\\network_validate_report.txt >> %result_dir%\result.txt
findstr "X-cross" %result_dir%\\network_validate_report.txt >> %result_dir%\result.txt
@echo off
)
PAUSE
Copyright (c) 2022 STMicroelectronics. All rights reserved.