![]() |
Coming Soon! |
Sensing is a major part of the smart objects and equipment, for example, condition monitoring for predictive maintenance, which enables context awareness and production performance improvement, and results in a drastic decrease in the downtime due to preventive maintenance.
The FP-AI-MONITOR1 function pack for STM32Cube is a multi-sensor AI data monitoring framework on the wireless industrial node.
For more information about how to use FP-AI-MONITOR1 look at the FP-AI-MONITOR1 user manual
The rest of the article discusses some of the key technologies and concepts behind the function pack v2.0.0, and it guides the reader trough the source code of the embedded software.
1. Introduction
The firmware in FP-AI-MONITOR1 implements a complex multi-tasking embedded application that takes full advantage of STM32 power. The following image gives an idea of the complexity managed by the firmware: the left side of the image displays fourteen tasks (each task is an independent execution flow) running in parallel, together with several Interrupt Service Routine (ISR), in STM32L4R9ZI single-core microcontroller.
At the same time, we can see in the right part of the image that, despite the high number of context switches, the average load percentage of the MCU core, with a clock frequency set to 120MHz, is below 50%. These results are made possible by the use of an application framework optimized for STM32, and a set of firmware components designed on top of the framework.
1.1. Who should read this document?
This document is intended for firmware developers who develop or support the development of AI applications on the edge. Users of this document should have some knowledge of the following:
- Real Time Operating System (RTOS). FreeRTOSTM is part of the kernel of FP-AI-MONITOR1.
- Principle of Object Oriented programming (like inheritance, polymorphism, virtual function).
- Unified Modeling Language (UML)
1.2. Main components of the firmware
We can look at the complex architecture of FP-AI-MONITOR1 from different perspectives, from the high-level view presented in the User Manual up to the more detailed diagram that we can find, in the developer documentation available in FP-AI-MONITOR1 local installation folder at this location:
Projects\STM32L4R9ZI-STWIN\Applications\FP-AI-MONITOR1\doc
The next sections look at the main components of the firmware. They are:
- eLooM: the application framework.
- Sensor Manager: an eLooM component to configure and get raw data from the sensors on the board.
- Digital Processing Unit (DPU): an eLooM component to process data.
On top of the above main components the application implements a set of AI-related processing tasks:
- AI_USC_Task_t
- AITask_t
- MfccTask_t
- NeaiTask_t
2. eLooM application framework (main concepts)
eLooM stands for embedded Light object-oriented fraMework for STM32. It is an application framework designed for STM32 and specifically for soft real-time, event drived, multi-tasking and low power embedded applications. It has been optimized over several years.
2.1. The Managed Task abstraction
The framework introduces the concept of Managed Task, which is an RTOS native task extended with new features. These new features are the result of analysis and generalization of problems common to STM32 applications, which leads us to a generic solution with an optimized trade-off between memory footprint and performance. The class diagram for the managed task is displayed in the following image:
If we think of a Managed Task as an OO class, then it implements a set of methods used by the framework to coordinate the task activities at runtime, like:
- System initialization: At startup, the system initializes all hardware resources as well as the software ones used by the Managed Tasks.
- Power management: The system coordinates the Managed Tasks to switch from one state to the other of a Power Mode State Machine (PM State Machine, or simply State Machine)[1] defined by the application.
- Error management: The system handles the errors reported by a Managed Task or its sub-components, and it checks that all Managed Tasks are working fine.
Not all methods are implemented by the AManagedTask or its subclass AManagedtTaskEx. Indeed, in the above image, the methods displayed in italic inside the Virtual methods block are pure virtual functions. Note that the prefix 'A' in front of the class name (AManagedTask) stands for abstract. This means that we cannot instantiate an object of the class (because it would be an incomplete object), but a developer can subclass one of the Managed Task classes and provide an application-specific implementation. This is what happens in FP-AI-MONITOR1. The following image shows the application-specific class we provide with the function pack as white rectangles, while the sky blue ones are provided by the framework.
By extending one of the base classes provided by the framework and implementing the pure virtual functions, the application tasks are well integrated and the application code is split from the base code provided by ST.
2.1.1. AI_USC_Task, a concrete example
Let us look at one of the managed tasks created for the function pack, the AI Ultrasound Classification Task ( AI_USC_Task_t). As a general recommendation, the implementation is split into three files, two header files, and one source file:
- AI_USC_Task.h: the main header file declares the type for the new managed task and its public API.
- AI_USC_Task_vtbl.h: the header file containing only all the virtual functions implemented by the managed task. Declaring all virtual functions in a separate file is a practical choice to understand at a glance which behaviors are redefined by the class. It is not a mandatory rule. Another way is to search the Outline view of the IDE for all function names that contain _vtbl (that stands for virtual table) as shown in the below image.
- AI_USC_Task.c: the source file defines the managed task. This file contains the implementation of the public as well as the private methods of the managed task.
How does a user-defined managed task extends the AManagedTask or the AManagedTaskEx base classes provided by the framework? The technique used is the inheritance by composition[2] because it is easy to implement in C.
/* file:AI_USC_Task.h */
/**
* Create a type name for _AI_USC_Task_t.
*/
typedef struct _AI_USC_Task_t AI_USC_Task_t;
/**
* AI_USC_Task_t internal structure.
*/
struct _AI_USC_Task_t
{
/**
* Base class object.
*/
AManagedTaskEx super;
/* Class-specific members must be declared here */
/**
* Task input message queue. The task receives messages of type struct AIMessage_t in this queue.
* This is one of the ways the task exposes its services at the application level.
*/
QueueHandle_t in_queue;
/* Task variables should be added here. */
/**
* Digital processing Unit specialized in the CubeAI library.
*/
AiUSC_DPU_t dpu;
/**
* Data buffer used by the DPU but allocated by the task. The size of the buffer depends
* on many parameters like:
* - the type of the data used as input by the DPU
* - the length of the signal
* - the number of signals to manage circularly to decouple the data producer and the data process.
* The correct size in bytes is computed by the DPU with the method AiUSC_DPUSetStreamsParam().
*/
void *p_dpu_buff;
};
The first member in the AI_USC_Task_t structure is a variable of the base class (AManagedTaskEx super), so, thanks to the way AManagedTask is defined, it is possible to use a pointer of type AI_USC_Task_t* with all the functions that require a parameter of type AManagedTask* or AManagedTaskEx*. For example:
AI_USC_Task_t my_task; ACAddTask(pAppContext, (AManagedTask*)&my_task);
In the above example, we use the explicit cast of the pointer to avoid compiler warnings.
There is one more thing to do: we need to use the virtual functions defined by the AI_USC_Task_t class to override those defined in the base class. This is done during the allocation of an instance of the class, as highlighted in the following snippet:
/* file:AI_USC_Task.c */
/**
* The only instance of the task object.
*/
static AI_USC_Task_t sTaskObj;
AManagedTaskEx *AI_USC_TaskAlloc(void)
{
/* In this application there is only one instance of the task,
* so this allocator implements the singleton design pattern.
*/
/* Initialize the super class */
AMTInitEx(&sTaskObj.super);
sTaskObj.super.vptr = &sTheClass.vtbl;
return (AManagedTaskEx*)&sTaskObj;
}
The virtual pointer (sTaskObj.super.vptr) points to a table, named virtual table, containing all the pointers to the virtual functions in the correct order, as defined by the base class:
/* file:AManagedTaskEx_vtbl.h */
/**
* Create type name for _AManagedTask_vtb.
*/
typedef struct _AManagedTaskEx_vtbl AManagedTaskEx_vtbl;
struct _AManagedTaskEx_vtbl {
sys_error_code_t (*HardwareInit)(AManagedTask *_this, void *pParams);
sys_error_code_t (*OnCreateTask)(AManagedTask *_this, TaskFunction_t *pvTaskCode, const char **pcName, unsigned short *pnStackDepth, void **pParams, UBaseType_t *pxPriority);
sys_error_code_t (*DoEnterPowerMode)(AManagedTask *_this, const EPowerMode eActivePowerMode, const EPowerMode eNewPowerMode);
sys_error_code_t (*HandleError)(AManagedTask *_this, SysEvent xError);
sys_error_code_t (*OnEnterTaskControlLoop)(AManagedTask *_this);
sys_error_code_t (*ForceExecuteStep)(AManagedTaskEx *_this, EPowerMode eActivePowerMode);
sys_error_code_t (*OnEnterPowerMode)(AManagedTaskEx *_this, const EPowerMode eActivePowerMode, const EPowerMode eNewPowerMode);
};
For the AI_USC_Task_t the virtual table is defined in the structure AI_USC_TaskClass_t, and in its initialization code, highlighted in the following snippet, we can see how the virtual functions of the AI_USC_Task_t class are linked with the base class:
/* file:AI_USC_Task.c */
/**
* Class object declaration. The class object encapsulates members that are shared between
* all instances of the class.
*/
typedef struct _AI_USC_TaskClass_t {
/**
* AI_USC_Task class virtual table.
*/
AManagedTaskEx_vtbl vtbl;
/**
* AI_USC_Task class (PM_STATE, ExecuteStepFunc) map. The map is implemented with an array and
* The key is the index. The number of items of this array must be equal to the number of PM state
* of the application. If the managed task does nothing in a PM state, then set to NULL the
* relative entry in the map.
*/
pExecuteStepFunc_t p_pm_state2func_map[];
} AI_USC_TaskClass_t;
};
/**
* The class object initialization.
*/
static const AI_USC_TaskClass_t sTheClass = {
/* Class virtual table */
{
AI_USC_Task_vtblHardwareInit,
AI_USC_Task_vtblOnCreateTask,
AI_USC_Task_vtblDoEnterPowerMode,
AI_USC_Task_vtblHandleError,
AI_USC_Task_vtblOnEnterTaskControlLoop,
AI_USC_Task_vtblForceExecuteStep,
AI_USC_Task_vtblOnEnterPowerMode
},
/* class (PM_STATE, ExecuteStepFunc) map */
{
AI_USC_TaskExecuteStepState1,
NULL,
NULL,
NULL,
AI_USC_TaskExecuteStepAIActive,
NULL,
AI_USC_TaskExecuteStepAIActive
}
};
At this point, the AI_USC_Task behaves as a managed task.
There is another question to be answered: how the framework knows about the managed tasks created by the application?
2.2. Application entry points
In a typical bare-metal application with a procedural programming model, a developer starts coding inside the main() function, that is the initial entry point. This is not the case for an eLooM based application where the main.c file is very simple like this:
/* file main.c */
#include <stdio.h>
#include "services/sysinit.h"
#include "task.h"
/* The main function initializes a minimum set of hardware resources and creates the INIT task, before giving the control to the scheduler.
* The main application entry points are defined in the file App.c
*/
int main()
{
// System initialization.
SysInit(FALSE);
vTaskStartScheduler();
while (1);
}
Normally the main.c file doesn't need to be modified. eLooM, instead, defines four entry points as weak functions as reported in the following table.
Call order | function prototype | Note |
---|---|---|
1 | IApplicationErrorDelegate *SysGetErrorDelegate(void) | Optional. This function is used by the system during the application startup to get an application-specific object that implements the IApplicationErrorDelegate interface. |
2 | IAppPowerModeHelper *SysGetPowerModeHelper(void) | Mandatory. This function is used by the system during the application startup to get an application-specific object that implements the IAppPowerModeHelper interface. |
3 | sys_error_code_t SysLoadApplicationContext(ApplicationContext *pAppContext) | Mandatory. Add all managed tasks to the application context |
4 | sys_error_code_t SysOnStartApplication(ApplicationContext *pAppContext) | Optional. This function is called by the framework at the end of the initialization process and before the INIT task releases the control to the application tasks. |
A developer must provide at least the SysGetPowerModeHelper() and the SysLoadApplicationContext() functions. They can be defined in an application file. For example FP-AI-MONITOR1 uses the file App.c for this purpose.
Let us look at the SysLoadApplicationContext() function defined in the function pack.
/* file: App.c */
sys_error_code_t SysLoadApplicationContext(ApplicationContext *pAppContext)
{
assert_param(pAppContext);
sys_error_code_t xRes = SYS_NO_ERROR_CODE;
// Allocate the task objects
spSPIBusObj = SPIBusTaskAlloc(&MX_SPI3InitParams);
spIMP23ABSUObj = IMP23ABSUTaskAlloc(&MX_DFSDMCH0F1InitParams, &MX_ADC1InitParams);
spISM330DHCXObj = ISM330DHCXTaskAlloc();
spIIS3DWBObj = IIS3DWBTaskAlloc();
spUtilObj = UtilTaskAlloc(&MX_TIM5InitParams, &MX_TIM16InitParams, &MX_GPIO_PF6InitParams);
spNeaiObj = NeaiTaskAlloc();
spAIObj = AITaskAlloc();
spAI_USC_Obj = AI_USC_TaskAlloc();
spMfccObj = MfccTaskAlloc();
spControllerObj = AppControllerAlloc();
DataInjectorTaskAllocStatic(&sDataInjObj);
// Add the task object to the context.
xRes = ACAddTask(pAppContext, (AManagedTask*)spSPIBusObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spIMP23ABSUObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spISM330DHCXObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spIIS3DWBObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spUtilObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spNeaiObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spAIObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spAI_USC_Obj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spMfccObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)spControllerObj);
xRes = ACAddTask(pAppContext, (AManagedTask*)&sDataInjObj);
return xRes;
}
In the beginning, all the managed task objects are allocated. The allocation strategy is an important topic for an embedded application, but it is not covered in this article. Nevertheless let us note that we prefer to use, whenever it is possible, static allocation, and the Singleton design pattern when it makes sense for the specific class.
Once a managed task object is allocated, we tell to the framework that this task is part of the application by using the function ACAddTask() provided by the Application Context API declared in the ApplicationContext.h file , for example:
xRes = ACAddTask(pAppContext, (AManagedTask*)spNeaiObj);
If a managed task is not added to the application context then it is not initialized, its resources are not allocated, the native RTOS task is not created, and so on. It doesn't exist during the application execution.
In the above example, the six tasks highlighted in yellow are the specific ones created for this function pack, the other tasks are provided by the Sensor Manager component, and we will introduce them in the next section.
The rest of the system initialization is done by the framework thanks to the INIT task that coordinates all managed tasks added to the application context as described in the section eLooM framework > System initialization of the developer documentation available in FP-AI-MONITOR1 local installation folder at this location:
Projects\STM32L4R9ZI-STWIN\Applications\FP-AI-MONITOR1\doc
3. Sensor Manager: main concepts
Sensor Manager is an eLooM-based application-level module that interfaces sensors and offers their data to other application modules. It is implemented as an acquisition engine that:
- Orchestrates multiple managed tasks accesses to sensor bus data as follows:
- One or more sensors for each managed task
- Read/write requests via a queue to handle concurrency on common buses (a physicals bus is represented as a resource controlled by a managed task acting as gate keeper)
- Defines interfaces to avoid implementation dependencies
- Dispatches events to notify when data is ready
The following image is a high-level class diagram showing how the Sensor Manager (pink boxes) extends the framework.
The current implementation of the Sensor Manager supports these sensors:
- HTS221
- IIS3DWB
- IMP23ABSU
- ISM330DHCX
- LPS22HB
- LPS22HH
More sensors will be supported with further releases of the eLooM component.
You find more information about the Sensor Manager in the section Sensor Manager of the developer documentation available in FP-AI-MONITOR1 local installation folder at this location:
Projects\STM32L4R9ZI-STWIN\Applications\FP-AI-MONITOR1\doc
3.1. Simple and advanced API exposed by the Sensor Manager
The first thing we need to understand is how to interact with a sensor supported by the Sensor Manager. We saw that sensors and buses are modeled as subclasses of AManagedTaskEx. It means that working with a sensor is a two steps process:
- To add the sensor to the Application Context, so that the framework knows about it, and it initializes the sensor subsystem.
- To interact with the sensor using the proper API.
A sensor task is added to the Application Context during the system initialization as each other managed tasks, as we saw in the code snippet of the function SysLoadApplicationContext(). If the physical sensor is connected to a bus then we need to do the same in the application code. This is normally done after all the objects have been initialized, in the SysOnStartApplication() entry point like in the FP code.
/* file: App.c */
sys_error_code_t SysOnStartApplication(ApplicationContext *pAppContext) {
UNUSED(pAppContext);
/* Re-map the state machine of the Sensor Manager tasks */
SensorManagerStateMachineRemap(spAppPMState2SMPMStateMap);
/* Disable the automatic low power mode timer */
UtilTaskSetAutoLowPowerModePeriod((UtilTask_t*)spUtilObj, 0);
/* connect the sensors tasks to the SPI bus. */
SPIBusTaskConnectDevice((SPIBusTask*)spSPIBusObj, ISM330DHCXTaskGetSensorIF((ISM330DHCXTask*)spISM330DHCXObj));
SPIBusTaskConnectDevice((SPIBusTask*)spSPIBusObj, IIS3DWBTaskGetSensorIF((IIS3DWBTask*)spIIS3DWBObj));
/* set the output queue for the USB CDC device. It is used to deliver all the incoming input */
CDC_SetOutQueue(AppControllerGetInQueue((AppController_t*)spControllerObj));
/* Connect the Util Task with the AppController task to propagate the push button event. */
UtilTaskSetCtrlInQueue((UtilTask_t*)spUtilObj, AppControllerGetInQueue((AppController_t*)spControllerObj));
/* register AI processing with the application controller. */
QueueHandle_t queueAi = AITaskGetInQueue((AITask_t*)spAIObj);
QueueHandle_t queueMfcc = MfccTaskGetInQueue((MfccTask_t*)spMfccObj);
QueueHandle_t queueUsc = AI_USC_TaskGetInQueue((AI_USC_Task_t*)spAI_USC_Obj);
QueueHandle_t queueNeai = NeaiTaskGetInQueue((NeaiTask_t*)spNeaiObj);
QueueHandle_t queueUtil = UtilTaskGetInQueue((UtilTask_t*)spUtilObj);
AppControllerSetAIProcessesInQueue((AppController_t*)spControllerObj, queueAi, queueMfcc, queueUsc,queueNeai,queueUtil);
/* set Mfcc DPU to controller */
IDPU * p_dpu = MfccTaskGetDpu((MfccTask_t*)spMfccObj);
AppControllerSetPreprocessDPU((AppController_t*)spControllerObj,p_dpu);
/* Set the memory storage area for the Data Injector task */
DataInjectorTaskSetMemStorageLocation(&sDataInjObj, GET_AI_DATA_STORAGE_ADDR(), AI_DATA_STORAGE_SIZE);
return SYS_NO_ERROR_CODE;
}
For the second step, the Sensor Manager provides a different set of APIs targeting a simple use of the sensor or a more advanced one. The simple way to operate a sensor is to use the API exported by the SensorManager class.
Given the ID of a sensor, it is possible to set its basic parameter like ODR, full scale, and so on. To get the actual value of the sensor 's parameter we can use the SMGetSensorObserver() function to get the ISourceObservable interface of the sensor. This interface has been designed to provide a uniform and immutable interface between all sensors. All SensorManager APIs are based on the idea that a sensor has an ID. To know the ID of a sensor it is possible to use the SIterator or the SQuery services provided by the Sensor Manager. The SIterator is used to iterate through the sensor collection managed by the Sensor Manager. The SQuery is used to search for sensors that match a given query. This is an example:
/* using a SIterator object. */
SIterator_t iterator;
SIInit(&iterator, SMGetSensorManager());
while(SIHasNext(&iterator))
{
uint16_t sensor_id = SINext(&iterator);
// do something with the sensor
ISourceObservable *p_sensor_observer = SMGetSensorObserver(sensor_id);
float odr = ISourceGetODR(p_sensor_observer);
SMSensorSetODR(sensor_id, odr+1000);
}
/* using a SQuery object. */
SQuery_t query;
SQInit(&query, SMGetSensorManager());
sensor_id = SQNextByNameAndType(&query, "ism330dhcx", COM_TYPE_ACC);
if (sensor_id != SI_NULL_SENSOR_ID)
{
SMSensorEnable(sensor_id);
SMSensorSetODR(sensor_id, 1666);
SMSensorSetFS(sensor_id, 4.0);
}
Of course, the Sensor Manager allows an advanced use of the sensor. It is possible to subclass a sensor class to access all the sensor internal data and also the low-level PID, but this is out of the scope of this tutorial.
3.2. Sensors used in FP-AI-MONITOR1
The current implementation of the Sensor Manager supports six sensors. Only three sensors are used by FP-AI-MONITOR1:
- IIS3DWB
- IMP23ABSU
- ISM330DHCX
In fact in the project three there are only the managed tasks for the used sensor, as displayed in the following image:
It shows how easy is to use a sensor supported by the Sensor Manager thanks to the modularity of an eLooM based component. To use other sensors we need only to link the relative files (two headers files and one source file) to the project.
4. DPU: main concepts
Digital Processing Unit (DPU) is an eLooM-based application-level module that provides:
- A set of processing objects ready to use to process data coming from a data source (like the sensors of the Sensor Manager).
- An abstract class and a set of interfaces to simplify the creation of new DPU.
The above image shows the class diagram of the DPU engine. Starting from the definition of a generic DPU interface (IDPU), it provides an abstract class (ADPU) that implements the basic behavior of a DPU. The ADPU class is then used as base class to implement the concrete DPU used in the function pack.
4.1. DPU programming model
DPU are software objects that are able to do few things:
- To connect to a data source, like a sensor.
- To transform the input data in output data by applying a specific processing.
- To dispatch the output data to all registered listeners.
4.1.1. Connect a DPU to a data source
To attach an input data source to a DPU we use the API sys_error_code_t IDPU_AttachToSensor(IDPU *_this, ISourceObservable *s, void *buffer)
. The parameter buffer
is an optional input parameter used to pass to the DPU a memory buffer allocated by the application. This buffer is used by the DPU to store the data coming the data source, as well as to take advantage of the multi-tasking system. In fact in a typical scenario a DPU stores the data coming from a data producer task (like a sensor), while, at the same time, it process the data ready in a dedicated processing task as showed in the following image.
Let's give a look at a concrete example from FP-AI-MONITOR1: how the NeaiTask (that is a processing task) connects the NeaiDPU to a sensor.
// file NeaiTask.c
sys_error_code_t NeaiTaskAttachToSensorEx(NeaiTask_t *_this, ISourceObservable *p_sensor, uint16_t signal_size, uint8_t axes, uint8_t cb_items)
{
assert_param(_this != NULL);
sys_error_code_t res = SYS_NO_ERROR_CODE;
/* check if there is a sensor already attached */
if (_this->p_dpu_buff != NULL)
{
vPortFree(_this->p_dpu_buff);
_this->p_dpu_buff = NULL;
}
uint32_t buff_size = NeaiDPUSetStreamsParam(&_this->dpu, signal_size, axes, cb_items);
_this->p_dpu_buff = pvPortMalloc(buff_size);
if (_this->p_dpu_buff != NULL)
{
res = IDPU_AttachToSensor((IDPU*)&_this->dpu, p_sensor, _this->p_dpu_buff);
SYS_DEBUGF(SYS_DBG_LEVEL_VERBOSE, ("NAI: dpu buffer = %i byte\r\n", buff_size));
}
else
{
res = SYS_OUT_OF_MEMORY_ERROR_CODE;
SYS_SET_SERVICE_LEVEL_ERROR_CODE(SYS_OUT_OF_MEMORY_ERROR_CODE);
}
return res;
}
In the above code snippet we note that before calling the IDPU_AttachToSensor()
API, we use another function specific of NeaiDPU, that is NeaiDPUSetStreamsParam()
. This function, depending on the input parameters, well-known to an user of NanoEdge AI library, returns the size in byte of the memory buffer needed by the DPU. In this way the application can allocate a buffer of a proper size.
That buffer is optional, and, if it is not used then the DPU will process the data on the fly. Note that is not always possible to process data on the fly because the format of the input data coming from the data source maybe not compatible with the internal working data format needed by the DPU. In the case of the NeaiDPU attached to an inertial sensor, for example, sensor data are of type int16_t
, while the DPU need data of type float
. This data conversion is transparent to the application code and it is performed by the ADPU class.
4.1.2. Process a data when it is ready
When there are enough source data to be processed the DPU engine activates the processing function. While the data collection is performed in a generic way by the ADPU base class, the actual processing depends on the nature of the concrete DPU. This is why the NeaiDPU (as well as all others DPU) override the virtual function sys_error_code_t IDPU_Process(IDPU *_this)
to provide the concrete implementation sys_error_code_t NeaiDPU_vtblProcess(IDPU *_this
. In this case it calls the proper NanoEdge AI processing function.
4.1.3. Notify the listeners when a new processed data is ready
When the source data has been processed the DPU notify all the registered listeners. A DPU developer doesn't need to write the code to notify the listeners because it is provided by the ADPU class. all that is required is initialize a new ProcessEvent
and call the sys_error_code_t IDPU_DispatchEvents(IDPU *_this, ProcessEvent *pxEvt)
API. As example the following snippet show the last part of the NeaiDPU_vtblProcess()
function.
//file: NeaiDPU.c
sys_error_code_t NeaiDPU_vtblProcess(IDPU *_this)
{
assert_param(_this != NULL);
sys_error_code_t xRes = SYS_NO_ERROR_CODE;
ADPU * super = (ADPU*)_this;
NeaiDPU_t *p_obj = (NeaiDPU_t*)_this;
//...
{
ProcessEvent evt_neai;
ProcessEventInit((IEvent*)&evt_neai, super->pProcessEventSrc, (ai_logging_packet_t*)&super->dpuOutStream, ADPU_GetTag(super));
IDPU_DispatchEvents(_this, &evt_acc);
}
return xRes;
}
To receive a ProcessEvent
an object must implement the IProcessEventListener
interface and register itself to the DPU:
NeaiDPU dpu; IProcessEventListener *p_process_listener = GetProcessListenerIF(&an_obj); IEventSrc *p_evt_src = ADPU_GetEventSrcIF((ADPU*)&dpu); res = IEventSrcAddEventListener(p_evt_src, (IEventListener*)p_process_listener );
In FP-AI-MONITOR1 an example is provided in the AppController
task that, before entering its control loop, it register itself as a IProcessListener
with the NeaiTask
.
// file: AppController.c
// function: sys_error_code_t AppController_vtblOnEnterTaskControlLoop(AManagedTask *_this)
struct NeaiMessage_t msg1 = {
.msgId = APP_MESSAGE_ID_NEAI,
.cmd_id = NAI_CMD_ADD_DPU_LISTENER,
.param.n_param = (uint32_t)&p_obj->listenetIF
};
if (pdTRUE != xQueueSendToBack(p_obj->neai_in_queue, &msg1, pdMS_TO_TICKS(100)))
{
res = SYS_NAI_TASK_IN_QUEUE_FULL_ERROR_CODE;
SYS_SET_SERVICE_LEVEL_ERROR_CODE(SYS_NAI_TASK_IN_QUEUE_FULL_ERROR_CODE);
}
The NeaiTask
is the owner of the NeaiDPU
and it forwards the request to the NeaiDPU
when it process the command NAI_CMD_ADD_DPU_LISTENER
in its task control loop.
4.2. DPU used in FP-AI-MONITOR1
5. Footnote and References
- ↑ The PM State machine is a generic implementation of a state machine. It is named Power Mode State Machine only because in the first products the main purpose was to manage the low power mode of the embedded application.
- ↑ eLooM supports single inheritance and multiple interfaces. This is different from the multiple inheritances supported by C++, but it is simple to implement in C and it adds flexibility to an embedded application.
6. Appendix A: UML and color convention
The UML diagrams presented in this article describe the architecture of some of the mains elements of the function pack. Because of the dependency between the elements, a color convention is used to identify the package to which each element belongs, as displayed in the following image.
When the color is not specified (black for foreground and text, and white for the background), then the element belongs to the main component described in the section.