1. STM32WB - Bluetooth® LE Coprocessor Binaries
This is a description about the Bluetooth® LE Wireless stack available for the secure CM0+ coprocessor of the STM32WB.
Most of the information can be found within the Release Note for STM32WBxx Copro Wireless Binaries.
For more information on how to bring up the hardware to run simple Bluetooth® LE application check the Bluetooth® LE hardware setup page.
1.1. Link between wireless coprocessor binaries and Bluetooth® LE stack variant
STM32WB_BLE_Wireless_Interface.html [1] file and AN5270 [2] show which Application Commands Interface (ACI) and Host Commands Interface (HCI) are supported according to Bluetooth® LE stack variant. The following table shows the correspondence between the wireless coprocessor binaries and Bluetooth® LE stack variant:
Link between wireless coprocessor binaries and Bluetooth® LE stack variant | |||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
1.2. CubeWB v1.14.0 - Bluetooth® LE Wireless stack Summary
For Bluetooth® LE applications, 6 binaries are available and certified BLE 5.3. According to the type of application, the size of the flash, it is up to the developer to load the right binary:
BLE Stack 5.3 Certified | GAP Peripheral | GAP Central | GATT Server | GATT Client | PHY 2M | Data Length Extension | Legacy Pairing, LE secure connection | Privacy | Filter Accept List | HCI Interface | Direct Test Mode | L2CAP Connection Oriented channels support | Channel Selection #2 | Extended Advertising Scanning | BT SIG Declaration ID |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Full Extended | ● | ● | ● | ● | ● | ● | ● | ● | ● | ● | ● | ● | ● | ● | id123456 |
Full | ● | ● | ● | ● | ● | ● | ● | ● | ● | reduced | id123456 | ||||
Light | ● | ● | ● | ● | ● | ● | reduced | id123456 | |||||||
HCI Extended | ● | ● | ● | ● | ● | id123456 | |||||||||
HCI | ● | ● | ● | ● | id123456 | ||||||||||
AdvScan | reduced | id123456 |
- stm32wbxx_BLE_Stack_full_extended_fw.bin - 177KB - Link Layer, HCI, L2CAP, ATT, SM, GAP and GATT database
- To be used for Adverting/Scanning Extension - Full HCI/ACI/DTM commands/Event support
- To be used for GAP Central/Peripheral & GATT Server/Client applications
- support up to 8 connections with maximum 2 links as Slave
- stm32wbxx_BLE_Stack_full_fw.bin - 143KB - Link Layer, HCI(limited), L2CAP, ATT, SM, GAP and GATT database
- To be used for GAP Central/Peripheral & GATT Server/Client applications
- support up to 8 connections with maximum 2 links as Slave
- stm32wbxx_BLE_Stack_light_fw.bin - 112KB - Link Layer, HCI(limited), L2CAP, ATT, SM, GAP(limited) and GATT(limited) database
- To be used for GAP Peripheral & GATT Server applications
- support up to 2 links as Slave
- stm32wbxx_BLE_HCILayer_fw.bin - 93KB - Link Layer, HCI, DTM
- To be used for BLE Host Stack running on CM4 application processor (Arduino, Zephyr,..)
- stm32wbxx_BLE_HCILayer_extended_fw.bin - 93KB - Link Layer, HCI, DTM, Extended Advertising/Scanning
- To be used for BLE Host Stack running on CM4 application processor (Arduino, Zephyr,..)
- stm32wbxx_BLE_HCI_AdvScan_fw.bin - 34KB - Link Layer, HCI reduced
- To be used for advertising and scanning through HCI interface
1.3. Stack Extended Information
To use extended binaries, it is necessary to adapt the scatter file in the BLE applications as:
- The RAM_A shared range shall be reduced to memory range [0x20030000:0x200307FF]
- The Mail-box buffers(MB_MEM1, MB_MEM2) shall be located in RAM_B shared defined in memory range [0x20038000:0x2003A7FF]
- The RAM_B shared shall be added to Total_RAM_region
define symbol __ICFEDIT_region_RAM_SHARED_start__ = 0x20030000;
define symbol __ICFEDIT_region_RAM_SHARED_end__ = 0x200307FF;
define symbol __ICFEDIT_region_RAM_B_SHARED_start__ = 0x20038000;
define symbol __ICFEDIT_region_RAM_B_SHARED_end__ = 0x2003A7FF;
define region RAM_B_SHARED_region = mem:[from __ICFEDIT_region_RAM_B_SHARED_start__ to __ICFEDIT_region_RAM_B_SHARED_end__];
define region Total_RAM_region = RAM_region | RAM_SHARED_region | RAM_B_SHARED_region;
1.4. CubeWB Application & Bluetooth® LE Stacks association
The following table shows the Bluetooth® LE stack to be used for the different applications available within the CubeWB package TO BE UPDATED
Bluetooth® LE stack and Application compatibility | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|