FP-AI-MONITOR1 user manual

Revision as of 09:38, 6 April 2022 by Registered User (→‎Terms and definitions)

Sensing and condition monitoring are two of the major components of the IoT and predictive maintenance systems, enabling context awareness, production performance improvement, a drastic decrease in the downtime due to routine maintenance, and so, maintenance cost reduction.

The FP-AI-MONITOR1 function pack is a multi-sensor AI data monitoring framework on the wireless industrial node, function pack for STM32Cube. It helps to jump-start the implementation and development of sensor-monitoring-based applications designed with the X-CUBE-AI Expansion Package for STM32Cube or with the NanoEdge™ AI Studio. It covers the entire design of the Machine Learning cycle from the data set acquisition to the integration on a physical node.

The FP-AI-MONITOR1 runs learning and inference sessions in real-time on the SensorTile Wireless Industrial Node development kit (STEVAL-STWINKT1B), taking data from onboard sensors as input. The FP-AI-MONITOR1 implements a wired interactive CLI to configure the node and manages the learn and detect phases. For simple in the field operation, a standalone battery-operated mode allows basic controls through the user button, without using the console.

The STEVAL-STWINKT1B has an STM32L4R9ZI ultra-low-power microcontroller (Arm® Cortex®‑M4 at 120 MHz with 2 Mbytes of Flash memory and 640 Kbytes of SRAM). In addition, the STEVAL-STWINKT1B embeds industrial-grade sensors, including 6-axis IMU, 3-axis accelerometer and vibrometer, and analog microphones to record any inertial, vibrational and acoustic data with high accuracy at high sampling frequencies.

The rest of the article discusses the following topics:

  • The general information about the FP-AI-MONITOR1,
  • Setting up the hardware and software components,
  • Button-operated modes,
  • Command-line interface (CLI),
  • Human activity recognition, a classification application using accelerometer data, using a pre-trained model powered by X-CUBE-AI,
  • Anomaly detection using NanoEdge™ AI,
  • Anomaly classification using NanoEdge™ AI classification libraries based on vibration and inertial data,
  • Dual-mode to run the anomaly detection using the NanoEdge™ AI library and state classification of a USB fan based on the ultrasonic data from an analog microphone, using a pre-trained model powered by X-CUBE-AI,
  • Performing the data logging using onboard vibration sensors and a prebuilt binary of FP-SNS-DATALOG1, and
  • Some links to useful online resources, to help a user better understand and customize the project for specific needs.
Info white.png Information
NOTE: The NanoEdge™ library generation itself is out of the scope of this function pack and must be generated using NanoEdge™ AI Studio.

1. General information

1.1. Feature overview

  • Complete firmware to program an STM32L4+ sensor node for sensor-monitoring-based applications on the STEVAL-STWINKT1B SensorTile wireless industrial node
  • Runs classical Machine Learning (ML) and Artificial Neural Network (ANN) models generated by the X-CUBE-AI, an STM32Cube Expansion Package
  • Runs NanoEdge™ AI libraries generated by NanoEdge™ AI Studio for AI-based anomaly detection applications. Easy integration by replacing the pre-integrated stub
  • Application example of human activity classification based on motion sensors
  • Application example of combined anomaly detection based on vibration and anomaly classification based on ultrasound
  • Application binary of high-speed datalogger for STEVAL-STWINKT1B data record from any combination of sensors and microphones configured up to the maximum sampling rate on a microSD™ card
  • Sensor manager firmware module to configure any of the onboard sensors easily, and suitable for production applications
  • eLooM (embedded Light object-oriented fraMework) enabling efficient development of soft real-time, multi-tasking, and event-driven embedded applications on STM32L4+ Series microcontrollers
  • Digital processing unit (DPU) firmware module providing a set of processing blocks, which can be chained together, to apply mathematical transformations to the sensor data
  • Configurable autonomous mode controlled by user button,
  • Interactive command-line interface (CLI):
  • Node and sensor configuration
  • Configure the application running either an X-CUBE-AI (ML or ANN) model, or a NanoEdge™ AI Studio anomaly detection model with the learn-and-detect capability
  • Configure the application concurrently running an X-CUBE-AI ANN model and a NanoEdge™ AI Studio model with the learn-and-detect capability
  • Configure the application running a NanoEdge™ AI Studio model for classification using vibration data
  • Easy portability across STM32 microcontrollers using the STM32Cube ecosystem
  • Free and user-friendly license terms

1.2. Software architecture

The top-level architecture of the FP-AI-MONITOR1 function pack is shown in the following figure.

FP-AI-MONITOR1 V2 architecture.svg

The STM32Cube function packs leverage the modularity and interoperability of STM32 Nucleo and expansion boards running STM32Cube MCU Packages and Expansion Packages to create functional examples representing some of the most common use cases in certain applications. The function packs are designed to fully exploit the underlying STM32 ODE hardware and software components to best satisfy the final user application requirements.

Function packs may include additional libraries and frameworks, not present in the original STM32Cube Expansion Packages, which enable new functions and create more targeted and usable systems for developers.

STM32Cube ecosystem includes:

  • A set of user-friendly software development tools to cover project development from the design to the implementation, among which are:
    • STM32CubeMX, a graphical software configuration tool that allows the automatic generation of C initialization code using graphical wizards
    • STM32CubeIDE, an all-in-one development tool with peripheral configuration, code generation, code compilation, and debug features
    • STM32CubeProgrammer (STM32CubeProg), a programming tool available in graphical and command-line versions
    • STM32CubeMonitor (STM32CubeMonitor, STM32CubeMonPwr, STM32CubeMonRF, STM32CubeMonUCPD) powerful monitoring tools to fine-tune the behavior and performance of STM32 applications in real-time.
  • STM32Cube MCU & MPU Packages, comprehensive embedded-software platforms specific to each microcontroller and microprocessor series (such as STM32CubeL4 for the STM32L4+ Series), which include:
    • STM32Cube hardware abstraction layer (HAL), ensuring maximized portability across the STM32 portfolio
    • STM32Cube low-layer APIs, ensuring the best performance and footprints with a high degree of user control over the HW
    • A consistent set of middleware components such as FreeRTOS™, USB Device, USB PD, FAT file system, Touch library, Trusted Firmware (TF-M), mbedTLS, Parson, and mbed-crypto
    • All embedded software utilities with full sets of peripheral and application examples
  • STM32Cube Expansion Packages, which contain embedded software components that complement the functionalities of the STM32Cube MCU & MPU Packages with:
    • Middleware extensions and application layers
    • Examples running on some specific STMicroelectronics development boards

To access and use the sensor expansion board, the application software uses:

  • STM32Cube hardware abstraction layer (HAL): provides a simple, generic, and multi-instance set of generic and extension APIs (application programming interfaces) to interact with the upper layer applications, libraries, and stacks. It is directly based on a generic architecture and allows the layers that are built on it, such as the middleware layer, to implement their functions without requiring the specific hardware configuration for a given microcontroller unit (MCU). This structure improves library code reusability and guarantees easy portability across other devices.
  • Board support package (BSP) layer: supports the peripherals on the STM32 Nucleo boards.

1.3. Folder structure

FP-AI-MONITOR1 folder structure

The figure above shows the contents of the function pack folder. The content of each of these subfolders is as follows:

  • Documentation: contains a compiled .chm file generated from the source code, which details the software components and APIs.
  • Drivers: contains the HAL drivers, the board-specific drivers for each supported board or hardware platform (including the onboard components), and the CMSIS vendor-independent hardware abstraction layer for the Cortex®-M processors.
  • Middlewares: contains libraries and protocols for ST parts as well as for the third parties. The ST components include the eLoom libraries, X-Cube-AI runtime libraries, NanoEdge™ AI library substitutes, Audio Processing library, FFT library, and USB Device library.
  • Projects: contains a sample application software, which can be used to program the sensor board for classification and anomaly detection applications using the data from the motion sensors.
  • Utilities: contains python scripts and sample datasets. These python scripts can be used to create
  • Human Activity Recognition (HAR) models using
    • Convolutional Nural Networks (CNN),
    • Support Vector based Classifier (SVC), or
    • data preparation scripts for HAR with NanoEdge™ AI Studio.
  • Ultra Sound Classification (USC) models using Convolutional Neural Networks (CNN)
  • data preparation scripts for anomaly detection library generation from NanoEdge™ AI Studio.
  • data preparation scripts for anomaly classification library generation from NanoEdge™ AI Studio.

1.4. Terms and definitions

Acronym Definition
API Application Programming Interface
BSP Board Support Package
CLI Command-Line Interface
FP Function Pack
HAL Hardware Abstraction Layer
MCU Microcontroller Unit
ML Machine Learning
AI Artificial Intelligence
NEAI NanoEdge™ AI
SVC Support Vector Classifier
SVM Support Vector Machine
ANN Artificial Neural Network
CNN Convolutional Neural Network
ODE Open Development Environment
USC Ultrasound Classification
MFCC Mel-Frequency Cepstral Coefficient
Acronyms used in this article.

1.5. References

References Description Source
[1] X-CUBE-AI X-CUBE-AI
[2] NanoEdge™ AI Studio st.com/nanoedge
[3] STEVAL-STWINKT1B STWINKT1B
References

1.6. Licenses

FP-AI-MONITOR1 is delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement (SLA0048).

The software components provided in this package come with different license schemes as shown in the table below.

Software component Copyright License
Arm® Cortex®-M CMSIS Arm Limited Apache License 2.0
FreeRTOS™ Amazon.com, Inc. or its affiliates MIT
STM32L4xxx_HAL_Driver STMicroelectronics BSD-3-Clause
Board support package (BSP) STMicroelectronics BSD-3-Clause
STM32L4xx CMSIS Arm Limited - STMicroelectronics Apache License 2.0
eLooM application framework STMicroelectronics Proprietary
Python TM scripts STMicroelectronics BSD-3-Clause
Dataset STMicroelectronics Proprietary
Sensor Manager STMicroelectronics Proprietary
Audio preprocessing library STMicroelectronics Proprietary
Generic FFT library STMicroelectronics Proprietary
X-CUBE-AI runtime library STMicroelectronics Proprietary
X-CUBE-AI HAR model STMicroelectronics Proprietary
NanoEdge™ AI library stub STMicroelectronics Proprietary
Signal processing library STMicroelectronics Proprietary
Digital processing unit (DPU) STMicroelectronics Proprietary
Trace analyzer recorder Percepio AB Percepio Proprietary

2. Hardware and firmware setup

2.1. HW prerequisites and setup

To use the FP-AI-MONITOR1 function pack on STEVAL-STWINKT1B, the following hardware items are required:

  • STEVAL-STWINKT1B development kit board,
  • a microSD™ card and card reader to log and read the sensor data,
  • Windows® powered laptop/PC (Windows® 7, 8, or 10),
  • Two Micro USB cables, one to connect the sensor board to the PC, and another one for the STLINK-V3MINI, and
  • an STLINK-V3MINI.
FP-AI-MONITOR1-hardware.png

2.1.1. Presentation of the Target STM32 board

The STWIN SensorTile wireless industrial node (STEVAL-STWINKT1B) is a development kit and reference design that simplifies the prototyping and testing of advanced industrial IoT applications such as condition monitoring and predictive maintenance. It is powered with Ultra-low-power Arm® Cortex®-M4 MCU at 120 MHz with FPU, 2048 kbytes Flash memory (STM32L4R9). Other than this, STWIN SensorTile is equipped with a microSD™ card slot for standalone data logging applications, a wireless BLE4.2 (on-board), and Wi-Fi® (with STEVAL-STWINWFV1 expansion board), and wired RS485 and USB OTG connectivity, as well as Brand protection secure solution with STSAFE-A110. In terms of sensors, STWIN SensorTile is equipped with a wide range of industrial IoT sensors including:

  • an ultra-wide bandwidth (up to 6 kHz), low-noise, 3-axis digital vibration sensor (IIS3DWB)
  • a 6-axis digital accelerometer and gyroscope iNEMO inertial measurement unit (IMU) with machine learning (ISM330DHCX)
  • an ultra-low-power high-performance MEMS motion sensor (IIS2DH)
  • an ultra-low-power 3-axis magnetometer (IIS2MDC)
  • a digital absolute pressure sensor (LPS22HH)
  • a relative humidity and temperature sensor (HTS221)
  • a low-voltage digital local temperature sensor (STTS751)
  • an industrial-grade digital MEMS microphone (IMP34DT05), and
  • a wideband analog MEMS microphone (MP23ABS1)

Other attractive features include:

– a Li-Po battery 480 mAh to enable standalone working mode
STLINK-V3MINI debugger with programming cable to flash the board
– a Plastic box for ease of placing and planting the SensorTile on the machines for condition monitoring. For further details, the users are advised to visit this link

2.2. Software requirements

2.2.1. FP-AI-MONITOR1

  • Download the latest version of the FP-AI-MONITOR1, package from ST website, extract and copy the .zip file contents into a folder on the PC. The package contains binaries, source code and utilities for the sensor board STEVAL-STWINKT1B.

2.2.2. IDE

Info white.png Information
In this document all the steps presented are carried out with STM32CubeIDE but the same can also be done with any of the other two IDEs.

2.2.3. STM32CubeProgrammer

  • STM32CubeProgrammer (STM32CubeProg) is an all-in-one multi-OS software tool for programming STM32 products. It provides an easy-to-use and efficient environment for reading, writing, and verifying device memory through both the debug interface (JTAG and SWD) and the bootloader interface (UART, USB DFU, I2C, SPI, and CAN). STM32CubeProgrammer offers a wide range of features to program STM32 internal memories (such as Flash, RAM, and OTP) as well as external memory. FP-AI-MONITOR1 requires STM32CubeProgrammer 2.10.0.
  • This software is available from STM32CubeProg.

2.2.4. Tera Term

  • Tera Term is an open-source and freely available software terminal emulator, which is used to host the CLI of the FP-AI-MONITOR1 through a serial connection.
  • Users can download and install the latest version available from Tera Term website.

2.2.5. STM32CubeMX

STM32CubeMX is a graphical tool that allows a very easy configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization C code for the Arm® Cortex®-M core or a partial Linux® Device Tree for Arm® Cortex®-A core), through a step-by-step process. Its salient features include:

  • Intuitive STM32 microcontroller and microprocessor selection.
  • Generation of initialization C code project, compliant with IAR™, Keil® and STM32CubeIDE (GCC compilers) for Arm®Cortex®-M core
  • Development of enhanced STM32Cube Expansion Packages thanks to STM32PackCreator, and
  • Integration of STM32Cube Expansion packages into the project.

FP-AI-MONITOR1 requires STM32CubeMX V 6.5.0. To download the STM32CubeMX and obtain details of all the features please visit st.com.

2.2.6. X-Cube-AI

X-CUBE-AI is an STM32Cube Expansion Package part of the STM32Cube.AI ecosystem and extending STM32CubeMX capabilities with automatic conversion of pre-trained Artificial Intelligence models and integration of generated optimized library into the user project. The easiest way to use it is to download it inside the STM32CubeMX tool (version 7.1.0 or newer) as described in the user manual Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI) (UM2526). The X-CUBE-AI Expansion Package offers also several means to validate the AI models (both Neural Network and Scikit-Learn models) both on desktop PC and STM32, as well as to measure performance on STM32 devices (Computational and memory footprints) without ad-hoc handmade user C code.

2.2.7. Python 3.7.3

Python is an interpreted high-level general-purpose programming language. Python's design philosophy emphasizes code readability with its notable use of significant indentation. Its language constructs, as well as its object-oriented approach, aim to help programmers write clear, logical code for small and large-scale projects. To build and export AI models the reader requires to set up a Python environment with a list of packages. The list of the required packages along with their versions is available as a text file in /FP-AI-MONITOR1_V2.0.0/Utilities/requirements.txt directory. The following command is used in the command terminal of the anaconda prompt or Ubuntu to install all the packages specified in the configuration file requirements.txt:

pip install -r requirements.txt
Info white.png Information
NOTE: The FP-AI-MONITOR1 is tested with exactly the same versions of all the libraries. We noticed that different versions of few dependencies can cause some problems. In addition we recommend to use pip version 20.2.4 or 21.2.4.

2.2.8. NanoEdge™ AI Studio

NanoEdge™ AI Studio is a new Machine Learning (ML) technology to bring true innovation easily to the end-users. In just a few steps, developers can create optimal ML libraries for Anomaly Detection, 1-class classification, n-class classification, and extrapolation, based on a minimal amount of data. The main features of NanoEdge™ AI Studio are:

  • Desktop tool for design and generation of an STM32-optimized library for anomaly detection and feature classification of temporal and multi-variable signals
  • Anomaly detection libraries are designed using very small datasets. They can learn normality directly on the STM32 microcontroller and detect defects in real-time
  • Classification libraries are designed with a very small, labeled dataset. They classify signals in real-time
  • Supports any type of sensor: vibration, magnetometer, current, voltage, multi-axis accelerometer, temperature, acoustic and more
  • Explore millions of possible algorithms to find the optimal library in terms of accuracy, confidence, inference time, and memory footprint
  • Generate very small footprint libraries running down to the smallest Arm® Cortex®-M0 microcontrollers
  • Embedded emulator to test library performance live with an attached STM32 board or from test data files
  • Easy portability across the various STM32 microcontroller series

This function pack supports the Anomaly Detection and n-class Classification libraries generated by NanoEdge™ AI Studio for STEVAL-STWINKT1B. It facilitates users to log the data, prepare and condition it to generate the libraries from the NanoEdge™ AI Studio and then embed these libraries in the FP-AI-MONITOR1. NanoEdge™ AI Studio is available from www.st.com/stm32nanoedgeai under several options such as a single user or team license, or trial version, and personalized support based sprints. FP-AI-MONITOR1 is tested using NanoEdge™ AI Studio V3.0.2.

Info white.png Information
An evaluation version of the NanoEdge™ AI Studio can be freely downloaded to generate development libraries for selected STM32 Nucleo boards and Discovery kits, like STEVAL-STWINKT1B.

.

2.3. Program firmware into the STM32 microcontroller

This section explains how to select a binary file for the firmware and program it into the STM32 microcontroller. A precompiled binary file is delivered as part of the FP-AI-MONITOR1 function pack. It is located in the FP-AI-MONITOR1_V2.0.0/Projects/STM32L4R9ZI-STWIN/Applications/FP-AI-MONITOR1/Binary/ folder. When the STM32 board and PC are connected through the USB cable on the STLINK-V3E connector, the STEVAL-STWINKT1B appears as a drive on the PC. The selected binary file for the firmware can be installed on the STM32 board by simply performing a drag and drop operation as shown in the figure below. This will create a dialog to copy the file and once it is disappeared (without any error) this indicates that the firmware is programmed in the STM32 microcontroller.

FP-AI-MONITOR1 V2 drag drop installation.png

2.4. Using the serial console

A serial console is used to interact with the host board (Virtual COM port over USB). With the Windows® operating system, the use of the Tera Term software is recommended. Following are the steps to configure the Tera Term console for CLI over a serial connection.

2.4.1. Set the serial terminal configuration

Start Tera Term, select the proper connection, featuring the [USB Serial Device]. For the screenshot below this is COM10 but it could vary for different users.

tera term connection port choice.png

Set the parameters:

  • Terminal
    • [New line]:
      • [Receive]: CR
      • [Transmit]: CR
tera term connection new line.png
  • Serial
    The interactive console can be used with the default values.

2.4.2. Start FP-AI-MONITOR1 firmware

Restart the board by pressing the RESET button. The following welcome screen is displayed on the terminal.

FP-AI-MONITOR1 Console Welcome Message

From this point, start entering the commands directly or type help to get the list of available commands along with their usage guidelines.

Note: The firmware provided is generated with a HAR model based on SVC and users can test it straight out of the box. However, for the NanoEdge™ AI Library, a substitute is provided in place of the library. The user must generate the library with the help of the NanoEdge™ AI Studio, replace the substitute with this library, and rebuild the firmware. These steps will be described in detail in the article later.

3. Button-operated modes

This section provides details of the button-operated mode for FP-AI-MONITOR1. The purpose of the extended mode is to enable the users to operate the FP-AI-MONITOR1 on STWIN even in the absence of the CLI console.

In button-operated mode, the sensor node can be controlled through the user button instead of the interactive CLI console. The default values for node parameters and settings for the operations during auto-mode are provided in the FW. Based on these configurations, different modes such as ai, neai_detect, and neai_learn can be started and stopped through the user button on the node.

3.1. Interaction with user

The button-operated mode can work with or without the CLI and is fully compatible and consistent with the current definition of the serial console and its command-line interface (CLI).

The supporting hardware for this version of the function-pack (STEVAL-STWINKT1B) is fitted with three buttons:

  1. User Button, the only button usable by the SW,
  2. Reset Button, connected to STM32 MCU reset pin,
  3. Power Button connected to power management,

and three LEDs:

  1. LED_1 (green), controlled by Software,
  2. LED_2 (orange), controlled by Software,
  3. LED_C (red), controlled by Hardware, indicates charging status when powered through a USB cable.

So, the basic user interaction for button-operated operations is to be done through two buttons (user and reset) and two LEDs (green and orange). The following provides details on how these resources are allocated to show the users what execution phases are active or to report the status of the sensor node.

3.1.1. LED Allocation

In the function pack six execution phases exist:

idle: the system waits for user input.
ai detect: all data coming from the sensors are passed to the X-CUBE-AI library to detect anomalies.
neai learn: all data coming from the sensors are passed to the NanoEdge™ AI library to train the model.
neai detect: all data coming from the sensors are passed to the NanoEdge™ AI library to detect anomalies.
neai class: all data coming from the sensors are passed to the NanoEdge™ AI library to perform classification.
dual mode: all data coming from the sensors are passed to the NanoEdge™ AI library to detect anomalies and to X-CUBE-AI library to classify them.


At any given time, the user needs to be aware of the current active execution phase. We also need to report on the outcome of the detection when the detect execution phase is active, telling the user if an anomaly has been detected, or what activity is being performed by the user with the HAR application when the "ai" context is running.

The onboard LEDs indicate the status of the current execution phase by showing which context is running and also by showing the output of the context (anomaly or one of the four activities in the HAR case).

The green LED is used to show the user which execution context is being run.

Pattern Task
OFF -
ON IDLE
BLINK_SHORT X-CUBE-AI Running
BLINK_NORMAL NanoEdge™ AI learn
BLINK_LONG NanoEdge™ AI detection or classification or dual-mode

The Orange LED is used to indicate the output of the running context as shown in the table below:

Pattern Reporting
OFF Stationary (HAR) when in X-CUBE-AI mode, Normal Behavior when in NEAI mode
ON Biking (HAR)
BLINK_SHORT Jogging (HAR)
BLINK_LONG Walking (HAR) or anomaly detected (NanoEdge™ AI detection or dual-mode)

Looking at these LED patterns the user is aware of the state of the sensor node even when CLI is not connected.

3.1.2. Button Allocation

In the extended autonomous mode, the user can trigger any of the four execution phases. The available modes are:

  1. idle: the system is waiting for a command.
  2. ai: run the X-CUBE-AI library and print the results of the live inference on the CLI (if CLI is available).
  3. neai_learn: all data coming from the sensor is passed to the NanoEdge™ AI library to train the model.
  4. neai_detect: all data coming from the sensor is passed to the NanoEdge™ AI library to detect anomalies.

To trigger these phases, the FP-AI-MONITOR1 is equipped with the support of the user button. In the STEVAL-STWINKT1B sensor node, there are two software usable buttons:

  1. The user button: This button is fully programmable and is under the control of the application developer.
  2. The reset button: This button is used to reset the sensor node and is connected to the hardware reset pin, thus is used to control the software reset. It resets the knowledge of the NanoEdge™ AI libraries and reset all the context variables and sensor configurations to the default values.

To control the executions phases, we need to define and detect at least three different button press modes of the user button.

The following are the types of the press available for the user button and their assignments to perform different operations:

Button Press Description Action
SHORT_PRESS The button is pressed for less than (200 ms) and released Start AI inferences for X-CUBE-AI model.
LONG_PRESS The button is pressed for more than (200 ms) and released Starts the learning for NanoEdge™ AI Library.
DOUBLE_PRESS A succession of two SHORT_PRESS in less than (500 ms) Starts the inference for NanoEdge™ AI Library.
ANY_PRESS The button is pressed and released (overlaps with the three other modes) Stops the current running execution phase.

4. Command-line interface

The command-line interface (CLI) is a simple method for the user to control the application by sending command-line inputs to be processed on the device.

4.1. Command execution model

The commands are grouped into three main sets:

  • (CS1) Generic commands
    This command set allows the user to get the generic information from the device like the firmware version, UID, compilation date and time, and so on, and to start and stop an execution phase.
  • (CS2) AI commands
    This command set contains commands which are AI-specific. These commands enable users to work with the X-CUBE-AI and NanoEdge™ AI libraries.
  • (CS3) Sensor configuration commands
    This command set allows the user to configure the supported sensors and to get the current configurations of these sensors.

4.2. Execution phases and execution context

The five system execution phases are:

  • X-CUBE-AI: Data coming from the sensors is passed through the X-CUBE-AI models to run the inference on the HAR classification.
  • NanoEdge™ AI learning: Data coming from the sensors is passed to the NanoEdge™ AI library to train the model.
  • NanoEdge™ AI detection: Data coming from the sensors is passed to the NanoEdge™ AI library to detect anomalies.
  • NanoEdge™ AI Classification: Data coming from the sensor is passed to the NanoEdge™ AI n-class Classification library to perform n-class classification.
  • Dual-mode: The data coming from the accelerometer sensor is passed to the NanoEdge™ AI library to detect the anomalies and if an anomaly is detected the data from the analog microphone is passed to an ANN model to perform the classification of the running class of the setup.

Each execution phase can be started and stopped with a user command $ start <execution phase> issued through the CLI, where valid values for the execution phase are:

  • ai,
  • neai_learn,
  • neai_detect,
  • neai_class, and
  • dual.

An execution context, which is a set of parameters controlling execution, is associated with each execution phase. One single parameter can belong to more than one execution context.

The CLI provides commands to set and get execution context parameters. The execution context cannot be changed while an execution phase is active. If the user attempts to set a parameter belonging to any active execution context, the requested parameter is not modified.

4.3. Command summary

Command name Command string Note
CS1 - Generic commands
help help Lists all registered commands with brief usage guidelines. Including the list of the applicable parameters.
info info Shows firmware details and version.
uid uid Shows STM32 UID.
reset reset Resets the MCU system.
CS2 - AI specific commands
start start <phase> Starts an execution phase according to its execution context. Available execution phases are:
  • ai for the HAR classification based on a pre-trained model converted using CUBE-AI,
  • neai_learn for learning the normal conditions using NanoEdge™ AI library for anomaly detection,
  • neai_detect for starting the detection of the anomalies using the NanoEdge™ AI anomaly detection library,
  • neai_class for the classification using the NanoEdge™ AI classification library and finally,
  • dual for the combination of anomaly detection using the NanoEdge™ AI anomaly detection library and classification using the pre-trained model converted and deployed using CUBE-AI.
neai_init neai_init (Re)Initializes the NanoEdge™ AI model and forgets any learning made on the device. Used in the beginning or to reinitialize the NanoEdge™ AI anomaly detection to start from scratch at any time.
neai_set neai_set <parameter> <value> Sets a NanoEdge™ AI specific parameter. Valid parameters and values are
  • sensitivity: float [0, 100]
  • threshold: integer [0, 100]
  • signals: integer [0, MAX_SIGNALS]
  • timer: integer [0, MAX_TIME_MS]
  • sensor: integer [0, 4]
neai_get neai_get <parameter> Displays the value of the NanoEdge™ AI parameter. Valid parameters are
  • sensitivity
  • threshold
  • signals
  • timer
  • sensor
  • all.
ai_set ai_set <parameter> <value> Sets a X-CUBE-AI specific parameter. Valid parameters are
  • sensor: integer [0,4]
ai_get ai_get <parameter> Displays the value of the X-CUBE-AI parameters. Valid parameters are
  • info: information on the models
  • sensor: associated sensor id
  • all: all the information regarding X-CUBE-AI model for HAR.
dual_set dual_set <parameter> <value> Sets a dual AI specific parameter. Valid parameters and values are

sensor: sensor for classification, values can be integer [0, 4].

dual_get dual_get <parameter> Gets a dual AI specific parameter. Valid parameters could be
  • info,
  • sensor, and
  • all.
CS3 - Sensor configuration commands
sensor_info sensor_info Get a list of all supported sensors and their ID.
sensor_set sensor_set <id> <parameter> <value> Sets the value of a parameter for a sensor with sensor id provided in id. The settable parameters are
  • FS: full scale,
  • ODR: output data rate, and

enable: active.

sensor_get sensor_get <id> <parameter> Gets the value of a parameter for a sensor with sensor id provided in id. Valid parameters are:
  • enable: active
  • ODR: output data rate
  • ODR_List: list of supported ODRs
  • FS: full scale
  • FS_List: list of supported FSs
  • all: all sensor configurations.
Available commands in command-line interface (CLI) application of FP-AI-MONITOR1

4.4. Configuring the sensors

Through the CLI interface, a user can configure the supported sensors for sensing and condition monitoring applications. The list of all the supported sensors can be displayed on the CLI console by entering the command sensor_info. This command prints the list of the supported sensors along with their ids as shown in the image below. The user can configure these sensors using these ids. The configurable options for these sensors include:

  • enable: to activate or deactivate the sensor,
  • ODR: to set the output data rate of the sensor from the list of available options, and
  • FS: to set the full-scale range from the list of available options.

The current value of any of the parameters for a given sensor can be printed using the command,

$ sensor_get <sensor_id> <param>

or all the information about the sensor can be printed using the command:

$ sensor_get <sensor_id> all

Similarly, the values for any of the available configurable parameters can be set through the command:

$ sensor_set <sensor_id> <param> <val>

The figure below shows the complete example of getting and setting these values along with old and changed values.

FP-AI-MONITOR1 V2 sensor configurations.png
Info white.png Information
Note: VSENS is a virtual sensor is used for data injection applications for debugging and validation purposes during development phase.

5. Available Applications

5.1. NanoEdge™ AI Anomaly Detection

This section provides a complete anomaly detection method using the NanoEdge™ AI library. FP-AI-MONITOR1 includes a pre-integrated stub which is easily replaced by an AI condition monitoring library generated and provided by NanoEdge™ AI Studio. This stub simulates the NanoEdge™ AI-related functionalities, such as running learning and detection phases on the edge.

The learning phase is started by issuing a command $ start neai_learn from the CLI console or by long-pressing the [USR] button. The learning process is reported either by slowly blinking the green LED light on STEVAL-STWINKT1B or in the CLI as shown below:

 
NanoEdge AI: learn
$ CTRL: ! This is a stubbed version, please install the NanoEdge AI library!
{"signal": 1, "status": need more signals}
{"signal": 2, "status": need more signals}
:
:
{"signal": 10, "status": need more signals}
{"signal": 11, "status": success}
{"signal": 12, "status": success}
{"signal": 13, "status": success}
:
:
:
End of execution phase

The CLI shows that the learning is to be performed for at least 10 signals and reports that more signals are needed until it has learned 10 signals. After 10 signals are learned, the status message of learning changes to success for every learning of the new signal. The learning can be stopped by pressing the ESC key on the keyboard or simply by pressing the [USR] button.

Similarly, the user starts the condition monitoring process by issuing the command $ start neai_detect command or by double-pressing the [USR] button. This starts the inference phase and checks the similarity of the presented signal with the learned normal signals. If the similarity is less than the set threshold default: 90%, a message is printed in the CLI showing the occurrence of an anomaly along with the similarity of the anomaly signal. The process is stopped by pressing the ESC key on the keyboard or pressing the [USR] button. This behavior is shown in the snippet below:

$ start neai_detect
NanoEdge AI: starting detect phase.

NanoEdge AI: detect
$ CTRL: ! This is a stubbed version, please install the NanoEdge  AI library!
{"signal": 1, "similarity": 0, "status": anomaly}
{"signal": 2, "similarity": 1, "status": anomaly}
{"signal": 3, "similarity": 2, "status": anomaly}
:
:
{"signal": 90, "similarity": 89, "status": anomaly}
{"signal": 91, "similarity": 90, "status": anomaly}
{"signal": 102, "similarity": 0, "status": anomaly}
{"signal": 103, "similarity": 1, "status": anomaly}
{"signal": 104, "similarity": 2, "status": anomaly}
End of execution phase

Other than CLI, the status is also presented using the LED lights on the STEVAL-STWINKT1B. Fast blinking green LED light shows the detection is in progress. Whenever an anomaly is detected, the orange LED light is blinked twice to report an anomaly.

NOTE : This behavior is simulated using a STUB library where the similarity starts from 0 when the detection phase is started and increments with the signal count. Once the similarity is reached to 100 it resets to 0. One can see that the anomalies are not reported when similarity is between 90 and 100.

Info white.png Information
Note : The message CTRL: ! This is a stubbed version, please install the NanoEdge AI library! shows that the library embedded in the function pack is just a stub and a real library is not present. This message is replaced by a new message saying CTRL:!Powered by NanoEdge AI Library! once a real library is embedded.

5.1.1. Additional parameters in condition monitoring

For user convenience, the CLI application also provides handy options to easily fine-tune the inference and learning processes. The list of all the configurable variables is available by issuing the following command:

$ neai_get all
NanoEdgeAI: signals = 0
NanoEdgeAI: sensitivity = 1.000000
NanoEdgeAI: threshold = 95
NanoEdgeAI: timer = 0
NanoEdge AI: sensor = 2

Each of the these parameters is configurable using the neai_set <param> <val> command.

This section provides information on how to use these parameters to control the learning and detection phase. By setting the "signals" and "timer" parameters, the user can control how many signals or for how long the learning and detection is performed (if both parameters are set the learning or detection phase stops whenever the first condition is met). For example, to learn 10 signals, the user issues this command, before starting the learning phase as shown below.

$ neai_set signals 10
NanoEdge AI: signals set to 10
$ start neai_learn
NanoEdgeAI: starting
$ {"signal": 1, "status": success}
{"signal": 2, "status": success}
{"signal": 3, "status": success}
:
:
{"signal": 10, "status": success}
NanoEdge AI: stopped

If both of these parameters are set to "0" (default value), the learning and detection phases will run indefinitely.

The threshold parameter is used to report any anomalies. For any signal which has similarities below the threshold value, an anomaly is reported. The default threshold value used in the CLI application is 90. Users can change this value by using neai_set threshold <val> command.

Finally, the sensitivity parameter is used as an emphasis parameter. The default value is set to 1. Increasing this sensitivity will mean that the signal matching is to be performed more strictly, reducing it will relax the similarity calculation process, meaning resulting in higher matching values.

Info white.png Information
Note: For the best performance, the user must expose all the normal conditions to the sensor board during the learning and library generation process. For example, in the case of motor monitoring, the required speeds and ramps that need to be monitored must be exposed.

For further details on how NanoEdge™ AI libraries work users are invited to read the detailed documentation of NanoEdge™ AI Studio.

5.2. NanoEdge™ AI Classification

This section provides an overview of the classification application provided in FP-AI-MONITOR1 based on the NanoEdge™ AI classification library. FP-AI-MONITOR1 includes a pre-integrated stub which is easily replaced by an AI classification library generated using NanoEdge™ AI Studio. This stub simulates the NanoEdge™ AI-classification-related functionality, such as running the classification by simply iterating between two classes for ten consecutive signals on the edge.

Unlike the anomaly detection library, the classification library from the NanoEdge™ AI Studio comes with static knowledge of the data and does not require any learning on the device. This library contains the functions based on the provided sample data to best classify one class from another and rightfully assign a label to it when performing the detection on the edge. The classification application powered by NanoEdge™ AI can be simply started by issuing a command $ start neai_class as shown in the snippet below.

 
$ start neai_class
NanoEdgeAI: starting classification phase...

$ CTRL: ! This is a stubbed version, please install the NanoEdge AI library!
NanoEdge AI: classification
{"signal": 1, "class": Class1}
{"signal": 2, "class": Class1}
:
:
{"signal": 10, "class": Class1}
{"signal": 11, "class": Class2}
{"signal": 12, "class": Class2}
:
:
{"signal": 20, "class": Class2}
{"signal": 21, "class": Class1}
:
:
End of execution phase

The CLI shows that for the first ten samples the class is detected as "Class1" while for the upcoming ten samples "Class2" is detected as the current class. The classification phase can be stopped by pressing the ESC key on the keyboard or simply by pressing the [USR] button.


NOTE : This behavior is simulated using a STUB library where the classes are iterated by displaying ten consecutive labels for one class and then ten labels for the next class and so on.

Info white.png Information
Note : The message CTRL: ! This is a stubbed version, please install the NanoEdge AI library! shows that the library embedded in the function pack is just a stub and a real library is not present. Once a real library is embedded, this message is replaced by another message saying CTRL:!Powered by NanoEdge AI Library! .

5.3. X-CUBE-AI HAR

The CLI application comes with a prebuilt Human Activity Recognition model. This functionality is started by typing the command:

$ start ai

Note that the provided HAR model is built with a dataset created using the IHM330DHCX_ACC sensor with ODR = 26, and FS = 4. To achieve the best performance, the user must set these parameters to the sensor configuration using the sensor_set command as provided in the Command Summary table. Running the $ start ai command starts doing the inference on the accelerometer data and predicts the performed activity along with the confidence. The supported activities are:

  • Stationary,
  • Walking,
  • Jogging, and
  • Biking.

The following figure is a screenshot of the normal working session of the AI command in the CLI application.

FP-AI-MONITOR1-HAR SVC with V2.png

5.4. Dual-mode application

In addition to the three applications described in the sections above the FP-AI-MONITOR1 also provides an advanced execution phase which we call the dual application mode. This mode uses anomaly detection based on the NanoEdge™ AI library and performs classification using a prebuilt ANN model based on an analog microphone. The dual-mode works in a power saver configuration. A low power anomaly detection algorithm based on the NanoEdge™ AI library is always running based on vibration data and an ANN classification based on a high-frequency analog microphone pipeline is only triggered if an anomaly is detected. Other than this both applications are independent of each other. This is also worth mentioning that the dual-mode is created to work for a USB fan when the fan is running at the maximum speed and does not work very well when tested on other speeds. The working of the applications is very simple.

To start testing the dual application execution phase, the user first needs to train the anomaly detection library using the $ start neai_learn at the highest speeds of the fan. Once the normal conditions have been learned the user can start the dual application by issuing a simple command as $ start dual as shown in the below snippet:

FP-AI-MONITOR1-dual mode.png

Whenever there is an anomaly detected, meaning a signal with a similarity of less than 90%, the ultrasound-based classifier is started. Both applications run in asynchronous mode. The ultrasound-based classification model takes almost one second of data, then preprocesses it using the mel-frequency cepstral coefficients (MFCC), and then feeds it to a pre-trained neural network. It then prints the label of the class along with the confidence. The network is trained for four classes [ 'Off', 'Normal', 'Clogging', 'Friction' ] to detect fan in 'Off' condition, or running in 'Normal' condition at max speed or clogged and running in 'Clogging' condition at maximum speed or finally if there is friction being applied on the rotating axis it is labeled as 'Friction' class. As soon as the anomaly detection detects the class to be normal, the ultrasound-based ANN is suspended.

6. Generating the AI models

6.1. NanoEdge™ AI anomaly detection

The following section shows how to generate an anomaly detection library using NanoEdge™ AI Studio and install and test it on STEVAL-STWINKT1B using FP-AI-MONITOR1. The steps are provided with brief details in the following figure.

FP-AI-MONITOR1 neai lib generation flow.png

6.1.1. Data logging for normal and abnormal conditions

The details on how to acquire the data are provided in the section data logging using HSDatalog.

Info white.png Information
Note: For the best performances, the user must expose the solution to the normal and abnormal behaviors, that are expected in real use (few signals only). For detailed information, the users are invited to read the detailed documentation of the NanoEdge™ AI Studio here.

6.1.2. Data preparation for library generation with NanoEdge™ AI Studio

The data logged through the datalogger is in the binary format and is not user readable nor compliant with the NanoEdge™ AI Studio format as it is. To convert this data to a useful form, users have two options.

  • Using the provided Python™ utility scripts on the path /FP-AI-MONITOR1_V2.0.0/Utilities/AI-resources/NanoEdgeAi/.
    • The Jupyter Notebook NanoEdgeAI_Utilities.ipynb provides a complete example of data preparation for a three-speed fan library generation running in normal and clogged conditions. In addition, there is a HSD_2_NEAISegments.py script provided if the user wants to prepare segments for given data acquisition. This script is used by issuing the following command for data acquisition with ISM330DHCX_ACC sensor.
    • >> python HSD_2_NEAISegments.py ../Datasets/Fan12CM/ISM330DHCX/normal/1000RPM/ command will generate a file named as ISM330DHCX_Cartesiam_segments_0.csv using the default parameter set. The file is generated with segments of length 1024 and stride 1024 plus the first 512 samples are skipped from the file.
    • If multiple acquisitions are used to acquire the data for the normal and abnormal conditions once the files *_Cartesiam_segments_0.csv are generated for different acquisitions, all the files for normal can be combined in a single file, and all the files for the abnormal in another file. This way the user has to provide only one normal and abnormal file to Studio.
  • Using the [FROM DATALOGGER (.DAT)] option in the data import in NanoEdge™ AI™ Studio
    • In the latest version of NanoEdge™ AI Studio it is possible to read the data from the acquisition directory of the HSDatalog directly.
    NOTE: In case there are multiple acquisitions for the normal behaviors, this has to be done for all the acquisitions, and for every normal acquisition added an abnormal acquisition is to be added also to create a pair.
Warning white.png Warning
If [FROM DATALOGGER (.DAT)] option is used, the user needs to apply the scaling for the sensor data in FP-AI-MONITOR1_prj/Application/dpu/Src/NeaiDPU.c as shown in the figure below.
FP-AI-MONITOR1-adding sensitivity neai ad.png

6.1.3. Library generation using NanoEdge™ AI Studio

Running the scripts in Jupyter Notebook will generate the normal_WL1024_segments.csv and clogged_WL1024_segments.csv files. This section describes how to generate the libraries using these normal and abnormal files.

The NanoEdge™ AI Studio can generate libraries for four types namely:

  • Anomaly Detection
  • 1-Class Classification
  • n-Class Classification
  • Extrapolation

To generate the anomaly detection library the first step is to create the project by clicking on the button for AD as shown in the figure below. The text shows the information on what Anomaly Detection is good for, and the project can be created by clicking on the CREATE NEW PROJECT button.

FP-AI-MONITOR1-NEAI STUDIO Project Types.png

The process to generate the anomaly detection library consists of six steps as described in the figure below:

FP-AI-MONITOR1-neai lib generation.png
  1. Project Settings
    • Choose a project name and description.
    • Hardware Configurations
      • Choosing the target STM32 platform or a microcontroller type: STEVAL-STWINKT1B Cortex-M4 is selected by default. If that is not the case select STEVAL-STWINKT1B from the list provided in the drop-down menu under Target.
      • Maximum amount of RAM to be allocated for the library: Usually, a few Kbytes is enough (but it depends on the data frame length used in the process of data preparation, 32 Kbytes is a good starting point).
      • Putting a limit or no limits for the Maximum Flash budget
      • Sensor type: 3-axis accelerometer is selected by default. If that is not the case select 3-axis accelerometer from the list in the drop-down under Sensor type.
  2. Providing the sample contextual data for normal segments to adjust and gauge the performance of the chosen model. Two options are available:
    • Provide directly an acquisition directory generated from the HSDatalog, (with all the *****.dat and DeviceConfig.json files unchanged), or
    • Provide the normal_WL1024_segments.csv generated using Jupyter notebook,
  3. Providing the sample contextual data for abnormal segments to adjust and gauge the performance of the chosen model. Two options are available:
    • Provide directly an acquisition directory generated from the HSDatalog, (with all the *****.dat and DeviceConfig.json files unchanged), or
    • Provide the clogged_WL1024_segments.csv generated using Jupyter notebook,
  4. Benchmark the available models and choose the one that complies with the requirements and provides the best performance.
  5. Validating the model for learning and testing through the provided emulator which emulates the behavior of the library on the STM32 target.
  6. The final step is to compile and download the libraries. In this process, the flag "-mfloat-abi" has to be checked for using libraries with hardware FPU. All the other flags can be left to the default state.
    • Note for using the library with μKeil also check -fshort-wchar in addition to -mfloat-abi.

Detailed documentation on the NanoEdge™ AI Studio.

Info white.png Information
An evaluation version of the NanoEdge™ AI Studio can be freely downloaded to generate development libraries for selected STM32 Nucleo boards and Discovery kits, like STEVAL-STWINKT1B.

.

6.2. NanoEdge™ AI classification

The following describes how to generate the NanoEdge™ AI-based classification library and download it. The figure below shows a full flow of generating the library, integrating and installing it with the firmware, and testing it on the sensor-tile to classify different conditions.

FP-AI-MONITOR1 neai class lib generation flow.png

6.2.1. Data logging for different conditions

The details on how to log the data are provided in the section Datalogging using HSDatalog. Using these steps the user needs to a separate acquisitions for each of the conditions/classes the user wants to monitor. For the simplicity purposes FP-AI-MONITOR1 provides the sample data for a USB fan in four different conditions namely [ Off, Normal, Clogging, Friction]. This data is measured using ISM330DHCX and IMP23ABSU sensors and can be found in FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/Datasets/HSD_Logged_Data/Fan12CM/ISM330DHCX+IMP23ABSU directory. For the configurations we used ACC subsensor of ISM330DHCX running at ODR = 1666 samples/sec and FS = 4G, and IMP23ABSU running at ODR = 192,000 samples/sec.

6.2.2. Data preparation for classification library generation using NanoEdge™ AI Studio

The data logged through the datalogger is in the binary format and is not user readable nor compliant with the NanoEdge™ AI Studio format as it is. To convert this data to a useful form, users have two options.

  • For the ease of the users we provided Python™ utilities to prepare this data to be ready to generate the n-class classification libraries using NanoEdge™ AI Studio. These scripts are provided in the form of a Jupyter Notebook and can be found in /FP-AI-MONITOR1_V2.0.0/Utilities/AI-resources/Training Scripts/Anomaly Classification/NanoEdgeAI_ACC/DataPreperation.ipynb.
Running all the sections of this notebook will generate the NanoEdge™ AI segments for all the acquisitions in the datalog folders which can be inputted to the NanoEdge™ AI Studio in the next step.
  • Using the [FROM DATALOGGER (.DAT)] option in the data import in NanoEdge™ AI Studio
In the latest version of NanoEdge™ AI Studio it is possible to read the data from the acquisition directory of the HSDatalog directly.
Warning white.png Warning
If [FROM DATALOGGER (.DAT)] option is used when the user needs to apply the sensitivity of the sensor to get the sensor data in physical units instead of using the register values. To do this the user needs to perform an extra steps as indicated in the figure below to edit the FP-AI-MONITOR1_prj/Application/dup/Src/NeaiDPU.c file.
FP-AI-MONITOR1-adding sensitivity neai ncc.png

6.2.3. Generation n-class classification library NanoEdge™ AI Studio

Running the scripts in Jupyter Notebook will generate the ISM330DHCX_Cartesiam_segments_0.csv csv files in each of the four datalog folders. This section describes how to use these files to generate the n-class classification library with NanoEdge™ AI Studio.

To generate the classification library the first step is to create the project by clicking on the button for nC as shown in the figure below. This will change the display and show what n-Class Classification libraries are good for and how does it work. Create a new project by clicking on the CREATE NEW PROJECT button.

FP-AI-MONITOR1-create ncc project.png

The process to generate the n-class classification library consists of five steps as described in the figure below:

FP-AI-MONITOR1-ncc project steps.png
  1. Project Settings
    • Choose a project name and description.
    • Hardware Configurations
      • Choosing the target STM32 platform or a microcontroller type: STEVAL-STWINKT1B Cortex-M4 is selected by default. If that is not the case select STEVAL-STWINKT1B from the list provided in the drop-down menu under Target.
      • Maximum amount of RAM to be allocated for the library: Usually, a few Kbytes is enough (but it depends on the data frame length used in the process of data preparation, 64 Kbytes is a good starting point).
      • Putting a limit or no limits for the Maximum Flash budget (we chose the no limits option)
      • Sensor type: 3-axis accelerometer is selected by default. If that is not the case select 3-axis accelerometer from the list in the drop-down under Sensor type.
  2. Providing the sample data for all four classes. Two options are available:
    • Provide directly an acquisition directory generated from the HSDatalog, (with all the *****.dat and DeviceConfig.json files unchanged), select ISM330DHCX>ACC from the sensor list and enter 1024 in the signal length field. Press CONTINUE button and then IMPORT button. Or
    • Provide the ISM330DHCX_Cartesiam_segments_0.csv generated using Jupyter notebook, directly
    NOTE: Assign a class label to the imported data in the Name field once the data is imported. This label is used to differentiate the classes and will be used in the emulation to show the predicted class.
    • Repeat the process for all four classes.
  3. Benchmark the available models and choose the one that complies with the requirements and provides the best performance.
  4. Validating the model performance through the provided emulator which emulates the behavior of the library on the STM32 target.
  5. The final step is to compile and download the libraries. As in FP-AI-MONITOR1, we support multiple NanoEdge™ AI libraries, this step will require a few precise settings to work with FP-AI-MONITOR1:
    • Check the Multi-library check-box and provide ncc in the suffix name field.
    • Check the "Float abi" flag for using libraries with hardware FPU. All the other flags can be left to the default state.
Info white.png Information
For using the library with μKeil also check -fshort-wchar in addition to Float abi

.

Detailed documentation on the NanoEdge™ AI Studio.

6.3. X-CUBE-AI models

This section explains how to generate the code for a pre-trained AI models using STM32 X-CUBE-AI. As the FP-AI-MONITOR1 runs two pre-trained AI models namely, USC and HAR, for the simplification and optimization purposes, we will generate the code for the both pre-trained models at the same time. We can either generate the code for the combination of har_IGN.h5 and usc_4_class.tflite or har_svc.onnx and usc_4_class.tflite. These pre-trained models are available in FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/models directory. As the package already contains the code for the HAR_SVC + USC combination, in the section below we will provide a step-by-step process for the code generation for the HAR_IGN and USC combination.

Step1 : Open the STM32CubeMX and click on the ACCESS TO BOARD SELECTOR button as shown in the image below.

FP-AI-MONITOR1-opening CubeMX.png

Step2 : Create a new project for STEVAL-STWINKT1B:

  1. Confirm the board selector tab is selected,
  2. Search for the right board, and in our case it is the STEVAL-STWINKT1B, by typing the name in the search bar,
  3. Select the board by clicking on either the board image or the name of the board,
  4. Start Project, and
  5. Chose NO for the Peripheral initialization option as this is not required for our purpose.
FP-AI-MONITOR1-CubeMX creating a project.png

Step3 : Configuring connectivity

  1. Click on the connectivity option in the left menu
  2. Select USART2
  3. Enable the "Asynchronous mode" by selecting it in the drop-down menu.
FP-AI-MONITOR1-CubeMX setting usart connectivity.png

Step4 : Add the X-CUBE-AI in the software packs for the project

  1. Click on the Software Packs, and select the Select Components option
  2. Click on the STMicroelectronics X-CUBE-AI. Use Version 7.1.0 as preference but any version from 7.1.0 or later can be used,
  3. Click on checkbox in front of Core to add the X-CUBE-AI code in the software stack.
  4. Expand the Device Application menu and from the drop-down menu under selection column select SystemPerformance.
  5. Click OK button to finish the addition of the X-CUBE-AI in the project.
FP-AI-MONITOR1-CubeMX adding X CUBE AI.png

Step 5 : Platform Settings

  1. Click on Software Packs,
  2. Choose STMicroelectronics.X-CUBE-AI,
  3. Select USART: Asynchronous option for the COM Port,
  4. Select USART2 in "Found Solutions" drop-down.
FP-AI-MONITOR1-CubeMX platform settings.png

Step6 : Adding the networks for code generation This step require the users to add two networks. HAR and USC. This can be done using following steps

  1. Adding HAR model
    • Click on the add network button,
    • In the first text field provide the text har_network as the network name. This is used to differentiate the name space of the model when code for multiple models is generated at once.
    • From drop down select the type of the network. X-CUBE-AI allows the user to generate code for the Keras, ONNX, and TFLite models. For using har_IGN.h5 file select the Keras option.
    • Click on the Browse button to select the model.
    • The har_IGN.h5 is located under FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/models . Select the model and click OK.
FP-AI-MONITOR1-CubeMX adding har network.png
  1. Adding USC model
    • Click on the add network button,
    • In the first text field provide the text usc_network as the network name. This is used to differentiate the name space of the model when code for multiple models is generated at once.
    • From drop down select the type of the network as TFLite model.
    • Click on the Browse button to select the model.
    • The usc_4_class.tflite is located under FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/models . Select the model and click OK.
FP-AI-MONITOR1-CubeMX adding usc network.png

Step7 : Generating the C-code

  1. Go to Project Manager
  2. Assign a "Project Name", in the figure below it is FP-AI-MONITOR1_AI-Code-Generation
  3. Choose a Project Location, in the figure below it is C:/Temp/
  4. Click on the GENERATE CODE button. A progress bar will start and shows progress across the different code generation steps.
  5. Upon completion of the code generation process the user will see a dialog as in the figure below. This shows completion of the code generation. Click on the Open Folder button to open the project with the generated code.
  6. The files present for the network model that have to be replaced in the provided project are located in the following directory: FP-AI-MONITOR1_AI-Code-Generation_X-CUBE-AI/App/ as shown in the figure below.
FP-AI-MONITOR1-CubeMX generating code dual.png

The next section shows how these files are used to replace the existing model embedded in the FP-AI-MONITOR1 software step-by-step and install it on the sensor board.

7. Updating the AI models

7.1. NanoEdge™ AI anomaly detection

Once the libraries are generated and downloaded from NanoEdge™ AI Studio, the next step is to link these libraries to FP-AI-MONITOR1 and run them on the STWIN. The FP-AI-MONITOR1, comes with the library stubs in the place of the actual libraries generated by NanoEdge™ AI Studio. This is done to simplify the linking of the generated libraries. In order to link the actual libraries, the user needs to copy the generated libraries and replace the existing stub/dummy libraries and header files NanoEdgeAI.h, and libneai.a files present in the folders Inc, and lib, respectively. The relative paths of these folders are /FP_AI_MONITOR1_V2.0.0/Middlewares/ST/NanoEdge_AI_Library/ as shown in the figure below.

FP-AI-MONITOR1-linking NEAI library.png

Once these files are copied, the project must be reconstructed and programmed on the sensor board to link the libraries correctly. For this, the user must open the project in STM32CubeIDE located in the /FP-AI-MONITOR1_V2.0.0/Projects/STWINL4R9ZI-STWIN/Applications/FP-AI-MONITOR1/STM32CubeIDE/ folder and double click .project file as shown in the figure below.

FP-AI-MONITOR1-V2 opening IDE project.png

To build and install the project click on the play button and wait for the successful download message as shown in the section Build and Install Project.

Once the sensor board is successfully programmed, the welcome message appears in the CLI (Tera Term terminal). If the message does not appear try to reset the board by pressing the RESET button.

Info white.png Information
NOTE: To be absolutely sure that a new software is installed in STEVAL-STWINKT1B, user can issue command info . This
will show the compile time and the user can confirm if the sensor board is programmed with a new or old binary code.

7.1.1. Testing the NanoEdge™ AI Machine Learning library

Once the STWIN is programmed with the FW containing a valid library, the condition monitoring libraries are ready to be tested on the sensor board. The learning and detection commands can be issued and now the user will not see the warning of the stub presence.

To achieve the best performance, the user must perform the learning using the same sensor configurations which were used during the contextual data acquisition. For example in the snippet below users can see commands to configure ISM330DHCX sensor with sensor_id 2 with following parameters:

  • enable = 1
  • ODR = 1666,
  • FS = 4.
$ sensor_set 2 enable 1
sensor 2: enable

$ sensor_set 2 ODR 1666
nominal ODR = 1666.00 Hz, latest measured ODR = 0.00 Hz

$ sensor_set 2 FS 4
sensor FS: 4.00
Info white.png Information
Note: The NanoEdge™ AI library comes with an incremental learning capability, so the learning and detection phases can be toggled depending on whether needs to be without forgetting the previous learning or not.

7.2. NanoEdge™ AI classification

The FP-AI-MONITOR1, comes with the library stubs in the place of the actual libraries generated by NanoEdge™ AI Studio. This is done to simplify the linking of the generated libraries. In n-Class classification library the features for the classes are learned and required in the form of the knowledge.h file in addition to .h and .a files. So unlike the anomaly detection library, in order to link the classification libraries, the user needs to copy two header files NanoEdgeAI_ncc.h and knowledge_ncc.h, and the library libneai_ncc.a file to replace the already present files in the folders Inc, and lib, respectively. The relative paths of these folders are /FP_AI_MONITOR1_V2.0.0/Middlewares/ST/NanoEdge_AI_Library/ as shown in the figure below.

FP-AI-MONITOR1-linking NEAI ncc library.png

In addition to this the user is required to add the labels of the classes to expect during classification process by updating the sNccClassLabels array in FP-AI-MONITOR1_prj/Application/Src/AppController.c file as shown in the figure below.

FP-AI-MONITOR1-ncc class labels.png

Note that the first label is "Unknown" and it is required to be left as it is. The real labels for the classification come after this. The order of the labels [Off, Normal, Clogging, Friction] has to be the same as was used to provide the data in the process of library generation in NanoEdge™ AI Studio.

Info white.png Information
The order of the labels for n-Class Classification library can be found in the NanoEdgeAI_ncc.h file. The users can simply copy and paste this array.

After this step, the project must be reconstructed and programmed on the sensor board to link the libraries correctly. To build and install the project click on the play button and wait for the successful download message as shown in the section Build and Install Project.

Once the sensor board is successfully programmed, the welcome message appears in the CLI (Tera Term terminal). If the message does not appear try to reset the board by pressing the RESET button.

7.3. X-CUBE-AI models

The CLI example has two prebuilt models integrated in it. One for HAR and another for the USC. Following the steps below user can update these models. As described in code generation process, for the simplicity sake, the code for the both models is generated at once. In this example the provided code for the combination of SVC and USC models(USC_4_Class_+_SVC_4_Class) is replaced with the prebuilt and converted C code from the HAR (CNN) and USC CNN models provided in the /FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/models/USC_4_Class_+_IGN_4_Class/ folder.

FP-AI-MONITOR1-copy pasting two networks c code.png

To update the model, the user must copy and replace following files in the /FP-AI-MONITOR1_V2.0.0/Projects/STM32L4R9ZI-STWIN/Applications/FP-AI-MONITOR1/X-CUBE-AI/App/ folder as shown in the figure above. Once the files are copied, the user must open the project with the CubeIDE. To do so, go to the /FP-AI-MONITOR1_V2.0.0/Projects/STWINL4R9ZI-STWIN/Applications/FP-AI-MONITOR1/STM32CubeIDE/ folder and double click .project file as shown in the figure below.

File: FP-AI-MONITOR1-V2 opening IDE project

Once the project is opened, go to FP-AI-MONITOR1_V2.0.0/Projects/STM32L4R9ZI-STWIN/Application/FP-AI-MONITOR1/X-CUBE-AI/App/app_x-cube-ai.c file and comment the following lines of the code as shown in the figure below.

FP-AI-MONITOR1-commenting app xcubeai c.png

7.3.1. Building and installing the project

Then build and install the project on the STWIN sensor board by pressing the play button as shown in the figure below.

FP-AI-MONITOR1-building and installing the project.png

A message saying Download verified successfully indicates the new firmware is programmed in the sensor board.

Info white.png Information
NOTE: To be absolutely sure that a new software is installed in STEVAL-STWINKT1B, user can issue command info . This will show the compile time and the user can confirm if the sensor board is programmed with new or old binary.

8. Python Utilities

Warning white.png Warning
This section needs to be simplified. This must give a simplified view of the main script files for HAR (SVC, CNN, NEAI), n-Class Classification, and USC.

8.1. Python Utilities for classification application

FP-AI-MONITOR1 comes equipped with two AI applications, a classification example for human activity recognition (HAR) based on X-CUBE-AI and an anomaly detection example based on the NanoEdge™ AI. This section describes the HAR classification application.

FP-AI-MONITOR1 comes with a Python utility code to generate the AI models for HAR both based on artificial neural networks and classical machine learning models using scikit-learn. These scripts are located under the FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/Training Scripts/HAR/ directory. The following figure shows the contents of the utilities.

FP-AI-MONITOR1 Python Utilities.png

The utilities include two folders, AI_Resources (all the Python resources related to AI) and DataLog (binary and helper scripts for High-Speed Datalogger). In the AI_Resources there are subdirectories of

  • Dataset: Contains different datasets/holders for the datasets used in the function pack
  • models: Contains the pre-generated and trained models for HAR along with their C-code
  • NanoEdgeAi: Contains the helper scripts to prepare the data for the NanoEdge™ AI Studio from the HSDatalogs
  • signal_processing_lib: Contains the code for various signal processing modules (there is equivalent embedded code available for all the modules in the function pack)
  • Training Scripts: Contains the Python scripts for HAR examples using SVC, CNN, and NEAI.

The HAR subdirectory at the path FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/Training Scripts/HAR/ contains three Jupyter notebooks:

  • HAR_with_CNN.ipynb (a complete step-by-step code to build an HAR model based on Convolutional Neural Networks),
  • HAR_with_SVC.ipynb (a complete step-by-step code to build an HAR model based on Support Vector Machine Classifier), and
  • HAR_with_NEAI.ipynb (a complete step-by-step code to build NanoEdge™ AI Studio compliant files for all activities).

The FP-AI-MONITOR1 comes with a prebuilt model for HAR based on SVC for recognizing four activities, namely [Stationary, Walking, Jogging, Biking]. The following figure shows a complete flow of building an HAR application using CNN or SVC, generating the C-code using X-CUBE-AI and embedding it in the FP-AI-MONITOR1, installing it and then finally running the inference on the edge.

FP-AI-MONITOR1 AI flow.png

The Jupyter Notebooks in FP-AI-MONITOR1_V2.0.0/Utilities/AI_Resources/Training Scripts/HAR/ directory contain very detailed step-by-step processes to create SVC, CNN, and NEAI-based HAR applications. This section describes briefly the steps to build this application in Python using the CNN and SVC scripts provided in this directory (yellow part). The steps are listed in the figure below:

FP-AI-MONITOR1 classification model training.png

The steps include:

  • Segmenting the data into segments of length 24 (any segment length can be used depending on the requirements, but the length used in this case is the length based on a famous model architecture).
  • Preprocess and condition the data, the gravity rotation is applied to the z-axis and suppression (any preprocessing chain can be applied depending on the user's needs)
  • a set of DSP feature extraction is provided in the subdirectory signal_processing_lib along with the equivalent embedded implementation.
  • Model building and optimization (learning)
  • In the case of CNN, this step includes building topology and training the weights.
  • In the case of SVC, this step includes finding the best hyperparameters for the model definition and performing the best dimension reduction to have the smallest models providing the best performance.
  • Validating the model using the unseen/test data.
  • Exporting the trained model as .h5 (in case of CNN) or .onnx (in case of SVC).

The next section shows how to take these pre-trained models and convert them into optimized C-code using X-CUBE-AI. The code can then be embedded and installed into the sensor board to run the inferences on the edge.

Info white.png Information
NOTE: The example shown here is for HAR, however, it is worth mentioning that using this pathway the readers can build an AI application for whichever use case they want. Also, the preprocessing chain can be changed to match the user's needs as a full set of preprocessing modules is available along with equivalent C-code implementation to facilitate the task for the readers.

9. Data collection

The data collection functionality is out of the scope of this function pack, however, to simplify this for the users this section provides the step-by-step guide to logging the data on STEVAL-STWINKT1B using the high-speed data logger.

Step 1: Program the STEVAL-STWINKT1 with the HSDatalog FW

In the scope of this function pack and article, the STEVAL-STWINKT1 can be programmed with HSDatalog firmware in two ways.

  • Using the binary provided in the function pack
    To simplify the task of the users and to allow them the possibility to perform a data log, the precompiled HSDatalog.bin file for FP-SNS-DATALOG1 is provided in the Utilities directory, which is located under path /FP-AI-MONITOR1_V2.0.0/Utilities/Datalog/. The sensor tile can be programmed by simply following the drag-and-drop action shown in section 2.3.
  • Using the NanoEdge™ AI Studio
    The new version of NanoEdgeTM AI Studio has a new feature to program the high-speed datalogger in the STEVAL-STWINKT1B. To do this follow the steps in the figure below.
    1. click on the Datalogger button in the home menu,
    2. connect the STEVAL-STWINKT1B to the computer as shown in the figure below (connect the USB to STWIN first and STLINK after),
    3. wait for the status to change to connect,
    4. click the LOAD BINARY button,
    5. wait for the Success message,
    the STWIN is now programmed with the high-speed datalogger firmware.
FP-AI-MONITOR1 flashing HSD in STWIN from Studio.png

Step 2: Place a DeviceConfig.json file on the SD card

The next step is to copy a DeviceConfig.json on the SD card. This file contains the sensors configurations to be used for the data logging. These sample files can be either:

  • interactively generated through studio by clicking on the Configure datalogger button in the datalogger menu as shown in the figure below, or,
Creating DeviceConfig.json file from NanoEdge™ AI Studio
  • the users can simply use one of the provided some sample .json files in the package in FP-AI-MONITOR1_V2.0.0/Utilities/Datalog/STWIN_config_examples/ directory.
Info white.png Information
The configuration files are to be precisely named DeviceConfig.json or the process will not work.
Warning white.png Warning
Provide a little more detail on what are the important fields and structures in the DeviceConfig.json and how to change them

Step 3: Insert the SD card into the STWIN board Insert an SD card in the STEVAL-STWINKT1B sensor tile.

Info white.png Information
For data logging using the high speed datalogger user needs a FAT32-FS formatted microSDTM card.

Step 4: Reset the board

Reset the board. Orange LED blinks once per second. The custom sensor configurations provided in DeviceConfig.json are loaded from the file.

Step 5: Start the data log

Press the [USR] button to start data acquisition on the SD card. The orange LED turns off and the green LED starts blinking to signal sensor data is being written into the SD card.

Step 6: Stop the data logging

Press the [USR] button again to stop data acquisition. Do not unplug the SD card, turn the board off or perform a [RESET] before stopping the acquisition otherwise the data on the SD card will be corrupted.

Step 7: Retrieve data from SD card

Remove the SD card and insert it into an appropriate SD card slot on the PC. The log files are stored in STWIN_### folders for every acquisition, where ### is a sequential number determined by the application to ensure log file names are unique. Each folder contains a file for each active sub-sensor called SensorName_subSensorName.dat containing raw sensor data coupled with timestamps, a DeviceConfig.json with specific information about the device configuration (confirm if the sensor configurations in the DeviceConfig.json are the ones you desired), necessary for correct data interpretation, and an AcquisitionInfo.json with information about the acquisition.

Info white.png Information
For details on how to use all the features of the provided HSDatalog.bin binary the users are invited to refer to the user manual of FP-SNS-DATALOG1.

10. Documents and related resources