STM32WB-WBA BLE security

Under construction.png Coming soon

1. STM32WB - BLE security

Vocabulary and BLE security configuration. Legacy Pairing and Secure Connection

The BLE security model includes 5 security features:

  • Pairing: process for creating one or more shared secret keys.
  • Bonding: act of storing the keys created during pairing for use in subsequent connections in order to form a trusted device pair.
  • Device authentication: verification that the two devices have the same keys.
  • Encryption: provides message confidentiality.
  • Message integrity: protects against fake messages.(4 bytes Message Integrity Check MIC)

BLE uses 2 security levels:

  • Legacy Pairing – Short Temporary Key (STK). STK will be created to encrypt connection. Then, if bonding, LTK will be used for subsequent connections.
  • Secure Connection – Long Term Key (LTK). LTK will be created to encrypt connection.

1.1. Legacy pairing and no fixed pin

Initialization (when no link is established)

Set the IO capability of the device with *aci_gap_set_io_capability Parameter: IO capability aci_gap_set_io_capability(0x04) (IO_CAP_KEYBOARD_DISPLAY)

Set the authentication requirements for the device with *aci_gap_set_authentication_req Parameters: Bonding_mode, mitm_mode, sc_support, keypress notification, min_encryption_key_size, max_encryption_key_size, use_fixed_pin,fixed_pin, identity_address_type aci_gap_set_authentication_req(0,1,0,0,7,16,1,111111,0) (no bonding, MITM, secure connection pairing not supported, keypress notification not supported, min encryption key size, max encryption key size, no use of fixed pin, fixed pin (not used), public address type)


1.2. Legacy pairing and fixed pin

initiated by the peripheral

aci_gap_set_io_capability(0x00) (IO_CAP_DISPLAY_ONLY)

aci_gap_set_authentication_req(0,0,0,0,7,16,0 (use fixed pin), 111111 (used fixed pin),0) (no bonding, no MITM, secure connection pairing not supported, keypress notification not supported, min encryption key size, max encryption key size, use of fixed pin, fixed pin (used), public address type)


1.3. Secure connection

aci_gap_set_io_capability(0x04) (IO_CAP_KEYBOARD_DISPLAY)

aci_gap_set_authentication_req(0,1,1,1,7,16,1,111111, 0) (no bonding, MITM, secure connection pairing not supported, keypress notification not supported, min encryption key size, max encryption key size, no use of fixed pin, fixed pin (not used), public address type)

2. Additional information - BLE characteristics and security permissions

2.1. STM32WB - BLE GATT characteristic

When a characteristic is created (aci_gatt_add_char), following security permissions could be given: 0x00: none 0x01: AUTHEN_READ (need authentication to read) 0x02: AUTHOR_READ (need authorization to read) 0x04: ENCRY_READ (need encryption to read) 0x08: AUTHEN_WRITE (need authentication to write) 0x10: AUTHOR_WRITE (need authorization to write) 0x20: ENCRY_WRITE (need encryption to write)

2.2. Example 1

If a characteristic is created with properties READ and WRITE and if the security permission is set to ENCR_READ and ENCR_WRITE After the discovery of service and characteristic, if the client tries to read or write this characteristic, an error is returned (ACI_GATT_ERROR_RESP_EVENT) with error_code=0x0F (insufficient encryption) If the devices are paired and encryption is started, read and write operations can be done.

2.3. Example 2

Security permission 'need authentication' is more restrictive than 'need encryption'.

You need to set MITM (in aci_gap_set_authentication_requirement) and need of start pairing to be able to read/write the characteristic with 'need authentication' No need to set MITM and need of start pairing to be able to read/write the characteristic with 'need encryption'

2.4. Example 3

The way to use characteristic with 'need authorization': after the connection_complete_event, the server sends the command aci_gap_set_authorization_requirement (for current connection handle) the master initiates pairing. When the pairing is complete, ACI_GAP_AUTHORIZATION_REQ_EVENT is generated on server side which sends aci_gap_authorization_resp(conn_handle, authorize) then the client can read/write the characteristic.

2.5. References