1. Embedded Provisioner Introduction
Embedded Provisioner is a proprietary solution to provision a Bluetooth® LE-Mesh network from a STM32WB platform instead of using a smartphone or tablet.
2. Requirements
Software and System requirements
The software required are the following (minimum IDEs version):
- IAR Embedded Workbench for ARM (EWARM) toolchain V8.20.2
- RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.23
- STM32CubeIDE toolchain V1.7.0 [1].
Programmer:
- STM32CubeProgrammer[2] : To flash the board with an already generated binary
More information about software and system requirements are available in the ST Bluetooth® LE-Mesh Application Note[3].
Hardware requirements
P-NUCLEO-WB55 Nucleo board[4] is necessary to setup the demonstration.
STM32WB Nucleo board |
---|
3. Setup
Embedded Provisioner project can be found in STM32CubeWB MCU Package[5] at the following emplacement.
Embedded provisioner project directory |
---|
To build and flash Embedded Provisioner project, process on the same way as for ST BLE-Mesh Proxy-Relay-Friend example.
Before building the project, choose between the 2 available configurations by modifying mesh_cfg_usr.h code as described below.
3.1. Embedded Provisioner Feature
With this setup, the provisioner node configure and initialize itself without action required from the user.
#define ENABLE_RELAY_FEATURE
#define ENABLE_PROXY_FEATURE
#define ENABLE_FRIEND_FEATURE
#define ENABLE_PROVISIONER_FEATURE
//#define DYNAMIC_PROVISIONER
[…]
#define ENABLE_SERIAL_PRVN 1
3.2. Dynamic Provisioner Feature
With this setup, the provisioner node need to be configured and initialized by user. The configuration setup is described in the below chapters.
#define ENABLE_RELAY_FEATURE
#define ENABLE_PROXY_FEATURE
#define ENABLE_FRIEND_FEATURE
//#define ENABLE_PROVISIONER_FEATURE
#define DYNAMIC_PROVISIONER
[…]
#define ENABLE_SERIAL_PRVN
For both setup, ensure the serial commands are enabled, in order to pilot the provisioner from Terminal window.
/* Enables the serial interface using Uart */
#define ENABLE_SERIAL_INTERFACE 1
#define ENABLE_SIG_MODELS_AT_COMMANDS 1
#define ENABLE_VENDOR_MODELS_AT_COMMANDS 0
#define ENABLE_UT 1
4. Getting Started
Before following the steps described below, ensure your project is setup to support the desired feature (embedded or Dynamic provisioner) and flashed into the STM32WB platform.
Open a terminal to communicate with the platform. Terminal setup and utilization is described in ST Bluetooth® LE-Mesh Proxy-Relay-Friend example page.
If you build the provisioner application using ENABLE_PROVISIONER_FEATURE, you can skip the Step 1, as the board is automatically setup and initialized.
4.1. Step 1: Starting provisioner node
In the case of DYNAMIC_PROVISIONER feature, logs on terminal should display:
Unprovisioned device
NEXT NVM ADDRESS […]
BLE-Mesh Lighting Demo v1.[…]
BLE-Mesh Library v01.[…]
BD_MACAddress = […]
UUID Address = […]
Write below command on Serial terminal to make one node ROOT node for network creation:
ATEP ROOT (Case insensitive)
This command configures the provisioner and bind all the embedded models:
Terminal logs: ATEP ROOT |
---|
4.2. Step 2: Scan unprovisioned devices
Write below command on Serial terminal to scan unprovisioned devices in range:
ATEP SCAN (Case insensitive)
Log on terminal indicates unprovisioned devices with their corresponding UUIDs:
Terminal logs: ATEP SCAN |
---|
In the example, two devices (device-0 and device-1) are not provisioned to the network.
4.3. Step 3: Provision and configure devices
Write below command to start provisioning of device-0:
ATEP PRVN-0 (Here 0 indicate the device–0)
Below Log will appear on terminal indicating the device-0 has been provisioned by the provisioner by making the PB-Adv connection link:
Test command executed successfully
PB-ADV Link opened successfully
Device Key: […]
App Key: […]
Device is provisioned by provisioner
Log on provisioned Node terminal will indicates that the node is provisioned by the provisioner. Finally, the PB-Adv connection link is closed and device-0 will be configured, and models bind.
Terminal logs: Node provisioned |
---|
4.4. Step 4: Provision other devices
To provision and configure new nodes, reproduce Step 2 and Step 3.
5. References