Revision as of 18:01, 2 November 2021 by Registered User

This category groups together all articles related to the Security and Cryptographic.

Safety & security.png

STM32L5 security

Learn how to use STM32 security and enable/disable TrustZone on STM32L5
Security Shield.png

STM32 cryptograhic

Learn how to use STM32 cryptographic
Security Shield.png

'

How to use available security features



1. Concepts of security in STM32

For a long time the general purpose microcontrollers had little on no security features and secure applications relied on purpose built smartcard or secure element ICs. These are also based on a microcontroller architecture, but the two worlds were clearly separated for decades. Proliferation of microcontrollers to various connected devices or sensitive applications gradually began to blur the borderline. A modern microcontroller usually provides a developer with means to thwart all but the very sophisticated attacks. It’s important to establish 3 terms:

  • Asset – value to be protected
  • Threat – type of attack
  • Vulnerability – a weakness that can be exploited

There are several reasons to try to improve security of a device – the obvious assets.

  1. Protection of own intellectual property. Make it more difficult for indecent competition trying to steal your ideas.
  2. Protection of user data. Some customers may care about their privacy.
  3. Reliability – in some cases a DoS attack is major threat. Even worse case is a hijacked device being abused for attackers own purposes.
  4. Brand image bolstered by a security certificate (or damaged by a history of successful hacks)

While there is no such thing as a perfect security, it’s important to balance the security efforts with the expected efforts the attacker could be willing to invest. Popular device with lots of assets to protect needs security countermeasures, while application with low production volume or no assets to protect may not need any. To make informed decision (risk analysis) it’s necessary to identify the assets, threats and vulnerabilities. A topic that stands out as a particularly important is the security of deploying patches or firmware updates securely for products that are already in the field. Secure solution called SBSFU is template for such situation.

Subcategories

This category has the following 4 subcategories, out of 4 total.

1

2

3