1. NanoEdge AI Studio: CLI
1.1. I. Purpose of NanoEdge AI Studio CLI
NanoEdgeAI Studio CLI is a Command Line Interface for the NanoEdge AI Studio.
It makes all NanoEdge AI Studio's features usable without the graphical user interface, directly from the terminal.
1.2. II. Requirements
1.2.1. 1. Windows
NanoEdgeAI Studio CLI is tested to run on Windows 10 64 bits.
1.2.2. 2. Linux
NanoEdge AI Studio CLI is tested to run on Ubuntu, Debian 64 bits.
It has a dependency on libnss3 and glibc. Please be sure to install libnss3 and glibc before running the CLI.
$ apt-get update -qy && apt-get -y install procps libnss3
1.3. III. Install
Download and unzip neai_cli_***_v***.zip to any folder.
This folder includes:
- neai_cli: the executable
- docs: this documentation
- bin: the NanoEdge AI Studio Engine (not included in the slim version)
1.4. IV. Getting started
1.4.1. 1. Engine: Launch or connect to the NanoEdge AI Studio Engine
- Launch NanoEdge AI Studio Engine on the local computer:
$ neai_cli engine -launch
- Connect to an already running NanoEdge AI Studio Engine
$ neai_cli engine -set -host "<my_host>" -port "<my_port>"
You can also use NanoEdge AI Studio Engine launched by NanoEdge AI Studio. To do so, please launch NanoEdge AI Studio and set port to use to 5000 (or the port you set during NanoEdge AI Studio setup)
$ neai_cli engine -set -port 5000
A NanoEdge AI Studio Engine must be running to use neai_cli.
Usage:
$ neai_cli engine <command> <attributes> Command: -get Get host and port used to connect to NanoEdge AI Studio Engine -launch Launch NanoEdge AI Studio Engine Optional attributes: port, workspace -set Set host and port to use to connect to NanoEdge AI Studio Engine Mandatory attributes: host, port -shutdown Shutdown NanoEdge AI Studio Engine -test Test connection to NanoEdge AI Studio Engine Attributes: -host string Host running NanoEdge AI Studio Engine (default "http://localhost") -port int Port of NanoEdge AI Studio Engine (default 8000) -workspace string Path to the workspace directory (default "./bin/workspace")
1.4.2. 2. License: Activate and manage license
- Activate a license:
$ neai_cli license -activate -key "<my_license_key>"
A license must be activated to use a NanoEdge AI Studio Engine.
Usage:
license <command> <attributes> Command: -activate Set a license Mandatory attributes: key -deactivate Delete the license -info Get license info Attributes: -key string License key
Response:
Name | Type | Description | Example |
---|---|---|---|
expiration_date | date | Expiration date of the license | "2020-02-13T09:58:12+00:00" |
is_offline_activation | bool | If the license key has been offline activated | false |
is_set | bool | If the license is set | true |
is_trial | bool | If the license is a trial license | false |
is_valid | bool | If the license is activated | true |
license_key | string | License key | <LICENSE_KEY> |
license_type | string | License type | <LICENSE_TYPE> |
user_email | string | Email of the user associated with the license key | john.smith@company.com |
user_name | string | Name of the user associated with the license key | John Smith |
valid_reason | string | License validity reason | "License is genuinely activated!" |
1.4.3. 3. Project: Create or manage project
- Create a new project:
$ neai_cli project -create -anomaly_detection -slug_name "<my_slug_name>" -mcu "<my_mcu>" -max_ram <max_ram_value> -number_axis <number_of_axis_value>
The project slug name can contain only letters, numbers and dash.
For an existing project, it can be found using:
$ neai_cli project -list
Usage:
project <command> <attributes> Command: -create Create and open a project Mandatory attributes: name, anomaly_detection or classification, mcu Optional attributes: description, max_ram, max_flash, number_axis -delete Delete a project Mandatory attributes: slug_name -info Get project info Mandatory attributes: slug_name -list List projects Attributes: -anomaly_detection Set project of type Anomaly Detection -classification Set project of type Classification -description string Description of the project -max_flash int Maximum Flash available for the library in bytes (default 128000 bytes) -max_ram int Maximum RAM available for the library in bytes (default 32000 bytes) -mcu string MCU compilation target (default "cortex-m4"). MCU list: - Generic: cortex-m0plus, cortex-m1, cortex-m3, cortex-m4, cortex-m23, cortex-m33, cortex-m7 - Specific: cortex-m4_st_nucleo-f401re, cortex-m4_st_nucleo-l432kc, cortex-m33_st_stm32l562qe-dk, cortex-m4_st_steval-stwinkt1 -name string Name of the project -number_axis int Number of axis of the signals. (default 1) -slug_name string Slug name of the project. Can contain only letters, numbers and dash. You can find the slug name of an existing project by listing projects with -list.
Response:
Name | Type | Description | Example |
---|---|---|---|
creation_date | date | Expiration date of the license | "2020-02-13T09:58:12+00:00" |
description | bool | If the license key has been offline activated | false |
folder_name | string | Name of the folder containing the project | project_test-cli |
is_compatible | bool | If the project is compatible with current NanoEdge AI Studio Engine version | true |
is_multivariate | bool | If the project is multivariate | false |
last_update_date | string | Last update date of the project | "2020-01-09T09:47:04+00:00" |
max_flash | int | Maximum amount of Flash (in bytes) you wish to dedicate to NanoEdgeAI on the microcontroller | 20000 |
max_ram | int | Maximum amount of RAM (in bytes) you wish to dedicate to NanoEdgeAI on the microcontroller | 20000 |
mcu | string | Type of microcontroller used | "cortex-m4" |
name | string | Project's name | "test_cli" |
number_axis | int | Number of axis of the sensors | 1 |
project_type | string | Type of project ("on_board_training" for Anomaly Detection and "classifier" for Classification) | on_board_training |
slug_name | string | Project's slug name. The slug name is the identifier of the project. | "test-cli" |
1.4.4. 4. Signal: Import a new signal
- Import a signal
$ neai_cli signal -import -file_path "<my_file_path>" -nominal -delimiter "," -project <my_project_slug_name>
Usage:
signal <command> <attributes> Command: -delete Delete a signal Mandatory attributes: id, project -info Get info on a signal Mandatory attributes: id, project -import Import a signal Mandatory attributes: file_path, nominal or anomaly or class, project Optional attributes: name -list List signals Mandatory attributes: project Attributes: -anomaly Is anomaly signal -class Is class signal -delimiter string Signal file values delimiter (1 char max) -file_path string File path to the signal -id int ID of the signal -name string Name of the signal -nominal Is nominal signal -project string Project slug name
Response:
Name | Type | Description | Example |
---|---|---|---|
class_name | string | Name of the class | "my_class" |
file_found | bool | If the signal file has been found on the machine | "2020-02-13T09:58:12+00:00" |
file_name | string | Signal file name | "1.csv" |
file_path | string | Signal file path | "C:\Users\<my_name>\ Documents\workspaceNanoEdgeAi\ project_test-cli\signals\nominal\1.csv" |
file_type | string | Signal file type (nominal or anomaly or class) | "nominal" |
id | int | Signal id | 1 |
name | string | Signal name | "signal_test" |
number_axis | int | Number of axis of the sensors | 1 |
passed | bool | If tests on signal data has been successfully passed | true |
signalq_metadata | json | Metadata on the signal | {...} |
signalq_result | json | Results of tests on signal data | {...} |
1.4.5. 5. Optimization: Launch an optimization, retrieve progress and get result
- Launch an optimization:
$ neai_cli optimization -launch -signals "<my_signal_ids>" -project <my_project_slug_name>
- Get progress of an optimization
$ neai_cli optimization -progress -id <my_optimization_id> -project <my_project_slug_name>
- Get result of an optimization
$ neai_cli optimization -result -id <my_optimization_id> -project <my_project_slug_name>
- Stop an optimization
$ neai_cli optimization -stop
Usage:
optimization <command> <attributes> Command: -delete Delete an optimization Mandatory attributes: id, project -info Get optimization info Mandatory attributes: id, project -launch Launch an optimization Mandatory attributes: signals, project Optional attributes: max_ram, name, nb_cores -list List optimizations Mandatory attributes: project -progress Get progression of an optim Mandatory attributes: id, project -result Get the best result of an optimization Mandatory attributes: id, project -stop Stop current optimization Attributes: -id int ID of the optimization -name string Name of the optimization (default "my_optimization") -nb_cores int Number of cores to use for the optimization. Default min(machine's nb cores - 2, 1) -project string Project slug name -signals string List of Signal IDs to be used by the optimization. Ex: -signals="1,2"
Response:
- For launch, info and list:
- {| !width="11%"| Name !width="6%"| Type !width="62%"| Description !width="20%"| Example |- | creation_date | bool | If the license key has been offline activated | false |- | elapsed_time | int | Elapsed time (s) | 588 |- | id | string | ID of the optimization | 1 |- | name | string | Optimization name | "my_optimization" |- | state | string | Status of optimization | "finished" |}
- For progress:
- {| !width="15%"| Name !width="5%"| Type !width="58%"| Description !width="19%"| Example |- | done | int | Number of libraries tested | 789 |- | elapsed_time | int | Elapsed time (s) | 588 |- | optimization | int | ID of the optimization | 1 |- | progress | float | Progression of the optimization (0 to 1) | 0.95 |}
- For result:
- {| !width="14%"| Name !width="6%"| Type !width="60%"| Description !width="20%"| Example |- | buffer_size | int | Size of the buffer (bytes) | 2048 |- | confidence | float | Confidence performance | 0.9876 |- | estimated_flash | float | Estimated flash used by the library (bytes) | 4560.0 |- | estimated_ram | string | Estimated RAM used by the library (bytes) | 3215.0 |- | id | int | ID of the result | 1 |- | learning_curve | {} | Learning curve of the library (only for Anomaly Detection) | {...} |- | loss | float | Loss value used for internal optimization | -0.9878 |- | max_ram | int | Maximum RAM that was available (bytes) | 32000 |- | id | int | ID of the result | 1 |- | mcu | string | MCU set | cortex-m4 |- | optimization | int | ID of the optimization | 1 |- | precision | int | Accuracy performance | 0.9754 |}
1.4.6. 6. Emulator: Get a NanoEdge AI Emulator
- Compile an emulator:
$ neai_cli emulator -compile -id <my_optimization_id> -output_zip <my_emulator_path> -project <my_project_slug_name>
Usage:
emulator <command> <attributes> Command: -compile Compile a NanoEdge AI Emulator for an optimization Mandatory attributes: id, output_zip, project Attributes: -id int ID of the optimization -output_zip file path Output zip file path to store the NanoEdge AI Library -project string Project slug name
Response:
Name | Type | Description | Example |
---|---|---|---|
library_id | bool | Library code id. It should be used to communicate with Cartesiam support. | <LIBRARY_ID> |
mcu | string | Type of microcontroller used | "cortex-m4" |
file_path | string | Path to library zip | "library.zip" |
size_bytes | int | Size of the library (bytes) | 705502 |
1.4.7. 7. Library: Compile a NanoEdge AI Library
- Compile a library:
$ neai_cli library -compile -id <my_optimization_id> -output_zip <my_library_path> -project <my_project_slug_name>
Usage:
library <command> <attributes> Command: -compile Compile a NanoEdge AI Library for an optimization Mandatory attributes: id, output_zip, project Optional attributes: float_abi, short_wchar, fshort_enums Attributes: -float_abi string Float Abi: soft or hard (default "soft") -fshort_enums Use fshort enums -id int ID of the optimization -output_zip file path Output zip file path to store the NanoEdge AI Library -project string Project slug name -short_wchar Use short wchar
Response:
Name | Type | Description | Example |
---|---|---|---|
library_id | bool | Library code id. It should be used to communicate with Cartesiam support. | <LIBRARY_ID> |
gcc_version | string | Version of GNU ARM GCC compiler used | "arm-none-eabi-gcc-cli ..." |
mcu | string | Type of microcontroller used | "cortex-m4" |
compilation_flags_set | json | GNU ARM GCC compiler flags used | {...} |
file_path | string | Path to library zip | "library.zip" |
size_bytes | int | Size of the library (bytes) | 705502 |
1.5. V. Options
1.5.1. Display: Customize CLI outputs
- Use pretty printing:
$ neai_cli display -print -pretty_print
- Do not use pretty printing
$ neai_cli display -print -no_pretty_print
1.6. Resources
Documentation
All NanoEdge AI Studio documentation is available here <index>.
Tutorials
Step-by-step tutorials, to use NanoEdge AI Studio to build a smart device from A to Z:
Anomaly Detection:
- Smart vibration sensor (STM32) <vibration>
- Smart vibration sensor (Arduino) <vib_arduino>
- Smart current sensor (STM32) <current>
- Smart ukulele chord checker (STM32) <ukulele>
- Smart Italian coffee watcher (STM32) <coffee>
Classification:
- Multispeed fan classifier (STM32) <class_multispeed_fan>
Useful links:
*
- For technical issues, please create a ticket using the .
- For any question, contact us at [mailto:support@cartesiam.com support@cartesiam.com].
- For commercial enquiries, reach us via [mailto:contact@cartesiam.com contact@cartesiam.com].