Revision as of 08:30, 11 May 2021 by Registered User (Escoda Michael moved page STM32 MC SDK Overmodulation (new in V5.Y) to STM32MotorControl:STM32 MC SDK Overmodulation (new in V5.Y) without leaving a redirect)


1. Principle of SVPWM

Space vector modulation index is limited to (√3)/2 but there is way to extend this limit with the over-modulation. This technique is required when the modulation index (the length of the reference space vector Us) exceeds the edges of the hexagon.


1.1. Linear mode

STM32 MC Overmodulation slide9 1.png

In the linear area, V'cmd can keep both the amplitude and angle of Vcmd ,
then V'cmd = T'1 * V1 + T'2 * V2 with T'1 = T1 and T'2 = T2 .

1.2. TOVM mode 1

STM32 MC Overmodulation slide10 1.png

There are two cases:

    • In the green area: T1 + T2 ≤ 1 .

Vcmd is unmodified and the timings remain unchanged T'1 = T1 and T'2 = T2 . In that region V'cmd follows the circle.

    • In the blue area: T1 + T2 > 1 .

Then In order to keep V'cmd on the edge of the hexagon and keep the angle 𝜃, | V'cmd | is shrunk to make T'1 + T'2 = 1. V'cmd = T'1 * V1 + T'2 * V2 with T'1 = T1 / (T1 + T2) and T'2 = T2 / (T1 + T2).
In that region V'cmd follows the hexagon edge.

1.3. OVM mode 2

STM32 MC Overmodulation slide11 1.png


1.4. Example: F4 three shunt with Shinano motor at 4000rpm

STM32 MC Overmodulation slide17.jpg