This page explains the differences between the previous Cryptographic Library version V3.x.x and the current one V4.x.x.
1. What's new in the V4.x.x version
Cryptographic Library V4.x.x, in addition to new algorithms, brings more simplicity and more performances (both speed and size)
1.1. New algorithms
Here are the new algorithms available:
- Hash
- SHA3, SHAKE, SM3
- MAC
- KMAC
- Cipher
- SM4
- ECC
- SM2, ECDH on Curve448, EdDSA on edwards448 curve
- RSA
- PKCS#1 v2.2, CRT, Bellcore Attack protection
- DRBG
- CTR_DRBG-AES256
1.2. Simplicity
Here is an example on simpler interface brought by the Cryptographic Library V4.x.x in performing ECDSA verification:
V3.x.x | V4.0.0 |
---|---|
int32_t rv;
EC_stt EC_st;
membuf_stt Crypto_Buffer;
ECpoint_stt *PubKey = NULL;
ECDSAsignature_stt *sign = NULL;
uint8_t membuf[MAX_MEMBUF_SIZE];
ECDSAverifyCtx_stt verctx;
uint8_t pub_x[] = {…}, pub_y[] = {…};
uint8_t sign_r[] = {…}, sign_s[] = {…};
uint8_t digest[] = {…};
Crypto_Buf.pmBuf = membuf;
Crypto_Buf.mUsed = 0;
Crypto_Buf.mSize = sizeof(membuf);
// ToDo: manually fill EC_st with
// curve parameters!!!
/* Init the EC main struct */
rv = ECCinitEC(&EC_st, &Crypto_Buf);
/* Init the public key */
ECCinitPoint(&PubKey,
&EC_st,
&Crypto_Buf);
ECCsetPointCoordinate(PubKey,
E_ECC_POINT_COORDINATE_X,
pub_x,
sizeof(pub_x));
ECCsetPointCoordinate(PubKey,
E_ECC_POINT_COORDINATE_Y,
pub_y,
sizeof(pub_y));
/* Init the signature */
ECDSAinitSign(&sign,
&EC_st,
&Crypto_Buf);
ECDSAsetSignature(sign,
E_ECDSA_SIGNATURE_R_VALUE,
sign_r, sizeof(sign_r));
ECDSAsetSignature(sign,
E_ECDSA_SIGNATURE_S_VALUE,
sign_s, sizeof(sign_s));
/* Verification */
verif_ctx.pmEC = &EC_st;
verif_ctx.pmPubKey = PubKey;
rv = ECDSAverify(digest,
sizeof(digest),
sign,
&verif_ctx,
&Crypto_Buf); |
cmox_ecc_retval_t rv;
cmox_ecc_handle_t Ecc_Ctx;
uint8_t membuf[MAX_MEMBUF_SIZE];
uint32_t fault_check = CMOX_ECC_AUTH_FAIL;
uint8_t pubkey[] = {…}, digest[] = {…};
uint8_t signature[] = {…};
/* Construct a ECC context */
cmox_ecc_construct(&Ecc_Ctx,
CMOX_ECC256_MATH_FUNCS,
membuf, sizeof(membuf));
/* Verify directly the signature passing
all the needed parameters */
rv = cmox_ecdsa_verify(&Ecc_Ctx,
CMOX_ECC_CURVE_SECP256R1,
pubkey, pubkey(Public_Key),
digest, sizeof(digest),
signature, sizeof(signature),
&fault_check); |
Here is another example on simpler interface brought by the Cryptographic Library V4.x.x in performing AES GCM AEAD Encryption:
V3.x.x | V4.0.0 |
---|---|
AESGCMctx_stt AESctx;
uint32_t error_status = AES_SUCCESS;
AESctx.mFlags = E_SK_DEFAULT;
AESctx.mKeySize = sizeof(Key);
AESctx.mIvSize = sizeof(IV);
AESctx.mTagSize = 16;
/* Initialize the operation, by passing key and IV */
error_status = AES_GCM_Encrypt_Init(&AESctx,
Key, IV);
/* Append AAD */
error_status = AES_GCM_Header_Append(&AESctx,
AddData, sizeof(AddData));
/* Append plaintext */
error_status = AES_GCM_Encrypt_Append(&AESctx,
Plaintext, sizeof(Plaintext),
Computed_Ciphertext, &computed_size);
/* Finalize and compute tag */
error_status = AES_GCM_Encrypt_Finish(&AESctx,
Tag, &tag_size); |
cmox_cipher_retval_t rv;
rv = cmox_aead_encrypt(CMOX_AES_GCM_ENC_ALGO,
Plaintext, sizeof(Plaintext),
sizeof(Expected_Tag),
Key, sizeof(Key),
IV, sizeof(IV),
AddData, sizeof(AddData),
Computed_Ciphertext, &computed_size);
/* NB: tag included in Computed_Ciphertext */ |
1.3. Performances
Here is a comparative view of the best performances achievable on a STM32G4 using both the Cryptographic Library V3.x.x and V4.x.x versions.
Use cases | V3.1.3 Cycles | V4.0.0 Cycles | Improvements | V3.1.3 Code Size | V4.0.0 Code size | Improvements |
---|---|---|---|---|---|---|
AES CBC 64 Bytes encryption | 11,189 | 8,660 | 22.6% | 8,218 | 4,592 | 44.1% |
AES CBC 64 Bytes decryption | 12,000 | 10,098 | 15.8% | 8,218 | 4,592 | 44.1% |
SHA256 16 bytes Digest | 9,630 | 6,137 | 36.2% | 2,204 | 2,144 | 2.7% |
ECDSA SECP256R1 Signature | 20,298,504 | 2,957,360 | 85.4% | 21,616 | 14,610 | 32.41% |
ECDSA SECP256R1 Verification | 26,891,792 | 6,575,536 | 75.55% | 21,616 | 15,110 | 30.10% |
2. Deprecated algorithms
Some algorithms available in the V3.x.x are no more supported, cause they have been deprecated for security reason.
Algorithm | Comment |
---|---|
MD5 | More details on MD5 vulnerabilities are available here rfc6151 |
ARC4 | More details on RC4/ARC4 vulnerabilities are available here rfc7465 |
DES | Withdrawn by NIST on May 19, 2005:FIPS46-3 |
T-DES | Withdrawn by NIST on September 26, 2018:NIST-SP800-20 |
3. V3.x.x to V4.x.x migration information and links
In the Cryptographic Library middleware legacy_v3 folder, we provide migration helpers.
This files are provided to help you migrate your software designed upon V3.x.x APIs onto the V4.x.x APIs.
3.1. Switch your project from V3.x.x to V4.x.x
- Remove the old V3.x.x library from your project, including the path to the V3.x.x library header folder.
- Update your project to include the V4.x.x as describe in Creating a project
- Add to your project settings the path to the legacy_v3/include folder
- Add to your project settings the path to the legacy_v3/src folder
- Add to your project settings the sources to the legacy_v3/src files coresponding to the algorithms you are using
- Rebuild all your project, it should work as before
ECC particular case:
In the V4.x.x library ECC module, to avoid specific attacks (invalid point/curve attacks), the parameter B is mandatory and must be given to successfully instantiate an ECC curve.
Thus, if your code running on the V3.x.x library is not providing it in the curve's parameter of structure EC_stt to the ECCinitEC function, you need to change this part of your code to have it working using the helpers+V4.x.x.
3.2. Migrate your project from V3.x.x to V4.x.x
You can now rewrite your application progressively to use the V4.x.x APIs and then fully benefit of all the V4.x.x improvements.