STM32 MCSDK Single Shunt Phase Shift support (new in V5.Y)

Revision as of 10:14, 13 April 2021 by Registered User (Table bug fix)


1. Single shunt phase shift overview

In the context of a single shunt topology, the purpose of the phase shifting is to shift one or two duty cycles in order to have to be able to sample current signal in the boundary zones instead of inserting a distortion window. The benefit are:

  • Less commutations
  • Less switching losses
  • Less acoustical noise
  • Better current shape

2. Single shunt phase shift comparison

  • Single shunt with distortion window
  • Single shunt with phase shift
  • and Three shunts


3. Phase shift principle

Boundary zone 1:

  • FW shifts on the right the smallest duty cycle by TMIN (minimum window time for sampling)
STM32 MC Image 008.png


Boundary zone 2:

  • FW shifts on the right the middlest duty cycle by TMIN (minimum window time for sampling)
STM32 MC Image 009.png


Boundary zone 3:

  • FW shifts on the right the smallest duty cycle and on the left the highest duty cycle by TMIN (minimum window time for sampling)
STM32 MC Image 010.png


4. Peripheral usage

Phase shifting needs the following peripherals to create the shifting. According to the advanced timer capabilities, one or two DMA channels will be used

MCU TIM DMA IRQ
F0 TIM1 DMA1_Ch5 DMA1_Ch4 DMA1_Ch5 HT and TC
G0 TIM1 DMA1_Ch4 DMA1_Ch4 HT and TC
F3 TIM1 DMA1_Ch4 DMA1_Ch4 HT and TC
TIM8 DMA1_Ch2 DMA1_Ch2 HT and TC
F4 TIM1 DMA2_stream4 DMA2_stream5 DMA_stream5 HT and TC
TIM8 DMA2_stream7 DMA2_stream1 DMA_Stream1 HT and TC
G4 TIM1 DMA1_Ch1 DMA1_Ch1 HT and TC
TIM8 DMA2_Ch1 DMA2_Ch4 HT and TC
L4 TIM1 DMA1_Ch4 DMA1_Ch4 HT and TC
TIM8 DMA2_Ch2 DMA2_Ch2 HT and TC
F7 TIM1 DMA2_stream4 DMA2_Stream4 HT and TC
TIM8 DMA2_stream7 DMA2_Stream7 HT and TC

5. Single shunt phase shift scheduling

6 channels advanced timer and execution rate = 1 (G0,G4,F3,L4,F7)

STM32 MC Image 016.png

6 channels advanced timer and execution rate = 2 (G0,G4,F3,L4,F7)

4 channels advanced timer and execution rate = 1 (F4)

4 channels advanced timer and execution rate = 2 (F4)

4 channels advanced timer and execution rate = 2 (F0)

6. Single shunt phase shift in the MCSDK

Single shunt is divided in 4 template files

  • r1_ps_pwm_fdbk.c/.h.ftl processed when the MC project uses a MCU with 6 channels advanced timer (G0,F3,G4,L4,F7)
  • r1_ps_4ch_pwm_fdbk.c/.h.ftl processed when the MC project uses a MCU with 4 channels advanced timer