1. Introduction
The ACIM Software Development Kit (SDK) is a set of firmware plugins implementing different kinds of motor control algorithms for Alternate Current Induction Motors (ACIM), the kit is based on X-Cube-MCSDK.
The package includes an application example to drive an induction motor using the NUCLEO-F303RE and the STEVAL-IPM10B boards (connected together using the X-NUCLEO-IHM09M1 expansion board).
2. Main features
- STM32 F3 Support of induction motors.
- Vector control algorithms:
- Field Oriented Control with speed sensor (I-FOC)
- Self-sensing Field Oriented Control (LSO-FOC) (Sensorless)
- Scalar control algorithms:
- Open Loop V/f
- Closed Loop V/f
- API function available to send the application commands to the motor driver using the ST Motor Control Workbench tool.
- PC GUI for firmware configuration and dedicated induction motor parameters settings (ACIM GUI).
3. Hardware and Software setup
3.1. Hardware prerequisites
- 1x High voltage 3 phase motor driver board: (STEVAL-IPM10B),
- 1x STM32 Nucleo development board: (NUCLEO-F303RE),
- 1x Motor control connector expansion board: (X-NUCLEO-IHM09M1),
- 1x DC power supply (max 400 Vdc),
- 1x DC power supply (max 15 Vdc),
- 1x USB type A to mini-B USB cable,
- 1x 3-Phase ACIM up to 1 kW.
3.2. Software prerequisites
- STSW-LINK009: ST-LINK/V2-1 USB driver,
- STSW-LINK004: STM32 ST-LINK utility,
- Only to update ST-LINK firmware to last version.
- A Windows PC with the supported development toolchain:
- IAR Embedded Workbench IDE – ARM 7.80.4.
- X-CUBE-MCSDK version 5.0.x
- ST Motor Control Workbench (Only for monitoring purpose).
For more information, please refer to the related documentation available on http://www.st.com .
3.3. Field Oriented Control FW example for Induction Motors
3.3.1. Hardware configuration
- NUCLEO-F303RE
- Remove SB21 to disable the LED2.
- If the Nucleo board is powered by USB during the motor test (JP5 is mounted between 1-2 pins), in case of encoder sensor usage: connect a DC voltage source (7V to 12V) on the VIN pin (in order to provide the required E5V voltage to the MC_25 pin of the Motor control connector), refer to UM1724 for more info.
- X-NUCLEO-IHM09M1
- Remove R2, R3, R13, R18 R21, R22, R23 resistors.
- Stack the X-NUCLEO-IHM09M1 on the STM32 Nucleo board using the ST morpho-connector.
- Connect the X-NUCLEO-IHM09M1 to the STEVAL-IPM10B using the Motor control connector (see the ACIM User Guide for more details).
- Connect the STM32 Nucleo board to the PC through the USB cable. (see the ACIM User Guide for more details).
- STEVAL-IPM10B
- Connect a DC power supply (between 15-20 Vdc) on J4 connector.
- Mount the Bulk capacitor C1 (the value to be used is linked to the application parameters. i.e. voltage ripple, load condition).
- Connect a DC power supply (up to 400 Vdc) on J1 connector.
- Connect the motor phase cables on J3 connector.
- To evaluate motors with load, assemble an appropriate heatsink on the power module on the bottom of the board.
3.3.2. How to use the FW package
- Unzip the “ACIM SDK ver.1.0.0.zip” in a working folder. This working folder will contain the ACIMGUI, the source code and the IAR project to build the executable FW. You can relocate the working folder to any other folder on the PC just keeping the internal folder structure as it has been provided.
- Open the “ACIMGUI.exe” available on “InductionMotor/ACIMGUI” path, and fill the required fields (according to you motor and drive settings) and then generate all required .h files required by the FW.
Do not use the ST MCWB to generate the FW configuration, the ST MCWB will be used only for the real time communication with the board.
The next slides will explain how to use the ACIM GUI and the ST MCWB monitor window, respectively, to configure the FW and to send commands to the motor and to perform the debug of the solution.
For more information, please refer to the related documentation available on http://www.st.com .
The ACIM GUI therefore carries out the following tasks:
- Tuning of the PI controllers used by the motor control firmware.
- Generation of the necessary header files for firmware compiling.
4. How to use the software tools
4.1. ACIM GUI
4.1.1. V/f Open loop mode
- Select the MAIN_VF_OL mode from ACIM Mode menu.
- Set the required parameters. (see Note 1)
- Save the project (Optional) in a user folder for load it in the future.
- Click on the Generate command.
Note 1:
- Ensure to avoid inserting letters in the numerical fields or not valid values, due to typing errors, in order to avoid undesired behavior of the motor and/or the hardware. In fact, the ACIM GUI does not perform any validity check on the inserted values.
4.1.2. Indirect Field Oriented Control (IFOC) mode (with speed sensor)
- Select the MAIN_IFOC mode from ACIM Mode menu.
- Set the required parameters. (see Note 3)
- Please see Appendix A of this document to have more info about the measure of some parameters.
- Save the project (Optional) in a user folder for load it in the future.
- Click on the Generate command.
- The header (.h) file generated will contain also the value of the gains (Kp and Ki) of the speed and current PI regulators.
- If the user intends to modify manually the gains can select the Manual Edit checkbox and adjust their value.
- In this case, make sure the divisors are power of 2 in order to avoid compiling errors of the FW.
Note 3:
- Ensure to avoid inserting letters in the numerical fields or not valid values, due to typing errors, in order to avoid undesired behavior of the motor and/or the hardware. In fact, the ACIM GUI does not perform any validity check on the inserted values.
4.1.3. Luenberger State Observer - Field Oriented Control (LSO-FOC) mode (without speed sensor)
- Select the MAIN_LSO_FOC mode from ACIM Mode menu.
- Set the required parameters. (see note 4)
- Please see Appendix A of this document to have more info about the measure of some parameters.
- Save the project (Optional) in a user folder for load it in the future.
- Click on the Generate command.
- The header (.h) file generated will contain also the value of the gains (Kp and Ki) of the speed and current PI regulators.
- If the user intends to modify manually the gains can select the Manual Edit checkbox and adjust their value.
- In this case, make sure the divisors are power of 2 in order to avoid compiling errors of the FW.
Note 4:
- Ensure to avoid inserting letters in the numerical fields or not valid values, due to typing errors, in order to avoid undesired behavior of the motor and/or the hardware. In fact, the ACIM GUI does not perform any validity check on the inserted values.
4.1.4. Information about the parameter to be inserted
- Pole pairs is the number of rotor electromagnetic pole pairs.
- Rr is the rotor phase resistance expressed in Ohm.
- Rs is the stator phase resistance expressed in Ohm.
- Lls is the stator phase leakage inductance expressed in Henry.
- Llr is the rotor phase leakage inductance expressed in Henry.
- Lms is the rotor phase magnetizing inductance expressed in Henry.
- In is the rated nominal phase motor current expressed in Ampere rms.
- Im is the magnetizing phase current that corresponds to the no-load test phase current. In the case of FOC it will be the value fixed for Id current. It is expressed in Ampere rms.
- Vn is the rated phase to neutral voltage expressed in Voltage rms.
- Fn is the rated motor frequency expressed in Hz.
- PWM frequency is the frequency of gate signals and of the High Frequency Task, which manages the electromagnetic field angle computation and the duty cycle computation.
- Validation Tick is the number of consecutive Speed Loop task ticks when the measured Id current is into the [Low BW limit, UP BW limit] bandwidth. It is used at any startup to magnetize the motor before to generate torque.
- Low BW limit and UP BW limit are the bandwidth limits and they are expressed in %
- Execution frequency of speed regulator section is the frequency of Medium Frequency task that manages the motor control state machine and then the speed loop execution.
- LSO gain is the empiric value to set in order to guarantee the stability of the LSO (between 1-1.5)
- Target Speed is the default value that the speed control will take into account at the first Start Motor command; in the case, the user has not previously executed the Exec ramp command. (For more details of STMCWB monitor window commands, please see dedicated slides of this document).
- Max Speed is the maximum mechanical speed that FW will allow to set as target speed. It can be chosen considering the minimum value between the max motor speed and the max speed readable by sensor; or simply considering the max application speed, if it is not higher than the motor and sensor max velocity.
Inertia is the rotor + load inertia coefficient. Friction is the rotor + load friction coefficient.
Encored PPR is the Pulses Per mechanical Revolution. Encoder inv. dir. inverts the sign of the measured speed. The user has to choose the state of this checkbox in order to match the sign convention of the encoder with the firmware’s one, according to the motor phases connection.
Kf (Vrms/Hz) Flux constant is the value of the flux maintained constant during the V/f control. The user can calculate it dividing the nominal phase peak voltage for nominal frequency. If necessary, he can adjust in order to find the best value that provides the maximum torque with the maximum speed range according to the user’s application. Voltage offset is the peak value of voltage used to compensate the voltage drop on the stator winding at very low frequency. (Below the Min Frequency). Min Frequency is used to fix the Voltage offset if the applied frequency is below the threshold.
The Bandwidth field is the PI regulator bandwidth used for its tuning. High values increase the reactivity of the regulator but can introduce noise and fast oscillation on the controlled quantity.
4.2. Project building and MCU programming
- Open the “Project.eww” file located in the \InductionMotor\EWARM\
- Build the project using the Rebuild All command (at the first time is better to us it) or simply using the Make command, from Project menu.
- Download the firmware into the MCU using the Download and Debug command
4.3. ST MC Workbench
4.3.1. Advanced Monitor window
Starting from the MCSDK 5.0 version, the STMC WB tool can generate the entire project (Source and header files of library and the IDE workspace too) according to the user hardware configuration (Control board, power board, current sensing topology, motor speed/position sensor and so on).
Using the ACIM SDK the user shall not use the generation of the project using STMCWB because this will erase the project for ACIM.
Use the STMC Workbench only to establish the UART serial communication. The user shall use the Monitor Window. We suggest to use the Advanced tab because it allows the control of more parameters than Basic one.
Open the InductionMotor.stmcx project and click on the Monitor button and select the Advanced tab as shown in the figure.
The user can change the Currents and Speed regulators gains when the active control is the FOC (Indirect or LSO).
When the selected control is V/f (Closed or Open loop), these gains will not have any effect.
5. Firmware architecture overview
This ACIM SDK is a firmware plugin to develop applications based on induction motors.
The package includes an application example to drive a high voltage induction motor using the NUCLEO-F303RE and the STEVAL-IPM10B boards (connected together using the X-NUCLEO-IHM09M1 expansion board). In the Figure 1 the overall system architecture is shown.
6. Appendix A - How to measure the motor electrical parameters with standard tests
6.1. Measurement setup
6.2. Electrical model of the motor at steady state
Where:
Parameter | Comment |
---|---|
R_s (Ω) | Stator phase winding resistance |
L_ls (H) | Stator Leakage inductance |
R_Fe (Ω) | Equivalent iron loss resistance |
L_ms(H) | Magnetizing inductance |
L_lr^'(H) | Rotor leakage inductance referred to stator |
R_r^'(Ω) | Equivalent rotor phase resistance |
Φ_n(Wb) | Nominal magnetizing flux |
6.3. DC Test
During the DC test, a continuous electromagnetic field is generated. It means the equivalent impedance of the motor is resistive and only the stator has to be considered.
It consists in measuring resistance between two stator windings with a multimeter.
6.4. No-Load test – Rotating test
No-load: slip s = 0 (ωre ≅ ωe)
Since the I0 is equal to the magnetizing current it is lower than the nominal current, In, the voltage drop on the Rs and Lls parameters is negligible respect of the nominal phase voltage, Vn. It is so possible to consider the following equivalent circuit:
The term R_Fe represent the iron-losses and it is value is higher than the magnetizing impedance module, Z_m= ω_e L_ms, so it is reasonable to consider, I_(m,rms)≅ I_(0,rms)
6.5. Blocked-Rotor test
The rotor is mechanically blocked: slip s = 1 (ωre = 0)
Since the I_br=I_n and it is higher than the magnetizing current (no-load current), I_br, (I_br >> I_m) the magnetizing branch is negligible respect of the series one. It is so possible to consider the following equivalent circuit:
7. Appendix B - Block diagrams and principles about the implemented ACIM control methods
7.1. Legend of symbols
- fe = stator frequency, Hz
- e = stator pulsation, rad/s
- re = rotor electrical pulsation, rad/s
- slip = slip pulsation, rad/s
- n*r = mech. target speed, rpm
- nr,fbk = mech. target speed, rpm
- τr = Lr/Rr = electrical rotor time constant, s
- I*qd = q-d reference frame reference current vector
- Iqd,fbk = q-d reference frame measured current vector
- Vqd = q-d reference frame voltage vector
- Vαβ = α-β reference frame voltage vector
- θλr = rotor flux position
7.2. Constant airgap flux operation - V/f
7.2.1. Open loop block diagram
Advantages
- Simple control.
- No speed sensors.
- Motor electrical model not required.
Drawback and Limitations
- Low efficiency.
- Low control dynamics.
- No speed control.
- Although the stable region curve slope remains constant, maintaining the V/f = const., an increase/decrease of the mechanical load causes a variation of the rotor speed (modifying the slip frequency in order to provide the required torque).
7.2.2. Closed loop block diagram
Advantages
- Simple control.
- Motor electrical model not required.
- Speed control modify the slip frequency in order to provide the required mech. Load and to maintain the rotor speed target.
Drawback and Limitations
- Low efficiency.
- Low control dynamics.
7.3. Field Oriented control
7.3.1. Indirect Field Oriented control (IFOC) – solution with speed sensor
Advantages
- High efficiency.
- High control dynamics.
- Simple estimation of rotor flux position.
Drawback and Limitations
- Some motor parameters are required (τ_r)
- Motor parameters variation dependency (i.e. variation of resistances with the temperature) badly affecting the efficiency.
- Speed sensor is required both for rotor flux position estimation and for speed loop execution.
7.4. = Luenberger State Observer–FOC (LSO-FOC) – solution without speed sensor
Advantages
- High efficiency.
- High control dynamics.
- Speed sensor not required both for rotor flux position estimation and for speed loop execution.
Drawback and Limitations
- Motor electrical model is required.
- Motor parameters variation dependency (i.e. variation of resistances with the temperature) badly affecting the efficiency and/or the speed estimation accuracy.
- Complexity of estimator model.
- Empiric setting of the observer gain.
8. Experimental results
8.1. Motor data
ABB Motor
- 3-Phase AC Induction Motor 750 W
- 380-420 V (Y) – 1.9 A (Y) – 50Hz
8.2. Hardware setup
8.3. V/f open Loop - No load
8.4. V/f Closed Loop – No load
8.5. Indirect Field Oriented control (IFOC) – No load
8.6. Indirect Field Oriented control (IFOC) – Mech. Load 1 Nm
8.7. Luenberger State Observer–FOC (LSO-FOC) – No load
8.8. Luenberger State Observer–FOC (LSO-FOC) – Mech. Load 1 Nm