Cellular hardware setup

Revision as of 08:30, 1 April 2021 by Registered User (Escoda Michael moved page Cellular Hardware setup to Cellular hardware setup without leaving a redirect)
Renaming.png This page is a candidate for renaming (move).
The requested new name is: Cellular hardware setup .
The supplied reason is: No need to capitalize "hardware" .
-- Registered User (-) 21:35, 30 March 2021 (CEST).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.

Click here for Cellular overview

1. Introduction

This wiki page contains information to help users with their hardware setups.
X-CUBE-CELLULAR V6.0.0 supports different types of hardware setups.
Some are based on a module that contains both an STM32 and modem while some others are based on two boards, an STM32 board associated with a separate modem board.
If the STM32 board has no STMod+ connector, use an ARDUINO® / STMod+ adaptor. This is the case for the B-L4S5I-IOT01A.
Separate STM32 and modem boards are sometimes available as one pack composed of two boards in the same blister. This is the case for the P-L496G-CELL02.
In case of issue, do not forget to check the ST-LINK firmware version and upgrade it if needed. Use for instance the STM32CubeProgrammer tool (STM32CubeProg) for this purpose.

2. B-L462E-CELL1

2.1. Boards and ST-LINK USB cable connections

B-L462E-CELL1

The red USB cable from the PC is used to power and interact with the STM32.

3. P-L496G-CELL02

3.1. Boards and ST-LINK USB cable connections

P-L496G-CELL02

The red USB cable from the PC is used to power and interact with the STM32.

4. B-L4S5I-IOT01A + X-NUCLEO-STMODA1 + B-CELL-GM01Q or STEVAL-STMODLTE

4.1. Boards and ST-LINK USB cable connections

B-L4S5I-IOT01A + X-NUCLEO-STMODA1 + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable from the PC is used to power and interact with the STM32.

5. 32L496GDISCOVERY + B-CELL-GM01Q or STEVAL-STMODLTE

5.1. Boards and ST-LINK USB cable connections

32L496GDISCOVERY + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable from the PC is used to power and interact with the STM32.

6. STEVAL-STWINKT1B + B-CELL-GM01Q or STEVAL-STMODLTE

6.1. Boards and ST-LINK USB cable connections

STEVAL-STWINKT1 + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable from the PC is used to interact with the STM32 through the STLINK-V3. This cable is provided in the blister.
A second USB cable (not provided) is needed to power the STEVAL-STWINKT1B through its USB connector.

7. Previous X-CUBE-CELLULAR versions before V6.0.0

The former X-CUBE-CELLULAR versions support other hardware setups such as P-L496G-CELL01 (similar to P-L496G-CELL02 but with the UG96 Quectel 2G/3G modem), and B-L475E-IOT01A.
UG96 is no more used because, nowadays, LTE Cat M and NB-IoT networks are available and much more low-power friendly than 3G.
B-L475E-IOT01A (also known as "IoT node V1") is replaced with B-L4S5I-IOT01A (also known as "IoT node V1.5").