STM32WBA Bluetooth® LE - STM32CubeMX Application Conception

Click here for Bluetooth® Low Energy Overview.

1. Introduction

STM32CubeMX tool is a graphical tool that helps you to generate an application targeting the STMicroelectronics MCU of your choice, with initialization code based on the configuration you specify. In the tools interface, you can select the right STMicroelectronics MCU, configure pins, clocks, peripherals, middleware, and it generates code project based on your setup.

This wiki page defines how to generate a Bluetooth® Low Energy (BLE) server application for STM32WBA52CG MCU using STM32CubeMX software.

2. Build a Bluetooth® Low Energy application on STM32WBA with STM32CubeMX

The STM32WBA Nucleo board, flashed with the application generated by STM32CubeMX, can send data to a smartphone (using ST BLE ToolBox application), and receive commands from it through Bluetooth® Low Energy.

System presentation
Connectivity WBA CMX System Presentation


This GATT Server application shall be able to expose two services:

  • First service exposes two characteristics
  • Second service exposes three characteristics

The first service (My_P2P_Server) looks like P2P Server (STM proprietary) with two characteristics:

  • Characteristic 1 has Write property
  • Characteristic 2 has Notify property

Writing to characteristic 1 toggles blue LED.
Pressing B1 on Nucleo board send data to the phone

Custom Service
Connectivity WBA CMX Custom Service


The following steps are recommended to build this application example:

Step by step 1 logo.png

Step 1: STM32CubeMX initialization for STM32WB52CG
Initialize a STM32CubeMX project targeting STM32WB52GG platform.

Step by step 2 logo.png

Step 2: STM32WBA IP configuration
Enable required system resources and peripherals to make BLE application to work.

Step by step 3 logo.png

Step 3: Clock configuration
Setup project clocks.

Step by step 4 logo.png
Step 4: Project Setup
Define project settings for C code generation as project name, IDE, Firmware location.

Step by step 5 logo.png
Step 5: Bluetooth® LE GAP/GATT Custom Application Configuration
Define BLE Application as Advertising parameters, Services and Characteristics.


Service and Characteristics configuration are given in the following table:

Service Long Name My_P2P_Server
Service Short Name My_P2P
UUID Type 128 bits
UUID 0xFE40
Characteristic Long Name My_LED_Char My_Switch_Char
Characteristic Short Name LED_C SWITCH_C
UUID Type 128 bits 128 bits
UUID 0xFE41 0xFE42
Char Properties Read + Write w/o response Notify
Char Permissions None None
Char GATT Events GATT_NOTIFY_ATTRIBUTE_WRITE GATT_NOTIFY_ATTRIBUTE_WRITE

3. Tools

3.1. Software tools

To make and use this project, the needed software tools to complete the application are:

  • STM32CubeMX[1] software (from v6.9.0)
  • STM32CubeWBA MCU Package[2] (from v1.0.0)
  • IDE: STM32CubeIDE[3] or IAR[4]
  • Serial Terminal (TeraTerm[5])
  • Smartphone application ST BLE ToolBox

3.2. Hardware tools

A STM32WB Nucleo board and a micro-B to Type-A USB cable are also needed.

Hardware presentation
Connectivity WBA CMX Hardware Presentation.jpg


4. STM32CubeMX initialization for STM32WBA Nucleo Board

4.1. STM32CubeMX initial setup

Open STM32CubeMX and start a new project from the Access to MCU selector button

New Project Menu
Connectivity wiki photo 03.png


Chose the MCU and then start the new project:

puce1.png
In MCU/MPU Selector, open the Series menu in PODUCT INFO
puce2.png
Check the STM32WBA
puce3.png
Select the STM32WBA52CGU6 part number
puce4.png
Start the project
Project Interface
Connectivity WBA CMX Project Interface.jpg


Start the new project without TrustZone activated

Connectivity WBA CMX Trust Zone Activation.jpg

4.2. Pinout and IP configuration

To configure the system, enable all the required system resource and peripherals clicking on A->Z to display all IPs.

Pinout & configuration interface
Connectivity WBA CMX pinout Config Interface.jpg


BLE mode is reachable once the following system resources and peripherals are turned to enable.

  • ADC4 :activate Temperature Sensor Channel
  • CRC :Activated
  • RAMCFC :Activate SRAM1
  • ICACHE :1 way (direct mapped cache)
  • RNG :Activated
  • RCC : HSE and LSE on Crystal/Ceramic resonator
  • RF :Activated
  • RTC : Activate clock source
  • USART1 : Turn Mode to Asynchronous
  • GPDMA1 : Configure channel 0 & 1
  • NVIC : Verify NVIC settings
IP list
Connectivity WBA CMX IP List.jpg

4.2.1. ADC4

The 12-bit analog to digital converter has sever (ADC4) has external and two internal (temperature sensor, voltage reference measurement) channels and performs conversions in single-shots or scan modes.

puce1.png
Select ADC4
puce2.png
Check Temperature Sensor Channel
puce3.png
Set sampling Time Common 1 to 814.5
ADC4 configuration
Connectivity WBA CMX ADC4 Configuration.jpg

4.2.2. CRC

The Cyclic Redundancy Check (CRC) is used to verify data transmission or storage integrity.

puce1.png
Select CRC
puce2.png
Activate it
CRC activation
Connectivity WBA CMX CRC Configuration.jpg

4.2.3. RAMCFG

The RAMs ConFiGuration Controller (RAMCFG) configures the features of the internal SRAMs

puce1.png
Select RAMCFG
puce2.png
Select RAMCFG SRAM1
RAMCFG Activation
Connectivity WBA CMX RAMCFG Configuration.jpg

4.2.4. ICACHE

The Instruction CACHE (ICACHE) is introduced on C-AHB code bus of ARM Cortex-M33® processor to improve performance when fetching instruction and data from internal memories.

Configuration of ICACHE is done as follows:

puce1.png
Select ICACHE
puce2.png
Choose 1-way (direct mapped cache) for Mode
ICACHE Activation
Connectivity WBA CMX ICACHE Configuration.jpg

4.2.5. RNG

The Random Number Generator (RNG) provides full entropy outputs to the application as 32-bit samples.

puce1.png
Select RNG
puce2.png
Activate it
puce3.png
Select NVIC panel
puce4.png
Enable RNG Global interrupt

RNG Activation
Connectivity WBA CMX RNG Configuration.jpg

4.2.6. RCC

Reset and Clock Control (RCC) manages the different kind of reset and generates all clocks for the bus and peripherals.

puce1.png
Select RCC
puce2.png
Choose Crystal/Ceramic Resonator for HSE
puce3.png
Choose Crystal/Ceramic Resonator for LSE
puce4.png
Select NVIC panel
puce5.png
Enable RCC non-secure global interrupt
RCC Activation & Setup
Connectivity WBA CMX RCC Configuration.jpg

4.2.7. RF

Activate RF

puce1.png
Select RF
puce2.png
Activate RF
RF Activation
Connectivity WBA CMX RF Configuration.jpg

4.2.8. RTC

Real Time Clock (RTC) provides an automatic wakeup to manage all low-power modes.

puce1.png
Select RTC
puce2.png
Activate Calendar
puce3.png
Set Alarm A to Internal Alarm A
puce4.png
Select Parameter Settings tab
puce5.png
Set Asynchronous Predivider value to 31
puce5.png
Set Bin Mode to Free running Binary mode
RTC Configuration (1/2)
Connectivity WBA CMX RTC1 Configuration.jpg
puce8.png
Select NVIC Settings tab
Enable RTC non-secure interrupt (in Parameter Settings tab, SSRU Underflow Interrupt will be turned to Enabled automatically)
RTC Configuration (2/2)
Connectivity WBA CMX RTC2 Configuration.jpg


4.2.9. USART1

USART1 is enabled to allow display of traces on a terminal.

puce1.png
Select USART1
puce2.png
Turn Mode to Asynchronous
puce3.png
Select Parameters Settings tab
puce4.png
In Advanced Parameters, set Over Sampling to 8 samples (other settings are already fine)
puce5.png
Once USART1 is activated, USART1_TX and USART1_RX are affected to pin PB12 and PA8
USART1 Configuration (1/2)
Connectivity WBA CMX USART1 1 Configuration.jpg
puce6.png
Select RF
puce7.png
Activate RF
USART1 Configuration (2/2)
Connectivity WBA CMX USART1 2 Configuration.jpg



4.2.10. GPDMA1

The General Purpose Direct Memory Access (GPDMA) controller is a bus master and system peripheral. The GPDMA is used to perform programmable data transfers between memory-mapped peripherals and/or memories via linked-list, upon the control of an off-loaded CPU.

puce1.png
Select GPDMA1
puce2.png
Set Channel 0 and Chanel 1 to Standard Request Mode
GPDMA1 Configuration (1/4)
Connectivity WBA CMX GPDMA 14 Configuration.jpg



puce1.png
In CH0 tab
puce2.png
Under Request Configuration, set Request to USART1_TX
puce3.png
Under Channel Configuration, set Direction to Memory to Peripheral
puce4.png
In Source Data Setting, enable Source Address Increment After Transfer
GPDMA1 Configuration (2/4)
Connectivity WBA CMX GPDMA 24 Configuration.jpg



puce1.png
In CH1 tab
puce2.png
Under Request Configuration, set Request to USART1_RX
puce3.png
Under Channel Configuration, set Direction to Peripheral to Memory
puce4.png
In Destination Data Setting, enable Destination Address Increment After Transfer
GPDMA1 Configuration (3/4)
Connectivity WBA CMX GPDMA 34 Configuration.jpg



puce1.png
In All Channels tab
puce2.png
The channels configuration shall be displayed
GPDMA1 Configuration (4/4)
Connectivity WBA CMX GPDMA 44 Configuration.jpg


4.2.11. NVIC

The Nested Vector Interrupt Controller (NVIC) ans the processor core interface are closely coupled, enabling low-latency interrupt processing and efficient processing of late arriving interrupts. All interrupts including the core exceptions are managed by the NVIC.

puce1.png
Go to NVIC setting interface
puce2.png
Enable all the needed Interrupt
puce2.png
Set the Preemption priority
NVIC Configuration
Connectivity WBA CMX NVIC Configuration.jpg

4.3. Clock configuration

On Clock Configuration tab, run the automatic clock issue solver (if requested).

This following configuration is defined for initial startup phase. At runtime, clocks will be managed dynamicly by System Clock Manager (SCM) module.

Connectivity WBA CMX Clock Configuration 12.jpg

Then:

puce1.png
ADC4 Clock Mux on HCLK1
puce2.png
RTC Clock Mux on LSE
puce3.png
System Clock Mux on HSE
puce4.png
PLL1 *N on x8
puce5.png
Radio Sleep Timer Clock Mux on LSE
puce4.png
RNG Clock Mux on HSI
puce5.png
USART1 Clock Mux on HSI (reachable only when USART1 turned ON)
Clock configuration
Connectivity WBA CMX Clock Configuration 22.jpg

5. BLE GAP/GATT Custom application configuration

Now, we can start configuring and defining the STM32 WPAN.

  • Bluetooth® LE Peripheral Custom Template GATT Server Application can be defined:
    • On STM32WBA
    • With STM32CubeMX (available from Version 6.8.0)
  • GAP peripheral : advertising configuration
  • GATT server configuration:
    • 25 services maximum
    • 25 characteristics maximum per service
  • ACI commands:
    • AN5270: STM32WBx5 Bluetooth® Low Energy (BLE) wireless interface[6].

5.1. Enable BLE

To configure your application :

puce1.png
Select STM32_WPAN
puce2.png
In Mode panel, chose Select and configure your Server application
STM32_WPAN Mode and Configuration
Connectivity WBA CMX STM32WPAN.jpg


5.2. Advertising configuration

Advertising parameters are defined under BLE Advertising tab:

  • advertising configuration data are located in app_conf.h and ble_conf.h files
  • advertising elements data are located in app_ble.c file
STM32_WPAN Interface: Bluetooth® LE Advertising tab
Connectivity WBA CMX STM32WPAN ADV Configuration 14.jpg


Open Advertising Configuration and set the CFG_GAP_DEVICE_NAME to something of your liking, for example MY_APPLI.
This array is defined in app_ble.c file as :

static const char a_GapDeviceName[] = {  'M', 'y', '_', 'A', 'p', 'p', 'l', 'i' }; /* Gap Device Name */


In the generated code these parameters are defined in :
1. app_conf.h file:

#define ADV_TYPE
#define BLE_ADDR_TYPE
#define FILTER
#define ADV_LPINTERVAL_MIN
#define ADV_LPINTERVAL_MAX

2. ble_conf.h file:

#define BLE_CFG_PERIPHERAL
#define BLE_CFG_CENTRAL
STM32_WPAN Interface: Bluetooth® LE Advertising configuration
Connectivity WBA CMX STM32WPAN ADV Configuration 24.jpg


In Advertising elements, included in the advertising packet payload :

puce1.png
Turn to “yes” the elements to add in the advertising packet payload
puce2.png
Enter the value for these elements
STM32_WPAN Interface: Advertising elements
Connectivity WBA CMX STM32WPAN ADV Configuration 34.jpg


The generated code corresponding to advertising packet elements is located in app_ble.c file.

/**
 * Advertising Data
 */
uint8_t a_AdvData[25] =
{
  8, AD_TYPE_COMPLETE_LOCAL_NAME, 'p', '2', 'p', 'S', '_', 'X', 'X',  /* Complete name */
  15, AD_TYPE_MANUFACTURER_SPECIFIC_DATA, 0x30, 0x00, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */, 0x00 /*  */,
};

METTRE UN LIEN VERS MANUF / SDK V2

In this case, we will set 2 advertising data elements; local name, and a manufacturer specific field. Make sure to set the fields as you see here:
In our example, we set 2 advertising elements (Advertising packet structure’s length = 25 bytes):

  • Complete local name
  • Manufacturer specific data

The advertising information is represented by advertising data elements, which are standardized on the Bluetooth SIG.

Manufacturer specific data are updated at runtime (specific function in app_ble.c file)

Warning white.png Warning
Pay attention to not oversize the ad_data[ ] length array.

This array size is automatically calculated by STM32CubeMX and can't exceed 28 bytes


5.3. Services and characteristics definition

All created services and characteristics are managed in an associated xxx.c file (one file per service, xxx = Service short name defined in SERVICEx panel). Each Service and Characteristic are added in XXX_Init(void) function (XXX = Service short name (capitalized) defined in SERVICEx panel) using :

  • aci_gatt_add_service(…) for services
  • aci_gatt_add_char(…) for characteristics

5.3.1. BLE Applications and Services

To start the definition of the Bluetooth LE application :

puce1.png
Go to BLE Applications and Services tab,
puce2.png
Enter the number of services to define (one in our example),
puce3.png
Note : For each number of service, a tab to configure it is created.
Bluetooth® LE Applications and Services
Connectivity WBA CMX STM32WPAN Applications and Services.jpg

5.3.2. Services definition

Each created Service is defined in a dedicated tab (SERVICE 1 to 25) :

  • Up to 25 Characteristics per Service
  • UUID type can be defined as 16 or 128 bits (full or reduced)
  • UUID definition
  • Type value is Primary or Secondary Service

Once the number of service has been defined, in our example we defined one service with two characteristics, update the service information.

puce1.png
From SERVICE1 tab,
puce2.png
Set the number of characteristics and all the parameters required to define the service.
Service Definition
Connectivity WBA CMX STM32WPAN Service Definition.jpg

5.3.3. Characteristics definition

For each characteristic the following parameters must be defined

  • General
  • Properties
  • Permissions
  • GATT events

Our example defines 2 characteristics:

Characteristic 1 Characteristic 2
UUID type 128 bits UUID (0x02) 128 bits UUID (0x02)
UUID 128 Input type Reduced Reduced
UUID FE 41 FE 42
Characteristic long name My_LED_Char My_Switch_Char
Characteristic Short Name LED_C SWITCH_C
Value length 2 2
Length characteristic Variable Variable
Encryption key size 0x10 0x10
Char Properties READ WRITE_WITHOUT_RESP NOTIFY
GATT events GATT_NOTIFY_ATTRIBUTE_WRITE GATT_NOTIFY_ATTRIBUTE_WRITE



Defined as follows:

SERVICE1 characteristics definition
Connectivity WBA CMX STM32WPAN Characteristic Definition.jpg


Info white.png Information
If UUID type is 128 bits reduced, the UUID value (on 16 bits) is encapsulated in a 128 bits data thanks to COPY_xxx_UUID macro (where xxx is service or characteristic long name) to bring it in 128 bits.

For example an UUID of 0xFE41 is encapsulated as : 0x00,0x00,0xfe,0x41,0x8e,0x22,0x45,0x41,0x9d,0x4c,0x21,0xed,0xae,0x82,0xed,0x19.

If UUID type is 16bits, the UUID value is used as this to create the service or characteristic.


5.4. Application Configuration

All the Application Configuration topics are reachable when :

puce1.png
Configuration pane has been selected
puce2.png
Open and configure the Application configuration chapters
Application Configuration (1/12)
Connectivity WBA CMX STM32WPAN Application Configuration 1-12.jpg


5.4.1. Project IP's Configuration

To display Application configuration recommendations:

puce1.png
Select Configuration tab
puce2.png
Select Application configuration recommandation line
puce3.png
Click on information logo
puce4.png
Display recommendations
Application Configuration (2/12)
Connectivity WBA CMX STM32WPAN Application Configuration 2-12.jpg


5.4.2. Application Parameter

Pairing is done to support secure connection method.
All parameters defined in this chapter are located in app_conf.h file.

puce1.png
Open Application parameters
puce2.png
Turn PAIRING_PARAMETERS ON, to configure the Pairing parameters
Application Configuration (3/12)
Connectivity WBA CMX STM32WPAN Application Configuration 3-12.jpg


5.4.3. BLE Stack

puce1.png
Open Application parameters
puce2.png
Set BLE stack parameters
Application Configuration (4/12)
Connectivity WBA CMX STM32WPAN Application Configuration 4-12.jpg


5.4.4. Low Power

puce1.png
Open Low Power
puce2.png
Define Low Power parameters
Application Configuration (5/12)
Connectivity WBA CMX STM32WPAN Application Configuration 5-12.jpg


5.4.5. Traces

puce1.png
Open Traces
puce2.png
Define Traces parameters
Application Configuration (6/12)


5.4.6. Log level

puce1.png
Open Log level
puce2.png
Define Traces parameters
Application Configuration (7/12)
Connectivity WBA CMX STM32WPAN Application Configuration 7-12.jpg


5.4.7. NVM

puce1.png
Open NVM
puce2.png
Define NVM parameters
Application Configuration (8/12)
Connectivity WBA CMX STM32WPAN Application Configuration 8-12.jpg


5.4.8. RT GPIO debug

puce1.png
Open RT GPIO debug
puce2.png
Define RT GPIO debug parameters
Application Configuration (9/12)
Connectivity WBA CMX STM32WPAN Application Configuration 9-12.jpg


5.4.9. HW Radio

puce1.png
Open HW Radio
puce2.png
Define HW Radio parameters
Application Configuration (10/12)
Connectivity WBA CMX STM32WPAN Application Configuration 10-12.jpg


5.4.10. HW_RNG

puce1.png
Open HW_RNG
puce2.png
Define HW_RNG parameters
Application Configuration (11/12)
Connectivity WBA CMX STM32WPAN Application Configuration 11-12.jpg


5.4.11. Memory manager

puce1.png
Open Memory manager
puce2.png
Define Memory manager
Application Configuration (12/12)
Connectivity WBA CMX STM32WPAN Application Configuration 12-12.jpg



5.5. Platefrom Settings

BSP settings :

puce1.png
Open Platform Setting tab
puce2.png
Set Serial Link for Traces to USART : Asynchronous
puce3.png
And USART1
Platform Settings
Connectivity WBA CMX STM32WPAN Platform Settings.jpg


6. Project Configuration

All the project configuration is done on the Project Manager pane within three sections:

  • Project
  • Code generator
  • Advanced Settings
puce1.png
Select Project Manager pane
puce2.png
In Project window
puce3.png
Define the project name
puce4.png
Chose the project location
puce5.png
Select the Toolchain IDE and version
puce6.png
Define the linker settings
puce7.png
Uncheck Use Default Firmware Location
puce8.png
To define your Firmware location a voir … si pas default FW location
Project Configuration (1/4)
Connectivity WBA CMX Project Configuration 1-4.jpg


Management of files, packages and embedded software packs are done from Code Generator panel.

puce1.png
Select Code Generator pane
puce2.png
Select Add necessary files as reference in the toolchain project configuration files
puce3.png
Check :
  • Keep User Code when re-generating
  • Delete previously generated files when not re-generated
Project Configuration (2/4)
Connectivity WBA CMX Project Configuration 2-4.jpg



puce1.png
To put the functions in the desired order, select the function line
puce2.png
And use the arrows
Project Configuration (3/4)
Connectivity WBA CMX Project Configuration 3-4.jpg


In Advanced Settings panel:

  • Do Not Generate Function Call shall be unticked for all IP’s associated to STM32WPAN configurationexcepted for CRC.
  • Visibility Static shall be unticked for all IP’s associated to STM32WPAN configuration excepted for GPDMA (when activated), ADC, and SystemPower_Config.
  • Generate code shall be ticked for all functions

Then turn UART to enable in Register Callback panel:

Project Configuration (4/4)
Connectivity WBA CMX Project Configuration 4-4.jpg


7. P2P Server notifications and writes management

In order to use P2P Server Notification and Write characteristics, several points have to be configured:

  • User Button and the related Interrupt, to Notify the P2P Client
  • Blue LED, to receive a P2P Client write operation
  • Custom application code to manage B1 and write operation on P2P Server service
STM32WBA Nucleo board
Connectivity WBA CMX STM32WBA Nucleo Board.jpg


7.1. User button and LED pinout

Connectivity WBA CMX Leds Pinout.jpg
Connectivity WBA CMX Button Pinout.jpg

In the Nucleo board, LED pinout is:

  • Blue LED : PB4
  • Red LED: PB8
  • Green LED: PA9

Switch (user button) pinout is:

  • B1: PC13
  • B2: PB6
  • B3: PB7

When used:

  • Switch pins are declared as GPIO_EXTIx (x = pin number)
  • LED pins are declared as GPIO_OUTPUT

7.2. LEDs setup

For the blue LED setup, go to Pinout and Configuration window, then :

puce1.png
Click on Pinout view
puce2.png
Open PB4 configuration
puce3.png
Chose GPIO Output
Blue LED Pinout


For the red LED :

puce1.png
Open PB8 configuration
puce2.png
Chose GPIO Output
Red LED Pinout
Connectivity WBA CMX Pinout Red Led.jpg


For the green LED :

puce1.png
Open PA9 configuration
puce2.png
Chose GPIO Output
GreenLED Pinout
Connectivity WBA CMX Pinout Green Led.jpg


Once the three Leds (Blue, Green, Red) have been added, their configuration can be done :

puce1.png
From under Pinout and Configuration tab
puce2.png
Click on GPIO window
puce2.png
Select the GPIO line (PB4, PA9 or PA8)
puce3.png
Configure the GPIO line pane as:
  • GPIO output level : Low
  • GPIO mode : Output Push Pull
  • GPIO Pull-up/Pull-down : No pull-up and no pull-down
  • Maximum output speed : High
  • User Label : Blue_Led (PB4), Green_Led (PA9), or Red_Led (PB8)
LEDs Configuration
Connectivity WBA CMX Pinout LEDs Configuration.jpg


7.3. Buttons setup

For B1 setup go to Pinout and Configuration window, then :

puce1.png
Open PC13 configuration
puce2.png
Chose GPIO_EXTI13
B1 Pinout
Connectivity WBA CMX Pinout Button1.jpg


For B2 setup :

puce1.png
Open PB6 configuration
puce2.png
Chose GPIO_EXTI6
B2 Pinout
Connectivity WBA CMX Pinout Button2.jpg


For B3 setup :

puce1.png
Open PB7 configuration
puce2.png
Chose GPIO_EXTI7
B3 Pinout
Connectivity WBA CMX Pinout Button3.jpg


Once the three Buttons (B1, B2, B3) have been added, their configuration can be done:

puce1.png
From under Pinout and Configuration tab
puce2.png
Click on GPIO window
puce2.png
Select the GPIO line (PC13, PB6 or PB7)
puce3.png
Configure the GPIO line pane as:
  • Pin Privilede access : Non priviliged access
  • GPIO mode : External Interrupt Mode with Rising edge
  • GPIO Pull-up/Pull-down : Pull-up
  • User Label : B1 (PC13), B2 (PB6) or B3 (PB7)
Buttons Configuration
Connectivity WBA CMX Pinout Buttons Configuration.jpg


7.4. NVIC Configuration

Once buttons have been defined, configure NVIC:

puce1.png
Go to NVIC setting interface
puce2.png
Enable all the EXTI linex (B1, B2 and B3) needed Interrupt
puce2.png
Set the Preemption priority (set to 9 in our example)
NVIC Configuration


8. Code Generation

Once configuration is done in STM32CubeMX:

puce1.png
Code can be generated by STM32CubeMX
puce2.png
Open the project in the IDE (if not done already)
Code Generation
Connectivity WBA CMX Code Generation.jpg


Info white.png Information

It is possible to modify the default IDE in the Project Manager window, Project pan, and then Toolchain / IDE.

9. Code modification: User sections

Once your Buttons and LEDs GPIOs are correctly setup, generate your project by following the steps described in Code Generation chapter.

The generated source code contains several sections called User Sections where users can add custom application code parts.
These sections are not erased/modified at project regeneration from STM32CubeMX.

In order to manage notify and write operation on P2P Server service, some code parts have to be added in User Sections of the following files and their respective header files:

Files to update
Connectivity WBA CMX Files to Update.jpg


  • In app_conf.h:

From app_conf.h, define the tasks for buttons, notifications and adv by adding code in CFG_Task_Id_t User Code Section:

typedef enum
{
  CFG_TASK_HCI_ASYNCH_EVT_ID,
  CFG_TASK_LINK_LAYER,
  CFG_TASK_LINK_LAYER_TEMP_MEAS,
  CFG_TASK_BLE_HOST,
  CFG_TASK_BPKA,
  CFG_TASK_HW_RNG,
  CFG_TASK_AMM_BCKGND,
  CFG_TASK_FLASH_MANAGER_BCKGND,
  CFG_TASK_BLE_TIMER_BCKGND,
  /* USER CODE BEGIN CFG_Task_Id_t */
  TASK_BUTTON_1,
  TASK_BUTTON_2,
  TASK_BUTTON_3,
  CFG_TASK_ADV_CANCEL_ID,
  CFG_TASK_SEND_NOTIF_ID,
  /* USER CODE END CFG_Task_Id_t */
  CFG_TASK_NBR /* Shall be LAST in the list */
} CFG_Task_Id_t;

Update also USER CODE Defines to support LED, Button and Debug :

/* USER CODE BEGIN Defines */
/**
 * User interaction
 * When CFG_LED_SUPPORTED is set, LEDS are activated if requested
 * When CFG_BUTTON_SUPPORTED is set, the push button are activated if requested
 * When CFG_DBG_SUPPORTED is set, the debugger is activated
 */

#define CFG_LED_SUPPORTED                       (1)
#define CFG_BUTTON_SUPPORTED                    (1)
#define CFG_DBG_SUPPORTED                       (1)

/**
 * If CFG_FULL_LOW_POWER is requested, make sure LED and debugger are disabled
 */
#if (CFG_FULL_LOW_POWER == 1)
  #undef  CFG_LED_SUPPORTED
  #define CFG_LED_SUPPORTED      (0)
  #undef  CFG_DBG_SUPPORTED
  #define CFG_DBG_SUPPORTED      (0)
#endif /* CFG_FULL_LOW_POWER */

/**
 * Timeout for advertising
 */
#define ADV_TIMEOUT_MS         (60*1000) /**< 60s */
/* USER CODE END Defines */


  • In main.c:
  /* USER CODE BEGIN ICACHE_Init 1 */
  /* No retention for ICACHE in stop mode */
  LL_PWR_SetICacheRAMStopRetention(LL_PWR_ICACHERAM_STOP_NO_RETENTION);
  /* USER CODE END ICACHE_Init 1 */
  /* USER CODE BEGIN RNG_Init 0 */
  memset(&hrng, 0, sizeof(hrng));
  /* USER CODE END RNG_Init 0 */
  /* USER CODE BEGIN RNG_Init 2 */
  /* Disable RNG peripheral and its RCC clock */
  HW_RNG_Disable( );
  /* USER CODE END RNG_Init 2 */
/* USER CODE BEGIN MX_GPIO_Init_2 */
#if (CFG_DBG_SUPPORTED == 0)
  GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Pin = GPIO_PIN_14|GPIO_PIN_15|GPIO_PIN_13;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
  
  GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_4;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
#endif
/* USER CODE END MX_GPIO_Init_2 */
/* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  Error_Handler();
/* USER CODE END 6 */
  • In stm32wbaxx_it.c:
/* USER CODE BEGIN Includes */
#include "stm32wbaxx_nucleo.h"
/* USER CODE END Includes */
/* USER CODE BEGIN EXTI6_IRQn 1 */
BSP_PB_IRQHandler(B2);
/* USER CODE END EXTI6_IRQn 1 */
/* USER CODE BEGIN EXTI7_IRQn 1 */
BSP_PB_IRQHandler(B3);
/* USER CODE END EXTI7_IRQn 1 */
/* USER CODE BEGIN EXTI13_IRQn 1 */
BSP_PB_IRQHandler(B1);
/* USER CODE END EXTI13_IRQn 1 */


  • In app_entry.c:
/* USER CODE BEGIN Includes */
#include "stm32wbaxx_nucleo.h"
/* USER CODE END Includes */
/* USER CODE BEGIN PFP */
#if (CFG_LED_SUPPORTED == 1)
static void Led_Init(void);
#endif
#if (CFG_BUTTON_SUPPORTED == 1)
static void Button_Init(void);
#endif
/* USER CODE END PFP */
/* USER CODE BEGIN APPE_Init_1 */
#if (CFG_LED_SUPPORTED == 1)
  Led_Init();
#endif
#if (CFG_BUTTON_SUPPORTED == 1)
  Button_Init();
#endif
/* USER CODE END APPE_Init_1 */
/* USER CODE BEGIN APPE_Init_2 */
 #if (CFG_BUTTON_SUPPORTED == 1)
  /* Register Button Tasks */
  UTIL_SEQ_RegTask(1U << CFG_TASK_PB1_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, APP_BLE_Key_Button1_Action);
  UTIL_SEQ_RegTask(1U << CFG_TASK_PB2_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, APP_BLE_Key_Button2_Action);
  UTIL_SEQ_RegTask(1U << CFG_TASK_PB3_BUTTON_PUSHED_ID, UTIL_SEQ_RFU, APP_BLE_Key_Button3_Action);
#endif
 /* USER CODE END APPE_Init_2 */
/* USER CODE BEGIN FD_LOCAL_FUNCTIONS */
#if (CFG_LED_SUPPORTED == 1)
static void Led_Init( void )
{
  /* Leds Initialization */
  BSP_LED_Init(LED_BLUE);
  BSP_LED_Init(LED_GREEN);
  BSP_LED_Init(LED_RED);
 
  BSP_LED_On(LED_GREEN);
 
  return;
}
#endif

#if (CFG_BUTTON_SUPPORTED == 1)
static void Button_Init( void )
{
  /* Button Initialization */
  BSP_PB_Init(B1, BUTTON_MODE_EXTI);
  BSP_PB_Init(B2, BUTTON_MODE_EXTI);
  BSP_PB_Init(B3, BUTTON_MODE_EXTI);
 
  return;
}
#endif
/* USER CODE END FD_LOCAL_FUNCTIONS */
/* USER CODE BEGIN FD_WRAP_FUNCTIONS */
void BSP_PB_Callback(Button_TypeDef Button)
{
  switch (Button)
  {
    case B1:
      UTIL_SEQ_SetTask(1U << CFG_TASK_PB1_BUTTON_PUSHED_ID, CFG_SEQ_PRIO_0);
      break;
    case B2:
 UTIL_SEQ_SetTask(1U << CFG_TASK_PB2_BUTTON_PUSHED_ID, CFG_SEQ_PRIO_0);
      break;
 case B3:
      UTIL_SEQ_SetTask(1U << CFG_TASK_PB3_BUTTON_PUSHED_ID, CFG_SEQ_PRIO_0);
      break;
    default:
      break;
  }

  return;
}

void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == B1_PIN)
  {
    BSP_PB_Callback(B1);
  }
  if (GPIO_Pin == B2_PIN)
  {
    BSP_PB_Callback(B2);
  }
  if (GPIO_Pin == B3_PIN)
  {
    BSP_PB_Callback(B3);
  }
 
  return;
}
 
void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
  HAL_GPIO_EXTI_Rising_Callback(GPIO_Pin);
}
/* USER CODE END FD_WRAP_FUNCTIONS */
  • In app_ble.h:

From app_ble.h, declare button action functions, in EF User Code Section:

/* USER CODE BEGIN EF */
void APP_BLE_Key_Button1_Action(void);
void APP_BLE_Key_Button2_Action(void);
void APP_BLE_Key_Button3_Action(void);
 /* USER CODE END EF */


  • In app_ble.c:
/* USER CODE BEGIN Includes */
#include "stm32wbaxx_nucleo.h"
/* USER CODE END Includes */
/* USER CODE BEGIN PTD_1*/
/* Advertising timeout timerID*/
UTIL_TIMER_Object_t Advertising_mgr_timer_Id;
/* Led Timeout timerID */
UTIL_TIMER_Object_t SwitchOffGPIO_timer_Id;
 
uint8_t connIntervalFlag;
/* USER CODE END PTD_1 */
/* USER CODE BEGIN PD */
#define LED_ON_TIMEOUT                 (5)
/* USER CODE END PD */
/* USER CODE BEGIN PFP */
static void Adv_Cancel_Req(void *arg);
static void Adv_Cancel(void);
static void Switch_OFF_GPIO(void *arg);
static void fill_advData(uint8_t *p_adv_data, uint8_t tab_size, const uint8_t*p_bd_addr);
/* USER CODE END PFP */
/* USER CODE BEGIN APP_BLE_Init_1 */
tBleStatus ret = BLE_STATUS_INVALID_PARAMS;
/* USER CODE END APP_BLE_Init_1 */
/* USER CODE BEGIN APP_BLE_Init_4 */
UTIL_SEQ_RegTask(1<<CFG_TASK_ADV_CANCEL_ID, UTIL_SEQ_RFU, Adv_Cancel);
 
/* Create timer to handle the Advertising Stop */
UTIL_TIMER_Create(&(bleAppContext.Advertising_mgr_timer_Id),
                                  0,
                                  (UTIL_TIMER_Mode_t)hw_ts_SingleShot,
                                  &Adv_Cancel_Req,
                                  0);
/* Create timer to handle the Led Switch OFF */
UTIL_TIMER_Create(&(bleAppContext.SwitchOffGPIO_timer_Id),
                                  0,
                                  (UTIL_TIMER_Mode_t)hw_ts_SingleShot,
                                  &Switch_OFF_GPIO,
                                  0);
 /* USER CODE END APP_BLE_Init_4 */
/* USER CODE BEGIN APP_BLE_Init_3 */
ret = aci_hal_set_radio_activity_mask(0x0006);
if (ret != BLE_STATUS_SUCCESS)
{
  APP_DBG_MSG("  Fail   : aci_hal_set_radio_activity_mask command, result: 0x%2X\n", ret);
}
else
{
  APP_DBG_MSG("  Success: aci_hal_set_radio_activity_mask command\n\r");
}

/* Start to Advertise to accept a connection */
APP_BLE_Procedure_Gap_Peripheral(PROC_GAP_PERIPH_ADVERTISE_START_FAST);
 
/* Start a timer to stop advertising after a while */
UTIL_TIMER_StartWithPeriod(&bleAppContext.Advertising_mgr_timer_Id, INITIAL_ADV_TIMEOUT);
/* USER CODE END APP_BLE_Init_3 */
/* USER CODE BEGIN APP_BLE_Init_2 */
bleAppContext.connIntervalFlag = 0;
/* USER CODE END APP_BLE_Init_2 */
/* USER CODE BEGIN EVT_DISCONN_COMPLETE */
APP_BLE_Procedure_Gap_Peripheral(PROC_GAP_PERIPH_ADVERTISE_START_FAST);
UTIL_TIMER_StartWithPeriod(&bleAppContext.Advertising_mgr_timer_Id, INITIAL_ADV_TIMEOUT);
/* USER CODE END EVT_DISCONN_COMPLETE */
/* USER CODE BEGIN HCI_EVT_LE_ENHANCED_CONN_COMPLETE */
/* The connection is done, there is no need anymore to schedule the LP ADV */
UTIL_TIMER_Stop(&(bleAppContext.Advertising_mgr_timer_Id));
/* USER CODE END HCI_EVT_LE_ENHANCED_CONN_COMPLETE */
/* USER CODE BEGIN HCI_EVT_LE_CONN_COMPLETE */
/* The connection is done, there is no need anymore to schedule the LP ADV */
UTIL_TIMER_Stop(&(bleAppContext.Advertising_mgr_timer_Id));
/* USER CODE END HCI_EVT_LE_CONN_COMPLETE */
/* USER CODE BEGIN RADIO_ACTIVITY_EVENT*/
BSP_LED_On(LED_GREEN);
UTIL_TIMER_StartWithPeriod(&bleAppContext.SwitchOffGPIO_timer_Id, LED_ON_TIMEOUT);
/* USER CODE END RADIO_ACTIVITY_EVENT*/
/* USER CODE BEGIN CONN_PARAM_UPDATE */
if (bleAppContext.connIntervalFlag != 0)
{
  bleAppContext.connIntervalFlag = 0;
  paramA = CONN_INT_MS(50);
  paramB = CONN_INT_MS(50);
}
else
{
  bleAppContext.connIntervalFlag = 1;
  paramA = CONN_INT_MS(1000);
  paramB = CONN_INT_MS(1000);
}
/* USER CODE END CONN_PARAM_UPDATE */
/* USER CODE BEGIN FD*/
void APP_BLE_Key_Button1_Action(void)
{
  if (bleAppContext.Device_Connection_Status == APP_BLE_IDLE)
  {
    /* Relaunch advertising */
    APP_BLE_Procedure_Gap_Peripheral(PROC_GAP_PERIPH_ADVERTISE_START_FAST);
    UTIL_TIMER_StartWithPeriod(&bleAppContext.Advertising_mgr_timer_Id, INITIAL_ADV_TIMEOUT);
  }
  else
  {
    UTIL_SEQ_SetTask( 1<<CFG_TASK_SEND_NOTIF_ID, CFG_SCH_PRIO_0);
  }
  return;
}

void APP_BLE_Key_Button2_Action(void)
{
  tBleStatus ret = BLE_STATUS_INVALID_PARAMS;
  
  if (bleAppContext.Device_Connection_Status != APP_BLE_CONNECTED_SERVER)
  {
    ret = aci_gap_clear_security_db();
    if (ret != BLE_STATUS_SUCCESS)
    {
      APP_DBG_MSG("==>> aci_gap_clear_security_db - Fail, result: 0x%02X\n", ret);
    }
    else
    {
      APP_DBG_MSG("==>> aci_gap_clear_security_db - Success\n");
    }
  }
  else
  {
    /* Launch advertising for multi connection */
    APP_BLE_Procedure_Gap_Peripheral(PROC_GAP_PERIPH_ADVERTISE_START_FAST);
    UTIL_TIMER_StartWithPeriod(&bleAppContext.Advertising_mgr_timer_Id, INITIAL_ADV_TIMEOUT);
  }
 
  return;
}

void APP_BLE_Key_Button3_Action(void)
{
  if (bleAppContext.Device_Connection_Status != APP_BLE_CONNECTED_SERVER)
  {
 
  }
  else
  {
    APP_BLE_Procedure_Gap_Peripheral(PROC_GAP_PERIPH_CONN_PARAM_UPDATE);
  }
 
  return;
}
/* USER CODE END FD*/
  /* USER CODE BEGIN Ble_Hci_Gap_Gatt_Init_1*/
  fill_advData(&a_AdvData[0], sizeof(a_AdvData), p_bd_addr);
  /* USER CODE END Ble_Hci_Gap_Gatt_Init_1*/
/* USER CODE BEGIN FD_LOCAL_FUNCTION */
static void Adv_Cancel_Req(void *arg)
{
  UTIL_SEQ_SetTask(1 << CFG_TASK_ADV_CANCEL_ID, CFG_SCH_PRIO_0);
  return;
}
 
static void Switch_OFF_GPIO(void *arg)
{
  BSP_LED_Off(LED_GREEN);
  return;
}
 
static void Adv_Cancel(void)
{
  BSP_LED_Off(LED_GREEN);
 
  APP_BLE_Procedure_Gap_Peripheral(PROC_GAP_PERIPH_ADVERTISE_STOP);
  bleAppContext.Device_Connection_Status = APP_BLE_IDLE;
 
  return;
}

static void fill_advData(uint8_t *p_adv_data, uint8_t tab_size, const uint8_t* p_bd_addr)
{
  uint16_t i =0;
  uint8_t bd_addr_1, bd_addr_0;
  uint8_t ad_length, ad_type;  
  
  while(i < tab_size)
  {
    ad_length = p_adv_data[i];
    ad_type = p_adv_data[i + 1];
      
    switch (ad_type)
    {
    case AD_TYPE_FLAGS:
      break;
    case AD_TYPE_TX_POWER_LEVEL:
      break;
    case AD_TYPE_COMPLETE_LOCAL_NAME:
      {
        if((p_adv_data[i + ad_length] == 'X') && (p_adv_data[i + ad_length - 1] == 'X'))
        {
          bd_addr_1 = ((p_bd_addr[0] & 0xF0)>>4);
          bd_addr_0 = (p_bd_addr[0] & 0xF);
          /* Convert hex value into ascii */
          if(bd_addr_1 > 0x09)
          {
            p_adv_data[i + ad_length - 1] = bd_addr_1 + '7';
          }
          else
          {
            p_adv_data[i + ad_length - 1] = bd_addr_1 + '0';
          }
          
          if(bd_addr_0 > 0x09)
          {
            p_adv_data[i + ad_length] = bd_addr_0 + '7';
          }
          else
          {
            p_adv_data[i + ad_length] = bd_addr_0 + '0';
          }
        }
        break;
      }
    case AD_TYPE_MANUFACTURER_SPECIFIC_DATA:
      {
        p_adv_data[i+2] = 0x30;
        p_adv_data[i+3] = 0x00;
        p_adv_data[i+4] = 0x02; /* blueST SDK version */
        p_adv_data[i+5] = 0x8B; /* Board ID */
        p_adv_data[i+6] = 0x83; /* FW ID */
        p_adv_data[i+7] = 0x00; /* FW data 1 */
        p_adv_data[i+8] = 0x00; /* FW data 2 */
        p_adv_data[i+9] = 0x00; /* FW data 3 */
        p_adv_data[i+10] = p_bd_addr[5]; /* MSB BD address */
        p_adv_data[i+11] = p_bd_addr[4];
        p_adv_data[i+12] = p_bd_addr[3];
        p_adv_data[i+13] = p_bd_addr[2];
        p_adv_data[i+14] = p_bd_addr[1];
        p_adv_data[i+15] = p_bd_addr[0]; /* LSB BD address */
        break;
      }
    default:
      break;
    }
    i += ad_length + 1; /* increment the iterator to go on next element*/
  }
}
/* USER CODE END FD_LOCAL_FUNCTION */
  • In p2p_server.c:
/* USER CODE BEGIN Service1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
APP_DBG_MSG("-- GATT : LED CONFIGURATION RECEIVED\n");
notification.DataTransfered.Length = p_attribute_modified->Attr_Data_Length;
notification.DataTransfered.p_Payload = p_attribute_modified->Attr_Data;
/* USER CODE END Service1_Char_1_ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE */
/* USER CODE BEGIN BLECORE_EVT */
/* Manage ACI_GATT_INDICATION_VSEVT_CODE occurring on Android 12 */   
case ACI_GATT_INDICATION_VSEVT_CODE:
{
  tBleStatus status = BLE_STATUS_FAILED;
  aci_gatt_indication_event_rp0 *pr = (void*)p_blecore_evt->data;
  status = aci_gatt_confirm_indication(pr->Connection_Handle);
  if (status != BLE_STATUS_SUCCESS)
  {
    APP_DBG_MSG("  Fail   : aci_gatt_confirm_indication command, result: 0x%x \n", status);
  }
  else
  {
    APP_DBG_MSG("  Success: aci_gatt_confirm_indication command\n");
  }   
}
  break; /* end ACI_GATT_NOTIFICATION_VSEVT_CODE */
/* USER CODE END BLECORE_EVT */


  • In p2p_server_app.c:
/* USER CODE BEGIN Includes */
#include "stm32wbaxx_nucleo.h"
/* USER CODE END Includes */
/* USER CODE BEGIN PTD */
typedef struct{
  uint8_t             Device_Led_Selection;
  uint8_t             Led1;
}P2P_LedCharValue_t;
 
typedef struct{
  uint8_t             Device_Button_Selection;
  uint8_t             ButtonStatus;
}P2P_ButtonCharValue_t;
/* USER CODE END PTD */
/* USER CODE BEGIN Service1_APP_Context_t */
P2P_LedCharValue_t              LedControl;
P2P_ButtonCharValue_t          ButtonControl;
/* USER CODE END Service1_APP_Context_t */
/* USER CODE BEGIN PFP */
static void P2P_SERVER_APP_LED_BUTTON_context_Init(void);
/* USER CODE END PFP */
/* USER CODE BEGIN Service1Char1_WRITE_NO_RESP_EVT */
if(p_Notification->DataTransfered.p_Payload[1] == 0x01)
{
  BSP_LED_On(LED_BLUE);
  APP_DBG_MSG("-- P2P APPLICATION SERVER : LED1 ON\n"); 
  P2P_SERVER_APP_Context.LedControl.Led1 = 0x01; /* LED1 ON */
}
if(p_Notification->DataTransfered.p_Payload[1] == 0x00)
{
  BSP_LED_Off(LED_BLUE);
  APP_DBG_MSG("-- P2P APPLICATION SERVER : LED1 OFF\n"); 
  P2P_SERVER_APP_Context.LedControl.Led1 = 0x00; /* LED1 OFF */
}
/* USER CODE END Service1Char1_WRITE_NO_RESP_EVT */
/* USER CODE BEGIN Service1Char2_NOTIFY_ENABLED_EVT */
P2P_SERVER_APP_Context.Switch_c_Notification_Status = Switch_c_NOTIFICATION_ON;
APP_DBG_MSG("-- P2P APPLICATION SERVER : NOTIFICATION ENABLED\n"); 
APP_DBG_MSG(" \n\r");
/* USER CODE END Service1Char2_NOTIFY_ENABLED_EVT */
/* USER CODE BEGIN Service1Char2_NOTIFY_DISABLED_EVT */
P2P_SERVER_APP_Context.Switch_c_Notification_Status = Switch_c_NOTIFICATION_OFF;
APP_DBG_MSG("-- P2P APPLICATION SERVER : NOTIFICATION DISABLED\n"); 
APP_DBG_MSG(" \n\r");
/* USER CODE END Service1Char2_NOTIFY_DISABLED_EVT */
/* USER CODE BEGIN Service1_APP_DISCON_HANDLE_EVT */
P2P_SERVER_APP_LED_BUTTON_context_Init();
/* USER CODE END Service1_APP_DISCON_HANDLE_EVT */
/* USER CODE BEGIN Service1_APP_Init */
UTIL_SEQ_RegTask( 1U << CFG_TASK_SEND_NOTIF_ID, UTIL_SEQ_RFU, P2P_SERVER_Switch_c_SendNotification);
 
/**
 * Initialize LedButton Service
 */
P2P_SERVER_APP_Context.Switch_c_Notification_Status= Switch_c_NOTIFICATION_OFF;
P2P_SERVER_APP_LED_BUTTON_context_Init();
/* USER CODE END Service1_APP_Init */
/* USER CODE BEGIN FD */
void P2P_SERVER_APP_LED_BUTTON_context_Init(void)
{  
  BSP_LED_Off(LED_BLUE);
  P2P_SERVER_APP_Context.LedControl.Device_Led_Selection=0x01;   /* Device1 */
  P2P_SERVER_APP_Context.LedControl.Led1=0x00; /* led OFF */
  P2P_SERVER_APP_Context.ButtonControl.Device_Button_Selection=0x01;/* Device1 */
  P2P_SERVER_APP_Context.ButtonControl.ButtonStatus=0x00;
 
  return;
}
/* USER CODE END FD */
/* USER CODE BEGIN Service1Char2_NS_1*/
if(P2P_SERVER_APP_Context.ButtonControl.ButtonStatus == 0x00)
{
  P2P_SERVER_APP_Context.ButtonControl.ButtonStatus = 0x01;
} 
else
{
  P2P_SERVER_APP_Context.ButtonControl.ButtonStatus = 0x00;
}
a_P2P_SERVER_UpdateCharData[0] = 0x01; /* Device Led selection */
a_P2P_SERVER_UpdateCharData[1] = P2P_SERVER_APP_Context.ButtonControl.ButtonStatus;
/* Update notification data length */
p2p_server_notification_data.Length = (p2p_server_notification_data.Length) + 2; 
  
if(P2P_SERVER_APP_Context.Switch_c_Notification_Status == Switch_c_NOTIFICATION_ON)
{ 
  APP_DBG_MSG("-- P2P APPLICATION SERVER : INFORM CLIENT BUTTON 1 PUSHED\n");
  notification_on_off = Switch_c_NOTIFICATION_ON;
} 
else
{
  APP_DBG_MSG("-- P2P APPLICATION SERVER : CAN'T INFORM CLIENT - NOTIFICATION DISABLED\n"); 
}
/* USER CODE END Service1Char2_NS_1*/

10. Inserting external files

To complete the creation of our p2pServer project we will now add the following external BSP files:

  • stm32wbaxx_nucleo.c
  • stm32wbaxx_nucleo.h

You can download all BSP STM32WBAXX-NUCLEO Component here.
Those file provide a set of firmware functions to manage the LEDs and push buttons available on the STM32WBAxx-Nucleo kit.

To add external files, we recommend using the .extSettings file. However it is also possible to add them manually as described later.

10.1. Adding files using .extSettings

The .extsettings file allows you to add additional settings witch can be used when external tools call STM32CubeMX to generate the project and require specific project settings.

.extSettings file
Connectivity WBA CMX extSettings file.jpg


Your .extSettings file should be constituted as followed:

[ProjectFiles]
HeaderPath=..\Core\Inc\
[Others]

[Groups]
Drivers/BSP/STM32WBAxx_Nucleo = ../Core/Src/stm32wbaxx_nucleo.c;

In our case, the HearderPath indicate where stm32wbaxx_nucleo.h file is in your project. Then under Groups you need to specify where you want the code file to appear in your workspace, and where it is stored.

Now you can click Generate again in STM32CubeMX.
Here is how your space should look like now:

Connectivity WBA CMX Workspace.jpg

10.2. Adding files manually

The steps below were made with the IAR IDE.

To include manually the BSP code file :

puce1.png
In Workspace, right click on the "Drivers" folder
puce2.png
Go on Add
puce3.png
Click on Add Group...
Adding stm32wbaxx_nucleo.c


To specify manually the header path :

puce1.png
Right click on your project
puce2.png
Click on Options
Adding stm32wbaxx_nucleo.h (1/4)
puce1.png
Click on C/C++ Compiler
puce2.png
Click on the Preprocessor section
puce2.png
Click on : …
Adding stm32wbaxx_nucleo.h (2/4)
puce1.png
Click on Click to Add
puce2.png
Choose the folder containing the stm32wbaxx_nucleo.h file.
Adding stm32wbaxx_nucleo.h (3/4)
puce1.png
Click on the down arrow
puce2.png
Choose the second option to use relative path
Adding stm32wbaxx_nucleo.h (4/4)



You have just finished creating a p2pServer application with STM32CubeMX starting from the STM32WBA52CGU6 ship.

You can find more information about Peer 2 Peer Applications on: Connectivity:STM32WBA_Peer_To_Peer

11. References