Coming soon |
1. Peer to Peer Profile
The Peer to Peer Profile is a Generic Attribute Profile (GATT) based low-energy profile defined by STMicroelectronics with proprietary UUIDs(128 bits).
The Peer to Peer Profile, widely used for direct connection, defines the communication between a GATT-server of a Peer to Peer Server device, and a GATT-client Collector device, such as a smartphone, STM32WBA Peer to Peer Client or Peer to Peer Router devices.
- The Peer to Peer Server
-
- Contains the P2P Service, which expose two characteristics (Notification & Write) in order to create a bi-direction data communication.
- Is the GATT server
- The Collector
-
- Accesses the information exposed by Peer to Peer Server, controls it with the Write characteristics, receives Notification from it.
- Is the GATT client
This wiki page is the description of the Peer to Peer Server and Peer to Peer Client projects provided within the STM32CubeWBA MCU Package[1]
Follow this "link" for Peer to Peer Router project explanation.
Bluetooth® LE Peer to Peer Profile & STM32WBA |
---|
1.1. STM32WBA Peer to Peer Server application
The table below describes the structure of Peer to Peer service:
Bluetooth® LE Peer to Peer Service specification | ||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Peer To Peer Server is exported as a Service
- LED characteristic:
- Used to control LED1 (Blue) on STM32WBA platform by remote device .
Peer to Peer Service - LED Characteristic | |||||||||
---|---|---|---|---|---|---|---|---|---|
|
- SWITCH Characteristic:
- Used to switch LED or Lamp on Collector device.
Peer to Peer Service - SWITCH Characteristic | |||||||||
---|---|---|---|---|---|---|---|---|---|
|
Example of flow diagram between STM32WBA & ST BLE Toolbox |
---|
1.2. Advertising data
At start up, Peer To Peer Server application starts Advertising.
Data advertised are composed as follow:
P2P Server Advertising packet | ||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manufacturer data are encoded following STMicroelectronics BlueST SDK v2 as described below:
STMicroelectronics Manufacturer Advertising data | |||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
1.3. STM32WBA Peer to Peer Client application
It acts as a Central device with the support of GATT Client Layer.
At start up, by pressing B1 button, Peer To Peer Client application:
- Starts scanning to detect Peer To Peer Sever application by filtering the Firmware ID of the STMicroelectronics Manufacturer advertising data
- Stops Scanning once P2P server detected
- Connects to the P2P Server to establish the connection.
- Discovers GATT Service & Characteristics of the P2P server
- Enable all GATT server notification characteristics
Once connected, the Peer To Peer Client application:
- By pressing B1 button, write a message to toggle the Blue LED of the P2P Server
- Receive notification to toggle the on board Blue LED from remote P2P Server Application.
Example of flow diagram between STM32WBA P2P Server & P2P Client |
---|
1.4. On board buttons configuration
P2P Applications Nucleo-WBA buttons configuration | ||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
2. Requirements
2.1. Software and system requirements
The software required are the following (minimum IDEs version):
- IAR Embedded Workbench for ARM (EWARM) toolchain V9.20.1, plus a patch available in WBA Firmware Package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/EWARMv8_STM32WBAx_V1.2.zip
- RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.37, plus a patch available in WBA Firmware package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/Keil.STM32WBAx_DFP.1.0.0.zip
- STM32CubeIDE toolchain V1.12.0 [2].
Programmer:
- STM32CubeProgrammer[3] : To flash the board with an already generated binary
2.2. Hardware requirements
NUCLEO-WBA5 [4] is necessary to install the application.
Hardware platform illustration |
---|
|
2.3. Collector applications compatible
The STM32CubeWBA Health Thermometer Sensor project is compatible with the following collector:
3. STM32WBA P2P Server & P2P Client examples description
3.1. Project directory
The "BLE_p2pServer" & "BLE_p2pClient"applications are available by downloading STM32CubeWBA MCU Package[5].
Refer to How to Build a BLE Project wiki page for project directory information.
3.2. Project description
3.2.1. Structure
Software project structure with the most important parts:
P2P Server / Client project structure |
---|
WARNING: Do not modify the files in Middlewares folder |
3.2.2. Application initialization
The different steps of the application initialization are described below:
P2P Server project initialization |
---|
P2P Client project initialization |
3.2.3. GAP and GATT initialization and interaction
P2P Server:
and The Bluetooth LE P2P Server application initialization is done within app_ble.c
- Initialize the BLE stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init()
- Call the services controller initialization SVCCTL_Init() - svc_ctl.c
- Manage the GAP event - SVCCTL_App_Notification() - svc_ctl.c
- HCI_LE_CONNECTION_COMPLETE - provides information of the connection interval, slave latency, supervision timeout
- HCI_LE_CONNECTION_UPDATE_COMPLETE- provides the new information of the connection
- HCI_DISCONNECTION_COMPLETE - informs the application about the link disconnection and the reason
The Services management is done by the service controller, svc_ctl.c
- Initialize the number of registered handler - SVCCTL_Init()
- Manage events - SVCCTL_UserEvtRx()- from the BLE Host Stack and redirect them to the gap event handler - SVCCTL_App_Notification()
The application level of the P2P Server is done with p2p_server_app.c:
- Initialization of the services:
- P2P Server Service - P2P_SERVER_Init() - p2p_server.c
- Initialization of the context of the application
- Receive notification from the P2P Server Service - P2P_SERVER_Notification()
- When P2P_SERVER_LED_C_WRITE_NO_RESP_EVT event is received from the P2P Client, the blue LED is toggled.
- P2P_SERVER_Switch_c_SendNotification() function is called on Button B1 press, to notify the P2P Client:
- P2P_SERVER_UpdateValue() is called with the notification data - p2p_server.c
The Custom P2P Server Service p2p_server.c manages the specification of the service:
- Service Init - P2P_SERVER_Init()
- Register P2P Server Event Handle to Service Controller - SVCCTL_RegisterSvcHandler();
- Initialize Service UUID – add P2P Server service as Primary services
- Initialize LED_C characteristic
- Initialize SWITCH_C characteristic
- Manage the GATT event from BLE Stack - P2P_SERVER_EventHandler()
- ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
- Reception of an attribute modification - LED C Value : ON or OFF Indication
- Notify application of the Measurement Notification - P2P_SERVER_Notification(P2P_SERVER_LED_C_WRITE_NO_RESP_EVT)
- Reception of an attribute modification - LED C Value : ON or OFF Indication
- ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
P2P Server software module interaction |
---|
P2P Client:
and The Bluetooth LE P2P Client application initialization is done within app_ble.c
- Initialize the BLE stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init()
- Call the services controller initialization SVCCTL_Init() - svc_ctl.c
- Manage the GAP event - SVCCTL_App_Notification() - svc_ctl.c
- HCI_LE_CONNECTION_COMPLETE - provides information of the connection interval, slave latency, supervision timeout
- HCI_LE_CONNECTION_UPDATE_COMPLETE- provides the new information of the connection
- HCI_DISCONNECTION_COMPLETE - informs the application about the link disconnection and the reason
The Services management is done by the service controller, svc_ctl.c
- Initialize the number of registered handler - SVCCTL_Init()
- Manage events - SVCCTL_UserEvtRx()- from the BLE Host Stack and redirect them to the gap event handler - SVCCTL_App_Notification()
The application level of the P2P Client is done with gatt_client_app.c:
- Initialization of the application context
- Register Event Handler to BLE Controller - SVCCTL_RegisterCltHandler();
- Initialize LED data level and selection
- Manage the GATT event from BLE Stack - gatt_parse_notification()
- ACI_GATT_NOTIFICATION_VSEVT_CODE
- When the notification event is received from the P2P Server, the blue LED is toggled - gatt_Notification()
- ACI_GATT_NOTIFICATION_VSEVT_CODE
- Write characteristic to P2P Server (LED toggling) - P2Pclient_write_char() - by pressing Button B1 while connected.
P2P Client software module interaction |
---|
3.3. How to use
P2P Server VS Smartphone
Once the BLE P2P Server application is installed on the STM32WBA platform, launch ST BLE ToolBox smartphone application.
Then, scan and connect the device called p2pS_XX (where XX is replaced by the last byte of the BD address) to the application.
Once the Bluetooth® LE connection is established and the notification enabled by the smartphone (by clicking on P2P Server icon):
- LED_C value can be modified by clicking on the LED button on smartphone interface, the blue LED of the Nucleo board is switched On/Off accordingly.
- Pressing Button B1 on the board while connected send a SWITCH_C notification to the smartphone and the switch level is updated on the smartphone interface.
P2P Server VS P2P Client
At least two nucleo platforms are required, one flashed with the BLE P2P Server application and one with the BLE P2P Client application.
- On P2P Client side:
- Pressing Button B1 on P2P Client platform while not connected, start a scan procedure, and connection is done if a P2P Server platform is found.
- Pressing Button B1 on P2P Client platform while connected, send a GATT event to the P2P Server platform in order to switch On/Off server blue LED.
- On P2P Server side:
- Pressing Button B1 on P2P Server side while connected send a SWITCH_C notification to the P2P Client platform and toggle the blue LED on client side.
- Pressing Button B2 on P2P Server side while connected, start a new advertising in order to illustrate multi link feature.
- Pressing Button B2 on P2P Server side while not connected, clear the security DataBase of the platform.
3.4. UART debug trace
Thanks to the debug log via UART interface LINK TO UPDATE?, it is possible to trace the application project.
To enable the traces within the project, enable them within app_conf.h as described below:
/**
* Enable or Disable traces in application
*/
#define CFG_DEBUG_APP_TRACE (1)
P2P Server - Initialization phase | P2P Server - Connected Phase and LED On notification |
---|---|
==>> Start Ble_Hci_Gap_Gatt_Init function Success: hci_reset command Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET Public Bluetooth Address: 00:80:e1:2a:7c:ea Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET Success: aci_hal_set_tx_power_level command Success: aci_gatt_init command Success: aci_gap_init command Success: aci_gatt_update_char_value - Device Name Success: aci_gatt_update_char_value - Appearance Success: hci_le_set_default_phy command Success: aci_gap_set_io_capability command Success: aci_gap_set_authentication_requirement command Success: aci_gap_configure_whitelist command ==>> End Ble_Hci_Gap_Gatt_Init function Services and Characteristics creation Success: aci_gatt_add_service command: P2P_Server Success: aci_gatt_add_char command : LED_C Success: aci_gatt_add_char command : SWITCH_C End of Services and Characteristics creation Success: aci_hal_set_radio_activity_mask command ==>> aci_gap_set_discoverable - Success ==>> Success: Start Advertising |
>>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x0001 - Connection established with @:7d:64:80:ff:2e:4f - Connection Interval: 48.75 ms - Connection latency: 0 - Supervision Timeout: 5000 ms >>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - Connection Interval: 7.50 ms - Connection latency: 0 - Supervision Timeout: 5000 ms >>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - Connection Interval: 48.75 ms - Connection latency: 0 - Supervision Timeout: 5000 ms -- P2P APPLICATION SERVER : NOTIFICATION ENABLED -- GATT : LED CONFIGURATION RECEIVED -- P2P APPLICATION SERVER : LED1 ON |
P2P Client - Initialization phase | P2P Client - Connected Phase and LED On notification |
==>> Start Ble_Hci_Gap_Gatt_Init function Success: hci_reset command Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET Public Bluetooth Address: 00:80:e1:2a:7d:0c Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET Success: aci_hal_set_tx_power_level command Success: aci_gatt_init command Success: aci_gap_init command Success: aci_gatt_update_char_value - Appearance Success: aci_gap_set_io_capability command Success: aci_gap_set_authentication_requirement command Success: aci_gap_configure_whitelist command ==>> End Ble_Hci_Gap_Gatt_Init function |
==>> aci_gap_start_general_discovery_proc - Success P2P server, db addr 0x00:80:E1:2A:7C:EA ==>> aci_gap_terminate_gap_proc - Success >>== ACI_GAP_PROC_COMPLETE_VSEVT_CODE -- GAP_GENERAL_DISCOVERY_PROC completed Create connection to P2Pserver wait for event HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE >>== ACI_GAP_PROC_COMPLETE_VSEVT_CODE >>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x0001 - Connection established with @:00:80:e1:2a:7c:ea - Connection Interval: 50.00 ms - Connection latency: 0 - Supervision Timeout: 5000 ms Discover services, characteristics and descriptors for P2Pserver GATT services discovery GATT services discovery PROC_GATT_DISC_ALL_PRIMARY_SERVICES aci_gatt_disc_all_primary_services cmd NOK status =0x0C DISCOVER_ALL_CHARS ConnHdl=0x0001 ALLServiceHandle[0x0000 - 0x0000] All characteristics discovery Failed, status =0x0C DISCOVER_ALL_CHAR_DESCS [0x0000 - 0x0000] All characteristic descriptors discovery Failed, status =0x0C All notifications enabled Successfully ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0001 1/2 short UUID=0x1801, handle [0x0001 - 0x0004], GENERIC_ATTRIBUTE_SERVICE_UUID found 2/2 short UUID=0x1800, handle [0x0005 - 0x000B], GAP_SERVICE_UUID found ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0001 1/1 short UUID=0xFE40, handle [0x000C - 0x0011], P2P_SERVICE_UUID found PROC_GATT_DISC_ALL_PRIMARY_SERVICES services discovered Successfully DISCOVER_ALL_CHARS ConnHdl=0x0001 ALLServiceHandle[0x0001 - 0x0011] ACI_ATT_READ_BY_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0001 ConnHdl=0x0001, number of value pair = 3 1/3 short UUID=0x2A05, Properties=0x0020, CharHandle [0x0002 - 0x0003], GATT SERVICE_CHANGED_CHARACTERISTIC_UUID charac found 2/3 short UUID=0x2A00, Properties=0x000A, CharHandle [0x0006 - 0x0007], GAP DEVICE_NAME charac found 3/3 short UUID=0x2A01, Properties=0x0002, CharHandle [0x0008 - 0x0009], GAP APPEARANCE charac found ACI_ATT_READ_BY_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0001 ConnHdl=0x0001, number of value pair = 1 1/1 short UUID=0x2A04, Properties=0x0002, CharHandle [0x000A - 0x000B] ACI_ATT_READ_BY_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0001 ConnHdl=0x0001, number of value pair = 1 1/1 short UUID=0xFE41, Properties=0x0006, CharHandle [0x000D - 0x000E], ST_P2P_WRITE_CHAR_UUID charac found ACI_ATT_READ_BY_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0001 ConnHdl=0x0001, number of value pair = 1 1/1 short UUID=0xFE42, Properties=0x0010, CharHandle [0x000F - 0x0010], ST_P2P_NOTIFY_CHAR_UUID charac found All characteristics discovered Successfully DISCOVER_ALL_CHAR_DESCS [0x0001 - 0x0011] ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0002 UUID=0x2A05, handle=0x0003, found GATT SERVICE_CHANGED_CHARACTERISTIC_UUID Descriptor UUID=0x2902, handle=0x0002-0x0003-0x0004, Service Changed found PRIMARY_SERVICE_UUID=0x2800 handle=0x0005 reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0006 ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 UUID=0x2A00, handle=0x0007, found GAP DEVICE_NAME_UUID reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0008 UUID=0x2A01, handle=0x0009, found GAP APPEARANCE_UUID reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x000A UUID=0x2A04, handle=0x000B ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 PRIMARY_SERVICE_UUID=0x2800 handle=0x000C reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x000D ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 UUID=0xFE41, handle=0x000E, found ST_P2P_WRITE_CHAR_UUID ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x000F ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 UUID=0xFE42, handle=0x0010, found ST_P2P_NOTIFY_CHAR_UUID ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0001 Descriptor UUID=0x2902, handle=0x000F-0x0010-0x0011P2PNotification found : Desc UUID=0x2902 handle=0x000F-0x0010-0x0011 All characteristic descriptors discovered Successfully ServiceChangedCharDescHdl =0x0004 P2PNotificationDescHdl =0x0011 All notifications enabled Successfully ACI_GATT_NOTIFICATION_VSEVT_CODE - ConnHdl=0x0001, Attribute_Handle=0x0010 Incoming Nofification received P2P Server information P2P APPLICATION CLIENT : NOTIFICATION RECEIVED - LED ON |
4. P2P Client - smartphone application
4.1. ST BLE ToolBox application
Once the BLE P2P Server application is installed on the STM32WBA platform, launch the ST BLE ToolBox smartphone application. The application starts scanning and allows to see advertisement data or to connect to the device. Once the device is connected an interface allows to switch On/Off the blue LED of the platform, and a notification reflect the Switch_C characteristic status.
BLE P2P application on ST BLE ToolBox | ||
---|---|---|
5. References