This article provides explanations on how the STM32U0 battery less demo works and describes step-by-step how to reproduce it.
1. Presentation of the demo
1.1. Purpose
The aim of this demo is to illustrate the STM32U0's best-in-class ultra-low-power capabilities. It is running without battery thanks to Dracula technologies inkjet Printed Organic Photovoltaic module, which harvests energy for the STM32U0 MCU. This is a luxmeter and thermometer demo with data being displayed on an LCD segment display, and with the possibility to share measured data wirelessly.
1.2. Configurations
This demo can be configured in two versions.
- The first one is referred as the Data logger only configuration. It consists of one STM32U083C-Discovery kit powered by one Layer photovoltaic module. Every second, the measured temperature or illuminance is displayed on the LCD segment display. By pressing the joystick blue hat of the discovery kit, the user can change which data is being displayed.
- The second one is referred as the Data logger & RF configuration. It consists of two modules, the Data logger & Transmitter module, and the Receiver & Display module.
- The first one is based on the first configuration of the demo, on top of which an X-Nucleo-S2868A2, an RF expansion board, is plugged. In addition to measuring temperature and illuminance, and displaying one of the two measures on the LDC segment display, it sends each second the two measures thanks to the RF module.
- The second one is a module which receives the data and displays it on an LCD screen. It is based on a Nucleo-U083RC on top of which two expansion kits, an X-Nucleo-S2868A2, to receive the data, and an X-Nucleo-GFX01M2, with the LCD screen, are plugged. The two received measures are displayed in real time on the LCD screen, and variations are shown live on a graph chart. This module needs external power supply, such as USB.
2. How the demo works
2.1. Schematics
The figure below shows schematics of the Data logger only configuration on the left, and of the Data logger & RF configuration on the right.
2.2. Demo principle
The following flowchart and graph describe the three main phases of the Data logger module: the boot phase, the initialization phase, and the measurement phase.
After connecting the panel, the capacitor starts to charge (1). When voltage first reaches the POR voltage (1.65 V) (2), only the minimum instructions are done before entering stop 2 mode, to consume as little energy as possible. Hence, in this time frame, only PVD is set to level 6 to wake up the STM32U0 when voltage reach 3.0 V (3). This is the critical part of the initialization.
Once the voltage reaches 3.0 V for the first time (4), the initialization of the peripherals can start (5). GPIOs, LCD, ADC, communication with the temperature sensor, and, if present, communication with the RF module is initialized. PVD is set to level 0 (2.0 V). It is used to check that voltage is high enough before starting the measurement and sending process. It is set to this level to have the largest working range. RTC is also configured to wake-up the MCU every second. Then, the MCU enters stop 2 mode until wake-up from RTC (6).
At wake-up, and after checking voltage is high enough (7), the measurement phase is entered (8). Temperature is measured by the STT22H temperature sensor included in the discovery kit. Light is measured by measuring voltage provided by the panel, as explained in the following part. If the RF module is present, measured data is sent. The last step is to enter stop 2 again to harvest energy from the photovoltaic module (9).
2.3. Illuminance measurement
The figure below illustrates the flow of current outside of the illuminance measurement phase. PA0 is in open drain output high configuration, so current flows to the capacitor and the STM32U0.
The illuminance is deduced from the current supplied by the photovoltaic module as both are proportional. The current supplied by the photovoltaic module is deduced by measuring the voltage across the photovoltaic cell when its current is flowing through a resistor only. This voltage is measured by one of the ADC of the STM32U0.
So, the following formula is used to deduce illuminance from the measured ADC voltage:
Where:
is the ambient illuminance.
is the current provided by the photovoltaic module.
is the voltage measured by the ADC.
is a proportionality constant.
is the value of resistor R1.
To have the current of the photovoltaic module to flow through only, PA0 is configured in open drain output low, and a diode isolates the photovoltaic cell and the resistor from the capacitor. The figure below illustrates the flow of current during the illuminance measurement phase.
3. How to reproduce
3.1. Bill of material
Data logger & Transmission module
- 1x STM32U083C Discovery kit
- 1x Layer® inkjet Printed Organic photovoltaic product from Dracula Technologies
- 1x diode
- 1x 100 µF capacitor
- 1x 2.2 kΩ resistor
- 1x X-Nucleo-S2868A2
- 1x 300 kΩ resistor
Receiver & Display module
- 1x Nucleo-U083RC
- 1x X-Nucleo-S2868A2
- 1x X-Nucleo-GFX01M2
- 2x SSQ-119-03-T-D
3.2. Hardware
3.2.1. Reproduction of the Data logger & Transmission module
The figure below shows the modifications to be done on the front side of STM32U083-DK.
- 1. Remove JP5.
- 2. Close JP6 to connect the two right pins of the jumper (supply the temperature sensor by VDD_MCU).
- 3. Remove JP7.
- 4. Remove R57.
- 5. Connect the 100 µF capacitor in the dedicated slot of the DK.
The figure below shows the connections to be done on the bottom side of STM32U083-DK.
- 6. Close SB17.
- 7. Connect PV- to battery– pin.
- 8. Connect PV+ to CN7-38 (PC1).
- 9. Connect the diode between CN7-38 (PC1) and battery+ pin.
The figure below shows the modifications to be done on the front side of X-Nucleo-S2868A2.
- 10. Connect the 2.2 kΩ resistor between A4 (PC1) and A0 (PA0).
- 11. Connect the 300 kΩ pull-up resistor between VREF (CN5-3) and D7 (CN9-8).
- 12. Remove JP1.
The figure below shows the modifications to be done on the bottom side of X-Nucleo-S2868A2.
- 13. Cut CN9-9 and CN9-10.
- 14. Connect CN5-8 to JP1-1.
- 15. Remove R12.
- 16. Plug the X-Nucleo-S2868A2 on the DK's Arduino connectors.
3.2.2. Reproduction of the Receiver & Display module
The figure below shows modifications to be done on the X-Nucleo-S2868A2.
The following solder bridges must be opened.
- A1. R10 - Disconnect SDN from D7.
- A2. R11 - Disconnect SPI SCLK from D3.
- A3. R12 - Disconnect GPIO0 from A0.
- A4. R13 - Disconnect CSN from A1.
- A5. R14 - Disconnect GPIO1 from A2.
- A6. R15 - Disconnect GPIO2 from A3.
- A7. R16 - Disconnect GPIO3 from A5.
The following solder bridges must be closed.
- B1. R6 - Connect SPI SCLK to D13.
- B2. R9 - Connect CSN to D10.
- B3. R18 - Connect GPIO0 to A4.
- B4. CN9-3 on R19 (or R10) - Connect SDN to D2. [1]
The figure below shows the connections and the modification to be done on the Nucleo-U083RC:
- C1. Cut CN7-36 (conflict on this pin between the 2 extension kits).
- C2. Plug the 2 SSQ-119-03-T-D 19x2 connectors on Nucleo-connectors.
- C3. Plug the X-Nucleo-S2868A2 on Arduino-connectors.
- C4. Plug the X-Nucleo-GFX01M2 on the SSQ-119-03-T-D connectors.
3.3. Software
![]() |
Coming soon |
3.3.1. Programming the Data logger & Transmission module
- 1. Download and open STM32CubeProgrammer.
- 2. Connect through USB the ST-LINK to your PC.
- 3. Close JP7.
- 4. Click on Connect.
- 5. Enter the Erasing & Programming menu.
- 6. Browse the “data_logger_and_transmission.hex” file.
- 7. Click on Start Programming.
- 8. Click on Disconnect.
- 9. Open JP7.
- 10. Disconnect the USB.
3.3.2. Programming the Receiver & Display module
- 1. Connect through USB the STLink to your PC.
- 2. Open the External loaders menu.
- 3. Search for “STM32U0”.
- 4. Select the “MX25L6433F_GFX01M2_STM32U0” external loader.
- 5. Click on Connect.
- 6. Enter the Erasing & Programming menu.
- 7. Browse the “reception_and_display.hex” file.
- 8. Click on Start Programming.
- 9. Click on Disconnect.
4. References
- ↑ D6 and D7 connectors are used by the display module, so neither of them can be used for SDN pin.
- STM32U0 new product for entry level battery operated devices, video in which you can see running demo.
- STM32U0 ULP Lux demo, video presenting the principle of this demo.
- STM32U0 new product for entry level battery operated devices, video in which you can see running demo.