![NanoEdgeAI logo rectangle.png](/stm32mcu/nsfr_img_auth.php/thumb/f/f5/NanoEdgeAI_logo_rectangle.png/600px-NanoEdgeAI_logo_rectangle.png)
NanoEdge AI Studio is a free software provided by ST to easily add AI into to any embedded project running on any Arm © Cortex M MCU.
It empowers embedded engineers, even those unfamiliar with AI, to almost effortlessly find the optimal AI model for their requirements through straightforward processes.
Operated locally on a PC, the software takes input data and generates a NanoEdge AI library that incorporates the model, its preprocessing, and functions for easy integration into new or existing embedded projects.
The main strength of NanoEdge AI Studio is its benchmark which will explore thousands of combinations of preprocessing, models and parameters. This iterative process identifies the most suitable algorithm tailored to the user's needs based on their data.
1. Getting Started
1.1. What is NanoEdge AI Studio?
NanoEdge AI Studio is a software designed for embedded machine learning. It acts like a search engine, finding the best AI libraries for your project. It needs data from you to figure out the right mix of data processing, model structure, and settings.
Once it finds the best setup for your data, it creates AI libraries. These libraries make it easy to use the data processing and model in your C code.
1.1.1. NanoEdge AI Library
NanoEdge™ AI Libraries are the output of NanoEdge AI Studio. They are static library for embedded C software on Arm® Cortex® microcontrollers (MCUs). Packaged as a precompiled .a file, it provides building blocks to integrate smart features into C code without requiring expertise in Mathematics, Machine Learning, or data science.
When embedded on microcontrollers, the NanoEdge AI Library enables them to automatically "understand" sensor patterns. Each library contains an AI model with easily implementable functions for tasks like learning signal patterns, detecting anomalies, classifying signals, and extrapolating data.
Each kind of project in NanoEdge has it own kind of AI Library with their functions but they share the same characteristics:
- Highly Optimized: Designed for MCUs (any Arm® Cortex®-M).
- Memory Efficient: Requires only 1-20 Kbytes of RAM/flash memory.
- Fast Inference: Executes in 1-20 ms on Cortex®-M4 at 80 MHz.
- Cloud Independent: Runs directly within the microcontroller.
- Easy Integration: Can be embedded into existing code/hardware.
- Energy Efficient: Minimal power consumption.
- Static Allocation: Preserves the stack.
- Data Privacy: No data transmission or saving.
- User-Friendly: No Machine Learning expertise required for deployment.
All NanoEdge AI Libraries are created using NanoEdge AI Studio.
1.1.2. Nanoedge AI Studio Capabilities
NanoEdge AI Studio can:
- Search for optimal AI libraries (preprocessing + model) given user data.
- Simplify the development of machine learning features for embedded developers.
- Minimize the need for extensive machine learning and data science knowledge.
- Utilize minimal input data compared to traditional approaches.
Using project parameters (MCU type, RAM, sensor type) and signal examples, the Studio outputs the most relevant NanoEdge AI Library. This library can be either untrained (learning post-embedding) or pre-trained. The library performs inference directly on the microcontroller, involving:
- Signal preprocessing algorithms (e.g., FFT, PCA, normalization).
- Machine learning models (e.g., kNN, SVM, neural networks, proprietary algorithms).
- Optimal hyperparameter settings.
The process is iterative: import signals, run a benchmark, test the library, adjust data, and repeat to improve results.
1.1.3. Nanoedge AI Studio Limitations
NanoEdge AI Studio:
- Requires user-provided input data (sensor signals) for satisfactory results.
- Libraries' performances are heavily correlated to the quality of the data imported
- Does not offer ready-to-use C code for final implementation. Users must write, compile, and integrate the code with the AI library.
In summary, NanoEdge AI Studio outputs a static library (.a file) based on user data, which must be linked and compiled with user-written C code for the target microcontroller.
1.2. License Activation
To use NanoEdge AI Studio, you need a license obtained during the software download at stm32ai.st.com.
Initial Setup
- Enter your license key
- Set your proxy settings if you need
- Save Settings
IP Authorization
You may need to authorize the following IP addresses:
ST API for library compilation: | 52.178.13.227 | or via URL: https://api.nanoedgeaistudio.net |
---|
Port Configuration
By default, NanoEdge AI Studio uses port 5000. If this port is unavailable, the Studio will automatically search for an available port. To manually configure the port:
- Press windows key + R, type %appdata% and press Enter.
- Navigate to nanoedgeaistudio folder and open config.json
- Locate the line where the port is set, modify it, and save the file.
Project Storage Location
You can change the location where projects are saved. Avoid selecting cloud-synced or shared folders for project storage.
1.2.1. Offline license activation
If you lack an Internet connection, you can activate your NanoEdge AI Studio license offline:
- Offline Activation: Click on "Offline Activation" and enter your license key.
- Copy the Activation String: A long string of characters will appear. Copy this string or click the provided link.
- Activate License: Paste the string if needed and click "Activate License".
- Receive Response String: You will receive a new string as a response. Copy this string.
- Finalize Activation: Return to NanoEdge AI Studio, paste the response string, and click "Activate".
1.3. Type of projects
The four different types of projects that can be created using the Studio, along with their characteristics, outputs, and possible use cases, are outlined below:
Anomaly detection differentiates normal behavior signals from abnormal ones.
- User Input: Datasets containing signals for both normal and abnormal situations.
- Studio Output: The optimal anomaly detection AI library, including preprocessing and the model identified during benchmarking.
- Library Output: The library provides a similarity score (0-100%) indicating the resemblance between the training data and the new signal.
- Retraining: This project type supports model retraining directly on the microcontroller. [More information here].
- C Library Functions: Includes initialization, learning, and detection functions. [More details here].
- Use Case Example: For preventive maintenance of multiple machines, collect nominal data and simulate possible anomalies. Use NanoEdge AI Studio to create a library that can distinguish normal and abnormal behaviors. Deploy the same model on all machines and retrain it for each specific machine to enhance specialization for their environments.
N-class classification assigns a signal to one of several predefined classes based on training data.
- User Input: A dataset for each class to be detected.
- Studio Output: The optimal N-class classification library, including preprocessing and the model identified during benchmarking.
- Library Output: The library produces a probability vector corresponding to the number of classes, indicating the likelihood of the signal belonging to each class. It also directly identifies the class with the highest probability.
- C Library Functions: Includes initialization and classification functions. [More details here].
- Use Case Example: For machines prone to various errors, use N-class classification to precisely identify the type of error occurring, rather than just detecting the presence of an issue.
One-class classification distinguishes normal behavior from abnormalities without needing abnormal examples, detecting outliers instead.
- User Input: A dataset containing only nominal (normal) examples.
- Studio Output: The optimal one-class classification library, including preprocessing and the model identified during benchmarking.
- Library Output: The library returns 0 for nominal signals and 1 for outliers.
- C Library Functions: Includes initialization and detection functions. [More details here].
- Use Case Example: For predictive maintenance when abnormal data is unavailable, one-class classification can identify outliers. However, for better performance, using anomaly detection is recommended.
Extrapolation predicts discrete values, commonly known as regression.
- User Input: A dataset containing pairs of target values to predict and corresponding signals. Data format differs from other projects in NanoEdge. [See here for details].
- Studio Output: The optimal extrapolation library, including preprocessing and the model identified during benchmarking.
- Library Output: The library predicts the target value based on the input signal.
- C Library Functions: Includes initialization and prediction functions. [More details here].
- Use Case Example: When monitoring a machine with multiple sensors, use extrapolation to predict the value of one sensor using data from other sensors. Create a dataset with signals representing the data evolution from the sensor to be kept and associate it with the values from the sensor to be replaced.
1.4. Data format
1.4.1. Defining important concepts
Here are some clarifications regarding important terms that are used in this document and in NanoEdge:
Axis/Axes:
In NanoEdge AI Studio, the axis/axes are the total number of variables outputted by the sensor used for a project. For example, a 3-axes accelerometer outputs a 3-variables sample (x,y,z) corresponding to the instantaneous acceleration measured in the 3 spatial directions.
In case of using multiple sensors, the number of axes is the total number of axes of all sensors. For example, if using a 3-axes accelerometer and a 3-axes gyroscope, the number of axes is 6.
Signal:
A signal is the continuous representation in time of a physical phenomenon. We are sampling a signal with a sensor to collect samples (discrete values). Example: vibration, current, sound.
Sample:
This refers to the instantaneous output of a sensor, and contains as many numerical values as the sensor has axes.
For example, a 3-axis accelerometer outputs 3 numerical values per sample, while a current sensor (1-axis) outputs only 1 numerical value per sample.
Data rate:
The data rate is the frequency at which we capture signal values (samples). The data rate must be chosen according to the phenomenon studied.
You must also pay attention to having a consistent data rate and number of samples to have buffers that represent a meaningful time frame.
Buffer:
A buffer is a concatenation of consecutive samples collected by a sensor. A dataset contains multiples buffers, the term Line is also used when talking about buffers of a dataset.
Buffers are the input for NanoEdge, being in the Studio or in the microcontroller.
1.4.2. Work with temporal buffers
NanoEdge AI Studio expects buffers and not just samples of data.
Buffer = sensor' number of axes * number of sample taken at a fixed data rate (Hz)
It's crucial to maintain a consistent sampling frequency and buffer size.
Why are buffers more useful than samples?
In machine learning, you want to work on buffer as they contains information on the evolution of the phenomenon studied. Samples are just a single point in time representing the phenomenon. It is easier to distinguish pattern in buffers than in simple values
Lets consider a simple example were we collect 2 signal being the same but one in temporal order (t0 to tn), and the other being the opposite (tn to t0). We consider these two signals being two classes and we want to classify a new signal into one of these two classes (here if it is equal to one of them).
- Left plot: Samples independently
- Right plot: Samples as temporal buffers
We collect a new signal that is for sure from one of the two classes and want to know which one:
- If we look at the samples (left approach), it is impossible as all the values are in the 2 classes. A single sample doesn't contains the information for it to be classified.
- On the other hand, if we use the temporal buffer, we directly see which one it is equal to.
1.4.3. General rules
The Studio requires:
- Each line in a dataset must represent a single, independent signal example composed of multiple samples.
- The buffer size to be a power of two and remain constant throughout the project.
- The sampling frequency to remain constant throughout the project.
- All signal examples for a specific "class" to be grouped in the same input file (e.g., all "nominal" regimes in one file and all "abnormal" regimes in another for anomaly detection).
General considerations for input file format:
- .txt / .csv files
- Numerical values only, no headers
- Uniform separators (single space, tab, comma, or semicolon)
- Decimal values formatted with a period (.)
- Fewer than 16,384 values per line
- Consistent number of numerical values on each line
- Minimum of 20 lines per sensor axis
- Fewer than ~100,000 total lines
- File size less than ~1 Gbit
Specific formatting rules:
- Anomaly detection, 1-class classification, and n-class classification projects share general rules.
- Extrapolation projects require target values for extrapolation.
1.4.4. Basic Format
Following the rules from the previous part, the format for anomaly detection (AD), N-class classification (NCC) or 1-class classification (1CC) is the same and is describe in the example below:
You want to collect 3-axes accelerometer data to monitor a motor. You estimate the highest-frequency component of this vibration to be below 500 Hz, therefore choose a sampling frequency of 1000 Hz for the sensor. You want to get signals that represent 250ms which mean that you will collect buffer of 256 samples as 256/1000 (nb sample / data rate) = 256 ms.
In this example all the parameters considered are:
- Number of axis: 3 axes
- Number of sample: 256samples
- Buffer size: 3*256 = 768
- Data rate: 1000Hz
- Temporal length: 256ms
All these parameters hold a major importance in the result that you will get in NanoEdge AI Studio. Find more on how to select them here.
1.4.5. Variant Format: Extrapolation projects
In Extrapolation (or Regression) the file format is slightly different.
The goal of extrapolation models is to predict a numerical value, called Target in NanoEdge based on an input buffer. To train such models, you need a dataset with a large variety of Target and the corresponding buffer.
When trained, you will then give a buffer as input to the model that will output the target that you are trying to predict.
Lets say that you want to predict the speed of a motor based on its vibration. Here your target is a speed corresponding to vibration, which is 3 axis accelerometer data. In this case, you will collect buffers of accelerometer data and for each buffer, associate the corresponding speed (the speed at the start of the acquisition, the end or an average depending on your use case):
The format is the same as in other project but with one more column that must be the first one.
This time, the buffer size in the dataset used by NanoEdge is: number of axes * number of sample + Target.
1.4.6. Designing a relevant sampling methodology
Recommended resource: NanoEdge AI Datalogging MOOC.
Compared to traditional machine learning approaches, which might require hundreds of thousands of signal examples to build a model, NanoEdge AI Studio requires minimal input datasets (as little as 50-100 signal examples, depending on the use case).
However, this data needs to be qualified, which means that it must contain relevant information about the physical phenomena to be monitored. For this reason, it is absolutely crucial to design the proper sampling methodology, in order to make sure that all the desired characteristics from the physical phenomena to be sampled are correctly extracted and translated into meaningful data.
To prepare input data for the Studio, the user must choose the most adequate sampling frequency.
The sampling frequency corresponds to the number of samples measured per second. For some sensors, the sampling frequency can be directly set by the user (such as digital sensors), but in other cases (such as analog sensors), a timer needs to be set up for constant time intervals between each sample.
The speed at which the samples are taken must allow the signal to be accurately described, or "reconstructed"; the sampling frequency must be high enough to account for the rapid variations of the signal. The question of choosing the sampling frequency therefore naturally arises:
- If the sampling frequency is too low, the readings are too far apart; if the signal contains relevant features between two samples, they are lost.
- If the sampling frequency is too high, it might negatively impact the costs, in terms of processing power, transmission capacity, or storage space for example.
The issues related to the choice of sampling frequency and the number of samples are illustrated below:
- Case 1: the sampling frequency and the number of samples make it possible to reproduce the variations of the signal.
- Case 2: the sampling frequency is not sufficient to reproduce the variations of the signal.
- Case 3: the sampling frequency is sufficient but the number of samples is not sufficient to reproduce the entire signal (meaning that only part of the input signal is reproduced).
The buffer size corresponds to the total number of samples recorded per signal, per axis. Together, the sampling frequency and the buffer size put a constraint on the effective signal temporal length.
Here are general recommendations. Make sure that:
- the sampling frequency is high enough to catch all desired signal features. To sample a 1000 Hz phenomenon, you must at least double the frequency (in this case, sample at 2000 Hz at least).
- your signal is long (or short) enough to be coherent with the phenomenon to be sampled. For example, if you want your signals to be 0.25 seconds long (
L
), you must haven / f = 0.25
. For example, choose a buffer size of 256 with a frequency of 1024 Hz, or a buffer of 1024 with a frequency of 4096 Hz, and so on.
2. Using NanoEdge AI Studio
2.1. Studio home screen
The Studio main (home) screen has four main elements:
1. Project Creation Bar (top): Create new projects (anomaly detection, 1-class classification, n-class classification, or extrapolation), and access the datalogger and data manipulation screens.
2. Existing Projects List (left side): Load, import/export, or search existing NanoEdge AI projects.
3. Useful Links and Inspiration (right side): Access resources like MOOC, documentation, and links to the Use Case Explorer data portal for downloadable datasets and performance summaries.
4. Toolbar (left extremity): Provides quick access to:
- Datalogger
- Data manipulation
- Sampling finder
- Studio settings (port, workspace folder path, license information, and proxy settings)
- NanoEdge AI documentation
- NanoEdge AI license agreement
- CLI (command line interface client) download
- Studio log files (for troubleshooting)
- Studio workspace folder
2.2. Project Steps
On the main screen, select your desired project type on the project creation bar, and click CREATE NEW PROJECT.
Each project is divided into 5 successive steps:
- Project settings, to set the global project parameters
- Signals, to import signal examples that are used for library selection.
Note: this step is divided in 2 substeps in anomaly detection projects (Regular signals / Abnormal signals) - Optimize & benchmark, where the best NanoEdge AI Library is automatically selected and optimized
- Emulator, to test the candidate libraries before embedding them into the microcontroller
- Validation to have a summary of the project benchmarks (data, performance, flows)
- Deployment, to compile and download the best library and its associated header files, ready to be linked to any C code.
A helper tool providing tips is available on the bottom right corner of the screen when in a project. We highly recommend to complete the tasks given and read the documentation highlighted by it!
2.2.1. Project settings
The first step in any project is Project settings.
Here, the following parameters parameters are set:
- Project name
- Description (optional)
- Max RAM: this is the maximum amount of RAM memory to be allocated to the AI library. It does not take into consideration the space taken by the sensor buffers.
- Limit Flash / No Flash limit: this is the maximum amount of flash memory to be allocated to the AI library.
- Sensor type: the type of sensor used to gather data in the project, and the number of axes / variables when using a "Generic" sensor or "Multi-sensor".
- Target: this is the type of board or microcontroller on which the final NanoEdge AI Library is deployed.
Look below for more information on the available targets.
2.2.1.1. Target selection
NanoEdge AI Studio allows compilation on a large variety of targets. These target are separated in three tabs:
Development boards: 140+ targets,
Greats for education or proof of concepts as development board generally embed sensors.
Microcontrollers: 550+ targets
- Any STM32 Arm © Cortex M MCU: All STM32 families with a Arm © Cortex M MCU can be selected as target.
- A large variety of non ST Arm © Cortex M MCUs for development purposes only.
Arduino Boards: 19 targets
Arduino Boards with Arm © Cortex M MCUs for development purposes only.
For non-ST target and production purposes, please contact ST.
It is possible to add a board as favorite by clicking on the star. Then, the board will always be displayed on the left.
2.2.1.2. Working with multiple sensors
When combining different sensor types together, three distinct approaches can be used:
1. Using the Generic sensor:
- The Generic sensor can be used to combine multiple sensor types together into a single, unified signal buffer that is treated by the library as one multi-variable input.
The Machine Learning algorithms therefore build a model based on the combination of these inputs. - All signal sources must have the same output data rate (sampling frequency).
- Example: combining accelerometer (3 axes) + gyroscope (3 axes) + current (1 axis) signals, into a unified 7-axis signal.
- The Generic sensor must be selected, with 7 axes.
- The buffers in the input files are formatted just like a generic 3-axis accelerometer (see the General formatting rules section), but each sample now has 7 variables.
Instead of the 3 linear accelerations [X Y Z], the 7-axis sample adds 3 angular accelerations [Gx Gy Gz] from the gyroscope, and 1 current value [C] from the current sensor. - This results in 7-axis samples [X Y Z Gx Gy Gz C], meaning that for a buffer size of 256, each line is composed of 1792 numerical values (7*256).
2. Using the Multi-library feature (selectable on the Studio Deployment screen):
- This approach is radically different, and consists in separating the different sensor types, to create a separate library for each one.
- Each signal is decoupled and treated on its own by a different library, that runs concurrently in the same microcontroller. See the Multi-library section.
- Here, the output data rates of the different sensors might be different.
2.3. Types of sensors in NanoEdge AI Studio
NanoEdge AI Studio and its output NanoEdge AI Libraries are compatible with any sensor type; they are sensor-agnostic. For example, users can use data coming from an accelerometer, a magnetometer, a microphone, a gas sensor, a time-of-flight sensor, a microphone, or a combination of any of these (list non exhaustive).
The Studio is designed to be able to work with raw sensor data that has not necessarily been pre-processed. However, in cases where users already have some knowledge and expertise about their signals, pre-processed signals can be imported instead.
Depending on the user's use case, the Studio needs to understand which data format to expect in the imported input files. There are 2 main categories of sensors selectable in the Studio:
- Generic (n axes) sensor, which is a generalization of some other sensor types, such as accelerometer 3 axes, magnetometer 1 axis, microphone (1 axis), current (1 axis), and so on. This sensor covers most typical use cases, and is selected most of the time.
- Multi-sensor (n variables), referred to as "Multi-sensor", which is specific to anomaly detection projects, and designed for niche use cases, for which the expected format is entirely different.
The Generic n-axis sensor (and all others except "Multi-sensor") expects a buffer of data as input, in other words, a signal example represented by a succession of instantaneous sensor samples. As a result, this "signal example" has an associated temporal length, which depends on the sampling frequency (output data rate of the sensor) and on the number of instantaneous samples composing the signal example (referred to as buffer size, or buffer length).
The Multi-sensor sensor, on the other hand, expects instantaneous samples of data. In other words, it uses a single sensor sample as input, as opposed to a temporal signal example composed of many samples.
In the remainder of this documentation, except when explicitly stated otherwise, the "Generic" sensor approach (using signal examples / buffers as input, rather than single samples) is used by default.
2.3.1. Signals
2.3.1.1. How to import signals
The input files, containing all the signal examples to be used by the Studio to select the best possible AI library, can be imported from three sources:
- From a file (in .txt / .csv format)
- From the serial port (USB) of a live datalogger
- From the FP-SNS-Datalog
1. From file:
- Click SELECT FILES, and select the input file to import.
- Rename the input file if needed.
- Repeat the operation to import more files.
- Click CONTINUE.
2. From serial port:
- Select the COM Port where your datalogger is connected, and select the correct Baudrate.
- If needed, tick the checkbox enter a maximum number of lines to be imported.
- Click START/STOP to record the desired number of signal examples from your datalogger.
- Rename your input file if needed.
- Click CONTINUE.
3. From Function pack (.dat):
To import .dat files from the ST function pack, the user needs to convert them to .csv and then use the From file option to import them in NanoEdge AI Studio.
- To import .dat file from FP-SNS-DATALOG to the NanoEdge AI Studio, refer to hsdatalog_to_nanoedge Python® script in FP-SNS-DATALOG/Utilities/Python_SDK to convert it into a .csv file.
- To import .dat file from FP-AI-PDMWBSOC to the NanoEdge AI Studio, refer to hsdatalog_to_nanoedge Python® script in FP-AI-PDMWBSOC/Utilities/HS_Datalog_BLE_FUOTA/Python_SDK to convert it into a .csv file.
2.3.1.2. Which signals to import
1. Anomaly detection:
In anomaly detection, you need to collect two types of data: regular (nominal) data and abnormal data:
- Regular Data: Represents normal states of a machine (e.g., different operating regimes of a normally functioning motor).
- Abnormal Data: Represents abnormal states of a machine (e.g., motor misalignment, pump clogging).
When logging data, ensure the setup closely matches the real deployment environment. Collect a wide variety of data. If the library performs poorly under specific conditions, log new data, add it to the training set, and rerun the benchmark. This is an iterative process.
Example:
To detect anomalies in a 3-speed fan using an accelerometer to monitor vibration patterns, I recorded signals for various behaviors:
Nominal Examples:
- 30 for "Speed 1"
- 25 for "Speed 2"
- 35 for "Speed 3"
- 30 for "Fan turned off"
Some signals include "transients" like fan speeding up or slowing down.
Abnormal Examples:
- 30 for "Fan airflow obstructed at speed 1"
- 35 for "Fan orientation tilted by 90 degrees"
- 25 for "Tapping on the fan with my finger"
- 25 for "Touching the rotating fan with my finger"
2. 1-class Classification:
For 1-class classification, all the imported data needs to be regular (nominal) data representing all the situations considered normal. The benchmark will then used these data to try to define what is the normality and its limit.
3. n-class classification:
For n-class classification, all signal examples corresponding to one given class must be gathered into the same input file.
N-class classification benchmarks are started using one input file per class.
Example: For the identification of types of failures on a motor, five classes can be considered, each corresponding to a behavior, such as:
- Normal behavior
- Misalignment
- Imbalance
- Bearing failure
- Excessive vibration
This results in the creation of five distinct classes (import one .txt / .csv file for each), each containing a minimum of 20-50 signal examples of said behavior.
4. Extrapolation:
For extrapolation, all signal examples must be gathered into the same input file.
This file contains all target values to be used for learning, along with their associated buffers of data (representing the known parameters).
2.3.1.3. Signal summary screen
The Signals screen contains a summary of all information related to the imported signals:
- List of imported input files
- Information about the input file selected, and basic checks
- Optional: frequency filtering for the signals
- Signal preview graphs
- Imported files [1]: in this example (n-class classification project) a total of 7 input files are imported, each corresponding to one of the 7 classes to distinguish on the system (here, a multispeed USB fan).
- File information [2]: The selected file ("speed_1") contains 100 lines (or signal examples), each composed of 768 numerical values.
- The Check for RAM and the next 5 checks are blocking, meaning that any error in the input file must be fixed before proceeding further.
Here, all checks were successfully passed (green icon). However, if a check returns an error, a red icon is displayed. - Click "Run optional checks" to scan your input file and run additional checks (search for duplicate signals, equal consecutive values, random values, outliers, or others).
Failing these additional checks gives warnings that suggest possible modifications on your input files. Click any warning for more information and suggestions.
- The Check for RAM and the next 5 checks are blocking, meaning that any error in the input file must be fixed before proceeding further.
- Signal previews [4]: these graphs show a summary of the data contained in each signal example within the input file. There are as many graphs as sensor axes.
- The graph x-axis corresponds to the columns' in the input file.
- The y-values contain an indication of the mean value of each column (across all lines, or signals), their min-max values, and standard deviation.
- Optionally, FFT (Fast Fourier Transform) plots can be displayed to transpose each signal from time domain to frequency domain.
- Frequency filtering [3]: this is used to alter the imported signals by filtering out unwanted frequencies.
- Click FILTER SETTINGS above the signal preview plots
- Toggle "filter activated / deactivated" as required
- Input the sampling frequency (output data rate) used on the sensor used for signal acquisition.
- Select the low and high cutoff frequencies you wish to use for the signals (maximum: half the sampling frequency).
Within the input signals, only the frequencies that fall between these two boundaries are kept; all frequencies outside the window are ignored. - In the example below (sampling rate: 1024 Hz) the decision is to cut off all the low frequencies under 100 Hz.
2.3.2. Benchmark
During the benchmarking process, NanoEdge AI Studio uses the signal examples imported in the previous step to automatically search for the best possible NanoEdge AI Library.
The benchmark screen, summarizing the benchmark process, contain the following sections:
- NEW BENCHMARK button, and list of benchmarks
- Benchmark results graph
- Search information window
- Benchmark PAUSE / STOP buttons
- Performance evolution graph
To start a benchmark:
- Click RUN NEW BENCHMARK
- Select which input files (signal examples) to use
- Optional: change the number of CPU cores to use
- Click START.
2.3.2.1. Benchmarking process
Each candidate library is composed of a signal preprocessing algorithm, a machine learning model, and some hyperparameters. Each of these three elements can come in many different forms, and use different methods or mathematical tools, depending on the use case. This results in a very large number of possible libraries (many hundreds of thousands), which need to be tested, to find the most relevant one (the one that gives the best results) given the signal examples provided by the user.
In a nutshell, the Studio automatically:
- divides all the imported signals into random subsets (same data, cut in different ways),
- uses these smaller random datasets to train, cross-validate, and test one single candidate library many times,
- takes the worst results obtained obtained from step #2 to rank this candidate library, then moves on to the next one,
- repeats the whole process until convergence (when no better candidate library can be found).
Therefore, at any point during benchmark, only the performance of the best candidate library found so far are displayed (and for a given library, the score shown is the worst result obtained on the randomized input data).
2.3.2.2. Performance indicators
During benchmark, all libraries are ranked based on one primary performance indicator called "Score", which is itself based on several secondary indicators. Which secondary indicators are used depends on the type of project created. Below is the list of secondary indicators involved in the calculation of the "Score" (more information about available here).
- Anomaly Detection:
- Balanced Accuracy (BA)
- Functional Margin
- RAM & flash memory requirements
- n-class Classification:
- Balanced Accuracy (BA)
- Accuracy
- F1-score
- Matthews Correlation Coefficient (MCC)
- A custom measurement which estimates the degree of certainty of a classification inference
- RAM & flash memory requirements
- 1-class Classification:
- Recall
- A custom measurement which takes into account the radius of the hypersphere containing nominal signals, and the Recall obtained on the training dataset
- RAM & flash memory requirements
- Extrapolation:
- R² (R-squared)
- SMAPE (Symmetric Mean Absolute Percentage Error)
- RAM & flash memory requirements
The main secondary indicators are "Balanced Accuracy" for Anomaly Detection and n-class Classification, "Recall" for 1-class Classification, and "R²" for Extrapolation. Like the Score, these metrics are constantly being optimized during benchmark, and are displayed for information.
- Balanced accuracy (anomaly detection, classification) is the library's ability to correctly attribute each input signal to the correct class. It is the percentage of signals that have been correctly identified.
- Recall (1-class classification) quantifies the number of correct positives predictions made, out of all possible positive predictions.
- R² (extrapolation) is the coefficient of determination, which provides a measurement of how well the observed outcomes are replicated by the model, based on the proportion of total variation of outcomes explained by the model.
Additional metrics related to memory footprints:
- RAM (all projects) is the maximum amount of RAM memory used by the library when it is integrated into the target microcontroller.
- Flash (all projects) is the maximum amount of flash memory used by the library when it is integrated into the target microcontroller.
2.3.2.3. Benchmark progress
Benchmark graph:
Along with the four performance indicators, a graph shows the position in real time of signal examples (data points) imported.
The type of graph depends on the type of project:
The anomaly detection plot (left side) shown similarity score (%) vs. the signal number. The threshold (decision boundary between the two classes, "nominal" and "anomaly") set at 90% similarity, is shown as a gray dashed line.
The n-class classification plot (right side) shows probability percentage of the signal (the % certainty associated to the class detected) vs. the signal number.
The 1-class classification plot (left side) shows a 2D projection of the decision boundary separating regular signals from outliers. The outliers are the few (~3-5%) signals examples, among all the signals imported as "regular" which appear to be most different from the rest (~95-97%) of the others.
The extrapolation plot (right side) shows the extrapolated value (estimated target) vs. the real value which was provided in the input files.
Information window:
When a benchmark is running, this window (top right side of the screen) displays additional information about the process, such as:
- Threads started / stopped
- New best libraries found, and their scored
- Search speed (evaluations per second for each thread)
Performance evolution plot:
This plot, located at the bottom right side of the screen, shows the time-evolution of the four performance indicators that are optimized during benchmark.
Every time a new best library is found, this plot shows which metric has been improved, and by how much.
Some secondary performance indicators (confidence / R², RAM, Flash) might deteriorate over time, only when it is to the benefit of one of the main indicators (accuracy / recall / R²).
2.3.2.4. Benchmark results
When the benchmark is complete, the a summary of the benchmark information appears:
Only the best library is shown. However, several other candidate libraries are saved for each benchmark.
Any candidate library may be selected by clicking "N libraries" (see above, "11 libraries"), and selecting the desired library by clicking the crown icon.
This feature is useful to select a library that has better performance in terms of a secondary indicator (for instance to prioritize libraries that have a very low RAM or flash memory footprint).
Here, information about the family of machine learning model contained in the candidate libraries is also displayed. For example, in the list displayed above, there are libraries based on the SVM model, and others based on SEFR.
[Anomaly detection only]: After the benchmark is complete, a plot of the library learning behavior is shown:
This graph shows the number of learning iterations needed to obtain optimal performance from the library, when it is embedded in your final hardware application. In this particular example, NanoEdge AI Studio recommended that the learn()
is called 30 times, at the very minimum.
2.3.2.5. Possible cause for poor benchmark results
If you keep getting poor benchmark results, try the following:
- Increase the "Max RAM" or "Max Flash"" parameters (such as 32 Kbytes or more).
- Adjust your sampling frequency; make sure it is coherent with the phenomenon you want to capture.
- Change your buffer size (and hence, signal length); make sure it is coherent with the phenomenon to sample.
- Make sure your buffer size (number of values per line) is a power of two (exception: Multi-sensor).
- If using a multi-axis sensor, treat each axis individually by running several benchmarks with a single-axis sensor.
- Increase (or decrease, more is not always better) the number of signal examples (lines) in your input files.
- Check the quality of your signal examples; make sure they contain the relevant features / characteristics.
- Check that your input files do not contain (too many) parasite signals (for instance no abnormal signals in the nominal file, for anomaly detection, and no signals belonging to another class, for classification).
- Increase (or decrease) the variety of signal examples in your input files (number of different regimes, classes, signal variations, or others).
- Check that the sampling methodology and sensor parameters are kept constant throughout the project for all signal examples recorded.
- Check that your signals are not too noisy, too low intensity, too similar, or lack repeatability.
- Remember that microcontrollers are resource-constrained (audio/video, image and voice recognition might be problematic).
You may also take a look at guidelines for a successful NanoEdge AI project
Low confidence scores are not necessarily an indication or poor benchmark performance, if the main benchmark metric (Accuracy, Recall, R²) is sufficiently high (> 80-90%).
Always use the associated Emulator to determine the performance of a library, preferably using data that has not been used before (for the benchmark).
2.3.3. Emulator
The NanoEdge AI Emulator is a tool intended to test NanoEdge AI Libraries, as if it they were already embedded, without having to compile them, link them to some code, or program them to their target microcontroller. Each library, among hundreds of thousands of possibilities, comes with its own emulator: it is a clone that makes testing libraries quick and easy, and guarantees the same behavior and performance.
The Emulator can be used within the Studio interface, or downloaded as a standalone .exe
(Windows®) or .deb
(Linux®) to be used in the terminal through the command line interface. This is especially useful for automation or scripting purposes.
The Emulator screen contains the following information:
- Select which benchmark to use, to load the associated emulator
- Click INITIALIZE EMULATOR when ready to start testing
- Download the emulator in its CLI version (command line interface), and check its documentation
- Check the information summary for the benchmark selected (progress, performance, input files used)
2.3.3.1. Learning signals (anomaly detection only)
After initializing the anomaly detection emulator, no knowledge base exists yet. It needs to be acquired in-situ, using real signals.
Note: only "regular signals" (translating the normal / nominal behavior of the target machine) can be used for learning. More generally, only learn what is considered as the norm on your system.
The "regular signals" imported previously (for benchmark) can be reused, but you can also use entirely new signal examples (feel free to test different things!).
Signals can also be imported from a live data logger (serial port).
- Anomaly detection emulator workflow: initialization, learning, detection.
- Select a file to import, or import data directly from serial (USB).
Optionally, define a custom number of lines to learn.
Then, click LEARN THIS FILE and repeat the operation is needed.
Click GO TO DETECTION to move on to the inference step. - Check the emulator function outputs (same responses as for CLI version of the emulator)
2.3.3.2. Running inference (detection)
To run inference, in any project type, simply import some data, either from file or from serial port (live data logger).
The detection / classification / extrapolation is automatically run using the signal examples provided, and the results displayed on a graph.
For more details, the raw inference outputs in text format are also available on the Emulator function outputs window (see [4] on the image above) on the right side of the screen.
To restrict the inference to a selected number of lines within the input file, just tick the Define lines box, input the first and last lines to consider, and click the DETECT button.
2.3.3.3. Possible causes of poor emulator results
Here are possible reasons for poor anomaly detection or classification results:
- The data used for library selection (benchmark) is not coherent with the one you are using for testing via Emulator/Library. The signals imported in the Studio must correspond to the same machine behaviors, regimes, and physical phenomena as the ones used for testing.
- Your main benchmark metric was well below 90% or your confidence score was too low to provide sufficient data separation.
- The sampling method is inadequate for the physical phenomena studied, in terms of frequency, buffer size, or duration for instance.
- The sampling method has changed between Benchmark and Emulator tests. The same parameters (frequency, signal lengths, buffer sizes) must be kept constant throughout the whole project.
- The machine status or working conditions might have drifted between Benchmark and Emulator tests. In that case, update the imported input files, and start a new benchmark.
- [Anomaly detection]: you have not run enough learning iterations (your Machine Learning model is not rich enough), or this data is not representative of the signal examples used for benchmark. Do not hesitate to run several learning cycles, as long as they all use nominal data as input (only normal, expected behavior must be learned).
2.3.4. Validation
In the validation step, you can compare the behavior of all the libraries saved during the benchmark on new dataset. The goal of this step is to make sure that the best library given by NanoEdge is indeed the best among all the other, but also to see if the libraries behave as they should.
In the page is the list of all the libraries found during the benchmark.
- Select several libraries
- Click 'new experience'
- Import test datasets (preferably dataset not used in the benchmark)
Each time a new experiment is done, an id will be associated. It permits the user to create multiples experiences, with different files and libraries and keep track, thanks to the ids, of the results of all those experiences.
You can filter the results of an experience by clicking the eye icon next to an experience id.
2.3.4.1. Execution time
NanoEdge AI Studio allows for the estimation of execution time for any library encountered during the benchmark with the STM32F411 simulator provided by ARM, utilizing a hardware floating-point unit.
The estimation is an average of multiple calls to the NanoEdge AI library functions tested. The tool doesn't use directly the user data but data of a similar range to make the estimation.
It's important to note that while this estimation mimics real hardware conditions, it should be treated as such, and variations in the exact signal may impact execution time. Keep in mind that using another hardware can lead to significant changes in execution time.
2.3.4.2. Validation report
For each library displayed, the user can click on the blank sheet of paper to open the validation report.
The validation report contains information about:
- The data:
- the name of each file used for the benchmark
- the data sensor type: sound, vibration, and others
- the signal length (with the total signal length and the signal length per axis)
- number of signals in each file
- the data repartition score (goes up to five stars)
- The performance:
- The main metrics: Score, balanced accuracy, RAM and flash memory usage
- More specific metrics: Accuracy, f1 score, ROC AUC Score, Precision, MCC
- The recall per class: To know which class perform well, which class perform badly
- The nested cross validation results (10 test): Show how the model performed on 10 test datasets (to monitor overfitting)
- An algorithm flowchart:
- The entry data shape
- The preprocessing applied to the data
- The model architecture name
The user can export the summary page as a PDF using the top right red pdf button.
2.3.5. Deployment
Here the NanoEdge AI library is compiled and downloaded, ready to be deployed to the target microcontroller to build the embedded application.
The Deployment screen is intended for four main purposes:
- Select a benchmark, and compile the associated library by clicking the COMPILE LIBRARY button.
- Optional: select Multi-library, in order to deploy multiple libraries to the same MCU. More information below.
- Optional: select compilations flags to be taken into account during library compilation.
- Optional: copy a "Hello, World!" code example, to be used for inspiration.
if the target selected at the beginning of the project is a production ready board, you will need to agree to the license agreement:
After clicking Compile and selecting your library type, a .zip file is downloaded to your computer.
It contains:
- the static precompiled NanoEdge AI library file
libneai.a
- the NanoEdge AI header file
NanoEdgeAI.h
- the knowledge header file
knowledge.h
(classification and extrapolation projects only) - the NanoEdge AI Emulators (both Windows® and Linux® versions)
- some library metadata information in
metadata.json
2.3.5.1. Arduino target compilation
If an Arduino board was selected in project settings, the .zip obtained in compilation will contains an additional arduino folder. This folder contains another .zip that can be imported directly in Arduino IDE to use Nanoedge.
In Arduino IDE:
- Click Sketch > Include library > Add .zip library...
- Select the .zip in the arduino folder
If you already used a NanoEdge AI library in the past, you might get an error saying that you already have a library with the same name. To solve it, go to Document/arduino/libraries and delete the nanoedge folder. Try importing your llibrary again in Arduino IDE.
2.3.5.2. Multi-library
The Multi-library feature can be activated on the Deployment screen just before compiling a library.
It is used to integrate multiple libraries into the same device / code, when there is a need to:
- monitor several signal sources coming from different sensor types, concurrently, independently,
- train Machine Learning models and gather knowledge from these different input sources,
- make decisions based on the outputs of the Machine Learning algorithms for each signal type.
For instance, one library can be created for 3-axis vibration analysis, and suffixed vibration
:
Later on, a second library can be created later on, for 1-axis electric current analysis, and suffixed current
:
All the NanoEdge AI functions in the corresponding libraries (as well as the header files, variables, and knowledge files if any) is suffixed appropriately, and is usable independently in your code. See below the header files and the suffixed functions and variables corresponding to this example:
Congratulations! You can now use your NanoEdge AI Library!
It is ready to be linked to your C code using your favorite IDE, and embedded in your microcontroller.
3. Integrated NanoEdge AI Studio tools
This section presents the tools integrated in NanoEdge AI Studio to help the realization of a project. They are:
- The Datalogger generator, to create code to collect data on development board in few clicks
- The Sampling finder, to estimate the data rate and signal length to use for a project in few seconds
- The data manipulation tool, to reshape dataset easily
These tools can be accessed:
- In the main NanoEdge AI Studio screen
- At any time, in the left vertical bar.
3.1. Datalogger
Importing signals from Serial (usb) is available when creating a project in the NanoEdge AI Studio provided the user has created a datalogger in the code beforehand (specific to the board and the sensor used).
The datalogger screen automatically generates that part for the user. The user only needs to select a board among the ones available and choose which sensor to use and its parameters.
This is the datalogger screen. It contains all the compatible boards that the Studio can generate a datalogger for:
Click on a board to access the page to choose a sensor and its parameters.
The parametrization screen contains:
- The selected board
- The list of sensors available on the board
- The list of parameters specific to the sensor selected
- A button to generate the datalogger
The user must select the options corresponding to the data to be used in a project and click generate datalogger. The Studio generates a zip file containing a binary file. The user only needs to load the binary file on the microcontroller to be able to import signals for a project directly from Serial (usb).
3.1.1. Continuous datalogger
For some sensors on some development boards, the "continuous" option is available as a parameter for the data rate (Hz). If selected, the datalogger will record data continuously at the maximum data rate available on the sensor.
When the continuous data rate is selected, the "sampling size per axis" parameter disappears, as the new signal size is simply the number of axes. For example, if you have a 3-axis accelerometer, each line of your file will contain 3 values.
For speed reasons, continuous data loggers use CDC USB instead of UART. In practice, this means that we use the board's USB port to send data to the PC instead of using the ST-Link port. So make sure you connect the card to the PC using its USB port, otherwise you won't get any data from the datalogger. This also means that once you've flashed the datalogger, you no longer need the ST-Link to record data.
3.1.2. Arduino data logger
NanoEdge Data logger also allow to generate code for Arduino boards. Because of how Arduino works, we don't need to select a specific board. Only the sensor that we want to use.
To be able to use the code generated, here are the steps to follow:
- Select Arduino in the data logger generator
- Select the sensor and set its parameters
- click Generate and get the .zip containing the code from NanoEdge
- Extract the .ino file from the Nanoedge's .zip
- Open it with Arduino IDE
- Select the board that you are using: Tools > board
- Include all the libraries called in the C code (generally the sensor and wire.h): Sketch > Include Library > manage Library...
- Flash the code
You are now ready to log data via serial.
3.2. Sampling finder
The sampling rate and sampling size are two parameters that have a considerable impact on the final results given by NanoEdge. A wrong choice can lead to very poor results, and it is difficult to know which sampling rate and sampling size to use.
The tool is designed to help users make informed decisions regarding the sampling rate and data length, leading to accurate and efficient analysis of time-series signals in IoT applications.
How does the sampling finder works:
The Sampling Finder needs continuous datasets logged with the highest data rate possible. The signals in a dataset need to have only one sample per line, meaning for example, 3 values per line if working with a 3 axes accelerometer.
The tool reshape these data to create buffers of multiple sizes (from 16 to 4096 values per axis).
When creating the buffers, the Sampling Finder also skips values to simulate data logged with a lower sampling rate. The range of frequencies tested goes from the base frequency to the frequency divided by 32. For example, to create a buffer with halve the initial data rate, the sampling finder only use one value every two values.
With the all the combinations of sampling sizes and sampling rates, the tool then apply features extraction algorithms to extract the most meaningful information from the buffers. Working with features instead of the whole buffers permit to be much faster.
The tool try to distinguish all the imported files using fast machine learning algorithms and estimate a score. The final recommend combination is the one that worked best, with both a good score and a small sampling duration.
How to use the Sampling Finder:
To use the sampling finder tool, first import continuous datasets with the highest data rate possible (see the file format above):
- If working with Anomaly detection, import one file of nominal signals and one file of abnormal signals.
- If working with N-class classification, import one file of each class.
The steps to use the sampling finder are the following:
- Import the files to distinguish
- Enter the number of axis in the files
- Enter the sampling frequency used
- Choose the minimum frequency to test (the maximum number of subdivision of the base sampling frequency)
- Start the research
The sampling finder will fill the matrix with the results, giving an estimation for each combination of sampling rate and sampling size and make a recommendation.
After that, the next step is to log data at the sampling rate and sampling size - recommended by the tool and create a new project in NanoEdge using these data.
3.3. Data manipulation
NanoEdge AI Studio provides the user a screen to manipulate data:
This page is composed of:
- The button to access the data manipulation screen.
- The file column: this part is used to manage your import.
- The actions column: this part is used to choose a modification to apply on your imported files.
- The result column: In this column are displayed your files after being modified.
The File section contains all the imported files displayed in this column:
- A button Drop files or click to import to import one or multiple files at once.
- All the imported files displayed in column. The name of the file and the number of lines and columns are displayed by default. Additionally, you can preview your entire file by clicking the arrow in the right down corner.
- A concatenate option is proposed if at least two files are imported. If you use the concatenation option, all the imported files are combined into one single file.
The Action section contains all the action to modify your file are displayed in this column:
The following actions are available:
- Extract lines: Truncate lines at the beginning and at the end of a files. Enter in the fields, or by using the blue bar, the lines to extract then click Run.
- Remove column(s): Enter the number of a single or multiple columns to delete (separated by commas) then click Run.
The user can enter columns to delete one by one separated by commas or directly enter range of columns to delete using dashes (example 10-20 deletes the columns from 10 to 20). The user can delete both single column and range at the same time as in the example.
- Change columns number: Reshape (change) the size of the signals in a file (the buffer size). Enter a signals length for the data to be reshaped as then click Run.
The user can enter the size desired (the number of columns) to reshape the data. For example, the user can modify signals of size 4096 to smaller signals of size 1024. After applying the data manipulation, all signals of size 4096 are divided into four signals of size 1024 (meaning that the user has four times more signals of size 1024 thans of size 4096 previously).
- Shuffle: Randomly mix all the lines of the imported file(s), just click on Run.
The result section contains files that went through a data manipulation:
For each imported file, a new result file is generated after performing any action. All the generated result files are displayed in column:
- For each result file, a name containing information about the action performed is generated. There is also between parenthesis the name of the original file. The number of lines and columns are also displayed. You can click the arrow in the down left corner to show more information about the file.
- You can save any file in the result column by clicking the Save as button. Additionally, you can choose to perform new actions on a result file by clicking the Run new action button. This results in moving the file from the result column to the file column (the imported files).
- Save all files appears if there is at least two result files. The user can use it to save all the result files at once.
3.3.1. Advanced manipulation (combination)
By repeating the same action many times or combining different actions, the user can perform other manipulations:
- Create sub datasets: The user can use the Extract lines action several times to split a dataset for example (extract the first half lines, save it, then extract the second half and save it). The user can also create a sub dataset by extracting 10 lines at a time for example and have multiples subsets.
- Remove an axis: By combining Create buffer and Remove column(s), the user can delete an axis in the signals. For example, if the user has 3 axis signals and wants to delete one of them, the user can reshape the signals to a size of 3, then remove the axis wanted using the remove columns action, and then reshape the data back to the original size.
4. Resources
Recommended: NanoEdge AI Datalogging MOOC.
Documentation
All NanoEdge AI Studio documentation is available here.
Tutorials
Step-by-step tutorials to use NanoEdge AI Studio to build a smart device from A to Z.