This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. STM32WBA Bluetooth® Low Energy Long Range feature
The Long Range or Low Energy Coded PHY feature extends the Bluetooth® Low Energy to a range of 1,6 km or more.
By using the advertising extension feature, the Bluetooth® Low Energy coded advertising Primary (and secondary) PHY becomes active as Bluetooth® Low Energy coded.
The HCI and ACI commands define new parameter values.
Based on the BLE_p2pClient_Ext and BLE_p2pServer_Ext applications, two new applications have been developed to demonstrate the feature and to provide range measurements: BLE_App_Long_Range_Central and BLE_App_Long_Range_Peripheral[1].
Application functionalities are derived from the BLE_p2pClient and BLE_p2pServer applications:
Refer to the following page for the Peer to Peer project explanation.
1.1. Principles
The advertising extension feature is required.
Modified or new GAP commands have been implemented to enable the Bluetooth® Low Energy coded feature.
- To set the advertising parameters:
aci_gap_adv_set_configuration: Adv_Mode parameter is equal to 0x02 (use Bluetooth® Low Energy coded as primary advertising PHY)
aci_gap_adv_set_configuration
|
Description
- This command is used to set the extended advertising configuration to one advertising set.
- Syntax
tBleStatus aci_gap_adv_set_configuration(uint8_t Adv_Mode, uint8_t Advertising_Handle, uint16_t Adv_Event_Properties,
uint32_t Primary_Adv_Interval_Min, uint32_t Primary_Adv_Interval_Max, uint8_t Primary_Adv_Channel_Map, uint8_t Own_Address_Type,
uint8_t Peer_Address_Type, const uint8_t* Peer_Address, uint8_t Adv_Filter_Policy, uint8_t Adv_TX_Power, uint8_t Secondary_Adv_Max_Skip,
uint8_t Secondary_Adv_PHY, uint8_t Adv_SID, uint8_t Scan_Req_Notification_Enable );
- Parameters
-
- [in] Adv_mode
- Type: uint8_t
- Description: Bitmap of the extended advertising modes.
- '[in] Advertising_handle
- Type: uint8_t
- Description: Used to identify an advertising set.
- [in] Adv_Event_Properties
- Type: uint16_t
- Description: Type of the advertising event.
- [in] Primary_adv_interval_min
- Type: uint32_t
- Description: Minimum advertising interval.
- [in] Primary_adv_interval_max
- Type: uint32_t
- Description: Maximum advertising interval.
- [in] Primary_adv_channel_map
- Type: uint8_t
- Description: Advertising channel map.
- [in] Own_address_type
- Type: uint8_t
- Description: Own address type: if Privacy is disabled, the address can be public or static random; otherwise, it can be a resolvable private address or a non-resolvable private address.
- [in] Peer_address_type
- Type: uint8_t
- Description: Address type of the peer device.
- [in] Peer_address
- Type: 6 bytes
- Description: Public Device Address, Random Device Address, Public Identity Address, or Random (static) Identity Address of the device to be connected.
- [in] Adv_filter_policy
- Type: uint8_t
- Description: Advertising filter policy.
- [in] Adv_Tx_power
- Type: uint8_t
- Description: Advertising TX power. Units: dBm.
- [in] Secondary_Adv_Max_Skip
- Type: uint8_t
- Description: Secondary advertising maximum skip.
- [in] Secondary_Adv_PHY
- Type: uint8_t
- Description: Secondary advertising PHY.
- [in] Adv_SID
- Type: uint8_t
- Description: Value of the Advertising SID subfield in the ADI field of the PDU.
- [in] Scan_Req_Notification_Enable
- Type: uint8_t
- Description: Scan request notifications.
- Return value
-
- [out] command status
- Type: uint8_t
|
- To set the scan procedure:
aci_gap_ext_start_scan: scanning_PHY parameter is equal to 0x04 (use of Bluetooth® Low Energy coded as scan PHY)
aci_gap_ext_start_scan
|
Description
- This command is used to start a scanning procedure when the extended advertising feature is supported.
- Syntax
tBleStatus aci_gap_ext_start_scan(uint8_t Scan_Mode, uint8_t Procedure, uint8_t Own_Address_Type, uint8_t Filter_Duplicates,
uint16_t Duration, uint16_t Period, uint8_t Scanning_Filter_Policy, uint8_t Scanning_PHYs, const Scan_Param_Phy_t* Scan_Param_Phy);
- Parameters
-
- [in] Scan_mode
- Type: uint8_t
- Description: not used.
- '[in] Procedure
- Type: uint8_t
- Description: Scan procedure.
- [in] Own_address_type
- Type: uint8_t
- Description: Own address type: if Privacy is disabled, the address can be public or static random; otherwise, it can be a resolvable private address or a non-resolvable private address.
- [in] Filter_duplicate
- Type: uint8_t
- Description: Enable/disable duplicate filtering.
- [in] Duration
- Type: uint16_t
- Description: Scan duration.
- [in] Period
- Type: uint16_t
- Description: Scan period.
- [in] Scanning_filter_policy
- Type: uint8_t
- Description: The scanning filter policy determines the scanner Link Layer process advertising, and scan response PDUs.
- [in] Scanning_PHYs
- Type: uint8_t
- Description: Scan PHYs.
- [in] Scan_type
- Type: uint8_t
- Description: Passive or active scanning. With passive scanning, no scan request PDUs are sent.
- Scan_Param_Phy_t
- [in] Scan_interval
- Type: uint16_t
- Description: Time interval starting at the last scan from the controller and finishing at the subsequent scan start on the primary advertising physical channel.
- [in] Scan_window
- Type: uint16_t
- Description: Duration of the scan on the primary advertising physical channel.
- Return value
-
- [out] command status
- Type: uint8_t
|
aci_gap_ext_create_connection: initiating PHYs parameter is equal to 0x04 (use of LE coded as scan connectable PHY)
aci_gap_ext_create_connection
|
Description:This command is used to create a connection with the local device in the central role to an advertiser when the extended advertising feature is supported.
- Syntax
tBleStatus aci_gap_ext_create_connection(uint8_t Initiating_Mode, uint8_t Procedure, uint8_t Own_Address_Type, uint8_t Peer_Address_Type,
const uint8_t* Peer_Address, uint8_t Advertising_Handle, uint8_t Subevent, uint8_t Initiator_Filter_Policy, uint8_t Initiating_PHYs,
const Init_Param_Phy_t* Init_Param_Phy);
- Parameters
-
- [in] Initiating_Mode
- Type: uint8_t
- Description: not used.
- '[in] Procedure
- Type: uint8_t
- Description: Scan procedure.
- [in] Own_address_type
- Type: uint8_t
- Description: Own address type: if Privacy is disabled, the address can be public or static random; otherwise, it can be a resolvable private address or a non-resolvable private address..
- [in] Peer_Address_Type
- Type: uint8_t
- Description: Enable/disable duplicate filtering..
- [in] Peer_Address
- Type: 6 bytes
- Description: Scan duration.
- [in] Advertising_Handle
- Type: uint16_t
- Description: Scan period.
- [in] Subevent
- Type: uint8_t
- Description: The scanning filter policy determines how the scanner's Link Layer processes advertising and scan response PDUs.
- [in] Initiator_Filter_Policy
- Type: uint8_t
- Description: Scan PHYs.
- [in] Initiating_PHYs
- Type: uint8_t
- Description: Passive or active scanning. With passive scanning, no scan request PDUs are sent.
- Init_Param_Phy_t
- [in] Scan_interval
- Type: uint16_t
- Description: Time interval from when the Controller started its last scan until it begins the subsequent scan on the primary advertising physical channel.
- [in] Scan_window
- Type: uint16_t
- Description: Duration of the scan on the primary advertising physical channel.
- [in] Conn_Interval_min
- Type: uint16_t
- Description: Minimum value for the connection event interval.
- [in] Conn_interval_max
- Type: uint16_t
- Description: Maximum value for the connection event interval.
- [in] Connection_latencyl
- Type: uint16_t
- Description: Maximum Peripheral latency for the connection in number of connection events.
- [in] Supervision_timeout
- Type: uint16_t
- Description: Supervision timeout for the LE Link.
- [in] Min_CE_length
- Type: uint16_t
- Description: Information parameter about the minimum length of connection needed for this LE connection.
- [in] Max_CE_length
- Type: uint16_t
- Description: Information parameter about the maximum length of connection needed for this LE connection.
- Return value
-
- [out] command status
- Type: uint8_t
|
1.2. Advertising data
At startup, Peer To Peer Server Long Range application starts advertising.
Data advertised are composed as follows:
P2P Server Long Range advertising packet
|
Description
|
Length
|
AD type
|
Value
|
Device name
|
8
|
0x09
|
p2pS_LR_XX (XX: last byte of BD address)
|
Manufacturer data
|
15
|
0xFF
|
See the table below
|
Flags
|
2
|
0x01
|
0x06 (GeneralDiscoverable, BrEdrNotSupported)
|
|
Manufacturer data are encoded following STMicroelectronics BlueST SDK v2 as described below:
STMicroelectronics manufacturer advertising data
|
Byte Index
|
0
|
1
|
2-3
|
4
|
5
|
6
|
7
|
8
|
9
|
10-15
|
Function
|
Length
|
Manufacturer ID
|
Company
|
BlueST SDK Version
|
Device ID
|
Firmware ID
|
Option 1
|
Option 2
|
Option 3
|
Device address
|
Value
|
0x0F
|
0xFF
|
0x0030 STMicro
|
0x02
|
0x8B Nucleo-WBA
|
0x8F - p2p Server Long Range
|
0x00
|
0x00
|
0x00
|
0x08E12Axxxx
|
|
1.3. On-board buttons configuration
Button configuration for Bluetooth® Low Energy Long Range application on Nucleo-WBA55CG boards
|
Application |
Condition |
B1 click |
B1 long press |
B2 Click |
B2 long press |
B3 click |
B3 long press
|
Long Range server
|
Idle
|
-
|
/
|
-
|
/
|
-
|
/
|
Connected
|
Starts/Stops notification
|
Change LE coded PHY options
|
Long Range client
|
Idle
|
Starts scan then connects
|
/
|
-
|
/
|
-
|
/
|
Connected
|
Starts/Stops write data
|
Change LE coded PHY Options
|
|
1.4. STM32WBA Long Range central and peripheral application
Long Range central acts as a central device with the support of GATT Client Layer.
At startup, by pressing the B1 button, the Long Range client application:
- Starts scanning to detect Long Range server application by filtering the firmware ID of the STMicroelectronics manufacturer advertising data.
- Stops Scanning once Long Range server detected.
- Connects to the Long Range server to establish the connection.
- Discovers the Long Range server GATT Service & Characteristics.
- Enables all GATT server notification characteristics.
Once connected, the Long Range client application:
- By pressing B1 button, writes a message to toggle the Blue LED of the Long Range server.
- Receive notification to toggle the on board Blue LED from the remote Long Range server Application.
Long Range peripheral acts as a peripheral device with the support of the GATT Client Layer.
At reset, the Long Range peripheral application starts one extended advertising set at primary and secondary LE coded PHY.
Once connected, on both applications:
- By pressing the B2 button, the HCI_LE_SET_PHY command is sent. It allows to toggle Phy_options parameter S=8/2 (red led is ON/OFF).
Information
|
Change in PHY coded option is not notified to remote device.
|
- Payload can be coded with two different rates: 125 kb/s (S = 2) or 500 kb/s (S = 8)
Refer to Bluetooth®Programming Manual PM0271 [2]. See chapter 5.7 STM32WBA LE Coded PHY.
Example of flow diagram between STM32WBA Long Range server & Long Range client
|
|
B2 to toggle Phy options: client writes with S=8, peripheral notifies with S=2
|
|
1.5. Collector applications compatibility
The BLE_App_Long_Range_Peripheral project is compatible with the following collector:
BLE_App_Long_Range_Central or a smartphone supporting the Bluetooth® Low Energy coded feature.
1.6. Code example
A STM32WBA Long Range code example has been shared on the STM32-Hotspot GitHub [1].
2. References