1. Introduction
STM32H5 MCUs are equipped with new security features, such as Product life cycle, Isolation, Debug Authentication, Secure Storage and Secure Boot.
To use these features on a stand-alone basis, solid security skills are required. However, STMicroelectronics offers a full solution, owned and maintained by STMicroelectronics, to use these security features, which are targeting SESIP and PSA Level 3 certification.
2. Secure Manager overview
The Secure Manager is an STMicroelectronics trusted execution environment security framework that is compliant with Arm® Platform Security Architecture (PSA) specifications for Cortex®-M (Armv8-M).
The Secure Manager is aiming at simplifying the security development cycle of embedded applications, by providing ready to use security services developed according to best practices.
Easy to install on STM32 products, the Secure Manager package offers a ready-to-use, high-performance and certified solution, supporting Secure Boot, root of trust, cryptography, internal trusted storage, initial attestation, as well as firmware update functions defined by the Arm® PSA specifications.
The Secure Manager main features are the following:
- Arm PSA standard and API compliancy
- Arm PSA services
- Secure Boot
- Cryptography
- Internal trusted storage
- Initial attestation
- Firmware update
- Multiple-tenant software IP protection
- Sandboxed secure services (PSA isolation level 3)
- Security certified (target)
- PSA Certified L3
- GlobalPlatform SESIP3
3. Secure Manager package ecosystem
The Secure Manager package is delivered with an ecosystem used to handle its life cycle.
This ecosystem is composed of:
- The Secure Manager access kit (SMAK): used to develop NS applications using Secure Manager services.
- The secure module development kit (SMDK): used to develop secure modules and associated APIs to access these modules from NS applications.
4. To go further
For details about Secure Manager generic solution, please see Secure Manager.
For details about SMAK for STM32H5, please see SMAK for STM32H5.
For details about SMDK for STM32H5, please see SMDK for STM32H5.
For details about Secure Manager manufacturing for STM32H5, please see SFI for STM32H5.
5. Getting started with Secure Manager
For an example on getting started with Secure Manager for STM32H5 MCUs, refer to the following pages:
Secure Manager STM32H5 How to Intro : Brief summary of the Secure Manager mechanism.
How to start with Secure Manager on STM32H573 Step by step lab to practice
6. References
- RM0481 STM32H5x3/562 reference manual
- UM2237 STM32CubeProgrammer software description
- UM2238 STM32TrustedPackageCreator tool software description
- AN5054 Secure programming using STM32CubeProgrammer
- AN2606 STM32 microcontroller system memory boot mode
- AN4992 STM32 MCUs secure firmware install (SFI) overview