This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
A set of practical trainings is proposed to get an overview and to understand the STM32H5 security solutions.
These trainings are based on the boards, tools and code examples provided by ST.
This article gives an overview of these proposed trainings.
For the examples listed below, each step to be done is described in detail.
It is advised to start with these examples before making your own trials or using other security related examples available in the STM32Cube_FW_H5.
In this article you will access the following security features of the STM32H5
Security functions embedded on: | |||
---|---|---|---|
Secure boot and firmware update | YES | YES | YES |
SBSFU legacy | YES | NO | NO |
SBSFU by mcuboot | NO | YES | YES |
STiROT | NO | YES | YES |
Isolation | YES | YES | YES |
HDP | YES | YES | YES |
TF-M | NO | YES | YES |
Secure manager | NO | NO | YES |
IP protection | YES | YES | YES |
Secure provisioning | YES | YES | YES |
Initial attesation | YES | YES | YES |
SMAK | NO | NO | YES |
SMDK | NO | NO | YES |
Cryptography | YES | YES | YES |
ST crypto lib | YES | YES | YES |
Crypto libraries | YES | YES | YES |
Crypto lib usage | YES | YES | YES |
Silicon device life cycle | YES | YES | YES |
Legacy RDP | NO | NO | NO |
Secure manufacturing | YES | YES | YES |
SFI | YES | YES | YES |
SFIx | YES | YES | YES |
Provisioning | YES | YES | YES |
Secure storage | NO | YES | YES |
Attestation | YES | YES | YES |
1. Secure Boot
pppppppp
1.1. Debug Authentication
pppppppp
1.2. OEMiROT
1.3. STiROT
2. Secure Manager
rrrr