Cellular X-CUBE-CELLULAR

Revision as of 11:42, 6 May 2020 by Registered User (→‎What is X-CUBE-CELLULAR)
Under construction.png Coming soon

Click here for Cellular overview

1. Introduction

This wiki page contains the information to ease the user's trip in ST Cellular software. When the information is already present in a databrief or a user manual, this wiki only redirects on those reference documents. So this wiki does not contain all the information but help you to find it.

2. What is X-CUBE-CELLULAR

What is X-CUBE-CELLULAR used for ? It is used to allow applications to send and receive data on the cellular network using BSD API sockets.

Do not forget the official web page on X-CUBE-CELLULAR on st.com. You will have access to multiple resources (software, documents, ...).

X-CUBE-CELLULAR consists of a set of libraries and application examples for STM32L4 Series MCUs acting as hosts for cellular connectivity applications.



The colors help to understand the different parts, Green for applications, light Blue for Middlewares, dark Blue for HAL, Purple for hardware.
Note that above the Cellular Middleware there is the Network_Library Middleware, it abstracts the cellular, Wifi, Ethernet ... So an application using Network_Library APIs, running on a bearer can be easily ported on another technology. Also note it is not mandatory to use Network_Library APIs, an application only using cellular can directly use X-CUBE-CELLULAR APIs.

3. Provided applications

Several applications are provided as examples:

  • PING Client application to test the access to a remote machine
  • ECHO Client application to provide an example of connection and data exchanges using the TCP or UDP (connected or not-connected mode) socket protocols
  • HTTP Client application to exchange data between the device and the cloud using HTTP protocol
  • MQTT Client application to exchange data between the device and the cloud using MQTT protocol (it uses TCP)
  • COM Client application to test the access to COM library services such as read information from ICC
  • CUSTOM Client application, an empty application already pre-integrated in X-CUBE-CELLULAR. It is provided to ease customers development.

By default, only one application is started at boot; ECHO Client.
Indeed PING Client is more a Command than an application so it starts when command is entered.
It is the same for COM Client, it is a Command.
HTTP Client is by default stopped, to start it just enter the following command: http on (http off to stop it)
CUSTOM Client must be activated with compilation switch, once activated by default this application only displays a message it is up to user to add his own content.
MQTT Client is more complicated to activate because it uses Network_Library and MbedTLS Middlewares but following the README.txt it is easy. see below for more details about MQTT

The X-CUBE-CELLULAR also contains modular tools like Command (to interact with the FW through terminal) and setup menu (to set parameters in the FW to avoid a new compilation)

4. What is the Getting started User Manual

This User Manual is an easy and quick document to read first. It explains the basis, Connect the HW, Activate the eSIM, Program the FW on the board and run it; all this in less than 10 pages.

5. How To ...

5.1. Introduction

This part is a guide to describe How To make main activities with X-CUBE-CELLULAR

5.2. ... start delivered Firmware binaries

A Firmware binaries is provided for each supported board. Summary to run the STM32L496 binary for BG96 modem follow the next steps: (Refer to UM2567 Getting started with the X-CUBE-CELLULAR cellular connectivity document for details)

  • insert an activated SIM in the BG96 modem
  • plug the BG96 modem on a STM32L496 board
  • plug an USB cable on the STM32L496 board (-> a new DIS_L496ZG volume appears on your PC)
  • flash the 32L496GDISCOVERY firmware
  • open a teraterm serial terminal and set the right parameters
  • enter right SIM APN using cellular setup menu
  • start the Firmware

5.3. ... access to the setup menu

The setup menu allows to update parameters of Firmware component and mainly cellular configuration (Refer to UM2567 Getting started with the X-CUBE-CELLULAR cellular connectivity document for details)

  • load a cellular firmware in the board flash.
  • open a open a teraterm serial terminal and set the right parameters.
  • reset the board and
  • select Cellular Service in Setup configuration menu
  • select the component configuration to update
  • the detail of menus and parameters is described in the Help option of the menus

5.4. ... set the SIM APN using the setup menu

Each operator own its APN. According to the SIM used the right APN must be set in the cellular configuration

  • start the setup menu (see above)
  • select Cellular Service in Setup configuration menu
  • type c to update configuration then the version number displayed
  • for each parameter (except APN), type enter to keep the default value (until the last parameter)
  • for the APN parameter type the right APN value (refer to SIM card)
  • start the Firmware

5.5. ... set the SIM APN by updating the plf_cellular_config.h file

According to the SIM/operator used, the cellular parameters can have to be updated in plf_cellular_config.h file that contains all the configurable cellular service parameters

5.6. ... know if the modem correctly configured after Firmware start

  • open a Teraterm serial terminal and set the right parameters.
  • start the Firmware
  • wait for the trace AUTOM TASK: MODEM_DATA_READY_STATE - NO_EVENT
  • The delay depends on Network attachment duration (from 30 seconds to several minutes)

5.7. ... to use console command commands to get modem and cellular network information

  • open a open a Teraterm serial terminal and set the right parameters.
  • remove trace display by typing commands
    • trace off
    • cst poll off
  • type the Cellular Service commands
    • cst
    • cst state
    • cst info
    • cst config

5.8. ... to configure modem radio band

  • open a Teraterm serial terminal and set the right parameters.
  • star firmware and select Modem power on option in the boot menu
  • type modem command to get help of modem configuration

5.9. ... to select components or application to include in cellular Firmware

The firmware can be customized by adding or removing some components or applications.
The configuration file plf_custom_config.h allows to select the component to include by define/undefine environment variables.
Refer to the User Manual document (UM2426) How to customize the software

5.10. ... to select the application to run

By default the delivered firmware contains several applications: httpclient, echoclient,...
Only echoclient application is activated by default at run time.
To activate/desactivate an application you can use the setup menu of the application.

  • go to to the setup menu of application to activate/desactivate
  • modify parameter: <application> enabled (or not) after boot

5.11. ... to add a personal application

Refer to the User Manual document (UM2426) How to customize the software for details. Sample applications are present in Middlewares\ST\STM32_Cellular\Samples\ directory. All these applications can be used as example. Custom sample is a template of application. All basic features are pre-configured (thread, Data Cache notification, commands, ...) You can develop your own application from this one.

5.12. ... to use MQTT client application

see detailed description below in this Wiki.

6. Setup for MQTT Client application

6.1. Introduction

As this application involves also the cloud, so 2 parts must be updated accordingly, the device (FW) part and the cloud (Server & Dashboard) part.

6.2. Device side

First, device side, either your FW already have the MQTT application activated or not. In case your FW have MQTT activated, you will only have to setup your personal parameter into the FW (using boot menu). If your FW is not yet MQTT enabled you must setup some parts in the source and rebuild (details below). During this setup you can choose to keep default values or decide to already provide your personal values (URL, login, password). If you know your personal values and decide to add them into the source file you will avoid to setup them manually at boot thanks the boot menu.

6.3. Cloud side

Cloud side, you have at least 2 possibilities, manual setup from scratch or use services that pre-install some configurations.

First solution, manually from scratch, 1/2 to 1h, for more advanced users:

  • setup a server instance on Internet
  • install MQTT server
  • install NodeRED server
  • configure NodeRED with json file provided by STMicroelectronics

2nd solution, less than 10mn, use pre-installed services from stackhero.io:

  • connect to https://www.stackhero.io
  • create an account
  • create a new stack, give it a name
  • select Node-RED by clicking on Start Node-RED
  • select an instance, Hobby is enough for this demo, click on Start now
  • in your stack you can see the Node-RED instance just created, select it
  • there are 2 URLs displayed to use first, Node-RED admin console and Node-RED dashboard (logins and passwords are in Configure item)
  • in one tab of you browser connect to Node-RED admin console, used to setup the Node-RED flow
  • in another tab connect to Node-RED dashboard, used to display the dashboard
  • in admin console import json file provided by STMicroelectronics (located into Utilities/MQTT/)
  • delete the 2 existing Flows (MQTT Auntentication & Flow 1)
  • Deploy the Node-RED, you can see the dashboard in the Dashboard tab of your browser
  • note your server address, example mqtts://yayer0.stackhero-network.com:8883/

Note that flows.json file is located here: Utilities/MQTT/flows.json in the X-CUBE-CELLULAR zip file. In this .json file we setup for user and password items a default user & password, it is user1 and 123abc, advice is to change it and to remove other users present in the list.

In case you don't receive email from stackhero to validate you account the reason could be that your email server blocks it. To solve this, just whitelist stackhero.io

Some video that illustrate the previous cloud steps with stackhero solution:

pc videol.png

How to create Node RED instance with Stackhero.io

pc videol.png

How to import json file in Node RED

pc videol.png

How to deploy and use the dashboard

pc videol.png

Where are MQTT login and password in Node RED

6.4. both sides

Whatever the solution you choose, you now need to provide server parameters to the STM32 FW. Those parameters are URL (something like yayer0.stackhero-network.com for stackhero solution or another url) user name (default is user1) and user password (default is 123abc) To update FW with thoses values, just use the boot menu.

6.5. How to modify the src files to add MQTT application in the FW

All the needed information for this can be found in the Readme file located in the zip file. The exact location is: \Middlewares\ST\STM32_Cellular\Samples\MQTT\README.txt

Indeed by MQTT example is not embedded in the default FW. However it is quick and simple to do this.

7. FAQ

Questions Answers
How to start Read UM 2567: Getting started and UM2426 for detailed explanations
Where to find the blueprint file for creating a Grovestreams organization? In \Middlewares\ST\STM32_Cellular\Samples\HTTP\Setup\Grovestreams_Blueprint.txt.
Where to find the text file for updating Grovestreams parameters? In \Middlewares\ST\STM32_Cellular\Samples\HTTP\Setup\Grovestreams_Setup.txt.
How to know if the cellular application is up and running? With the trace on Teraterm.
Nothing is displayed in Teraterm. Ensure that Teraterm options (such as Baud rate) are correctly set.
Wrong echo in Teraterm during setup. Ensure that Teraterm options (such as New-line and Transmit delay) are correctly set.
It boots but there is an issue with the network. Check that the correct SIM is selected (Plastic SIM or soldered UICC; Plastic SIM by default).
How to check that the EMnify profile on UICC is correctly activated? Connect to the EMnify account and check the status.
EMnify is correctly activated but it does not work. Check in the EMnify account if the correct tariff is selected.
The log indicates it is properly up and running but nothing change on Grovestreams dashboard. Check that the correct API keys are used (the ones associated with the organization used for the demonstration).
The voucher cannot be read because the initial image was overwritten (only for CELL01 and CELL02 kits). Browse to www.stm32-c2c.com, then download Restore factory firmware and flash it.
With the out-of-the-box FW, there is no information on the console. Set the correct parameter in Teraterm (Baud rate as 9600 to obtain the voucher) and make sure that the modem is not connected upside-down to the host board through the STMod+ connector.
Why cellular does is not operational after boot? There are multiple possibilities, the selected firmware does not correspond to the modem used, SIM card used is not valid on the available network, the modem firmware version see release note, too many bands selected and parsed by modem (see UM2567)
How to know if the cellular data service is operational Cellular operational after Trace displays -----> State : CST_MODEM_DATA_READY_STATE <-----
How to activate a 2nd C2C kit Once register on www.stm32-c2c.com note the BIC and connect directly on your EMnify account and ad the SIM with the BIC
What is the BIC It is not a bank number but only a Batch Identifier Code use at SIM creation