Secure Boot for STM32H5

Revision as of 17:11, 31 March 2023 by Registered User (Created page with "<big><big><big>''Secure Boot for STM32H5''</big></big></big> <br> <big><big>'''Target description'''</big></big><br> __TOC__ ==Intro== The secure boot ensures that applicat...")
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

Secure Boot for STM32H5

Target description

1. Intro

The secure boot ensures that applications are executed only after authentication and integrity verifications.

2. The different possible bootpaths for STM32H5

The possible bootpaths are depending on the chosen device, if it supports the embedded hardware cryptography and if Trust Zone is activated or not.

  • The STM32H57 is supporting TrustZone and hardware cryptography, so all bootpathes are possible with this device
  • The STM32H56 is supporting TrustZone but not the hardware cryptography (without export control constraints), so the STiROT (ST immutable Root of Trust) and the secure manager are not supported.
  • The STM32H503 is not supporting TrustZone and not supporting the hardware cryptography (without export control constraints), limiting the possible use cases as explained in next sections.

The bootpath is selected through option bytes programming, as explained in next sections.

2.1. STM32H57 Bootpaths

The STM32H57x devices support services available in the embedded system flash and services that can be installed. (add link to secure manager intro)
The figure below shows the possible bootpaths selected through the related user option bytes.

File:Bootpath1.png
Figure 1 STM32H57 possible bootpaths

2.2. STM32H56 Bootpaths

The STM32H6x is not supporting the STiROT and STuROT because the cryptographic hardware accelerator is not supported. The figure below shows the remaining possible bootpaths.

File:Bootpath2.png
Figure 2 STM32H56 possible bootpaths