Sensing and condition monitoring are two of the major components of the IoT and predictive maintenance systems, enabling context awareness, production performance improvement, a drastic decrease of the downtime due to routine maintenance, and so, maintenance cost reduction.
The FP-AI-MONITOR1 function pack is a Multi-sensor AI data monitoring framework on the wireless industrial node, function pack for STM32Cube. It helps to jump-start the implementation and development for sensor-monitoring-based applications designed with the X-CUBE-AI Expansion Package for STM32Cube or with the NanoEdge™ AI Studio. It covers the entire design of the Machine Learning cycle from the data set acquisition to the integration on a physical node.
The FP-AI-MONITOR1 runs learning and inference sessions in real-time on the SensorTile Wireless Industrial Node development kit (STEVAL-STWINKT1B), taking data from onboard sensors as input. The FP-AI-MONITOR1 implements a wired interactive CLI to configure the node and manages the learn and detect phases. For simple in the field operation, a standalone battery-operated mode allows basic controls through the user button, without using the console.
The STEVAL-STWINKT1B has an STM32L4R9ZI ultra-low-power microcontroller (Arm® Cortex®‑M4 at 120 MHz with 2 Mbytes of Flash memory and 640 Kbytes of SRAM). In addition, the STEVAL-STWINKT1B embeds industrial-grade sensors, including 6-axis IMU, 3-axis accelerometer and vibrometer and analog microphones to record any inertial, vibrational and acoustic data with high accuracy at high sampling frequencies.
The rest of the article discusses the following topics:
- The general information about the FP-AI-MONITOR1,
- Setting up the hardware and software components,
- Button-operated modes,
- Command-line interface (CLI),
- Human activity recognition, a classification application using accelerometer data,
- Anomaly detection using NanoEdge™ AI,
- Dual mode to run the anomaly detection using the NanoEdge AI library and state classification of a USB fan based on the ultra sonic data from analog microphone, using a pretrained model powered by X-CUBE-AI,
- Anomaly classification using NanoEdge™ AI classification libraries based on vibration and inertial data,
- Performing the data logging using onboard vibration sensors and a prebuilt binary of FP-SNS-DATALOG1, and
- Some links to useful online resources, to help a user better understand and customize the project for specific needs.
1. General information
1.1. Feature overview
- Complete firmware to program an STM32L4+ sensor node for sensor-monitoring-based applications on the STEVAL-STWINKT1B SensorTile wireless industrial node
- Runs classical Machine Learning (ML) and Artificial Neural Network (ANN) models generated by the X-CUBE-AI, an STM32Cube Expansion Package
- Runs NanoEdge™ AI libraries generated by NanoEdge™ AI Studio for AI-based anomaly detection applications. Easy integration by replacing the pre-integrated stub
- Application example of human activity classification based on motion sensors
- Application binary of high-speed datalogger for STEVAL-STWINKT1B data record from any combination of sensors and microphones configured up to the maximum sampling rate on a microSD™ card
- Sensor manager firmware module to configure any of the onboard sensors easily, and suitable for production applications
- eLooM (embedded Light object-oriented fraMework) enabling efficient development of soft real-time, multi-tasking, and event-driven embedded applications on STM32L4+ Series microcontrollers
- Digital processing unit (DPU) firmware module providing a set of processing blocks, which can be chained together, to apply mathematical transformations to the sensors data
- Configurable autonomous mode controlled by user button,
- Interactive command-line interface (CLI):
- Node and sensor configuration
- Configure application running either an X-CUBE-AI (ML or ANN) model, or a NanoEdge™ AI Studio anomaly detection model with the learn-and-detect capability
- Easy portability across STM32 microcontrollers using the STM32Cube ecosystem
- Free and user-friendly license terms
1.2. Software architecture
The top-level architecture of the FP-AI-MONITOR1 function pack is shown in the following figure.
The STM32Cube function packs leverage the modularity and interoperability of STM32 Nucleo and expansion boards running STM32Cube MCU Packages and Expansion Packages to create functional examples representing some of the most common use cases in certain applications. The function packs are designed to fully exploit the underlying STM32 ODE hardware and software components to best satisfy the final user application requirements.
Function packs may include additional libraries and frameworks, not present in the original STM32Cube Expansion Packages, which enable new functions and create more targeted and usable systems for developers.
STM32Cube ecosystem includes:
- A set of user-friendly software development tools to cover project development from the design to the implementation, among which are:
- STM32CubeMX, a graphical software configuration tool that allows the automatic generation of C initialization code using graphical wizards
- STM32CubeIDE, an all-in-one development tool with peripheral configuration, code generation, code compilation, and debug features
- STM32CubeProgrammer (STM32CubeProg), a programming tool available in graphical and command-line versions
- STM32CubeMonitor (STM32CubeMonitor, STM32CubeMonPwr, STM32CubeMonRF, STM32CubeMonUCPD) powerful monitoring tools to fine-tune the behavior and performance of STM32 applications in real-time.
- STM32Cube MCU & MPU Packages, comprehensive embedded-software platforms specific to each microcontroller and microprocessor series (such as STM32CubeL4 for the STM32L4+ Series), which include:
- STM32Cube hardware abstraction layer (HAL), ensuring maximized portability across the STM32 portfolio
- STM32Cube low-layer APIs, ensuring the best performance and footprints with a high degree of user control over the HW
- A consistent set of middleware components such as FreeRTOS™, USB Device, USB PD, FAT file system, Touch library, Trusted Firmware (TF-M), mbedTLS, Parson, and mbed-crypto
- All embedded software utilities with full sets of peripheral and application examples
- STM32Cube Expansion Packages, which contain embedded software components that complement the functionalities of the STM32Cube MCU & MPU Packages with:
- Middleware extensions and application layers
- Examples running on some specific STMicroelectronics development boards
To access and use the sensor expansion board, the application software uses:
- STM32Cube hardware abstraction layer (HAL): provides a simple, generic, and multi-instance set of generic and extension APIs (application programming interfaces) to interact with the upper layer applications, libraries, and stacks. It is directly based on a generic architecture and allows the layers that are built on it, such as the middleware layer, to implement their functions without requiring the specific hardware configuration for a given microcontroller unit (MCU). This structure improves library code reusability and guarantees easy portability across other devices.
- Board support package (BSP) layer: supports the peripherals on the STM32 Nucleo boards.
1.3. Folder structure
The figure above shows the contents of the function pack folder. The content of each of these subfolders is as follows:
- Documentation: contains a compiled
.chm
file generated from the source code, which details the software components and APIs. - Drivers: contains the HAL drivers, the board-specific drivers for each supported board or hardware platform (including the onboard components), and the CMSIS vendor-independent hardware abstraction layer for the Cortex®-M processors.
- Middlewares: contains libraries and protocols for ST parts as well as for the third parties. The ST components include the eLoom libraries, NanoEdge™ AI library stub, Audio Processing library, FFT library, and USB Device library.
- Projects: contains a sample application software, which can be used to program the sensor-board for classification and anomaly detection applications using the data from the motion sensors and manage the learning and detection phases of NanoEdge™ AI library provided for the STEVAL-STWINKT1B platforms through the STM32CubeIDE development environment.
- Utilities: contains python scripts and sample datasets. These python scripts can be used to create Human Activity Recognition (HAR) models using Convolutional Neural Networks (CNN) or Support Vector machine based Classifier (SVC). The FP-AI-MONITOR1 also enables a user to prepare the data logged using the High-Speed data logger on the STEVAL-STWINKT1B for the NanoEdge™ AI library generation.
1.4. Terms and definitions
Acronym | Definition |
---|---|
API | Application programming interface |
BSP | Board support package |
CLI | Command-line interface |
FP | Function pack |
HAL | Hardware abstraction layer |
MCU | Microcontroller unit |
ML | Machine learning |
AI | Artificial Intelligence |
SVC | Machine learning |
ANN | Artificial Neural Network |
CNN | Convolutional Neural Network |
ODE | Open development environment |
1.5. References
References | Description | Source |
---|---|---|
[1] | X-CUBE-AI | X-CUBE-AI |
[2] | NanoEdge™ AI Studio | st.com/nanoedge |
[3] | STEVAL-STWINKT1B | STWINKT1B |
1.6. Licenses
FP-AI-MONITOR1 is delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement (SLA0048).
The software components provided in this package come with different license schemes as shown in the table below.
Software component | Copyright | License |
---|---|---|
Arm® Cortex®-M CMSIS | Arm Limited | Apache License 2.0 |
FreeRTOS™ | Amazon.com, Inc. or its affiliates | MIT |
STM32L4xxx_HAL_Driver | STMicroelectronics | BSD-3-Clause |
Board support package (BSP) | STMicroelectronics | BSD-3-Clause |
STM32L4xx CMSIS | Arm Limited - STMicroelectronics | Apache License 2.0 |
eLooM application framework | STMicroelectronics | Proprietary |
Python TM scripts | STMicroelectronics | BSD-3-Clause |
Dataset | STMicroelectronics | Proprietary |
Sensor Manager | STMicroelectronics | Proprietary |
Audio preprocessing library | STMicroelectronics | Proprietary |
Generic FFT library | STMicroelectronics | Proprietary |
X-CUBE-AI runtime library | STMicroelectronics | Proprietary |
X-CUBE-AI HAR model | STMicroelectronics | Proprietary |
NanoEdge™ AI library stub | STMicroelectronics | Proprietary |
Signal processing library | STMicroelectronics | Proprietary |
Digital processing unit (DPU) | STMicroelectronics | Proprietary |
Trace analyzer recorder | Percepio AB | Percepio Proprietary |
2. Hardware and firmware setup
2.1. HW prerequisites and setup
To use the FP-AI-MONITOR1 function pack on STEVAL-STWINKT1B, the following hardware items are required:
- STEVAL-STWINKT1B development kit board,
- a microSD™ card and card reader to log and read the sensor data,
- Windows® powered laptop/PC (Windows® 7, 8, or 10),
- Two Micro USB cables, one to connect the sensor-board to the PC, and another one for the STLINK-V3MINI, and
- an STLINK-V3MINI.
2.1.1. Presentation of the Target STM32 board
The STWIN SensorTile wireless industrial node (STEVAL-STWINKT1B) is a development kit and reference design that simplifies the prototyping and testing of advanced industrial IoT applications such as condition monitoring and predictive maintenance. It is powered with Ultra-low-power Arm® Cortex®-M4 MCU at 120 MHz with FPU, 2048 kbytes Flash memory (STM32L4R9). Other than this, STWIN SensorTile is equipped with a microSD™ card slot for standalone data logging applications, a wireless BLE4.2 (on-board) and Wi-Fi (with STEVAL-STWINWFV1 expansion board), and wired RS485 and USB OTG connectivity, as well as Brand protection secure solution with STSAFE-A110. In terms of sensors, STWIN SensorTile is equipped with a wide range of industrial IoT sensors including:
- an ultra-wide bandwidth (up to 6 kHz), low-noise, 3-axis digital vibration sensor (IIS3DWB)
- a 6-axis digital accelerometer and gyroscope iNEMO inertial measurement unit (IMU) with machine learning (ISM330DHCX)
- an ultra-low-power high-performance MEMS motion sensor (IIS2DH)
- an ultra-low-power 3-axis magnetometer (IIS2MDC)
- a digital absolute pressure sensor (LPS22HH)
- a relative humidity and temperature sensor (HTS221)
- a low-voltage digital local temperature sensor (STTS751)
- an industrial-grade digital MEMS microphone (IMP34DT05), and
- a wideband analog MEMS microphone (MP23ABS1)
Other attractive features include:
- – a Li-Po battery 480 mAh to enable standalone working mode
- – STLINK-V3MINI debugger with programming cable to flash the board
- – a Plastic box for ease of placing and planting the SensorTile on the machines for condition monitoring. For further details, the users are advised to visit this link
2.2. Software requirements
2.2.1. FP-AI-MONITOR1
- Download the latest version of the FP-AI-MONITOR1, package from ST website, extract and copy the .zip file contents into a folder on the PC. The package contains binaries and source code, for the sensor-board STEVAL-STWINKT1B.
2.2.2. IDE
- One of the following IDEs must be installed:
- STMicroelectronics - STM32CubeIDE version 1.9.0,
- IAR Embedded Workbench for Arm (EWARM) toolchain version 9.20.1 or later,
- RealView Microcontroller Development Kit (MDK-ARM) toolchain version 5.32.
2.2.3. STM32CubeProgrammer
- STM32CubeProgrammer (STM32CubeProg) is an all-in-one multi-OS software tool for programming STM32 products. It provides an easy-to-use and efficient environment for reading, writing, and verifying device memory through both the debug interface (JTAG and SWD) and the bootloader interface (UART, USB DFU, I2C, SPI, and CAN). STM32CubeProgrammer offers a wide range of features to program STM32 internal memories (such as Flash, RAM, and OTP) as well as external memory.
- This software is available from STM32CubeProg.
2.2.4. Tera Term
- Tera Term is an open-source and freely available software terminal emulator, which is used to host the CLI of the FP-AI-MONITOR1 through a serial connection.
- Users can download and install the latest version available from Tera Term website.
2.2.5. STM32CubeMX
STM32CubeMX is a graphical tool that allows a very easy configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization C code for the Arm® Cortex®-M core or a partial Linux® Device Tree for Arm® Cortex®-A core), through a step-by-step process. Its salient features include:
- Intuitive STM32 microcontroller and microprocessor selection.
- Generation of initialization C code project, compliant with IAR™, Keil® and STM32CubeIDE (GCC compilers) for Arm®Cortex®-M core
- Development of enhanced STM32Cube Expansion Packages thanks to STM32PackCreator, and
- Integration of STM32Cube Expansion packages into the project.
To download the STM32CubeMX and obtain details of all the features please visit st.com.
2.2.6. X-Cube-AI
X-CUBE-AI is an STM32Cube Expansion Package part of the STM32Cube.AI ecosystem and extending STM32CubeMX capabilities with automatic conversion of pre-trained Artificial Intelligence models and integration of generated optimized library into the user project. The easiest way to use it is to download it inside the STM32CubeMX tool (version 7.0.0 or newer) as described in the user manual Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI) (UM2526). The X-CUBE-AI Expansion Package offers also several means to validate the AI models (both Neural Network and Scikit-Learn models) both on desktop PC and STM32, as well as to measure performance on STM32 devices (Computational and memory footprints) without ad-hoc handmade user C code.
2.2.7. Python 3.7.X
Python is an interpreted high-level general-purpose programming language. Python's design philosophy emphasizes code readability with its notable use of significant indentation. Its language constructs as well as its object-oriented approach aim to help programmers write clear, logical code for small and large-scale projects. To build and export the ONNX models the reader requires to set up a Python environment with a list of packages. The list of the required packages along with their versions is available as a text file in the package at location /FP-AI-MONITOR1_V1.1.0/Utilities/AI_resources/requirements.txt
. The following command is used in the command terminal of the anaconda prompt or Ubuntu to install all the packages specified in the configuration file requirements.txt
:
pip install -r requirements.txt
2.2.8. NanoEdge™ AI Studio
NanoEdge™ AI Studio is a new Machine Learning (ML) technology to bring true innovation easily to the end-users. In just a few steps, developers can create optimal ML libraries for Anomaly Detection, 1-class classification, n-class classification, and extrapolation, based on a minimal amount of data. The main features of NanoEdge AI Studio are:
- Desktop tool for design and generation of an STM32-optimized library for anomaly detection and feature classification of temporal and multi-variable signals
- Anomaly detection libraries are designed using very small datasets. They can learn normality directly on the STM32 microcontroller and detect defects in real-time
- Classification libraries are designed with a very small, labeled dataset. They classify signals in real-time
- Supports any type of sensor: vibration, magnetometer, current, voltage, multi-axis accelerometer, temperature, acoustic and more
- Explore millions of possible algorithms to find the optimal library in terms of accuracy, confidence, inference time, and memory footprint
- Generate very small footprint libraries running down to the smallest Arm® Cortex®-M0 microcontrollers
- Embedded emulator to test library performance live with an attached STM32 board or from test data files
- Easy portability across the various STM32 microcontroller series
This function pack supports the Anomaly Detection libraries generated by NanoEdge™ AI Studio for STEVAL-STWINKT1B. It facilitates users to log the data, prepare and condition it to generate the libraries from the NanoEdge™ AI Studio and then embed these libraries in the FP-AI-MONITOR1. NanoEdge™ AI Studio is available from www.st.com/stm32nanoedgeai under several options such as a single user or team license, or trial version, and personalized support based sprints.
2.3. Program firmware into the STM32 microcontroller
This section explains how to select a binary file for the firmware and program it into the STM32 microcontroller. A precompiled binary file is delivered as part of the FP-AI-MONITOR1 function pack. It is located in the FP-AI-MONITOR1_V1.1.0/Projects/STM32L4R9ZI-STWIN/Applications/FP-AI-MONITOR1/Binary/
folder. When the STM32 board and PC are connected through the USB cable on the STLINK-V3E connector, the STEVAL-STWINKT1B appears as a drive on the PC. The selected binary file for the firmware can be installed on the STM32 board by simply performing a drag and drop operation as shown in the figure below. This will create a dialog to copy the file and once it is disappeared (without any error) this indicates that the firmware is programmed in the STM32 microcontroller.
2.4. Using the serial console
A serial console is used to interact with the host board (Virtual COM port over USB). With the Windows® operating system, the use of the Tera Term software is recommended. Following are the steps to configure the Tera Term console for CLI over a serial connection.
2.4.1. Set the serial terminal configuration
Start Tera Term, select the proper connection (featuring the STMicroelectronics name),
Set the parameters:
- Terminal
- [New line]:
- [Receive]: CR
- [Transmit]: CR
- [New line]:
- Serial
- The interactive console can be used with the default values.
2.4.2. Start FP-AI-MONITOR1 firmware
Restart the board by pressing the RESET button. The following welcome screen is displayed on the terminal.
From this point, start entering the commands directly or type help to get the list of available commands along with their usage guidelines.
Note: The firmware provided is generated with a HAR model based on SVC and users can test it straight out of the box. However, for the NanoEdge™ AI Library, a stub is provided in place of the library. The user must generate the library with the help of the NanoEdge™ AI Studio, replace the stub with this library, and rebuild the firmware. These steps will be described in detail in the article later.
3. Button-operated modes
This section provides details of the button-operated mode for FP-AI-MONITOR1. The purpose of the extended mode is to enable the users to operate the FP-AI-MONITOR1 on STWIN even in the absence of the CLI console.
In button-operated mode, the sensor node can be controlled through the user button instead of the interactive CLI console. The default values for node parameters and settings for the operations during auto-mode are provided in the FW. Based on these configurations, different modes such as ai, neai_detect, and neai_learn can be started and stopped through the user button on the node.
3.1. Interaction with user
The button-operated mode can work with or without the CLI and is fully compatible and consistent with the current definition of the serial console and its command-line interface (CLI).
The supporting hardware for this version of the function-pack (STEVAL-STWINKT1B) is fitted with three buttons:
- User Button, the only button usable by the SW,
- Reset Button, connected to STM32 MCU reset pin,
- Power Button connected to power management,
and three LEDs:
- LED_1 (green), controlled by Software,
- LED_2 (orange), controlled by Software,
- LED_C (red), controlled by Hardware, indicates charging status when powered through a USB cable.
So, the basic user interaction for button-operated operations is to be done through two buttons (user and reset) and two LEDs (green and orange). The following provides details on how these resources are allocated to show the users what execution phases are active or to report the status of the sensor node.
3.1.1. LED Allocation
In the function pack four execution phases exist:
- idle: the system waits for user input.
- ai detect: all data coming from the sensors are passed to the X-CUBE-AI library to detect anomalies.
- neai learn: all data coming from the sensors are passed to the NanoEdge™ AI library to train the model.
- neai detect: all data coming from the sensors are passed to the NanoEdge™ AI library to detect anomalies.
At any given time, the user needs to be aware of the current active execution phase. We also need to report on the outcome of the detection when the detect execution phase is active, telling the user if an anomaly has been detected, or what activity is being performed by the user with the HAR application when the "ai" context is running.
The onboard LEDs indicate the status of the current execution phase by showing which context is running and also by showing the output of the context (anomaly or one of the four activities in the HAR case).
The green LED is used to show the user which execution context is being run.
Pattern | Task |
---|---|
OFF | - |
ON | IDLE |
BLINK_SHORT | X-CUBE-AI Running |
BLINK_NORMAL | NanoEdge™ AI learn |
BLINK_LONG | NanoEdge™ AI detection |
The Orange LED is used to indicate the output of the running context as shown in the table below:
Pattern | Reporting |
---|---|
OFF | Stationary if in X-CUBE-AI mode, Normal Behavior when in NEAI mode |
ON | Biking |
BLINK_SHORT | Jogging |
BLINK_LONG | Walking |
Looking at these LED patterns the user is aware of the state of the sensor node even when CLI is not connected.
3.1.2. Button Allocation
In the extended autonomous mode, the user can trigger any of the four execution phases. The available modes are:
- idle: the system is waiting for a command.
- ai: run the X-CUBE-AI library and print the results of the live inference on the CLI (if CLI is available).
- neai_learn: all data coming from the sensor is passed to the NanoEdge™ AI library to train the model.
- neai_detect: all data coming from the sensor is passed to the NanoEdge™ AI library to detect anomalies.
To trigger these phases, the FP-AI-MONITOR1 is equipped with the support of the user button. In the STEVAL-STWINKT1B sensor node, there are two software usable buttons:
- The user button: This button is fully programmable and is under the control of the application developer.
- The reset button: This button is used to reset the sensor node and is connected to the hardware reset pin, thus is used to control the software reset. It resets the knowledge of the NanoEdge™ AI libraries and reset all the context variables and sensor configurations to the default values.
To control the executions phases, we need to define and detect at least three different button press modes of the user button.
The following are the types of the press available for the user button and their assignments to perform different operations:
Button Press | Description | Action |
---|---|---|
SHORT_PRESS | The button is pressed for less than (200 ms) and released | Start AI inferences for X-CUBE-AI model. |
LONG_PRESS | The button is pressed for more than (200 ms) and released | Starts the learning for NanoEdge™ AI Library. |
DOUBLE_PRESS | A succession of two SHORT_PRESS in less than (500 ms) | Starts the inference for NanoEdge™ AI Library. |
ANY_PRESS | The button is pressed and released (overlaps with the three other modes) | Stops the current running execution phase. |
4. Command-line interface
The command-line interface (CLI) is a simple method for the user to control the application by sending command-line inputs to be processed on the device.
4.1. Command execution model
The commands are grouped into three main sets:
- (CS1) Generic commands
- This command set allows the user to get the generic information from the device like the firmware version, UID, compilation date and time, and so on, and to start and stop an execution phase.
- (CS2) AI commands
- This command set contains commands which are AI-specific. These commands enable users to work with the X-CUBE-AI and NanoEdge™ AI libraries.
- (CS3) Sensor configuration commands
- This command set allows the user to configure the supported sensors and to get the current configurations of these sensors.
4.2. Execution phases and execution context
The four system execution phases are:
- X-CUBE-AI: Data coming from the sensors is passed through the X-CUBE-AI models to run the inference on the HAR classification.
- NanoEdge™ AI learning: Data coming from the sensors is passed to the NanoEdge™ AI library to train the model.
- NanoEdge™ AI detection: Data coming from the sensors is passed to the NanoEdge™ AI library to detect anomalies.
Each execution phase can be started and stopped with a user command start <execution phase>
issued through the CLI.
An execution context, which is a set of parameters controlling execution, is associated with each execution phase. One single parameter can belong to more than one execution context.
The CLI provides commands to set and get execution context parameters. The execution context cannot be changed while an execution phase is active. If the user attempts to set a parameter belonging to any active execution context, the requested parameter is not modified.
4.3. Command summary
Command name | Command string | Note |
---|---|---|
CS1 - Generic commands | ||
help | help | Lists all registered commands with brief usage guidelines. Including the list of the applicable parameters. |
info | info | Shows firmware details and version. |
uid | uid | Shows STM32 UID. |
reset | reset | Resets the MCU system. |
CS2 - AI specific commands | ||
start | start <phase> | Starts an execution phase according to its execution context. Available execution phases are:
|
neai_init | neai_init | (Re)Initializes the NanoEdge™ AI model and forgets any learning made on the device. Used in the beginning or to reinit the NanoEdge™ AI anomaly detection to start from scratch at any time. |
neai_set | neai_set <parameter> <value> | Sets a NanoEdge AI specific parameter. Valid parameters and values are
|
neai_get | neai_get <parameter> | Displays the value of the NanoEdge AI parameter. Valid parameters are
|
ai_set | ai_set <parameter> <value> | Sets a X-CUBE-AI specific parameter. Valid parameters are
|
ai_get | ai_get <parameter> | Displays the value of the X-CUBE-AI parameters. Valid parameters are
|
dual_set | dual_set <parameter> <value> | Sets a dual AI specific parameter. Valid parameters and values are
sensor : sensor for classification, values can be integer [0, 4]. |
dual_get | dual_get <parameter> | Gets a dual AI specific parameter. Valid parameters could be
|
CS3 - Sensor configuration commands | ||
sensor_info | sensor_info | Get a list of all supported sensors and their ID. |
sensor_set | sensor_set <id> <parameter> <value> | Sets the value of a parameter for a sensor with sensor id provided in id. The settable parameters are
enable : active. |
sensor_get | sensor_get <id> <parameter> | Gets the value of a parameter for a sensor with sensor id provided in id. Valid parameters are:
|
4.4. Configuring the sensors
Through the CLI interface, a user can configure the supported sensors for sensing and condition monitoring applications. The list of all the supported sensors can be displayed on the CLI console by entering the command sensor_info
. This command prints the list of the supported sensors along with their ids as shown in the image below. The user can configure these sensors using these ids. The configurable options for these sensors include:
- enable: to activate or deactivate the sensor,
- ODR: to set the output data rate of the sensor from the list of available options, and
- FS: to set the full-scale range from the list of available options.
The current value of any of the parameters for a given sensor can be printed using the command,
$ sensor_get <sensor_id> <param>
or all the information about the sensor can be printed using the command:
$ sensor_get <sensor_id> all
Similarly, the values for any of the available configurable parameters can be set through the command:
$ sensor_set <sensor_id> <param> <val>
The figure below shows the complete example of getting and setting these values along with old and changed values.
5. Classification applications for sensing
5.1. Python Utilities for classification application
FP-AI-MONITOR1 comes equipped with two AI applications, a classification example for human activity recognition (HAR) based on X-CUBE-AI and an anomaly detection example based on NanoEdge™ AI. This section describes the HAR classification application.
FP-AI-MONITOR1 comes with a Python utility code to generate the AI models for HAR both based on artificial neural networks and classical machine learning models using scikit-learn. These scripts are located under the FP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/Training Scripts/HAR/
directory. The following figure shows the contents of the utilities.
The utilities include two folders, AI_Resources (all the Python resources related to AI) and DataLog (binary and helper scripts for High-Speed Datalogger). In the AI_Resources there are subdirectories of
- Dataset: Contains different datasets/holders for the datasets used in the function pack
- models: Contains the pre-generated and trained models for HAR along with their C-code
- NanoEdgeAi: Contains the helper scripts to prepare the data for the NanoEdge™ AI Studio from the HSDatalogs
- signal_processing_lib: Contains the code for various signal processing modules (there is equivalent embedded code available for all the modules in the function pack)
- Training Scripts: Contains the Python scripts for HAR examples using SVC, CNN, and NEAI.
The HAR subdirectory at the path FP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/Training Scripts/HAR/
contains three Jupyter notebooks:
- HAR_with_CNN.ipynb (a complete step-by-step code to build an HAR model based on Convolutional Neural Networks),
- HAR_with_SVC.ipynb (a complete step-by-step code to build an HAR model based on Support Vector Machine Classifier), and
- HAR_with_NEAI.ipynb (a complete step-by-step code to build NanoEdge™ AI Studio compliant files for all activities).
The FP-AI-MONITOR1 comes with a prebuilt model for HAR based on SVC for recognizing four activities, namely [Stationary, Walking, Jogging, Biking]. The following figure shows a complete flow of building an HAR application using CNN or SVC, generating the C-code using X-CUBE-AI and embedding it in the FP-AI-MONITOR1, installing it and then finally running the inference on the edge.
The Jupyter Notebooks in FP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/Training Scripts/HAR/
directory contain very detailed step-by-step processes to create SVC, CNN, and NEAI based HAR applications. This section describes briefly the steps to build this application in Python using the CNN and SVC scripts provided in this directory (yellow part). The steps are listed in the figure below:
The steps include:
- Segmenting the data into segments of length 24 (any segment length can be used depending on the requirements, but the length used in this case is the length based on a famous model architecture).
- Preprocess and condition the data, the gravity rotation is applied to the z-axis and suppression (any preprocessing chain can be applied depending on the user needs)
- a set of DSP feature extraction is provided in the subdirectory signal_processing_lib along with the equivalent embedded implementation.
- Model building and optimization (learning)
- In the case of CNN, this step includes building topology and training the weights.
- In the case of SVC, this step includes finding the best hyperparameters for the model definition and performing the best dimension reduction to have the smallest models providing the best performance.
- Validating the model using the unseen/test data.
- Exporting the trained model as .h5 (in case of CNN) or .onnx (in case of SVC).
The next section shows how to take these pre-trained models and convert them into optimized C-code using X-CUBE-AI. The code can then be embedded and installed into the sensor-board to run the inferences on the edge.
5.2. Generating C-code for the AI model using STM32 X-CUBE-AI
This section explains how to generate the code for a pre-trained AI model using STM32 X-CUBE-AI. For this purpose, the code is generated using the .h5 model provided. The readers can generate C-code for any .h5 or .onnx model using this method.
The following list gives a step-by-step guide for generating the C-code for the h5 model.
Step1 : Open the STM32CubeMX and click on the ACCESS TO BOARD SELECTOR
button as shown in the image below.
Step2 : Create a new project for STEVAL-STWINKT1B:
- Confirm the board selector tab is selected,
- Search for the right board, and in our case it is the
STEVAL-STWINKT1B
, by typing the name in the search bar, - Select the board by clicking on either the board image or the name of the board,
- Start Project, and
- Chose
NO
for the Peripheral initialization option as this is not required for our purpose.
Step3 : Configuring connectivity
- Click on the connectivity option in the left menu
- Select USART2
- Enable the "Asynchronous mode" by selecting it in the drop-down menu.
Step4 : Add the X-CUBE-AI in the software packs for the project
- Click on the
Software Packs
, and select theSelect Components
option - Click on the
STMicroelectronics X-CUBE-AI
. UseVersion 7.0.0
as preference but any version from 7.0 or later can be used, - Click on checkbox in front of
Core
to add the X-CUBE-AI code in the software stack. - Expand the
Device Application
menu and from the drop-down menu under selection column selectSystemPerformance
. - Click
OK
button to finish the addition of the X-CUBE-AI in the project.
Step 5 : Platform Settings
- Click on
Software Packs
, - Choose STMicroelectronics.X-CUBE-AI,
- Select
USART: Asynchronous
option for the COM Port, - Select USART2 in "Found Solutions" drop-down.
Step6 : Adding network for code generation
- Click on the add network button,
- From drop down select the type of the network. For the applications in this function pack these can be
Keras
orONNX
- Click on the
Browse
button to select the model. - The example in the figure below shows the
har_IGN.h5
being used, which is located underFP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/models
. Select the model and click OK.
Step7 : Generating the C-code
- Go to
Project Manager
- Assign a "Project Name", in the figure below it is
FP-AI-MONITOR1_AI-Code-Generation
- Choose a Project Location, in the figure below it is C:/Temp/
- Click on the GENERATE CODE button. A progress bar will start and shows progress across the different code generation steps.
- Upon completion of the code generation process the user will see a dialog as in the figure below. This shows completion of the code generation. Click on the Open Folder button to open the project with the generated code.
- The files present for the network model that have to be replaced in the provided project are located in the following directory:
FP-AI-MONITOR1_AI-Code-Generation_X-CUBE-AI/App/
as shown in the figure below.
The next section shows how these files are used to replace the existing model embedded in the FP-AI-MONITOR1 software step-by-step and install it on the sensor-board.
5.3. Replacing the prebuilt classification AI model with generated one
The prebuilt model provided in the CLI example binary is based on the Support Vector Classifier (SVC). The Python script along with detailed instructions on how to prepare the dataset, build the model, and convert it to onnx is provided in the Jupyter Notebook available in /FP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/Training Scripts/HAR/HAR_With_SVC.ipynb
. The building of these models and C-code generation is out of the scope of this article and readers are invited to refer to the user manual for detailed instructions. This article describes how a user replaces the default model provided in the function pack with a custom generated model once the C-code using the STM32CubeMX extension X-CUBE-AI is generated. In this example the provided SVC model is replaced with the prebuilt and converted CNN model provided in the /FP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/models/IGN4class/
folder. The details on the data used for training and the topology are located in the training scripts provided under /FP-AI-MONITOR1_V1.1.0/Utilities/AI_Resources/Training Scripts/HAR/HAR_With_CNN.ipynb
.
To update the model, the user must copy and replace following files in the /FP-AI-MONITOR1_V1.1.0/Projects/STM32L4R9ZI-STWIN/Applications/FP-AI-MONITOR1/X-CUBE-AI/App/
folder as shown in the figure above:
- app_x-cube-ai.c,
- app_x-cube-ai.h,
- network.c,
- network.h,
- network_config.h,
- netowrk_data.h,
- network_generate_report.h.
Once the files are copied, the user must open the project with the CubeIDE. To do so, go to the /FP-AI-MONITOR1_V1.1.0/Projects/STWINL4R9ZI-STWIN/Applications/FP-AI-MONITOR1/STM32CubeIDE/
folder and double click .project file as shown in the figure below.
Once the project is opened, go to FP-AI-MONITOR1_V1.1.0/Projects/STM32L4R9ZI-STWIN/Application/FP-AI-MONITOR1/X-CUBE-AI/App/app_x-cube-ai.c
file and comment the following lines of the code as shown in the figure below.
5.3.1. Building and installing the project
Then build and install the project in STWIN sensor-board by pressing the play button as shown in the figure below.
A message saying Download verified successfully indicates the new firmware is programmed in the sensor-board.
5.4. Running the AI application
The CLI application comes with a prebuilt Human Activity Recognition model. This functionality is started by typing the command:
$ start ai
Note that the provided HAR model is built with a dataset created using the IHM330DHCX_ACC sensor with ODR = 26, and FS = 4. To achieve the best performance, the user must set these parameters to the sensor configuration using the sensor_set command as provided in the Command Summary table.
Running the $ start ai
command starts doing the inference on the accelerometer data and predicts the performed activity along with the confidence. The supported activities are:
- Stationary,
- Walking,
- Jogging, and
- Biking.
The following figure is a screen shot of the normal working session of the AI command in CLI application.
6. Condition monitoring using NanoEdge™ AI Machine Learning library
This section provides a complete anomaly detection method using the NanoEdge™ AI library. FP-AI-MONITOR1 includes a pre-integrated stub which is easily replaced by an AI condition monitoring library generated and provided by NanoEdge™ AI Studio. This stub simulates the NanoEdge™ AI-related functionalities, such as running learning and detection phases on the edge.
The learning phase is started by issuing a command $ start neai_learn
from the CLI console or by long-pressing the [USR] button. The learning process is reported either by slowly blinking the green LED light on STEVAL-STWINKT1B or in the CLI as shown below:
$ CTRL: ! This is a stubbed version, please install NanoEdge AI library ! NanoEdge AI: learn {"signal": 1, "status": need more signals} {"signal": 2, "status": need more signals} : : {"signal": 10, "status": need more signals} {"signal": 11, "status": success} {"signal": 12, "status": success} {"signal": 13, "status": success} : : : End of execution phase
The CLI shows that the learning is to be performed for at least 10 signals and reports that more signals are needed until it has learned 10 signals. After 10 signals are learned, the status message of learning changes to success for every learning of the new signal. The learning can be stopped by pressing the ESC key on the keyboard or simply by pressing the [USR] button.
Similarly, the user starts the condition monitoring process by issuing the command $ start neai_detect
command or by double-pressing the [USR] button. This starts the inference phase and checks the similarity of the presented signal with the learned normal signals. If the similarity is less than the set threshold default: 90%
, a message is printed in the CLI showing the occurrence of an anomaly along with the similarity of the anomaly signal.
The process is stopped by pressing the ESC key on the keyboard or pressing the [USR] button.
This behavior is shown in the snippet below:
$ start neai_detect NanoEdge AI: starting detect phase. $ CTRL: ! This is a stubbed version, please install NanoEdge AI library ! NanoEdge AI: detect {"signal": 1, "similarity": 0, "status": anomaly} {"signal": 2, "similarity": 1, "status": anomaly} {"signal": 3, "similarity": 2, "status": anomaly} : : {"signal": 90, "similarity": 89, "status": anomaly} {"signal": 91, "similarity": 90, "status": anomaly} {"signal": 102, "similarity": 0, "status": anomaly} {"signal": 103, "similarity": 1, "status": anomaly} {"signal": 104, "similarity": 2, "status": anomaly} End of execution phase
Other than CLI, the status is also presented using the LED lights on the STEVAL-STWINKT1B. Fast blinking green LED light shows the detection is in progress. Whenever an anomaly is detected, the orange LED light is blinked twice to report an anomaly.
NOTE : This behavior is simulated using a STUB library where the similarity starts from 0 when the detection phase is started and increments with the signal count. Once the similarity is reached to 100 it resets to 0. One can see that the anomalies are not reported when similarity is between 90 and 100.
The following section shows how to generate an anomaly detection library using NanoEdge™ AI Studio and install and test it on STEVAL-STWINKT1B using FP-AI-MONITOR1. The steps are provided with brief details in the following figure.
6.1. Generating a condition monitoring library
6.1.1. Data logging for normal and abnormal conditions
The details on how to acquire the data are provided in the section data logging using HSDatalog.
6.1.2. Data preparation for library generation with NanoEdge™ AI Studio
The data logged through the datalogger is in the binary format and is not user readable nor compliant with the NanoEdge™ AI Studio format as it is. To convert this data to a useful form, users have two options.
- Using the provided Python™ utility scripts on the path
/FP-AI-MONITOR1_V1.1.0/Utilities/AI-resources/NanoEdgeAi/
.- The Jupyter Notebook
NanoEdgeAI_Utilities.ipynb
provides a complete example of data preparation for a three-speed fan library generation running in normal and clogged conditions. In addition, there is anHSD_2_NEAISegments.py
provided if the user wants to prepare segments for given data acquisition. This script is used by issuing the following command for a data acquisition withISM330DHCX_ACC
sensor. >> python HSD_2_NEAISegments.py ../Datasets/Fan12CM/ISM330DHCX/normal/1000RPM/
command will generate a file named asISM330DHCX_Cartesiam_segments_0.csv
using the default parameter set. The file is generated with segments of length1024
and stride1024
plus the first512
samples are skipped from the file.- If multiple acquisitions are used to acquire the data for the normal and abnormal conditions once the files
*_Cartesiam_segments_0.csv
are generated for different acquisitions, all the files for normal can be combined in a single file, and all the files for the abnormal in another file. This way the user has to provide only one normal and abnormal file to Studio.
- The Jupyter Notebook
- Using the [FROM SD CART (.DAT)] option in the data import in NanoEdge AI™ Studio
- In the latest version of NanoEdge™ AI Studio it is possible to read the data from the acquisition directory of the HSDatalog directly.
- NOTE: In case there are multiple acquisitions for the normal behaviors, this has to be done for all the acquisitions, and for every normal acquisition added an abnormal acquisition is to be added also to create a pair.
6.1.3. Library generation using NanoEdge™ AI Studio
Running the scripts in Jupyter Notebook will generate the normal_WL1024_segments.csv
and clogged_WL1024_segments.csv
files. This section describes how to generate the libraries using these normal and abnormal files.
The NanoEdge AI Studio can generate libraries for four types namely:
- Anomaly Detection
- 1-Class Classification
- n-Class Classification
- Extrapolation
In FP-AI-MONITOR1 users can only use the Anomaly Detection libraries. To generate the anomaly detection library the first step is to create the project by clicking on the button for AD as shown in the figure below. The text shows the information on what Anomaly Detection is good for, and the project can be created by clicking on the CREATE NEW PROJECT button.
The process to generate the anomaly detection library consists of six steps as described in the figure below:
- Project Settings
- Choose a project name and description.
- Hardware Configurations
- Choosing the target STM32 platform or a microcontroller type: STEVAL-STWINKT1B Cortex-M4 is selected by default. If that is not the case select STEVAL-STWINKT1B from the list provided in the drop-down menu under Target.
- Maximum amount of RAM to be allocated for the library: Usually, a few Kbytes is enough (but it depends on the data frame length used in the process of data preparation, 32 Kbytes is a good starting point).
- Putting a limit or no limits for the Maximum Flash budget
- Sensor type: 3-axis accelerometer is selected by default. If that is not the case select 3-axis accelerometer from the list in the drop-down under Sensor type.
- Providing the sample contextual data for normal segments to adjust and gauge the performance of the chosen model. Two options are available:
- Provide directly an acquisition directory generated from the HSDatalog, (with all the
*****.dat
andDeviceConfig.json
files unchanged), or - Provide the
normal_WL1024_segments.csv
generated using Jupyter notebook,
- Provide directly an acquisition directory generated from the HSDatalog, (with all the
- Providing the sample contextual data for abnormal segments to adjust and gauge the performance of the chosen model. Two options are available:
- Provide directly an acquisition directory generated from the HSDatalog, (with all the
*****.dat
andDeviceConfig.json
files unchanged), or - Provide the
clogged_WL1024_segments.csv
generated using Jupyter notebook,
- Provide directly an acquisition directory generated from the HSDatalog, (with all the
- Benchmarking of available models and choosing the one that complies with the requirements and provides the best performance.
- Validating the model for learning and testing through the provided emulator which emulates the behavior of the library on the STM32 target.
- The final step is to compile and download the libraries. In this process, the flag
"-mfloat-abi"
has to bechecked
for using libraries with hardware FPU. All the other flags can be left to the default state.- Note for using the library with μKeil also check -fshort-wchar in addition to -mfloat-abi.
Detailed documentation on the NanoEdge™ AI Studio.
.6.2. Installing the NanoEdge™ Machine Learning library
Once the libraries are generated and downloaded from NanoEdge™ AI Studio, the next step is to link these libraries to FP-AI-MONITOR1 and run them on the STWIN. The FP-AI-MONITOR1, comes with the library stubs in the place of the actual libraries generated by NanoEdge™ AI Studio. This is done to simplify the linking of the generated libraries. In order to link the actual libraries, the user needs to copy the generated libraries and replace the existing stub/dummy libraries and header files NanoEdgeAI.h
, and libneai.a
files present in the folders Inc
, and lib
, respectively. The relative paths of these folders are /FP_AI_MONITOR1_V1.1.0/Middlewares/ST/NanoEdge_AI_Library/
as shown in the figure below.
Once these files are copied, the project must be reconstructed and programmed on the sensor board to link the libraries correctly. For this, the user must open the project in STM32CubeIDE located in the /FP-AI-MONITOR1_V1.1.0/Projects/STWINL4R9ZI-STWIN/Applications/FP-AI-MONITOR1/STM32CubeIDE/
folder and double click .project file as shown in the figure below.
To build and install the project click on the play button and wait for the successful download message as shown in the section Build and Install Project.
Once the sensor-board is successfully programmed, the welcome message appears in the CLI (Tera Term terminal). If the message does not appear try to reset the board by pressing the RESET button.
6.3. Testing the NanoEdge™ AI Machine Learning library
Once the STWIN is programmed with the FW containing a valid library, the condition monitoring libraries are ready to be tested on the sensor board. The learning and detection commands can be issued and now the user will not see the warning of the stub presence.
To achieve the best performance, the user must perform the learning using the same sensor configurations which were used during the contextual data acquisition. For example in the snippet below users can see commands to configure ISM330DHCX sensor with sensor_id 1 with following parameters:
- enable = 1
- ODR = 1666,
- FS = 4.
$ sensor_set 1 enable 1 sensor 1: enable $ sensor_set 1 ODR 1666 nominal ODR = 1666.00 Hz, latest measured ODR = 0.00 Hz $ sensor_set 1 FS 4 sensor FS: 4.00
6.4. Additional parameters in condition monitoring
For user convenience, the CLI application also provides handy options to easily fine-tune the inference and learning processes. The list of all the configurable variables is available by issuing the following command:
$ neai_get all NanoEdgeAI: signals = 0 NanoEdgeAI: sensitivity = 1.000000 NanoEdgeAI: threshold = 95 NanoEdgeAI: timer = 0
Each of the these parameters is configurable using the neai_set <param> <val>
command.
This section provides information on how to use these parameters to control the learning and detection phase. By setting the "signals" and "timer" parameters, the user can control how many signals or for how long the learning and detection is performed (if both parameters are set the learning or detection phase stops whenever the first condition is met). For example, to learn 10 signals, the user issues this command, before starting the learning phase as shown below.
$ neai_set signals 10 NanoEdge AI: signals set to 10 $ start neai_learn NanoEdgeAI: starting $ {"signal": 1, "status": success} {"signal": 2, "status": success} {"signal": 3, "status": success} : : {"signal": 10, "status": success} NanoEdge AI: stopped
If both of these parameters are set to "0" (default value), the learning and detection phases will run indefinitely.
The threshold
parameter is used to report any anomalies. For any signal which has similarities below the threshold value, an anomaly is reported. The default threshold value used in the CLI application is 90. Users can change this value by using neai_set threshold <val>
command.
Finally, the sensitivity parameter is used as an emphasis parameter. The default value is set to 1. Increasing this sensitivity will mean that the signal matching is to be performed more strictly, reducing it will relax the similarity calculation process, i.e. resulting in higher matching values.
For further details on how NanoEdge™ AI libraries work users are invited to read the detailed documentation of NanoEdge™ AI Studio.
7. Data collection
The data collection functionality is out of the scope of this function pack, however, to simplify this for the users this section provides the step-by-step guide to log the data on STEVAL-STWINKT1B using the high-speed data logger.
Step 1: Program the STEVAL-STWINKT1 with the HSDatalog FW
In the scope of this function pack and article, the STEVAL-STWINKT1 can be programmed with HSDatalog firmware in two ways.
- Using the binary provided in the function pack
- To simplify the task of the users and to allow them the possibility to perform a data log, the precompiled
HSDatalog.bin
file for FP-SNS-DATALOG1 is provided in theUtilities
directory, which is located under path/FP-AI-MONITOR1_V1.1.0/Utilities/Datalog/
. The sensor tile can be programmed by simply following the drag-and-drop action shown in section 2.3.
- To simplify the task of the users and to allow them the possibility to perform a data log, the precompiled
- Using the NanoEdge AI Studio
- The new version of NanoEdgeTM AI Studio has a new feature to program the high-speed datalogger in the STEVAL-STWINKT1B. To do this follow the steps in the figure below.
- click on the Datalogger button in the home menu,
- connect the STEVAL-STWINKT1B to the computer as shown in the figure below (connect the USB to STWIN first and STLINK after),
- wait for the status to change to connect,
- click the LOAD BINARY button,
- weight for the Success message,
- the STWIN is now programmed with the high-speed datalogger firmware.
- The new version of NanoEdgeTM AI Studio has a new feature to program the high-speed datalogger in the STEVAL-STWINKT1B. To do this follow the steps in the figure below.
Step 2: Place a DeviceConfig.json
file on the SD card
The next step is to copy a DeviceConfig.json
on the SD card. This file contains the sensors configurations to be used for the data logging. These sample files can be either:
- interactively generated through studio by clicking on the Configure datalogger button in the datalogger menu as shown in the figure below, or,
- the users can simply use one of the provided some sample
.json
files in the package inFP-AI-MONITOR1_V1.1.0/Utilities/Datalog/Sample_STWIN_Config_Files/
directory.
Step 3: Insert the SD card into the STWIN board Insert an SD card in the STEVAL-STWINKT1B sensor tile.
Step 4: Reset the board
Reset the board. Orange LED blinks once per second. The custom sensor configurations provided in DeviceConfig.json
are loaded from the file.
Step 5: Start the data log
Press the [USR] button to start data acquisition on the SD card. The orange LED turns off and the green LED starts blinking to signal sensor data is being written into the SD card.
Step 6: Stop the data logging
Press the [USR] button again to stop data acquisition. Do not unplug the SD card, turn the board off or perform a [RESET] before stopping the acquisition otherwise the data on the SD card will be corrupted.
Step 7: Retrieve data from SD card
Remove the SD card and insert it into an appropriate SD card slot on the PC. The log files are stored in STWIN_###
folders for every acquisition, where ###
is a sequential number determined by the application to ensure log file names are unique. Each folder contains a file for each active sub-sensor called SensorName_subSensorName.dat
containing raw sensor data coupled with timestamps, a DeviceConfig.json
with specific information about the device configuration (confirm if the sensor configurations in the DeviceConfig.json
are the ones you desired), necessary for correct data interpretation, and an AcquisitionInfo.json
with information about the acquisition.
- FP-AI-MONITOR1: Multi-sensor AI data monitoring framework on wireless industrial node, function pack for STM32Cube
- Quick Start Guide: QSG for FP-AI-MONITOR1
- How to perform anomaly detection using FP-AI-MONITOR1 : A step-by-step guide to implement an Anomaly Detection solution for a USB powered fan.
- STEVAL-STWINKT1B: STWIN SensorTile Wireless Industrial Node development kit
- STM32CubeMX: STM32Cube initialization code generator
- X-CUBE-AI : expansion pack for STM32CubeMX
- NanoEdge™ AI Studio: NanoEdge™ AI the first Machine Learning Software, specifically developed to entirely run on microcontrollers.
- DB4345: Data brief for STEVAL-STWINKT1B.
- UM2777: How to use the STEVAL-STWINKT1B SensorTile Wireless Industrial Node for condition monitoring and predictive maintenance applications.