How to use Teachable Machine to create an image classification application on STM32

Revision as of 18:43, 12 June 2020 by Registered User (β†’β€ŽSTM32H747I-DISCO)

This article shows how to use the Teachable Machine online tool with STM32Cube.AI and the FP-AI-VISION function pack to create an image classifier running on the STM32H747I-DISCO board.

This tutorial is divided into three parts: we will first see how to use the Teachable Machine to train and export a deep learning model, then STM32Cube.AI will be used to convert this model into optimized C code for STM32 MCUs. In the last part, we will see how to integrate this new model into the FP-AI-VISION1 to run live inference on an STM32 board with a camera. The whole process is described below:

CLI_as_back-end
Teachable Machine with STM32 workflow


Info white.png Information
  • Teachable Machine is an online tool allowing to quickly train a deep learning model for various tasks including image classification. It is an educational tool not suitable for production purposes.
  • STM32Cube.AI is a software aiming at the generation of optimized C code for STM32 for neural network inference. It is delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement (SLA0048).
  • The FP-AI-VISION1 Function Pack is a software example of an image classifier running on the STM32H747I-DISCO board. It is delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement (SLA0048)

1. Prerequisites

1.1. Hardware

1.2. Software

2. Train a model using Teachable Machine

In this section, we will train deep neural network in the browser using Teachable Machine. We first need to choose something to classify. In the example below, we will classify ST boards and modules. The chosen boards are shown in the figure below:

Boards used for classification
Boards used for classification

You can choose whatever object you want to classify it: fruits, pasta, animals, people, etc...

Info white.png Information
Note: If you do not have any webcam, Teachable Machine allows to import images from your computer.

Let's get started. Open https://teachablemachine.withgoogle.com/, preferably from Chrome browser.

Click Get started, then select Image Project. You will be presented with the following interface.

Teachable Machine interface
Teachable Machine interface

2.1. Add training data

For each category you want to classify, edit the class name by clicking the pencil icon. In this example, we choose to start with SensorTile.

To add images with your webcam, click the webcam icon and record some images. If you have image files on your computer, click upload and select the directory containing your images.

Adding images with a webcam
Adding images with a webcam
Info white.png Information
No need to capture too many images, ~100 images per class is usually well enough. Try to vary camera angle, subject pose and scale as much as possible. To obtain the best results, a uniform background is recommended.

Once you have a satisfactory amount of images for this class, repeat the process for the next one until your dataset is complete.

Info white.png Information
Note: It can be nice to have a "Background/Nothing" class, so that the model is able to tell when nothing is presented to the camera.

2.2. Train the model

Now that we have a good amount of data, we are going to train a deep learning model for classifying these different objects. To do this, click the Train Model button as shown below:

Train a model
Train a model

This process can take a while, depending on the amount of data you have. To monitor the training progress, you can select Advanced and click Under the hood. A side panel displays training metrics.

When the training is complete, you can see the predictions of your network on the "Preview" panel. You can either choose a webcam input or an imported file.

Predictions from the model
Predictions from the model

2.2.1. What happens under the hood (for the curious)

Teachable Machine is based on Tensorflow.js to allow neural network training and inference in the browser. However, as image classification is a task that requires a lot of training time, Teachable Machine uses a technique called transfer learning: The webpage downloads a MobileNetV2 model that was previously trained on a big image dataset of 1000 categories. The convolution layers of this pre-trained model are very good at doing feature extraction so they do not need to be trained again. Only the last layers of the neural network are trained using Tensorflow.js, thus saving a lot of time.

2.3. Export the model


If you are happy with your model, it is time to export it. To do so, click the Export Model button. In the pop-up window, select Tensorflow Lite, check Quantized and click Download my model.

Export the model
Export the model

The model conversion is done in the cloud. This step can take a few minutes.

Your browser downloads a zip file containing the model as a .tflite file and a .txt file containing your label. Extract these two files in an empty directory that we will call workspace for the rest of this tutorial.

2.3.1. Inspect the model using Netron (optional)

It is always interesting to take a look at a model architecture, as well as its input and output formats and shapes. To do this, use the Netron webapp.

Visit https://lutzroeder.github.io/netron/ and select Open model, then choose the model.tflite file from Teachable Machine. Click sequental_1_input: we observe that the input type is uint8 and size [1, 244, 244, 3]. Now let's look at outputs: in this example we have 6 classes, so we see that the output shape s [1,6]. The quantization parameters are also reported. Refer to part 3 for how to use them.

Model visualization
Model visualization

3. Porting to target

3.1. STM32H747I-DISCO

In this part we will use the stm32ai command line tool to convert the TensorflowLite model to optimized C code for STM32.

Warning white.png Warning
Warning: FP-AI-VISION1 v1.1.0 is based on X-Cube-AI version 5.0.0. You can check your version of Cube.AI by running stm32ai --version


Start by opening a shell in your workspace directory, then execute the following command:

 cd <path to your workspace>
 stm32ai generate -m model.tflite -v 2

The expected output is:

Neural Network Tools for STM32 v1.2.0 (AI tools v5.0.0)
Running "generate" cmd...
-- Importing model
 model files : /path/to/workspace/model.tflite
 model type  : tflite (tflite)
-- Importing model - done (elapsed time 0.531s)
-- Rendering model
-- Rendering model - done (elapsed time 0.184s)
-- Generating C-code
Creating /path/to/workspace/stm32ai_output/network.c
Creating /path/to/workspace/stm32ai_output/network_data.c
Creating /path/to/workspace/stm32ai_output/network.h
Creating /path/to/workspace/stm32ai_output/network_data.h
-- Generating C-code - done (elapsed time 0.782s)

Creating report file /path/to/workspace/stm32ai_output/network_generate_report.txt

Exec/report summary (generate dur=1.500s err=0)
-----------------------------------------------------------------------------------------------------------------
model file         : /path/to/workspace/model.tflite
type               : tflite (tflite)
c_name             : network
compression        : None
quantize           : None
L2r error          : NOT EVALUATED
workspace dir      : /path/to/workspace/stm32ai_ws
output dir         : /path/to/workspace/stm32ai_output

model_name         : model
model_hash         : 2d2102c4ee97adb672ca9932853941b6
input              : input_0 [150,528 items, 147.00 KiB, ai_u8, scale=0.003921568859368563, zero=0, (224, 224, 3)]
input (total)      : 147.00 KiB
output             : nl_71 [6 items, 6 B, ai_i8, scale=0.00390625, zero=-128, (6,)]
output (total)     : 6 B
params #           : 517,794 items (526.59 KiB)
macc               : 63,758,922
weights (ro)       : 539,232 (526.59 KiB) 
activations (rw)   : 853,648 (833.64 KiB) 
ram (total)        : 1,004,182 (980.65 KiB) = 853,648 + 150,528 + 6

------------------------------------------------------------------------------------------------------------------
id  layer (type)               output shape      param #     connected to             macc           rom          
------------------------------------------------------------------------------------------------------------------
0   input_0 (Input)            (224, 224, 3)                                                                      
    conversion_0 (Conversion)  (224, 224, 3)                 input_0                  301,056                     
------------------------------------------------------------------------------------------------------------------
1   pad_1 (Pad)                (225, 225, 3)                 conversion_0                                         
------------------------------------------------------------------------------------------------------------------
2   conv2d_2 (Conv2D)          (112, 112, 16)    448         pad_1                    5,820,432      496          
    nl_2 (Nonlinearity)        (112, 112, 16)                conv2d_2                                             
------------------------------------------------------------------------------------------------------------------

( ... )

------------------------------------------------------------------------------------------------------------------
71  nl_71 (Nonlinearity)       (1, 1, 6)                     dense_70                 102                         
------------------------------------------------------------------------------------------------------------------
72  conversion_72 (Conversion) (1, 1, 6)                     nl_71                                                
------------------------------------------------------------------------------------------------------------------
model p=517794(526.59 KBytes) macc=63758922 rom=526.59 KBytes ram=833.64 KiB io_ram=147.01 KiB

 
Complexity per-layer - macc=63,758,922 rom=539,232
------------------------------------------------------------------------------------------------------------------
id      layer (type)               macc                                    rom                                    
------------------------------------------------------------------------------------------------------------------
0       conversion_0 (Conversion)  ||                                0.5%  |                                 0.0% 
2       conv2d_2 (Conv2D)          |||||||||||||||||||||||||         9.1%  |                                 0.1% 
3       conv2d_3 (Conv2D)          ||||||||||                        3.5%  |                                 0.0% 
4       conv2d_4 (Conv2D)          |||||||                           2.5%  |                                 0.0% 
5       conv2d_5 (Conv2D)          ||||||||||||||||||||||||||        9.4%  |                                 0.1% 
7       conv2d_7 (Conv2D)          |||||||                           2.6%  |                                 0.1% 

( ... )

64      conv2d_64 (Conv2D)         ||||                              1.5%  |||||                             3.7% 
65      conv2d_65 (Conv2D)         |                                 0.3%  |                                 0.8% 
66      conv2d_66 (Conv2D)         ||||||||                          2.9%  ||||||||                          7.1% 
67      conv2d_67 (Conv2D)         |||||||||||||||||||||||||||||||  11.3%  |||||||||||||||||||||||||||||||  27.5% 
69      dense_69 (Dense)           |                                 0.2%  ||||||||||||||||||||||||||       23.8% 
70      dense_70 (Dense)           |                                 0.0%  |                                 0.1% 
71      nl_71 (Nonlinearity)       |                                 0.0%  |                                 0.0% 
------------------------------------------------------------------------------------------------------------------

This command will generate 4 files:

  • network.c
  • network_data.c
  • network.h
  • network_data.h

under workspace/stm32ai_ouptut/.

Let's take a look at the highlighted lines: we learn that the model uses 526.59 Kbytes of weights (read-only memory) and 833.54 Kbytes of activations. As the STM32H747xx MCUs do not have 833 Kbytes of contiguous RAM, we need to use the external SDRAM present on the STM32H747-DISCO board. Refer to UM2411 section 5.8 "SDRAM" for more information.

3.1.1. Integration with FP-AI-VISION1

In this part we will import our brand new model into the FP-AI-VISION1 function pack. This function pack provides a software example for a food classification application. For more information on FP-AI-VISION1, refer to here.

The main objective of this step is to replace the network and network_data files in FP-AI-VISION1 by the newly generated files and make a few adjustments to the code.

3.1.1.1. Open the project

If it is not already done, download the zip file from ST website and extract the content to your workspace. It must now contain the following elements:

  • model.tflite
  • labels.txt
  • stm32ai_output
  • FP_AI_VISION1

If we take a look inside the function pack, we see two configurations for the model data type, as shown below.

FP-AI-VISION1 model data types
FP-AI-VISION1 model data types

Our model is a quantized one, so we choose the Quantized_Model directory.

Go into workspace/FP_AI_VISION1/Projects/STM32H747I-DISCO/Applications/FoodReco_MobileNetDerivative/Quantized_Model/STM32CubeIDE/STM32H747I_DISCO and double-click on .project. STM32CubeIDE starts with the project loaded.

3.1.1.2. Replace the network files

The model files are located in workspace/FP_AI_VISION1/Projects/STM32H747I-DISCO/Applications/FoodReco_MobileNetDerivative/Quantized_Model/CM7/ Src and Inc directory.

Delete the following files and replace them with the ones from workspace/stm32ai_output:

In Src:

  • network.c
  • network_data.c

In Inc:

  • network.h
  • network_data.h

3.1.1.3. Update the labels

In this step we will updates the labels for the network output. The label.txt file downloaded with Teachable Machine can help you doing this. In our example, the content of this file looks like this:

0 SensorTile
1 IoTNode
2 STLink
3 Craddle Ext
4 Fanout
5 Background

From STM32CubeIDE, open fp_vision_app.c. Go to line 129 where the g_food_classes is defined and update this variable with our label names:

// fp_vision_app.c line 129
const char* g_food_classes[AI_NET_OUTPUT_SIZE] = {
    "SensorTile", "IoTNode", "STLink", "Craddle Ext", "Fanout", "Background"};

3.1.1.4. Update the output format

In the original code, the neural network output is in floating point format (ai_float). With Teachable Machine, the output is an 8-bit integer (ai_i8). Update the code consequently.

In fp_vision_app.c line 97 modify the line as follows:

// fp_vision_app.c line 97
// ai_float nn_output_buff[AI_NET_OUTPUT_SIZE] = {0}; // Old code
ai_i8 nn_output_buff[AI_NET_OUTPUT_SIZE] = {0}; // New code code

Apply this change to fp_vision_app.h as well. You can open the file from the Include directory in the Project Explorer as shown bellow.

// fp_vision_app.h line 48
//extern ai_float nn_output_buff[]; // Old code
extern ai_i8 nn_output_buff[]; // New code

3.1.1.5. Dequantize the output

The last operation that needs to be done is the dequantization of the output from the model. As we can see from the output of stm32ai, the output is quantized in 8-bit signed integer format with the following parameters:

scale = 0.00390625
zero_point = -128

The formula for converting quantized to real is the following:

π‘…π‘’π‘Žπ‘™ = π‘†π‘π‘Žπ‘™π‘’ Γ— (π‘„π‘’π‘Žπ‘›π‘‘π‘–π‘§π‘’π‘‘ βˆ’ π‘π‘’π‘Ÿπ‘œπ‘ƒπ‘œπ‘–π‘›π‘‘)

Let's apply this transformation to the code: open main.c and visit the AI_Output_Display() function located line 562.

Just before calling the BubbleSort() function, perform the dequantization: add the following lines and update the BublleSort() call as following:

/* Added lines */
const ai_i32 zero_point = -128;
const ai_float scale = 0.00390625f;

ai_float float_output[NN_OUPUT_CLASS_NUMBER];

for(int i = 0; i < NN_OUPUT_CLASS_NUMBER; i++){
    float_output[i] = scale * ( (ai_float) (NN_OUTPUT_BUFFER[i]) - zero_point);
}
/* End added lines */

Bubblesort(float_output, ranking, NN_OUPUT_CLASS_NUMBER); /* Updated line */
Info white.png Information
For the sake of simplicity in this tutorial, we hardcode the values for zero_point and scale. However, it is cleaner to retrieve them through the API exposed by network.c. Refer to STM32Cube.AI documentation for details on how to do this.

We still need to add two modifications to this function:

  • First update the display mode by setting display_mode to 1 in order to see the image and label on the LCD display.
  • Then use float_output in the display function (as shown below).

All the modifications are highlighted in the snippet below

/**
 * Copyright (c) 2020 STMicroelectronics. All rights reserved.
 *
 * This software component is licensed by ST under Ultimate Liberty license
 * SLA0044, the "License"; You may not use this file except in compliance with
 * the License. You may obtain a copy of the License at:
 *                             www.st.com/SLA0044
 */

 /* (...) */

static void AI_Output_Display(void)
{
  static uint32_t occurrence_number = NN_OUTPUT_DISPLAY_REFRESH_RATE;
  static uint32_t display_mode=1; /* Updated line */

  occurrence_number--;

  if (occurrence_number == 0)
  {
    char msg[70];

    int ranking[NN_OUPUT_CLASS_NUMBER];
    occurrence_number = NN_OUTPUT_DISPLAY_REFRESH_RATE;

    for (int i = 0; i < NN_OUPUT_CLASS_NUMBER; i++)
    {
      ranking[i] = i;
    }
    /* Added lines */
    const ai_i32 zero_point = -128;
    const ai_float scale = 0.00390625f;

    ai_float float_output[NN_OUTPUT_CLASS_NUMBER];

    for(int i = 0; i < NN_OUPUT_CLASS_NUMBER; i++){
        float_output[i] = scale * ( (ai_float) (NN_OUTPUT_BUFFER[i]) - zero_point);
    }
    /* End added lines */

    Bubblesort(float_output, ranking, NN_OUPUT_CLASS_NUMBER); /* Updated line */
    
    /*Check if PB is pressed*/
    if (BSP_PB_GetState(BUTTON_WAKEUP) != RESET)
    {
      display_mode = !display_mode;
      
      BSP_LCD_Clear(LCD_COLOR_BLACK);
      
      if (display_mode == 1)
      {
        sprintf(msg, "Entering CAMERA PREVIEW mode");
      }
      else  if (display_mode == 0)
      {
        sprintf(msg, "Exiting CAMERA PREVIEW mode");
      }
      
      BSP_LCD_DisplayStringAt(0, LINE(9), (uint8_t*)msg, CENTER_MODE);
      
      sprintf(msg, "Please release button");
      BSP_LCD_DisplayStringAt(0, LINE(11), (uint8_t*)msg, CENTER_MODE);
      LCD_Refresh();
      
      /*Wait for PB release*/
      while (BSP_PB_GetState(BUTTON_WAKEUP) != RESET);
      HAL_Delay(200);
      
      BSP_LCD_Clear(LCD_COLOR_BLACK);
    }
    
    if (display_mode == 0)
    {
      BSP_LCD_Clear(LCD_COLOR_BLACK);/*To clear the camera capture*/
      
      DisplayFoodLogo(LCD_RES_WIDTH / 2 - 64, LCD_RES_HEIGHT / 2 -100, ranking[0]);
    }
    else  if (display_mode == 1)
    {      
      sprintf(msg, "CAMERA PREVIEW MODE");
      
      BSP_LCD_DisplayStringAt(0, LINE(DISPLAY_ACQU_MODE_LINE), (uint8_t*)msg, CENTER_MODE);
    }
  
    for (int i = 0; i < NN_TOP_N_DISPLAY; i++)
    {
      sprintf(msg, "%s %.0f%%", NN_OUTPUT_CLASS_LIST[ranking[i]], float_output[i] * 100); /* Updated Line */
      BSP_LCD_DisplayStringAt(0, LINE(DISPLAY_TOP_N_LAST_LINE - NN_TOP_N_DISPLAY + i), (uint8_t *)msg, CENTER_MODE);
    }

    sprintf(msg, "Inference: %ldms", *(NN_INFERENCE_TIME));
    BSP_LCD_DisplayStringAt(0, LINE(DISPLAY_INFER_TIME_LINE), (uint8_t *)msg, CENTER_MODE);

    sprintf(msg, "Fps: %.1f", 1000.0F / (float)(Tfps));
    BSP_LCD_DisplayStringAt(0, LINE(DISPLAY_FPS_LINE), (uint8_t *)msg, CENTER_MODE);

    LCD_Refresh();

    /* (...) */


3.1.1.6. Crop the image

Teachable Machine crops the webcam image to fit the model input size. In FP-AI-VISION1, the image is resized to the model input size, hence losing the aspect ratio, we will change this default behavior and implement a crop of the camera image.

In order to have square image and avoid image deformation we are going to crop the camera image using the DCMI. The goal of this step is to go from the 640x480 resolution to a 480x480 resolution.

First, edit fp_vision_app.h line 148 to update the CAMERA_WIDTH define to 480 pixels:

/****************************/
/***CAMERA related defines***/
/****************************/
#if CAMERA_CAPTURE_RES == VGA_640_480_RES
#define CAMERA_RESOLUTION RESOLUTION_R640x480
#define CAM_RES_WIDTH 480 /* was 640 */
#define CAM_RES_HEIGHT 480

Then, edit stm32h747i_discovery_camera_patch.c located in Drivers/BSP/STM32H747I_DISCO

Modify the BSP_CAMERA_Init function to configure DCMI cropping:

/**
  * @brief  Initializes the camera.
  * @param  Resolution : camera sensor requested resolution (x, y) : standard resolution
  *         naming QQVGA, QVGA, VGA ...
  * @retval Camera status
  */
uint8_t BSP_CAMERA_Init(uint32_t Resolution)
{
  DCMI_HandleTypeDef *phdcmi;
  uint8_t status = CAMERA_ERROR;

  /* Get the DCMI handle structure */
  phdcmi = &hdcmi_discovery;

  /*** Configures the DCMI to interface with the camera module ***/
  /* DCMI configuration */
  phdcmi->Init.CaptureRate      = DCMI_CR_ALL_FRAME;
  phdcmi->Init.HSPolarity       = DCMI_HSPOLARITY_LOW;
  phdcmi->Init.SynchroMode      = DCMI_SYNCHRO_HARDWARE;
  phdcmi->Init.VSPolarity       = DCMI_VSPOLARITY_HIGH;
  phdcmi->Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;
  phdcmi->Init.PCKPolarity      = DCMI_PCKPOLARITY_RISING;
  phdcmi->Instance              = DCMI;

  /* Power up camera */
  BSP_CAMERA_PwrUp();

  /* Read ID of Camera module via I2C */
  if(ov9655_ReadID(CAMERA_I2C_ADDRESS) == OV9655_ID)
  {
    /* Initialize the camera driver structure */
    camera_drv = &ov9655_drv;
    CameraHwAddress = CAMERA_I2C_ADDRESS;

    /* DCMI Initialization */
    BSP_CAMERA_MspInit(&hdcmi_discovery, NULL);
    HAL_DCMI_Init(phdcmi);

    /* Camera Module Initialization via I2C to the wanted 'Resolution' */
    if (Resolution == CAMERA_R480x272)
    {     /* For 480x272 resolution, the OV9655 sensor is set to VGA resolution
           * as OV9655 doesn't supports 480x272 resolution,
           * then DCMI is configured to output a 480x272 cropped window */
      camera_drv->Init(CameraHwAddress, CAMERA_R640x480);
      HAL_DCMI_ConfigCROP(phdcmi,           /* Crop in the middle of the VGA picture */
                         (CAMERA_VGA_RES_X - CAMERA_480x272_RES_X)/2,
                         (CAMERA_VGA_RES_Y - CAMERA_480x272_RES_Y)/2,
                         (CAMERA_480x272_RES_X * 2) - 1,
                          CAMERA_480x272_RES_Y - 1);
      HAL_DCMI_EnableCROP(phdcmi);
    }
    else
    {
      camera_drv->Init(CameraHwAddress, Resolution);
      /* Removed  HAL_DCMI_DisableCROP(phdcmi); */

      HAL_DCMI_ConfigCROP(phdcmi,           /* Crop in the middle of the VGA picture */
                         (CAMERA_VGA_RES_X - 480)/2,
                         (CAMERA_VGA_RES_Y - 480)/2,
                         (480 * 2) - 1,
                          480 - 1);

      HAL_DCMI_EnableCROP(phdcmi);

    }

    CameraCurrentResolution = Resolution;

    /* Return CAMERA_OK status */
    status = CAMERA_OK;
  }
  else
  {
    /* Return CAMERA_NOT_SUPPORTED status */
    status = CAMERA_NOT_SUPPORTED;
  }

  const uint8_t MVFP_REG = 0x1E;
  CAMERA_IO_Write(CameraHwAddress, MVFP_REG, 0x30);
  return status;
}


Lastly, in the same file, update the BSP_CAMERA_ContinuousStart function to start the DMA transfert with the correct size:

/**
  * @brief  Starts the camera capture in continuous mode.
  * @param  buff: pointer to the camera output buffer
  * @retval None
  */
void BSP_CAMERA_ContinuousStart(uint8_t *buff)
{
  /* Start the camera capture */
  /* Removed HAL_DCMI_Start_DMA(&hdcmi_discovery, DCMI_MODE_CONTINUOUS, (uint32_t)buff, GetSize(CameraCurrentResolution)); */
  HAL_DCMI_Start_DMA(&hdcmi_discovery, DCMI_MODE_CONTINUOUS, (uint32_t)buff, 480*480/2);
}

Now cropping is enabled and the image is square.

3.1.2. Compile the project

The function pack for quantized models comes in 4 memory configurations :

  • Quantized_Ext
  • Quantized_Int_Fps
  • Quantized_Int_Mem
  • Quantized_Int_Split

As we saw in Part 2, the activation buffer takes more than 800 KB of RAM, for this reason, we can only use the Quantized_Ext configuration in order to place activation buffer. For more details on the memory configuration, refer to UM2611 section 3.2.4 "Memory requirements".

In order to compile only the Quantized_Ext configuration, select Project > Properties from the top bar. Then select C/C++ Build from the left pane. Click on manage configuration and then delete all configurations which are not Quantized_Ext. You should be left with only one configuration.

Memory configuration settings
Memory configuration settings

Clean the project by selecting Project > Clean... and clicking Clean.

Finally, build the project clicking on Project > Build All.

At the end of compilation, a file named STM32H747I_DISCO_CM7.hex is generated in

workspace > FP_AI_VISION1 > Projects > STM32H747I-DISCO > Applications > FoodReco_MobileNetDerivative > Quantized_Model > STM32CubeIDE > STM32H747I_DISCO > Quantized_Ext

3.1.3. Flash the board

Connect the STM32H747I-DISCO to your PC via a micro-USB to USB cable. Open STM32CubeProgrammer and connect to ST-LINK. Then flash the board with the hex file.

3.1.4. Test the model

Plug the camera to the STM32H747I-DISCO board using a flex cable. In order the have the image in the upright position, the camera should be placed with the flex cable facing up as shown in the figure below. Once the camera is connected, power the board and press the reset button. After the "Welcome Screen", you will see the camera preview and output prediction of the model on the LCD Screen.

File:tm output.png
Model inference running on target

3.2. Troubleshooting

You may notice that once the model is running on STM32, the performance of the deep learning model is not as expected. This can be explained by a few things.

  • Quantization: The quantization process can reduce the performance of the model, as going from a 32-bit floating point to a 8-bit integer representation means a loss of precision.
  • Camera: The webcam used for training the model is different from the the camera on the DISCO board. This difference of data between the training and the inference can explain a loss of performance.