1. Heart rate profile
Heart Rate Profile (HRP) [1] is a generic attribute profile (GATT) based low-energy profile defined by the Bluetooth® Special Interest Group[2]
The HRP, widely used in fitness applications, defines the communication process between a GATT-server of a Heart Rate Sensor device, such as a wrist band, and a GATT-client Collector device, such as a smartphone or tablet.
- The Heart Rate Sensor:
- Measures the heart rate and exposes it via the Heart Rate Service[3].
- Contains the Device Information Service that includes information, for example, about the manufacturer of the device.
- Is the GATT server.
- The Heart Rate Collector:
- Accesses the information exposed by the heart rate sensor. It can display it to the end user, or store it on a nonvolatile memory for later analysis.
- Is the GATT client.
The description of the Heart Rate Sensor project provided within the STM32CubeWBA MCU Package[4] is below.
Bluetooth® Low Energy Heart Rate Profile & STM32WBA |
---|
The table below describes the structure of Heart Rate Sensor services:
Bluetooth® Low Energy Heart Rate Service specification | |||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
The Heart Rate Profile is a combination of a Heart Rate Collector and a Heart Rate Sensor. The goal is to connect and exchange data in different applications.
The GAP - Generic Access Profile defines and manages advertising and connection.
Collector Central device and Sensor Peripheral device |
---|
The GATT - Generic Attribute Profile defines and manages in/out data exchange.
Collector GATT client device and Sensor GATT service device |
---|
Example of flow diagram between STM32WBA & ST BLE Toolbox |
---|
1.1. Advertising Data
At start up, the Heart Rate Sensor application starts a fast advertising(80ms/100ms).
Data advertised are composed as follow:
Heart Rate Advertising packet | ||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
The manufacturer data are encoded following STMicroelectronics BlueST SDK v2 as described below:
STMicroelectronics Manufacturer Advertising data | |||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Advertising is switched to Low Power advertising (1s/2.5s) after 60s.
1.2. On board button configuration
Heart Rate Sensor application Nucleo-WBA button configuration | ||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
2. Requirements
2.1. Software and system requirements
The required softwares are the following ones (minimum IDEs version):
- IAR Embedded Workbench for ARM (EWARM) toolchain V9.20.1, plus a patch available in WBA Firmware Package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/EWARMv8_STM32WBAx_V1.2.zip
- RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.37, plus a patch available in WBA Firmware package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/Keil.STM32WBAx_DFP.1.0.0.zip
- STM32CubeIDE toolchain V1.12.0 [5].
The required programmer is the following one:
- STM32CubeProgrammer[6] : To flash the board with an already generated binary
2.2. Hardware requirements
The board NUCLEO-WBA5[7] is required to install the application.
Hardware platform illustration |
---|
|
2.3. Collector applications compatible
The STM32CubeWBA Heart Rate Sensor project is compatible with the following collectors:
3. STM32WB Heart Rate Sensor example description
3.1. Project directory
The "BLE_HeartRate" application is available by downloading STM32CubeWBA MCU Package[8].
Refer to How to Build a Bluetooth® LE project wiki page for project directory information.
3.2. Project description
3.2.1. Structure
Software project structure with the most important parts:
Heart Rate project structure |
---|
WARNING: Do not modify the files in Middlewares folder |
3.2.2. Application initialization
The different steps of the application initialization are described below:
Heart Rate project initialization |
---|
3.2.3. GAP and GATT initialization and interaction
and The Bluetooth LE Heart Rate Sensor application initialization is done within app_ble.c
- Initialize the BLE stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init()
- Call the services controller initialization SVCCTL_Init() - svc_ctl.c
- Manage the GAP event - SVCCTL_App_Notification()
- HCI_LE_CONNECTION_COMPLETE - provides information of the connection interval, slave latency, supervision timeout
- HCI_LE_CONNECTION_UPDATE_COMPLETE- provides the new information of the connection
- HCI_DISCONNECTION_COMPLETE - informs the application about the link disconnection and the reason
The Services management is done by the service controller, svc_ctl.c
- Initialize the number of registered handler - SVCCTL_Init()
- Manage events - SVCCTL_UserEvtRx()- from the BLE Host Stack and redirect them to the gap event handler - SVCCTL_App_Notification
The application level of the Heart Rate Sensor is done with hrs_app.c:
- Initialization of the services:
- Heart Rate Service - HRS_Init() - hrs.c
- Initialization of the context of the application
- Measurement value flags support
- Body sensor location - HRS_BODY_SENSOR_LOCATION_HAND
- Receive notification from the Heart Rate Service - HRS_Notification()
- When Heart rate measurement characteristics are enabled by the remote, simulate every 1 s the Heart Rate Measure (HRS_APP_Measurement) and increase the energy expended to transfer to the remote device (collector) - HRS_UpdateValue()
The Heart Rate Service hrs.c manages the specification of the service:
- Service Init - HRS_Init()
- Register Heart Rate Event Handle to Service Controller - SVCCTL_RegisterSvcHandler(HRS_EventHandler);
- Initialize Service UUID – add Heart Rate service as Primary services
- Initialize Heart rate measurement characteristic
- Initialize Body Sensor location characteristic
- Manage the GATT event from BLE Stack - HRS_EventHandler()
- ACI_GATT_WRITE_PERMIT_REQ_VSEVT_CODE
- Reception of a Write Command: HR Control Point Characterictic Value
- Send an aci_gatt_write_response() with an OK or KO status.
- Notify the application to Reset Energy Expended - HRS_Notification(HRS_RESET_ENERGY_EXPENDED_EVT)
- Reception of a Write Command: HR Control Point Characterictic Value
- ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
- Reception of an attribute modification - HR Measurement Characteristics Description Value : ENABLE or DISABLE Notification
- Notify application of the Measurement Notification - HRS_Notification(HRS_NOTIFICATION_ENABLED/DISABLED)
- Reception of an attribute modification - HR Measurement Characteristics Description Value : ENABLE or DISABLE Notification
- ACI_GATT_WRITE_PERMIT_REQ_VSEVT_CODE
Heart Rate Sensor software module interaction |
---|
3.3. How to use
Once the BLE Heart Rate application is installed on the STM32WBA platform, launch ST BLE Sensor or ST BLE ToolBox smartphone application. Then, scan and connect the device called HR_XX (where XX is replaced by the last byte of the BD address) to the application.
Once the Bluetooth® LE connection is established and the notification enabled by the smartphone:
- Heart Rate measurement is provided to remote every 1 s.
- thanks to the timer server and the task manager
BLE Heart Rate application support the pairing procedure
- Pressing B2 while not connected allows to clear the security database
- Pressing B2 while connected allows to request pairing
With the WBA5x.Nucleo board, it is also possible to change RF PHY modulation
- Pressing B1 while connected allows to switch between 2 Mbits and 1 Mbits PHY
BLE Heart Rate application allows other actions on button:
- Pressing B1 while not connected allows to restart the fast advertising
- Pressing B3 while connected allows to update the connection interval
3.4. Optimize low power
The project is delivered with the full system low-power enabled:
- no debug trace
- no debugger
It is possible to enable/disable the Low Power feature within app_conf.h
/******************************************************************************
* Low Power
*
* When CFG_FULL_LOW_POWER is set to 1, the system is configured in full
* low power mode. It means that all what can have an impact on the consumptions
* are powered down.(For instance LED, Access to Debugger, Etc.)
*
* When CFG_FULL_LOW_POWER is set to 0, the low power mode is not activated
*
******************************************************************************/
#define CFG_FULL_LOW_POWER (1)
3.5. UART debug trace
Thanks to the debug log via UART interface , it is possible to trace the application project.
To enable the traces within the project, enable them within app_conf.h as described below:
/**
* Enable or Disable traces in application
*/
#define CFG_DEBUG_APP_TRACE (0)
Debugger can also be supported by enabling it within app_conf.h as described below:
/**
* User interaction
* When CFG_LED_SUPPORTED is set, LEDS are activated if requested
* When CFG_BUTTON_SUPPORTED is set, the push button are activated if requested
* When CFG_DBG_SUPPORTED is set, the debugger is activated
*/
[...]
#define CFG_DBG_SUPPORTED (1)
Heart Rate Sensor - Initialization phase | Connected Phase |
---|---|
==>> Start Ble_Hci_Gap_Gatt_Init function Success: hci_reset command Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET Public Bluetooth Address: 00:80:e1:2a:7c:ea Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET Success: aci_hal_set_tx_power_level command Success: aci_gatt_init command Success: aci_gap_init command Success: aci_gatt_update_char_value - Device Name Success: aci_gatt_update_char_value - Appearance Success: hci_le_set_default_phy command Success: aci_gap_set_io_capability command Success: aci_gap_set_authentication_requirement command Success: aci_gap_configure_whitelist command ==>> End Ble_Hci_Gap_Gatt_Init function Services and Characteristics creation Success: aci_gatt_add_service command: HRS Success: aci_gatt_add_char command : HRME Success: aci_gatt_add_char command : BSL Success: aci_gatt_add_char command : HRCP Success: aci_gatt_update_char_value BSL command Success: aci_gatt_add_service command: DIS Success: aci_gatt_add_char command : MANS Success: aci_gatt_add_char command : MNBS Success: aci_gatt_add_char command : SNS Success: aci_gatt_add_char command : HRS Success: aci_gatt_add_char command : FRS Success: aci_gatt_update_char_value MANS command Success: aci_gatt_update_char_value MNBS command Success: aci_gatt_update_char_value SNS command Success: aci_gatt_update_char_value HRS command Success: aci_gatt_update_char_value FRS command End of Services and Characteristics creation ==>> aci_gap_set_discoverable - Success ==>> Success: Start Advertising |
>>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x0001 - Connection established with @:62:f1:e7:ab:a6:18 - Connection Interval: 48.75 ms - Connection latency: 0 - Supervision Timeout: 5000 ms >>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - Connection Interval: 7.50 ms - Connection latency: 0 - Supervision Timeout: 5000 ms >>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - Connection Interval: 48.75 ms - Connection latency: 0 - Supervision Timeout: 5000 ms ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE HRS_NOTIFICATION_ENABLED |
4. Heart Rate Collector - smartphone application
4.1. ST BLE ToolBox application
Once the BLE Heart Rate application is installed on the STM32WBA platform, launch the ST BLE ToolBox smartphone application. The application starts scanning and allows to see advertisement data or to connect to the device. Once the device is connected bpm and kcal measurements are displayed in real time.
BLE Heart Rate application on ST BLE ToolBox | ||
---|---|---|
5. References