Bluetooth® Low Energy audio - Stream Management

Revision as of 17:35, 18 June 2024 by Registered User


1. Introduction

The Bluetooth® LE Audio Stream Management section regroups

  • the Basic Audio Profile (BAP)
  • the Audio Stream Control Service (ASCS)
  • the Published Audio Capability Service (PACS)
  • the Broadcast Audio Scan Service (BASS)

These profile and services are used to configure and establish unicast and broadcast audio streams.

2. Basic Audio Profile (BAP)

The Basic Audio Profile defines roles and procedures to establish audio streams with remote devices. It's specified by the Bluetooth® SIG and the full specification is accessible on their website[1].

2.1. Roles

The BAP introduces 6 roles:

  • Unicast client: Establishes connection to Unicast server, discovers its capabilities and configure the audio stream. This role is used by a smartphone, a laptop, a television etc.
  • Unicast server: Advertises its role, exposes its capabilities, accepts the Unicast server to configure the audio stream. This role can be used by a headphone, a speaker, some hearing aids, some earbuds, or even a microphone.
  • Broadcast source: establishes a BIS and advertise all the information over extended advertising and periodic advertising.
  • Broadcast sink: scan advertising to find the broadcast source, and get synchronized to receive the audio stream
  • Scan delegator: exposes its capabilities and wait for a broadcast assistant to receive some information of a broadcast source and commands. The scan delegator also has the broadcast sink role to get synchronized to the selected broadcast source.
  • Broadcast assistant: scan advertising to find broadcast source, discovers the scan delegator capabilities. It sends the information of the broadcast source to the scan delegator.

2.2. Unicast Roles

The following diagram illustrates the interaction between the different unicast roles:
Interaction between a Unicast Client and a Unicast Server

2.2.1. Unicast Topologies

The BAP specifies 16 different topologies for the Unicast Roles. They define ways of establishing audio stream between one Central device and one or two Peripheral devices. The following table can be found in the BAP Specification and lists the possible topologies:

Audio
Configuration
Legend
C------S
Num Servers Sink ASEs Source ASEs Audio Channels
per Sink ASE
Min Sink Audio
Locations per
Server
Audio Channels
per Source ASE
Min Source Audio
Locations per
Server
CISes Audio Streams
1 --------> 1 1 1 1 1
2 <-------- 1 1 1 1 1
3 <-------> 1 1 1 1 1 1 2
4 ------->> 1 1 2 2 1 1
5 <----->> 1 1 1 2 1 1 2
6(i) -------->
-------->
1 2 1 2 2 2
6(ii) -------->
<--------
2 2 1 1 2 2
7(i) -------->
<--------
1 1 1 1 1 2 2
7(ii) -------->
<--------
2 1 1 1 1 2 2
8(i) -------->
<------->
1 2 1 1 2 1 2 3
8(ii) -------->
<------->
2 2 1 1 1 1 1 2 3
9(i) <--------
<--------
1 2 1 2 2 2
9(ii) <--------
<--------
2 2 1 1 2 2
10 <<------- 1 1 2 2 1 1
11(i) <------->
<------->
1 2 2 1 2 1 2 2 4
11(ii) <------->
<------->
2 2 2 1 1 1 1 2 4

The arrows in the "Legend" column illustrate the CIS(s) to establish between the devices. One arrow means 1 CIS. The arrow tip indicates the direction of the CIS (unidirectional or bidirectional). When the tip of the arrow is doubled, the CIS transport 2 channels. Topologies with "(i)" define interactions between 1 Central and 1 Peripheral, whereas topologies with "(ii)" define interactions between 1 Central and 2 Peripherals (earbud use-case for example).

For example:

  • The configuration 4 defines a unidirectional stereo stream on one CIS to 1 device, which could be applied to transmit media to a headphone.
  • The configuration 11(ii) defines two bidirectional CIS to 2 peripheral devices, which could be applied for a telephony use-case using earbuds where the two microphone on the earbuds would be used.


2.2.2. Unicast Codec Configurations

The BAP specifies LC3 codec configurations that can be used to establish audio streams between devices in Unicast mode. The following tables can be found in the BAP Specification and lists the possible configurations:

Low Latency:

Set Name Sampling
Frequency
(kHz)
Frame
Duration
(ms)
SDU
Interval
(µs)
Framing Maximum
SDU Size
(Octets)
RTN Max Transport
Latency
(ms)
Presentation
Delay
(µs)
8_1_1 8 7.5 7500 unframed 26 (27.734 kbps) 2 8 40000
8_2_1 8 10 10000 unframed 30 (24 kbps) 2 10 40000
16_1_1 16 7.5 7500 unframed 30 (32 kbps) 2 8 40000
16_2_1* 16 10 10000 unframed 40 (32 kbps) 2 10 40000
24_1_1 24 7.5 7500 unframed 45 (48 kbps) 2 8 40000
24_2_1 24 10 10000 unframed 60 (48 kbps) 2 10 40000
32_1_1 32 7.5 7500 unframed 60 (64 kbps) 2 8 40000
32_2_1 32 10 10000 unframed 80 (64 kbps) 2 10 40000
441_1_1 44.1 8.163 8163 framed 97 (95.06 kbps) 5 24 40000
441_2_1 44.1 10.884 10884 framed 130 (95.55 kbps) 5 31 40000
48_1_1 48 7.5 7500 unframed 75 (80 kbps) 5 15 40000
48_2_1 48 10 10000 unframed 100 (80 kbps) 5 20 40000
48_3_1 48 7.5 7500 unframed 90 (96 kbps) 5 15 40000
48_4_1 48 10 10000 unframed 120 (96 kbps) 5 20 40000
48_5_1 48 7.5 7500 unframed 117 (124.8 kbps) 5 15 40000
48_6_1 48 10 10000 unframed 155 (124 kbps) 5 20 40000

(*) Mandatory Configuration Unicast Client & Unicast Server

High reliability:

Set Name Sampling
Frequency
(kHz)
Frame
Duration
(ms)
SDU
Interval
(µs)
Framing Maximum
SDU Size
(Octets)
RTN Max Transport
Latency
(ms)
Presentation
Delay
(µs)
8_1_2 8 7.5 7500 unframed 26 (27.734 kbps) 13 75 40000
8_2_2 8 10 10000 unframed 30 (24 kbps) 13 95 40000
16_1_2 16 7.5 7500 unframed 30 (32 kbps) 13 75 40000
16_2_2 16 10 10000 unframed 40 (32 kbps) 13 95 40000
24_1_2 24 7.5 7500 unframed 45 (48 kbps) 13 75 40000
24_2_2 24 10 10000 unframed 60 (48 kbps) 13 95 40000
32_1_2 32 7.5 7500 unframed 60 (64 kbps) 13 75 40000
32_2_2 32 10 10000 unframed 80 (64 kbps) 13 95 40000
441_1_2 44.1 8.163 8163 framed 97 (95.06 kbps) 13 80 40000
441_2_2 44.1 10.884 10884 framed 130 (95.55 kbps) 13 85 40000
48_1_2 48 7.5 7500 unframed 75 (80 kbps) 13 75 40000
48_2_2 48 10 10000 unframed 100 (80 kbps) 13 95 40000
48_3_2 48 7.5 7500 unframed 90 (96 kbps) 13 75 40000
48_4_2 48 10 10000 unframed 120 (96 kbps) 13 100 40000
48_5_2 48 7.5 7500 unframed 117 (124.8 kbps) 13 75 40000
48_6_2 48 10 10000 unframed 155 (124 kbps) 13 100 40000

The configurations are separated between two tables: Low Latency and High Reliability. High Reliability configurations use a higher Retransmission Number (RTN) and higher maximum transport latency to ensure that the audio packets are all correctly transmitter, but induce higher latency due to increased buffering of the audio packets. Most of the configuration uses an "unframed" mode, meaning the spacing of the events on the air will be a multiple of the actual time between two audio Packets (SDU Interval).

2.3. Broadcast Roles

The following diagram illustrates the simple broadcast use-case, where a device acting as Broadcast Sink interacts with a Broadcast Source.
Broadcast Source and Broadcast Sink interaction

When the device acting as Broadcast Sink is not able to select which Broadcast Source to synchronize to, due to limited display or input capacity for example, the device may use the Scan Delegator role to ask a remote Broadcast Assistant to scan and select the Broadcast Source.
Broadcast Source, Broadcast Sink/Scan Delegator and Broadcast Assistant interaction

2.3.1. Broadcast Advertisement

A Broadcast Source advertises to be visible by remote Broadcast Sinks. It's advertisement is composed of two different types of advertising:

  • Extended Advertising: Partially on advertising channels (37-38-39) and on connection channels, it permits to be visible when a Broadcast Sink is scanning
  • Periodic Advertising: On connection channels, it contains large packets with information about the stream configuration

To synchronize for a Broadcast Source, a broadcast sink initiate a scanning procedure to find the extended advertising payload, which points to the Periodic Advertising payload, which itself points to the BIG.
Broadcast Source Advertising

2.3.1.1. BASE Structure

The Broadcast Audio Source Endpoint (BASE) structure is the data structure that permits to describe a Broadcast Source. It is located in the periodic advertising data and is constituted of 3 levels with the following items:

Level Parameter Description
1 (Group) Basic Audio Announcement Service UUID UUID defined in Bluetooth Assigned Numbers: 0x1851
1 (Group) Presentation Delay Presentation Delay parameter. Refer to the the LC3 codec and audio data path wiki page, section Audio Latency[2]
1 (Group) Num Subgroups Number of subgroups (level 2)
2 (Subgroup) Num BIS Number of BISes (level 3)
2 (Subgroup) Codec ID Codec ID for the subgroups. 0x0000000006 for the LC3 codec
2 (Subgroup) Codec Specific Configuration Series of LTV structures with common codec specific configuration for the subgroup
2 (Subgroup) Metadata Series of LTV Metadata structures
3 (BIS) BIS Index Unique index for the BIS
3 (BIS) Codec Specific Configuration Series of LTV structures with codec specific configuration for the bis

Example of a stereo Broadcast Source with one BIS:
BASE structure of a stereo Broadcast Source with one BIS


Example of a stereo Broadcast Source with 2 BISes:
BASE structure of a stereo Broadcast Source with two BIS

2.3.1.2. Broadcast Source Air Events

Over the air, a Broadcast Source emit 4 different types of packets

  • ADV_EXT_IND packets are sent on the 3 advertising channels (Extended Advertising)
  • AUX_ADV_IND packets are sent on connection channels and contains the remaining data of ADV_EXT_IND packets (Extended Advertising)
  • AUX_SYNC_IND packets are sent on connection channels (Periodic Advertising)
  • BIS ISO Packets are sent on connection channels during BIG Events (BIG)

The following diagrams illustrates a possible scheduling of those packets
Air Events of a Broadcast Source

2.3.2. Broadcast Topologies

The BAP specifies 3 different topologies for the Broadcast Roles. They define ways of establishing audio stream between one Central device and one or two Peripheral devices. The following table can be found in the BAP Specification and lists the possible topologies:

Audio
Configuration
Legend Audio Channels
per BIS
BISes Audio Streams
12 ---)))--> 1 1 1
13 ---)))-->
---)))-->
1 2 2
14 ---)))-->> 2 1 1

2.3.3. Broadcast Codec Configurations

The BAP specifies LC3 codec configurations that can be used to establish audio streams between devices in Broadcast mode. The following tables can be found in the BAP Specification and lists the possible configurations: Low Latency:

Set Name Sampling
Frequency
(kHz)
Frame
Duration
(ms)
SDU
Interval
(µs)
Framing Maximum
SDU Size
(Octets)
RTN Max Transport
Latency
(ms)
Presentation
Delay
(µs)
8_1_1 8 7.5 7500 unframed 26 (27.734 kbps) 2 8 40000
8_2_1 8 10 10000 unframed 30 (24 kbps) 2 10 40000
16_1_1 16 7.5 7500 unframed 30 (32 kbps) 2 8 40000
16_2_1* 16 10 10000 unframed 40 (32 kbps) 2 10 40000
24_1_1 24 7.5 7500 unframed 45 (48 kbps) 2 8 40000
24_2_1** 24 10 10000 unframed 60 (48 kbps) 2 10 40000
32_1_1 32 7.5 7500 unframed 60 (64 kbps) 2 8 40000
32_2_1 32 10 10000 unframed 80 (64 kbps) 2 10 40000
441_1_1 44.1 8.163 8163 framed 97 (95.06 kbps) 4 24 40000
441_2_1 44.1 10.884 10884 framed 130 (95.55 kbps) 4 31 40000
48_1_1 48 7.5 7500 unframed 75 (80 kbps) 4 15 40000
48_2_1 48 10 10000 unframed 100 (80 kbps) 4 20 40000
48_3_1 48 7.5 7500 unframed 90 (96 kbps) 4 15 40000
48_4_1 48 10 10000 unframed 120 (96 kbps) 4 20 40000
48_5_1 48 7.5 7500 unframed 117 (124.8 kbps) 4 15 40000
48_6_1 48 10 10000 unframed 155 (124 kbps) 4 20 40000

(*) Mandatory Configuration Broadcast Source & Broadcast Sink
(**) Mandatory Configuration Broadcast Sink

High reliability:

Set Name Sampling
Frequency
(kHz)
Frame
Duration
(ms)
SDU
Interval
(µs)
Framing Maximum
SDU Size
(Octets)
RTN Max Transport
Latency
(ms)
Presentation
Delay
(µs)
8_1_1 8 7.5 7500 unframed 26 (27.734 kbps) 4 45 40000
8_2_1 8 10 10000 unframed 30 (24 kbps) 4 60 40000
16_1_1 16 7.5 7500 unframed 30 (32 kbps) 4 45 40000
16_2_1 16 10 10000 unframed 40 (32 kbps) 4 60 40000
24_1_1 24 7.5 7500 unframed 45 (48 kbps) 4 45 40000
24_2_1 24 10 10000 unframed 60 (48 kbps) 4 60 40000
32_1_1 32 7.5 7500 unframed 60 (64 kbps) 4 45 40000
32_2_1 32 10 10000 unframed 80 (64 kbps) 4 60 40000
441_1_1 44.1 8.163 8163 framed 97 (95.06 kbps) 4 54 40000
441_2_1 44.1 10.884 10884 framed 130 (95.55 kbps) 4 60 40000
48_1_1 48 7.5 7500 unframed 75 (80 kbps) 4 50 40000
48_2_1 48 10 10000 unframed 100 (80 kbps) 4 65 40000
48_3_1 48 7.5 7500 unframed 90 (96 kbps) 4 50 40000
48_4_1 48 10 10000 unframed 120 (96 kbps) 4 65 40000
48_5_1 48 7.5 7500 unframed 117 (124.8 kbps) 4 50 40000
48_6_1 48 10 10000 unframed 155 (124 kbps) 4 65 40000

Like the Unicast codec configurations, the Broadcast codec configurations are separated between a Low Latency table and High Reliability table.


3. Audio Stream Control Service (ASCS)

The ASCS is hosted on a Unicast Server to permit remote Unicast Client to configure and establish audio streams between the two devices. It contains the current unicast state of the Unicast Server and its state machine. It's specified by the Bluetooth® SIG and the full specification is accessible on their website[3].

3.1. Audio Stream Endpoints (ASE)

3.2. Source ASE State Machine

3.3. Sink ASE State Machine

3.4. Unicast Streaming Procedure

4. Published Audio Capability Service (PACS)

The PACS permits to a Unicast Server to expose to remote Unicast Clients and Broadcast Assistants its audio capabilities. It's specified by the Bluetooth® SIG and the full specification is accessible on their website[4].

4.1. Published Audio Capability (PAC)

A PACS Server exposes one or multiple Published Audio Capability (PAC) records. These records indicates to a remote PACS Client which audio configuration are supported by the server.

Parameter Size (octets) Value
Codec_ID 5 Codec ID, 0x0000000006 for the LC3 Codec
Codec_Specific_Capabilities_Length 1 Length, in octets, of the Codec_Specific_Capabilities value
Codec_Specific_Capabilities Varies Sequence of LTVs (Length-Type-Value) of Codec Capabilities
Metadata_Length 1 Length of the Metadata field
Metadata Varies Sequence of LTVs (Length-Type-Value) of Metadata

5. Broadcast Audio Scan Service (BASS)

The Broadcast Audio Scan Service is hosted on a Scan Delegator collocated with a Broadcast Sink to communicate with a remote Broadcast Assistant and exchange information and commands about available Broadcast Sources. It's specified by the Bluetooth® SIG and the full specification is accessible on their website[5].

6. STM32Cube Firmware APIs

7. References


No categories assignedEdit