1 What is NanoEdge AI Library?
NanoEdge™ AI Library is an Artificial Intelligence (AI) static library originally developed by Cartesiam, for embedded C software running on Arm® Cortex® microcontrollers (MCUs). It comes in the form of a precompiled .a
file that provides building blocks to implement smart features into any C code.
When embedded on microcontrollers, the NanoEdge AI Library gives them the ability to "understand" sensor patterns automatically, by themselves, without the need for the user to have additional skills in Mathematics, Machine Learning, or data science.
Each NanoEdge AI static library contains an AI model (as a bundle of signal preprocessing, Machine Learning model, or optimally tuned hyperparameters) designed bring Machine Learning capabilities to any C code, in the form of easily implementable functions, such as learn, detect, or classify.
There are two different types of NanoEdge AI Libraries:
- NanoEdge AI Library for anomaly detection: it is used to detect anomalous behaviors on a machine, after an initial in-situ training phase, where only the "nominal" behaviors are learned.
- NanoEdge AI Library for classification: it is used to distinguish and recognize different types of behaviors, anomalous or not, and classify them into pre-established categories.
Each library, tailored for different goals, has unique features:
Anomaly detection library | Classification library |
---|---|
Comes optimized yet untrained | Comes optimized and pre-trained |
Gathers knowledge incrementally in the MCU | Includes static knowledge |
Learns dynamically and unsupervised in-situ | Does not require any additional learning |
Detects anomalies in the MCU | Classifies signals in the MCU |
However all NanoEdge AI Libraries:
- are ultra optimized to run on MCUs (any Arm® Cortex®-M)
- are ultra memory efficient (1-20 Kbytes of RAM/Flash memory)
- are ultra fast (1-20 ms inference on Cortex®-M4 at 80 MHz)
- run directly within the microcontroller
- can be integrated into existing code / hardware
- consume very little energy
- preserve the stack (static allocation only)
- are inherently independent from the cloud
- transmit or save no data
- require no Machine Learning expertise to be deployed
All NanoEdge AI Libraries are created by using NanoEdge AI Studio.
2 Purpose of NanoEdge AI Studio
2.1 What the Studio can do
NanoEdge AI Libraries contains a range of Machine Learning models, and each of these models can be optimized by tuning a wide range of hyperparameters. This results in a very large number of potential combinations, each one being tailored for a specific use-case (one static libraries for each combination). Therefore, a tool is needed to find the best possible library for each project.
NanoEdge AI Studio (NanoEdgeAIStudio), also called the Studio,
- is a search engine for AI Libraries
- is built for embedded developers
- abstracts away all aspects of Machine Learning and data science
- enables the quick and easy development of Machine Learning capabilities into any C code
Its purpose is to find the best possible NanoEdge AI static library for a given hardware application, where the only requirements in terms of user knowledge are embedded development (software/hardware), C coding, and basic signal sampling notions.
NanoEdge AI Studio takes as input project parameters (such as MCU type, RAM and sensor type) and some signal examples, and outputs the most relevant NanoEdge AI Library (that then do all the learning in-situ, when embedded).
Each NanoEdge AI static library is the result of the benchmark of virtually all possible AI libraries (combinations of signal treatment, ML model, tuned hyperparameters), tested against the minimal data given by the user. It therefore contains the best possible model, for a given project, given the signal examples provided as input.
2.2 What the Studio cannot do
In a nutshell, NanoEdge AI Studio takes user data as input (in the form of sensor signal examples), and produces a static library (.a) file as output. This is a straightforward and relatively quick procedure.
However, the Studio does not provide any input data. The user needs to have qualified data in order to obtain satisfactory results from the Studio. These data can be raw sensor signals, or pre-treated signals, and need to be formatted properly (see below). For example, for anomaly detection on a machine, the user needs to collect signal examples of "normal" behavior on this machine, as well as a few examples (non-exhaustive) of "anomalies". This data collection process is crucial, and can be tedious, as some expertise is needed to design the correct signal acquisition and sampling methodology, which can vary dramatically from one project to the other.
Additionally, NanoEdge AI Studio does not provide any ready-to-use C code to implement in your final project. This code, which includes some of the NanoEdge AI Library smart functions (such as initialize, learn and detect), needs to be written and compiled by the user. The user is free to call these functions as needed, and implement all the smart features imaginable.
In summary, the static (.a) library file, outputted by the Studio from user-generated input data, must be linked to some C code written by the user, and compiled/flashed by the user on the target microcontroller.
3 Getting started
3.1 Running NanoEdge AI Studio for the first time
When running NanoEdge AI Studio for the first time, you are prompted for:
- Your proxy settings: if you are using a proxy, use the settings below, otherwise, click NO.
- Here are the IP addresses that need to be authorized:
Licensing API: Cartesiam API for library compilation: 54.147.158.222 40.113.111.93 54.147.163.93 - 54.144.124.187 - 54.144.46.201 - or via URL: https://api.cryptlex.com:443 or via URL: https://apidev.cartesiam.net
- The port you want to use.
- It can be changed to any port available on your machine (port 5000 by default).
- Your license key.
- If you do not know your license key, log in to the Cryptex licensing platform to retrieve it.
- If you have lost your login credentials, reset your password using the email address used to download NanoEdge AI Studio.
- If you do not know your license key, log in to the Cryptex licensing platform to retrieve it.
3.2 Preparing signal files
During the library selection process, NanoEdge AI Studio uses user data (input files containing signal examples) to test and benchmark many Machine Learning models and parameters. The way those input files are structured, formatted, and the way the signal were recorded is therefore very important.
This section is composed of the following sub-sections:
- Anomaly detection vs. classification
- General formatting approach
- Variant: the "Multi-sensor" sensor
- Choosing sampling frequency and buffer size
- Which signals to put in which files
3.2.1 Anomaly detection vs. classification
Here is an overview of the two different approaches:
Anomaly detection | Classification (N classes) | |
---|---|---|
Studio purpose |
|
|
Embedded functions (MCU) |
|
|
Studio steps |
|
|
Input signals |
|
|
Different regimes |
|
|
File contents | All files contain several examples (or repetitions, or variations) of the same signal, be it “nominal”, “abnormal”, or corresponding to a given “class” or regime. | (same) |
The following sub-sections are applicable to both anomaly detection and classification.
3.2.2 General approach for formatting input files properly
For both anomaly detection (AD) and classification (Cl), the expected input file format is the same:
- .txt / .csv file
- at least 20-50 lines representing independent signal examples
- multiple numerical values on each line
- same number of numerical values per line
- numerical values only
- uniform separators (such as comma, semicolon or other)
Each input file contains several signals, each made of many samples.
Signals:
Each line in the input file, corresponds to an observation of a signal during a given time. It is a signal example.
Each of these line comes from a sampling process that involves reading values from a signal at defined intervals, generally constant, producing a series of discrete values called samples.
Samples:
During sampling, the signal values are read, generally at regular intervals. Keeping a constant sampling frequency during data acquisition is recommended, regardless of the final application.
The number of samples per signal, or buffer size, is set by the user depending on this sampling frequency (see next section), and depends on each particular use case. You need enough samples to cover the whole physical phenomenon studied, to get a proper and meaningful signal snapshot.
Example:
Here is an example of signal file corresponding to a 3-axis sensor, such as a collection of m signal examples (m readings, or lines) on a 3-axis accelerometer with a buffer size of 256 on each axis, where each numerical value is separated by a single space:
3.2.3 Variant: aggregating multiple variables into "states"
The above procedure described how to treat signals that contain a succession of samples, often resulting from real time acquisition of a temporal signal.
However, it is also possible to create artificial signals from higher-level features, resulting from the aggregation of multiple variables, possibly coming from multiple sensors. Such signal represent instantaneous states rather than time-evolving signals.
For this purpose, "Multi-sensor" can be selected in the Studio, on the project creation screen, where you would normally select your sensors:
Make sure that you select the correct number of variables (for example creating a 5-variable state using a 3-axis magnetometer + temperature sensor + pressure sensor).
Example:
For example, for an application where a state can be represented via a combination of magnetism, temperature, and pressure: it is possible to aggregate data from a 3-axis magnetometer, a (1-axis) thermometer, and a (1-axis) pressure sensor. Temperature and pressure, if they vary slowly, can be read directly, but magnetometer data needs to be summarized using (for example) average values across a 50 millisecond window along all 3 axes.
This would result in 3 extracted magnetic features, followed by temperature, followed by pressure, to represent a 5-variable state.
It is also possible to build a more complex state from the 50-millisecond magnetometer buffer, including not only average magnetometer values, but also minimums and maximums, for all 3 axes. This would result in 3x3 = 9 extracted magnetometer values (3 each for average, minimum, maximum), followed by temperature and pressure, to represent a 11-variable state.
3.2.4 Choosing a relevant sampling frequency and buffer size (except multi-sensor)
To prepare input data (except when using multi-sensor), it is crucial to choose the most adequate sampling frequency and buffer size for your sensors.
The sampling frequency corresponds to the number of samples measured per second. For some sensors, the sampling frequency can be directly set by the user, but in other cases, a timer needs to be set up for constant time intervals between each sample.
The speed at which the samples are taken must allow the signal to be accurately described, or "reconstructed"; the sampling frequency must be high enough to account for the rapid variations of the signal. The question of choosing the sampling frequency therefore naturally arises:
- If the sampling frequency is too low, the readings are too far apart; if the signal contains relevant features between two samples, they are lost.
- If the sampling frequency is too high, it may negatively impact the costs, in terms of processing power, transmission capacity, or storage space for example.
The issues related to the choice of sampling frequency and the number of samples are illustrated below:
- Case 1: the sampling frequency and the number of samples make it possible to reproduce the variations of the signal.
- Case 2: the sampling frequency is not sufficient to reproduce the variations of the signal.
- Case 3: the sampling frequency is sufficient but the number of samples is not sufficient to reproduce the entire signal (meaning that only part of the input signal is reproduced).
The buffer size corresponds to the total number of samples recorded per signal, per axis. Together with the sampling frequency, they put a constraint on the effective signal temporal length.
Here are general recommendations. Make sure that:
- the sampling frequency is high enough to catch all desired signal features. To sample a 1000 Hz phenomenon, you must at least double the frequency (in this case, sample at 2000 Hz at least).
- your signal is long (or short) enough to be coherent with the phenomenon to be sampled. For example, if you want your signals to be 0.25 seconds long (
L
), you must haven / f = 0.25
. For example, choose a buffer size of 256 with a frequency of 1024 Hz, or a buffer of 1024 with a frequency of 4096 Hz, and so on.
3.2.5 Which signals to put in which files
For classification, each category of signal examples that wish to be classified / separated must be put into distinct files and imported separately into different "Classes".
For anomaly detection, the general guideline is to concatenate all signal examples corresponding to the same category into the same file (like "nominal").
Example:
I want to detect anomalies on a 3-speed fan by monitoring its vibration patterns using an accelerometer. I recorded many signals corresponding to different behaviors, both "nominal" and "abnormal". I have the following signal examples (numbers are arbitrary):
- 30 examples for "Speed 1", which I consider nominal,
- 25 examples for "Speed 2", which I consider nominal,
- 35 examples for "Speed 3", which I consider nominal,
- 30 examples for "Fan turned off", which I also consider nominal,
- Some of these signals contain "transients", like fan speeding up, or slowing down.
- 30 examples for "fan air flow obstructed at speed 1", which I consider abnormal,
- 35 examples for "fan orientation tilted by 90 degrees", which I consider abnormal,
- 25 examples for "tapping on the fan with my finger", which I consider abnormal,
- 25 examples for "touching the rotating fan with my finger", which I consider abnormal.
Here, I create
- Only 1 nominal input file containing all 120 signal examples (30+25+35+30) covering 4 nominal regimes + transients.
- Only 1 abnormal input file containing all 115 signal examples (30+35+25+25) covering 4 abnormal regimes.
And start a benchmark using only this couple of input files.
4 Using NanoEdge AI Studio
In order to generate a static library, NanoEdge AI Studio walks the user through several steps:
- Creating a new project and setting up its parameters,
- Importing "signal examples" into the studio for context,
- Running the library selection process,
- Testing the best library found by the Studio,
- Compiling and downloading the library [Full version / Featured boards only].
For anomaly detection:
For classification:
4.1 Creating a new project
In the main window, you can:
- Create a new project
- Load an existing project
Projects can be imported from and exported to .zip
format:
The 3 projects most recently opened are listed first.
4.1.2 Project creation
- Choose project type: Anomaly detection or Classification:
- Enter name and description;
- Choose the target (microcontroller type);
- Arm® Cortex®-M MCUs currently supported: M0, M0+, M1, M3, M4, M23, M33 and M7.
- Selecting an authorized board enables library download and compilation when using NanoEdge AI Studio TRIAL version.
- Here is the list of the authorized boards currently available:
- STMicroelectronics:
- Choose the maximum amount of RAM allocated to the library (maximum: 10 000 Kbytes);
- (optional) Choose the maximum amount of FLASH allocated to the library;
- Choose the sensor type used to collect data (with the correct number of axes);
- Click CREATE.
4.1.3 Which sensor to use for which case
Single-sensor temporal buffer:
This is the typical single-sensor use case where a signal example is composed of a buffer made out of several samples (such as current, magnetometer, accelerometer, or others) Valid sensors to use would be:
Multi-sensor temporal buffer:
To work with temporal buffers coming from multiple sensors of different types, there are 2 different approaches:
- Separate each sensor signal, and create a library for each one, using Multi-library.
- Each signal is decoupled and treated on its own by a different library. See the Multi-library section. This is very similar to the Single-sensor buffer case above, but this time there is a need to monitor several buffers coming from several sensors, concurrently, in the same device.
- Each signal is decoupled and treated on its own by a different library. See the Multi-library section. This is very similar to the Single-sensor buffer case above, but this time there is a need to monitor several buffers coming from several sensors, concurrently, in the same device.
- Combine all signals into a single buffer, by using a generic N-axis sensor.
- All signals are treated concurrently by the same library. The Machine Learning algorithms build therefore a model based on the combination of these inputs (unlike option #1).
- Example:
- To combine accelerometer (3 axes) + gyroscope (3 axes) + current (1 axis) signals, you would select a generic 7-axis sensor.
- The buffers in the input files are formatted just like a generic 3-axis accelerometer (see this section formatting), but each sample now has 7 variables. Instead of the 3 linear accelerations [X Y Z], the 7-axis sample adds 3 angular accelerations [Gx Gy Gz] from the gyroscope, and 1 current value [C] from the current sensor.
- This would result in 7-axis samples [X Y Z Gx Gy Gz C], meaning that for a buffer size of 256, each line would be composed of 7x256 = 1792 numerical values.
- To combine accelerometer (3 axes) + gyroscope (3 axes) + current (1 axis) signals, you would select a generic 7-axis sensor.
Multi-sensor non-temporal state:
See the Multi-sensor section. This is a niche use case, where machine states need to be monitored at defined intervals. Each state is composed of several "variables" (there is no buffer anymore), possibly coming from sensors of different types.
4.2 Importing signal files
4.2.1 Anomaly detection
For anomaly detection, two types of signals examples are required. They are imported respectively in Step 2: Regular signals and Step 3: Abnormal signals.
- The Regular signals correspond to nominal machine behavior, corresponding to data acquired by sensors during normal use, when everything is functioning as expected.
Include data corresponding to all the different regimes, or behaviors, that you wish to consider as "nominal". For example, when monitoring a fan, you may need to log vibration data corresponding to different speeds, possibly including the transients.
- The Abnormal signals correspond to abnormal machine behavior, corresponding to data acquired by sensors during a phase of anomaly.
The anomalies do not have to be exhaustive. In practice, it would be impossible to predict (and include) all the different kinds of anomalies that could happen on your machine. Just include examples of some anomalies that you've already encountered, or that you suspect could happen. If needed, do not hesitate to create "anomalies" manually. However, if the library is expected to be sensitive enough to detect very "subtle anomalies", it is recommended that the data provided as abnormal signals includes at least some examples of subtle anomalies as well, and not only very gross, obvious ones.
To import a new file, simply click "Choose Signals".
4.2.2 Classification
For classification, you need as many signal types as you have classes to distinguish.
For example, for the identification of types of failures on a motor, 5 classes can be considered, each corresponding to a behavior, such as:
- normal behavior
- misalignment
- imbalance
- bearing failure
- excessive vibration
This would result in the creation of 5 distinct classes (import one .txt / .csv file for each), each containing a minimum of 20-50 signal examples of said behavior.
To add a new class, simply click "Add Class" and then "Choose Signals".
4.2.3 Importing signals from file
Make sure that your input files are formatted properly (see Studio: Formatting input files).
- Click Select file, and choose a valid input file.
- Select the separator you are using.
- Validate import.
If your input file is valid, you are able to import it. Otherwise, double-check your data (numerical values, uniform separators, or constant number of samples per line).
Any imported signal can be plotted and displayed by clicking the icon:
Plots can then be saved to .png format.
4.2.4 Importing signals "live" from Serial port (USB)
It is possible to import signals directly within the Studio, by logging it through your computer serial port (USB).
You need a USB data logger in order to do it. For instructions on how to make a simple data logger, check the tutorials: Smart vibration sensor and Smart current sensor, under section Making a data logger.
- Select your Serial / COM port. Refresh if needed.
- Choose your preferred baudrate.
- If needed, select a maximum number of lines to be recorded.
- Click the red "Record" round button to start the data logging.
- Click the grey "Stop" square button to interrupt the logging.
- Choose your delimiter.
- Validate import.
If your data is valid, you are able to import it. Otherwise, double-check your data logger parameters.
The data logged via serial is plotted in real-time at the bottom of the screen:
This serial plotter window can be toggled on/off by clicking the signal icon, above numlerical data preview:
If any error is found during the real-time data logging via serial, a pop-up window appears, letting you delete or edit the lines where issues were detected.
4.2.5 Checks, errors and warnings
Supported file formats are .txt / .csv. Recommended separators are single spaces, commas or semicolons. Make sure that your input file is correctly formatted.
In this example, an input file contains 200 examples of nominal data (200 lines), for a 3-axis accelerometer that uses a buffer size of 256 (which gives 256x3 = 768 numerical values per line).
The "Check for RAM"" and the next 5 checks are blocking, meaning that you need to fix any error in your input file before proceeding further.
Click "Run optional checks"" to scan your input file and run additional checks, for instance. to search for duplicate signals, equal consecutive values, random values, outliers, and others. Failing these additional checks gives warnings that suggest possible modifications on your input files. Click any warning for more information and advice.
4.2.6 Data plots
On the right of the screen, you can see a preview of data contained in your input files.
These graphs show a summary of the data contained in each line of your input files. There are as many graphs as sensor axes.
The graph x-axis corresponds to the columns of your input file. The y-values contain an indication of the mean value of each column (across all lines, or signals), their min-max values, and their standard deviation.
The FFT plots can be displayed by toggling "Show FFT" at the top-right of the graphs.
Several input files can be loaded (shown on the left of the screen, see below), either for "regular" or "abnormal" signals, but only one (for each) at a time is used for library selection.
4.2.7 Frequency filtering
Since v2.1, it is now possible to alter the imported signals by filtering out unwanted frequencies.
Click Advanced settings above the list of imported signals.
In the Advanced settings menu, you may toggle Activate FFT to force the library to include a fast Fourier transform in its signal pre-processing step. The library treats imported signals in the frequency domain rather than the time domain.
- Input the sampling frequency used to collect your signals (here 6660 Hz)
- Select the range of frequencies to exclude (meaning that everything is excluded under 500 Hz and above 2000 Hz)
- Validate
The FFT plots of your signals are displayed under signal previews, with greyed out zones corresponding to the excluded frequencies (below, only the frequencies between 500 Hz and 2000 Hz are kept).
4.3 Running the library selection process
Here (Step: Optimize and Benchmark), you start and monitor the library benchmark. NanoEdge AI Studio searches for the best possible library given the contextual signal examples provided in the previous step(s).
4.3.1 Starting the benchmark
Click START to open the signal selection window:
[Anomaly detection]:
Select a couple of signal files (regular + abnormal signals) that you wish to use for benchmark.
Those signals can be compared visually across all sensor axes by clicking Compare these signals.
[Classification]:
Select the classes to take into consideration for benchmarking.
Then, select the number of microprocessor cores from your computer that you wish to dedicate to the benchmark process (see below). Selecting more CPU cores parallelizes the workload of algorithms, and greatly speed up the process. Use as many as you can, but be aware that using all available CPU cores might temporarily slow down your computer performance.
When you are ready to start the benchmark, click Validate.
4.3.2 Library performance indicators
NanoEdge AI Studio uses 3 indicators to translate the performance and relevance of candidate libraries, in the following order of priority:
- (Balanced) accuracy (most important by far)
- Confidence
- RAM
- Fèlash memory
Balanced Accuracy (anomaly detection) | Accuracy (classification) |
|
|
Optimizing this indicator is the top priority of the algorithms. |
Confidence (anomaly detection) | Confidence (classification) |
|
|
Increasing this indicator is the algorithms' second priority. |
RAM and Flash memory (anomaly detection and classification) |
This is the maximum amount of RAM and Flash memory space needed by the library after your integrate it on your microcontroller. |
The amounts of Flash memory and RAM used by the libraries are optimized last. |
Along with those 3 indicators, a graph shows a plot of all data points, against a percentage of similarity (on the y-axis). Similarity is a measure of the how much a given data point fits in with (how much it resembles) the existing knowledge base of the library.
[Anomaly detection]:
Regular signals are shown as blue dots, and abnormal signals as red dots. The x-axis represents the number of the signal example in the corresponding file, and the y-axis represents the similarity score (%). The threshold (decision boundary between the two classes, "nominal" and "anomaly") set at 90% similarity, is shown as a gray dashed line.
For example:
- The blue dot below refers to a signal from the imported "nominal signals" input file, and it is ranked at 67% similarity. It is (incorrectly) detected as anomaly.
- The red dot below refers to a signal from the imported "abnormal signals" input file, and it is ranked at 60% similarity. It is (correctly) detected as anomaly.
[Classification]:
The graph is subdivided into sections, one for each class. The x-axis shows the number of the signal example in the corresponding class file, while the y-axis represents the probability associated to this signal (the % certainty associated to the class detected).
All signal examples are represented as dots, either green if their associated probability is higher than 50%, or red otherwise.
For example:
- The red dot below, pertaining to the class / input file "Obstructed" was (incorrectly) classified as "Nominal".
- All other dots (green) were correcly identified as their respective classes.
4.3.3 Benchmark progress and summary
As soon as the library selection process is initiated, a graph is displayed on the right hand side of the screen (see below), showing the evolution of the 3 performance indicators (see above section) over time, as thousands of candidate library are tested.
The selection algorithms first try to maximise balanced accuracy, then confidence, and finally to decrease the RAM / Flash memory needed as much as possible.
While a benchmark is running, a small log window displays notable information / events such as benchmark status, search speed per thread, and new libraries found.
When the benchmark is complete, the progress graph is be replaced by a summary.
Several successive benchmarks can be run; all results are saved. They can be loaded by clicking them on the left hand side of the screen.
[Anomaly detection only]: After the benchmark is complete, a plot of the library learning behavior is shown:
This graph shows the number of learning iterations needed to obtain optimal performance from the library, when it is embedded in your final hardware application. In this particular example, NanoEdge AI Studio recommended that the learn()
is called 70 times, at the very minimum.
4.3.4 Possible cause for poor benchmark results
If your keep getting poor benchmark results, you may try the following:
- Increase the "Max RAM" or "Max Flash"" parameters (such as 32 Kbytes or more).
- Adjust your sampling frequency; make sure it is coherent with the phenomenon you want to capture.
- Change your buffer size (and hence, signal length); make sure it is coherent with the phenomenon to sample.
- Make sure your buffer size (number of values per line) is a power of two (except for multi-sensor).
- If using a multi-axis sensor, treat each axis individually by running several benchmarks with a single-axis sensor.
- Include more signal examples (lines) in your input files.
- Check the quality of your signal examples; make sure they contain the relevant features / characteristics.
- Check that your input files do not contain (too many) parasite signals (for instance no anomalous signals in the nominal file, for anomaly detection, and no signals belonging to another class, for classification).
- Increase the variety of your signal examples (more nominal regime, or more anomalies, or more classes).
- Decrease the variety of your signal examples ( fewer nominal regime, or fewer anomalies, or fewer classes).
- Check that the sampling methodology and sensor parameters are kept constant throughout the project for all signal examples recorded (in all input files; nominal, abnormal or class files).
- Check that your signals are not too noisy, too low intensity, too similar, or unrepeatable.
- Remember that microcontrollers are resource-constrained (audio/video, image and voice recognition are not be supported).
Low confidence scores are not necessarily an indication or poor benchmark performance, if the (balanced) accuracy is sufficiently high (> 80-90%). Always use the associated Emulator to determine the performance of a library, preferably using data that has not been used before (for the benchmark).
4.4 Testing the NanoEdge AI Library
Here (Step: Emulator), you are able to test the library that was selected during the benchmark process (Step: Optimize and Benchmark) using NanoEdge AI Emulator.
NanoEdge AI Emulator is a clone of the library that emulates its behavior, and is directly usable within the Studio interface. There is no need to embed a library in order to test its performance with real, "unseen" data. Therefore, each library, among hundreds of thousands of possibilities, comes with its own Emulator.
The Emulator can be also be downloaded as a standalone .exe
(Windows®) or .deb
(Linux®) to be used in the terminal through the command line interface.
This screen gives a summary of the selected benchmark (progress, performance, input files used):
Select the benchmark to use, on the left side of the screen, to load the associated emulator.
When you are ready to start testing, click Initialize Emulator.
4.4.1 Anomaly detection
Functions:
Here are the functions of the anomaly detection library that are available through its Emulator:
initialize()
|
run first before learning/detecting, or to reset the knowledge of the library/emulator |
set_sensitivity()
|
adjust the pre-set, internal detection sensitivity (does not affect learning, only returned similarity scores) |
learn()
|
start a number of learning iterations (to establish an initial knowledge, or enrich an existing one) |
detect()
|
start a number detection iterations (inference), once a minimum knowledge base has been established |
For more information, see the Emulator and Library documentations for anomaly detection.
The testing procedure goes as follows:
Learning:
After initialization, no knowledge base exists yet. It needs to be acquired in-situ, using real signals. Your library is not pre-trained with the signals imported before benchmark, in Steps 2 and Step 3. Therefore, you need to learn some signals.
To learn some signals from a file, click Select file and open the file containing your training data.
To learn some signals "live" from your Serial port, using your own data logger, click Serial data. Then, select your Serial / COM port (refresh if needed), choose your preferred baudrate, and Start recording by clicking the red button.
As soon as some signals are learned, the number of learned signals is indicated.
Click Go to detection after all relevant signals (nominal, by definition) have been learned.
Detection:
When a first knowledge base has been established, you can use Detection using any signals, to check if they would be classified as nominal or anomaly by the library, and make sure this library performs as intended.
As usual, the signals to use for detection can be imported from file, or from Serial port using a data logger.
Select the signals that you wish to use, and adjust the sensitivity if needed. A pie chart summarizes the detection results.
When detecting using live data from the Serial port, a graph shows how the detection performance (similarity percentage) evolves in real time.
4.4.2 Classification
Here are the functions of the classification library that are available through its Emulator:
knowledge_init()
|
run first to initialize the knowledge |
classifier()
|
run an inference iteration (detect which class the input signal belongs to) |
For more information, see the Emulator and Library documentations for classification.
Just like in anomaly detection (see "Important" section above), the classifier
function can be called dynamically whenever needed. It can be triggered by external data (for example from sensors, buttons, to account for and adapt to environment changes), and the class / probabilities returned can trigger all kinds of behaviors on your device.
To classify signals from a file, click Select file and open the file containing the signal examples to classify. You can see a pie chart summarizing the classification.
The image below shows data from a 3-speed fan:
- 3 signals were detected at "speed 1"
- 7 at "speed 2"
- 17 at "speed 3"
- 6 when the fan air flow was obstructed
- and so on
You see a pie chart summarizing the classification, as well as a graph showing the probabilities associated to each classification iteration (the image below shows data from a 3-speed fan, and "speed 1" is currently being detected).
4.4.3 Possible causes of poor emulator results
Here are possible reasons for poor anomaly detection or classification results:
- The data used for library selection (benchmark) is not coherent with the one you are using for testing via Emulator/Library. The regular/abnormal or class signals imported in the Studio must correspond to the same machine behaviors, regimes, and physical phenomena as the ones used for testing.
- Your (balanced) accuracy score was well below 90% or your confidence score was too low to provide sufficient data separation.
- You used an insufficient number or signals in either regular/abnormal or class signal files. Make sure that you used enough lines in your input files (minimum 20-50). For anomaly detection, make sure that you use at least the minimum number recommended by the Studio, and possibly more.
- The sampling method is inadequate for the physical phenomena studied, in terms of frequency, buffer size, or duration for instance.
- The sampling method has changed between Benchmark and Emulator tests. The same parameters (frequency, signal lengths, buffer sizes) must be kept constant throughout the whole project.
- [Anomaly detection]: you have not run enough learning iterations (your Machine Learning model is not rich enough), or this data is not representative of the signal examples used for benchmark. Do not hesitate to run several learning cycles, as long as they all use nominal data as input (only normal, expected behavior should be learned).
- [Classification]: the machine status or working conditions have drifted between Benchmark and Emulator tests, and classes are not recognized anymore. In that case, update the imported "class" files, and start a new benchmark.
4.5 Downloading the NanoEdge AI Library
This feature is only available:
- in the Trial version of NanoEdge AI Studio, limited to the featured boards which can be selected during project creation
- in the Paid version of NanoEdge AI Studio
4.5.1 General case
In this step (Step: Deploy), the library is compiled and downloaded, ready to be used on your microcontroller for your embedded application.
Before compiling the library, several compilation flags are available:
- [[File:NanoEdgeAI_compilation_flags.png]
If you ran several benchmarks, make sure that the correct benchmark is selected. Then, when you are ready to download the NanoEdge AI Library, click Compile.
Select Development version to get a library that is intended for testing and prototyping. If you would like to start producing your device, integrating NanoEdge AI Library, contact STMicroelectronics for more details and to get the proper library version.
After a short delay, a .zip file is downloaded to your computer.
It contains all relevant documentation, the NanoEdge AI Emulator (both Windows® and Linux® versions), the NanoEdge AI header file (C and C++), a .json file containing some library details, and the model knowledge (for classification only).
You can also re-download any previously compiled library, via the archived libraries list:
4.5.2 Multi-library
In this final step (Step: Deploy) you also have the possibility to add a suffix to the library you are about to compile and download.
This is useful to integrate multiple libraries into the same device / code, when there is a need to:
- monitor several signal sources coming from different sensor types, concurrently, independently,
- train Machine Learning models and gather knowledge from these different input sources,
- take decisions based on the outputs of the Machine Learning algorithms for each signal type.
For instance, one library can be created for 3-axis vibration analysis, and suffixed vibration
:
Later on, a second library can be created later on, for 1-axis electric current analysis, and suffixed current
:
All the NanoEdge AI functions in the corresponding libraries (as well as the header files, variables, and knowledge files if any) is suffixed appropriately, and is usable independently in your code. See below the header files and the suffixed functions and variables corresponding to this example:
Congratulations! You can now use your NanoEdge AI Library!
It is ready to be linked to your C code using your favorite IDE, and embedded in your microcontroller.
For more info, check the library documentation (AD library, CL library), as well as the code snippets on the right side of the screen, which provide general guidelines about how your code could be structured, and how the NanoEdge AI Library functions must be called.
5 Resources
Documentation
All NanoEdge AI Studio documentation is available here.
Tutorials
Step-by-step tutorials, to use NanoEdge AI Studio to build a smart device from A to Z.