This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.- How to start the coprocessor from the bootloader
- How to stop and start Weston
- How to stream camera over network
- How to structure the software to develop STM32Cube examples
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to test and benchmark OpenGLES
- How to transfer a file over network
- How to transfer a file over serial console
- How to transfer files to Discovery kit using Tera Term on Windows PC
- How to tune a NN model using TVM
- How to update OTP with U-Boot
- How to use AI features
- How to use SPI from Linux userland with spidev
- How to use STM32CubeProgrammer to populate a board
- How to use TCP console in STM32CubeIDE
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
- How to use engineering and production modes
- How to use the IIO user space interface
- How to use the RTC
- How to use the Target Status widget in STM32CubeIDE
- How to use the kernel dynamic debug
- I-LINUX-INFINEON-WLAN OpenSTLinux Expansion Package
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S Linux driver
- I2S device tree configuration
- IDE
- IIO Linux kernel tools
- IIO libiio
- IIO overview
- IKS01A2 MEMS expansion board
- IKS01A3 MEMS expansion board
- IKS01Ax MEMS expansion board
- IO expander hardware components
- IPCC device tree configuration
- IPCC internal peripheral
- IP Linux command line
- ISSI
- IWDG device tree configuration
- IWDG internal peripheral
- IWave Systems
- Ifconfig
- Install STM32CubeMP1 package
- Install the IDE
- Install the SDK
- Interrupt overview
- Introduction to Azure RTOS with STM32
- Introduction to FILEX
- Introduction to LEVELX
- Introduction to NETXDUO
- Introduction to THREADX
- Introduction to USBX
- Ka-Ro
- KeyGen release note
- KeyGen tool
- Kmemleak
- LEDs and buttons on STM32 MPU boards
- LPTIM Linux driver
- LPTIM device tree configuration
- LPTIM internal peripheral
- LTDC device tree configuration
- LTDC internal peripheral
- LTTng
- Linaro
- Linux Mailbox framework overview
- Linux RPMsg framework overview
- Linux application frameworks overview
- Linux remoteproc framework overview
- Linux tracing, monitoring and debugging
- Ltrace
- MB1230
- MB1262
- MB1263
- MB1272
- MB1379
- MB1407
- MDMA device tree configuration
- MDMA internal peripheral
- MMC overview
- MTD overview
- Macronix
- Main Page
- Marius-test-01
- Media-ctl
- Menuconfig or how to configure kernel
- Minutes
- Modify, rebuild and reload a firmware
- Modify, rebuild and reload the Linux® kernel
- NEON overview
- NVIC internal peripheral
- NVMEM overview
- Netdata
- Netstat
- Network tools
- Networking overview
- Networking troubleshooting grid
- ONNX Cpp object detection
- ONNX Python image classification
- ONNX Python object detection
- OP-TEE Calibration PTA overview
- OP-TEE OTP overview
- OP-TEE overview
- OPC UA overview
- OTG device tree configuration
- OTG internal peripheral
- Octavo Systems
- Online Linux trainings
- OpenEmbedded
- OpenEmbedded - devtool
- OpenSTLinux BSP architecture overview
- OpenSTLinux architecture overview
- OpenSTLinux directory structure
- OpenSTLinux distribution
- OpenSTLinux filesystem
- OpenSTLinux licenses
- OpenVG overview
- Other resources
- Overview of GPIO pins
- Overview of embedded software architectures
- PC prerequisites
- PC prerequisites about STM32MPU distribution for Android
- PHYTEC
- PHY overview
- PKA device tree configuration
- PKA internal peripheral
- PMIC hardware components
- PRG-TOOLBOX-DFU
- PRG-TOOLBOX-DFU release note
- PRG-TOOLBOX-FB
- PRG-TOOLBOX-FB release note
- PWM overview
- PWR internal peripheral
- Package repository for OpenSTLinux distribution
- Partner program
- Pengutronix
- Perf
- Pinctrl device tree configuration
- Pinctrl overview
- Populate the target and boot the image
- Power overview
- Prevas
- ProvenRun
- Pseudo filesystem
- QT overview
- QUADSPI device tree configuration
- QUADSPI internal peripheral
- Qt
- RCC internal peripheral
- RETRAM internal memory
- RGMII GTX clock delay
- RNG device tree configuration
- RNG internal peripheral
- RTC device tree configuration
- RTC internal peripheral
- RTC overview
- Reading tips
- Regulator overview
- Reserved memory
- Reset device tree configuration
- Reset overview
- Resource manager for coprocessing
- SAES device tree configuration
- SAES internal peripheral
- SAI Linux driver
- SAI device tree configuration
- SAI internal peripheral
- SCMI device tree configuration
- SCMI overview
- SDK for OpenSTLinux distribution
- SDMMC device tree configuration
- SDMMC internal peripheral
- SIANA Systems
- SPDIFRX Linux driver
- SPDIFRX device tree configuration
- SPDIFRX internal peripheral
- SPI device tree configuration
- SPI internal peripheral
- SPI overview
- ST-LINK
- STGEN internal peripheral
- STM32CubeIDE
- STM32CubeIDE release note
- STM32CubeMP13 Package
- STM32CubeMP13 Package - Getting started
- STM32CubeMP13 Package architecture
- STM32CubeMP13 Package release note
- STM32CubeMP13 Package release note - v1.0.0
- STM32CubeMP13 Package release note - v1.1.0
- STM32CubeMP13 ecosystem release note
- STM32CubeMP13 ecosystem release note - v1.0.0
- STM32CubeMP13 ecosystem release note - v1.1.0
- STM32CubeMP13 licenses
- STM32CubeMP13 package - boot architecture
- STM32CubeMP15 Package
- STM32CubeMP15 Package - Getting started
- STM32CubeMP15 Package architecture
- STM32CubeMP15 Package release note
- STM32CubeMP15 Package release note - v1.6.0
- STM32CubeMP15 licenses
- STM32CubeMP1 Package
- STM32CubeMP1 Package release note
- STM32CubeMP1 Package release note - v1.6.0
- STM32CubeMP1 architecture
- STM32CubeMP1 licenses
- STM32CubeMX
- STM32CubeMX release note
- STM32CubeProgrammer
- STM32CubeProgrammer OTP management
- STM32CubeProgrammer STPMIC1 NVM management
- STM32CubeProgrammer flashlayout
- STM32CubeProgrammer release note
- STM32DDRFW-UTIL
- STM32DDRFW-UTIL release note
- STM32MP135x-DK - board assembly
- STM32MP135x-DK - board connections
- STM32MP135x-DK - hardware description
- STM32MP135x-DK - software distributions
- STM32MP13 ADC internal peripheral
- STM32MP13 Developer Package - STM32CubeMP13 Package
- STM32MP13 Discovery kits - Starter Package
- STM32MP13 Discovery kits - getting started
- STM32MP13 Discovery kits - required material
- STM32MP13 Discovery kits - starting for the first time
- STM32MP13 Linux kernel overview
- STM32MP13 OTP mapping
- STM32MP13 PWR internal peripheral
- STM32MP13 RAM mapping
- STM32MP13 SRAM internal memory
- STM32MP13 U-Boot
- STM32MP13 V4L2 camera overview
- STM32MP13 VREFBUF internal peripheral
- STM32MP13 backup registers
- STM32MP13 boards
- STM32MP13 clock tree
- STM32MP13 ecosystem errata sheet
- STM32MP13 internal peripherals assignment table template
- STM32MP13 internal peripherals software table template
- STM32MP13 microprocessor
- STM32MP13 peripherals overview
- STM32MP13 resources
- STM32MP157x-DKx - board assembly
- STM32MP157x-DKx - board connections
- STM32MP157x-DKx - hardware description
- STM32MP157x-DKx - software distributions
- STM32MP157x-EV1 - board assembly
- STM32MP157x-EV1 - board connections
- STM32MP157x-EV1 - hardware description
- STM32MP157x-EV1 - software distributions
- STM32MP15 ADC internal peripheral
- STM32MP15 Discovery kits - Starter Package
- STM32MP15 Discovery kits - getting started
- STM32MP15 Discovery kits - required material
- STM32MP15 Discovery kits - starting for the first time
- STM32MP15 Evaluation boards - Starter Package
- STM32MP15 Evaluation boards - Starter Package for Android
- STM32MP15 Evaluation boards - getting started
- STM32MP15 Evaluation boards - required material
- STM32MP15 Evaluation boards - starting for the first time
- STM32MP15 Linux kernel overview
- STM32MP15 MCU SRAM internal memory
- STM32MP15 OTP mapping
- STM32MP15 PWR internal peripheral
- STM32MP15 RAM mapping
- STM32MP15 U-Boot
- STM32MP15 V4L2 camera overview
- STM32MP15 VREFBUF internal peripheral
- STM32MP15 backup registers
- STM32MP15 boards
- STM32MP15 clock tree
- STM32MP15 distribution for Android release note
- STM32MP15 distribution for Android release note - v1.0.0
- STM32MP15 distribution for Android release note - v1.1.0
- STM32MP15 distribution for Android release note - v2.0.0
- STM32MP15 ecosystem errata sheet
- STM32MP15 internal peripherals assignment table template
- STM32MP15 internal peripherals software table template
- STM32MP15 microprocessor
- STM32MP15 peripherals overview
- STM32MP15 resources
- STM32MP1 DMA
- STM32MP1 Developer Package
- STM32MP1 Developer Package - OpenSTLinux BSP
- STM32MP1 Developer Package - SDK
- STM32MP1 Developer Package - STM32CubeMP1 Package
- STM32MP1 Developer Package for Android
- STM32MP1 Distribution Package
- STM32MP1 Distribution Package - OpenSTLinux distribution
- STM32MP1 Distribution Package for Android
- STM32MP1 Platform trace and debug environment overview
- STM32MP1 Platform trace and debug environment overview for Android
- STM32MP1 Starter Package - images
- STM32MP1 internal peripherals assignment table template
- STM32MPU Embedded Software architecture overview
- STM32MPU Embedded Software distribution
- STM32MPU Embedded Software distribution for Android
- STM32MPU Embedded Software for Android architecture overview
- STM32MPU distribution for Android
- STM32MPU distribution for Android licenses - v1.0.0
- STM32MPU distribution for Android licenses - v1.1.0
- STM32MPU distribution for Android licenses - v2.0.0
- STM32PRGFW-UTIL
- STM32PRGFW-UTIL release note
- STM32 MPU Flash mapping
- STM32 MPU Linux kernel overview
- STM32 MPU OpenSTLinux release note
- STM32 MPU OpenSTLinux release note/Changes notification
- STM32 MPU OpenSTLinux release note - v5.0.0
- STM32 MPU OpenSTLinux release note - v5.0.0/Changes notification – v5.0.0
- STM32 MPU ROM code overview
- STM32 MPU ROM code secure boot
- STM32 MPU ROM trace analyzer
- STM32 MPU boards
- STM32 MPU device tree
- STM32 MPU ecosystem release note
- STM32 MPU ecosystem release note - v5.0.0
- STM32 MPU resources
- STM32 MPU trainings
- STM32 MPUs Community FAQ
- STM32 header for binary files
- STM internal peripheral
- STPM4RasPI expansion board
- SYSCFG internal peripheral
- SYSRAM internal memory
- Savoir-Faire Linux
- Secure Firmware Update
- Secure Secret Provisioning (SSP)
- Security overview
- Sequitur Labs
- Serial TTY device tree configuration
- Serial TTY overview
- Signing tool
- Signing tool release note
- SoMLabs
- Soundcard configuration
- Standard SDK directory structure
- Strace
- Subpart - STM32MP1 - Starter Package
- Sysdig
- Sysprof