This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:=:
Displayed 205 items.
- How to get Terminal (transclusion) (← links)
- Blktrace (transclusion) (← links)
- Ethtool (transclusion) (← links)
- Ifconfig (transclusion) (← links)
- Ltrace (transclusion) (← links)
- OpenEmbedded - devtool (transclusion) (← links)
- Tcpdump (transclusion) (← links)
- How to setup a WLAN connection (transclusion) (← links)
- IP Linux command line (transclusion) (← links)
- Wayland Weston overview (transclusion) (← links)
- I2C overview (transclusion) (← links)
- I2C i2c-tools (transclusion) (← links)
- IIO overview (transclusion) (← links)
- GDB (transclusion) (← links)
- PC prerequisites (transclusion) (← links)
- How to avoid proxy issues (transclusion) (← links)
- WLAN overview (transclusion) (← links)
- How to use the IIO user space interface (transclusion) (← links)
- Strace (transclusion) (← links)
- Netstat (transclusion) (← links)
- Perf (transclusion) (← links)
- Sysstat tool suite (transclusion) (← links)
- LTTng (transclusion) (← links)
- Menuconfig or how to configure kernel (transclusion) (← links)
- Ftrace (transclusion) (← links)
- CAN overview (transclusion) (← links)
- Crypto API overview (transclusion) (← links)
- CEC overview (transclusion) (← links)
- U-Boot overview (transclusion) (← links)
- How to debug Weston (transclusion) (← links)
- How to launch Khronos OpenGLES conformance tests (transclusion) (← links)
- How to launch glmark2 benchmark (transclusion) (← links)
- Serial TTY overview (transclusion) (← links)
- How to use TTY with User Terminal (transclusion) (← links)
- Pinctrl overview (transclusion) (← links)
- GPIOLib overview (transclusion) (← links)
- How to control a GPIO in userspace (transclusion) (← links)
- How to control a GPIO in kernel space (transclusion) (← links)
- STM32MP15 V4L2 camera overview (transclusion) (← links)
- STM32MP15 Evaluation boards - starting for the first time (transclusion) (← links)
- STM32MP15 Evaluation boards - required material (transclusion) (← links)
- STM32CubeProgrammer (transclusion) (← links)
- How to use the kernel dynamic debug (transclusion) (← links)
- Watchdog overview (transclusion) (← links)
- Regulator overview (transclusion) (← links)
- PWM overview (transclusion) (← links)
- U-Boot - How to debug (transclusion) (← links)
- STM32MP15 U-Boot (transclusion) (← links)
- Pseudo filesystem (transclusion) (← links)
- How to populate the SD card with dd command (transclusion) (← links)
- How to cross-compile with the Developer Package (transclusion) (← links)
- STM32MP157x-EV1 - board connections (transclusion) (← links)
- STM32MP157x-EV1 - board assembly (transclusion) (← links)
- STM32MP157x-EV1 - hardware description (transclusion) (← links)
- How to configure TF-A BL2 (transclusion) (← links)
- How to create an SDK for OpenSTLinux distribution (transclusion) (← links)
- How to debug TF-A BL2 (transclusion) (← links)
- Weston keyboard shortcuts (transclusion) (← links)
- Power overview (transclusion) (← links)
- Clock overview (transclusion) (← links)
- How to transfer a file over serial console (transclusion) (← links)
- STM32CubeProgrammer flashlayout (transclusion) (← links)
- Dmesg and Linux kernel log (transclusion) (← links)
- V4l2-ctl (transclusion) (← links)
- How to use USB mass storage in U-Boot (transclusion) (← links)
- Gst-play (transclusion) (← links)
- STM32 MPU OpenSTLinux release note (transclusion) (← links)
- STM32CubeProgrammer release note (transclusion) (← links)
- Example of directory structure for Packages (transclusion) (← links)
- Netdata (transclusion) (← links)
- Gdbgui (transclusion) (← links)
- Gst-typefind (transclusion) (← links)
- STM32MP1 Distribution Package - OpenSTLinux distribution (transclusion) (← links)
- Ethernet overview (transclusion) (← links)
- GDB commands (transclusion) (← links)
- Kmemleak (transclusion) (← links)
- Sysprof (transclusion) (← links)
- Valgrind (transclusion) (← links)
- How to transfer a file over network (transclusion) (← links)
- ADC OpenSTLinux drivers (transclusion) (← links)
- How to find Linux kernel driver associated to a device (transclusion) (← links)
- Gst-discoverer (transclusion) (← links)
- Core dump (transclusion) (← links)
- Trace-cmd and kernelshark trace viewer (transclusion) (← links)
- Subpart - STM32MP1 - Starter Package (transclusion) (← links)
- MB1272 (transclusion) (← links)
- STM32MP157x-DKx - board connections (transclusion) (← links)
- STM32MP15 Discovery kits - starting for the first time (transclusion) (← links)
- STM32MP157x-DKx - board assembly (transclusion) (← links)
- STM32MP157x-DKx - hardware description (transclusion) (← links)
- STM32MP15 Discovery kits - required material (transclusion) (← links)
- How to display on HDMI (transclusion) (← links)
- How to create your own distribution (transclusion) (← links)
- DAC Linux driver (transclusion) (← links)
- Debugging the Linux kernel using the GDB (transclusion) (← links)
- Hardware random overview (transclusion) (← links)
- GStreamer troubleshooting grid (transclusion) (← links)
- Wayland Weston troubleshooting grid (transclusion) (← links)
- How to add a customer application (transclusion) (← links)
- How to customize the Linux kernel (transclusion) (← links)
- DFSDM Linux driver (transclusion) (← links)
- Ethernet device tree configuration (transclusion) (← links)
- NVMEM overview (transclusion) (← links)
- How to configure the Weston keyboard layout (transclusion) (← links)
- How to integrate an external software package (transclusion) (← links)
- How to boot the kernel via TFTP from U-Boot (transclusion) (← links)
- How to manually update bootloaders (transclusion) (← links)
- How to stop and start Weston (transclusion) (← links)
- How to stream camera over network (transclusion) (← links)
- Trace and debug scenario - UART issue (transclusion) (← links)
- How to set up a SocketCAN interface (transclusion) (← links)
- How to send or receive CAN data (transclusion) (← links)
- How to support UBIFS through MTD (transclusion) (← links)
- How to support EXT4 through MMC (transclusion) (← links)
- How to configure ethernet interface (transclusion) (← links)
- How to perform ssh connection (transclusion) (← links)
- How to perform ping test (transclusion) (← links)
- Configfs (transclusion) (← links)
- How to configure a WLAN interface on hotspot mode (transclusion) (← links)
- WLAN and Bluetooth hardware component (transclusion) (← links)
- Visual troubleshooting grid (transclusion) (← links)
- How to set up a Bluetooth connection (transclusion) (← links)
- How to scan Bluetooth devices (transclusion) (← links)
- How to scan BLE devices (transclusion) (← links)
- How to profile video framerate (transclusion) (← links)
- How to monitor the display framerate (transclusion) (← links)
- Top Linux command line (transclusion) (← links)
- How to control a RNG in userspace (transclusion) (← links)
- How to retrieve Cortex-M4 logs after crash (transclusion) (← links)
- How to monitor the GCNANO GPU load (transclusion) (← links)
- DRM KMS troubleshooting grid (transclusion) (← links)
- How to play audio (transclusion) (← links)
- Reading tips (transclusion) (← links)
- How to assign an internal peripheral to an execution context (transclusion) (← links)
- Debugfs (transclusion) (← links)
- USB overview (transclusion) (← links)
- SPI overview (transclusion) (← links)
- How to cross-compile with the Distribution Package (transclusion) (← links)
- HDP Linux driver (transclusion) (← links)
- DRM KMS overview (transclusion) (← links)
- CMSIS-SVD environment and scripts (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Populate the target and boot the image (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-DK2/Develop on Arm® Cortex®-M4/Modify, rebuild and reload a firmware (transclusion) (← links)
- How to start the coprocessor from the bootloader (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image (transclusion) (← links)
- Sysdig (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands (transclusion) (← links)
- Systemtap (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-M4/Modify, rebuild and reload a firmware (transclusion) (← links)
- Create a simple hello-world application (transclusion) (← links)
- Populate the target and boot the image (transclusion) (← links)
- How to accelerate JPEG compression and decompression (transclusion) (← links)
- How to calibrate the touchscreen (transclusion) (← links)
- How to configure system resources (transclusion) (← links)
- How to get name and current status of a DRM connector (transclusion) (← links)
- How to install JAVA JDK (transclusion) (← links)
- How to modify the panel backlight (transclusion) (← links)
- How to optimize the boot time (transclusion) (← links)
- How to record audio (transclusion) (← links)
- How to configure OP-TEE (transclusion) (← links)
- Modify, rebuild and reload a firmware (transclusion) (← links)
- How to build Linux kernel user space tools (transclusion) (← links)
- IKS01Ax MEMS expansion board (transclusion) (← links)
- How to protect the coprocessor firmware (transclusion) (← links)
- How to use SPI from Linux userland with spidev (transclusion) (← links)
- How to use the RTC (transclusion) (← links)
- Coprocessor management troubleshooting grid (transclusion) (← links)
- Package repository for OpenSTLinux distribution (transclusion) (← links)
- Wrapper for FSBL images (transclusion) (← links)
- How to update OTP with U-Boot (transclusion) (← links)
- How to configure U-Boot for your board (transclusion) (← links)
- STPM4RasPI expansion board (transclusion) (← links)
- How to read or write peripheral registers (transclusion) (← links)
- How to build and use an SDK for QT (transclusion) (← links)
- How to install Node-RED (transclusion) (← links)
- How to install a simple web browser (transclusion) (← links)
- How to load U-Boot with STM32CubeProgrammer (transclusion) (← links)
- How to configure TF-A FIP (transclusion) (← links)
- How to configure TF-A FW CONFIG (transclusion) (← links)
- IKS01A3 MEMS expansion board (transclusion) (← links)
- IKS01A2 MEMS expansion board (transclusion) (← links)
- STM32MP13 U-Boot (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Populate the target and boot the image (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Execute basic commands (transclusion) (← links)
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Create a simple hello-world application (transclusion) (← links)
- How to load U-Boot with dfu-util (transclusion) (← links)
- How to measure the DDR throughput (transclusion) (← links)
- How to integrate Azure IoT Edge on OpenSTLinux (transclusion) (← links)
- STM32MP13 V4L2 camera overview (transclusion) (← links)
- How to use UART as serial boot device with STM32CubeProgrammer (transclusion) (← links)
- How to configure a WLAN gateway (transclusion) (← links)
- Media-ctl (transclusion) (← links)
- STM32MP135x-DK - board assembly (transclusion) (← links)
- STM32MP13 Discovery kits - starting for the first time (transclusion) (← links)
- How to install OPC UA (transclusion) (← links)
- How to add a new parallel or serial NAND flash memory device in Yocto (transclusion) (← links)
- How to use U-Boot stm32key command (transclusion) (← links)
- TF-A BL2 Trusted Board Boot (transclusion) (← links)
- STM32MP135x-DK - hardware description (transclusion) (← links)
- How to prevent the year 2038 bug (transclusion) (← links)
- How to deploy SSP: a step-by-step approach (transclusion) (← links)
- STM32 MPU OpenSTLinux release note/Changes notification (transclusion) (← links)