Approved version. Approved on: 13:06, 21 May 2021
- Last edited 2 years ago ago
STM32MP13x
This category groups together all articles that are applicable for the STM32MP13x lines
Subcategories
This category has the following 7 subcategories, out of 7 total.
M
P
S
U
Pages in category "STM32MP13x"
The following 200 pages are in this category, out of 511 total.
(previous page) (next page)H
- How to manage OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure acceleration and orientation
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure performance of your NN models using the Coral Edge TPU
- How to measure temperature and humidity
- How to measure the DDR throughput
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to optimize the boot time
- How to perform digital signature with TPM
- How to perform ping test
- How to perform Secure Boot from Distribution package
- How to perform ssh connection
- How to play a video
- How to play audio
- How to populate and boot a board with OP-TEE
- How to populate the SD card with dd command
- How to prevent the year 2038 bug
- How to profile video framerate
- How to read or write peripheral registers
- How to record audio
- How to reproduce an example using PyCoral API
- How to run Coral Edge TPU inference using Python TensorFlow Lite API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to secure STM32 MPU
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to set up proxy and P2P Ethernet connection with STM32CubeIDE
- How to setup a WLAN connection
- How to setup target password in STM32CubeIDE
- How to stop and start Weston
- How to stream camera over network
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to transfer a file over network
- How to transfer a file over serial console
- How to update OTP with U-Boot
- How to use SPI from Linux userland with spidev
- How to use STM32CubeProgrammer to populate a board
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- How to use the RTC
- How to use the Target Status widget in STM32CubeIDE
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
I
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S device tree configuration
- I2S Linux driver
- Ifconfig
- IIO libiio
- IIO Linux kernel tools
- IIO overview
- Interrupt overview
- IO expander hardware components
- IP Linux command line
- IWDG device tree configuration
- IWDG internal peripheral
L
M
N
O
- Online Linux trainings
- OP-TEE Calibration PTA overview
- OP-TEE OTP overview
- OP-TEE overview
- OPC UA overview
- OpenEmbedded
- OpenEmbedded - devtool
- OpenSTLinux architecture overview
- OpenSTLinux BSP architecture overview
- OpenSTLinux directory structure
- OpenSTLinux distribution
- OpenSTLinux filesystem
- OpenSTLinux licenses
- LegalInformation:OpenSTLinux licenses - v4.0.0
- LegalInformation:OpenSTLinux licenses - v4.1.0
- OTG device tree configuration
- OTG internal peripheral
- Overview of GPIO pins
P
R
S
- SAES device tree configuration
- SAES internal peripheral
- SAI device tree configuration
- SAI internal peripheral
- SAI Linux driver
- SCMI device tree configuration
- SCMI overview
- SDK for OpenSTLinux distribution
- SDMMC device tree configuration
- SDMMC internal peripheral
- Secure Firmware Update
- Secure Secret Provisioning (SSP)
- Security overview
- Serial TTY device tree configuration
- Serial TTY overview
- Signing tool
- Signing tool release note
- SPDIFRX device tree configuration
- SPDIFRX internal peripheral
- SPDIFRX Linux driver
- SPI device tree configuration
- SPI internal peripheral
- SPI overview
- ST-LINK
- Standard SDK directory structure
- STGEN internal peripheral
- STM32 header for binary files
- STM32 MPU device tree
- STM32 MPU ecosystem release note
- STM32 MPU ecosystem release note - v4.0.0
- STM32 MPU ecosystem release note - v4.1.0
- STM32 MPU Flash mapping
- STM32 MPU Linux kernel overview
- STM32 MPU OpenSTLinux release note
- STM32 MPU OpenSTLinux release note - v4.0.0
- STM32 MPU OpenSTLinux release note - v4.0.0/Changes notification – v4.0.0
- STM32 MPU OpenSTLinux release note - v4.1.0
- STM32 MPU OpenSTLinux release note - v4.1.0/Changes notification – v4.1.0
- STM32 MPU OpenSTLinux release note/Changes notification
- STM32 MPU resources
- STM32 MPU ROM code overview
- STM32 MPU ROM code secure boot
- STM32 MPU ROM trace analyzer
- STM32 MPU trainings
- STM32 MPUs Community FAQ
- STM32CubeIDE
- STM32CubeIDE release note
- STM32CubeMX
- STM32CubeProgrammer
- STM32CubeProgrammer flashlayout
- STM32CubeProgrammer OTP management
- STM32CubeProgrammer release note
- STM32DDRFW-UTIL
- STM32DDRFW-UTIL release note
- STM32MP1 Developer Package
- STM32MP1 Developer Package - SDK
- STM32MP1 Distribution Package
- STM32MP1 Distribution Package - OpenSTLinux distribution
- STM32MP1 DMA
- STM32MP1 Platform trace and debug environment overview
- STM32MP1 Starter Package - images