This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This category groups together all articles that are applicable for the STM32MP13x lines
Subcategories
This category has the following 9 subcategories, out of 9 total.
A
M
P
S
U
Pages in category "STM32MP13x"
The following 200 pages are in this category, out of 568 total.
(previous page) (next page)D
- DFSDM Linux driver
- DH electronics
- Display bridges hardware components
- Display panels hardware components
- DMA device tree configuration
- DMA internal peripheral
- Dmaengine overview
- DMAMUX device tree configuration
- DMAMUX internal peripheral
- Dmesg and Linux kernel log
- Dpkg
- DRM KMS overview
- DRM KMS troubleshooting grid
- DTS internal peripheral
E
- Embedded software
- Embedded Wizard
- Emcraft Systems
- Emotas
- Emtrion
- Engicam
- ETH internal peripheral
- Ethernet device tree configuration
- Ethernet overview
- Ethtool
- ETM internal peripheral
- ETZPC device tree configuration
- ETZPC internal peripheral
- Example of directory structure for Packages
- EXTI internal peripheral
F
G
- GDB
- GDB commands
- Gdbgui
- Getting started
- Getting started with software distributions
- Getting started/STM32MP1 boards
- Getting started/STM32MP1 boards/STM32MP135x-DK
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Create a simple hello-world application
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Install the SDK
- Getting started/STM32MP1 boards/STM32MP135x-DK/Develop on Arm® Cortex®-A7/Modify, rebuild and reload the Linux® kernel
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Execute basic commands
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Populate the target and boot the image
- Getting started/STM32MP1 boards/STM32MP135x-DK/Let's start/Use the demo launcher
- Getting started/STM32MP1 boards/STM32MP135x-DK/What's next
- GIC internal peripheral
- Git
- GPIO device tree configuration
- GPIO internal peripheral
- GPIOLib overview
- Gst-discoverer
- Gst-play
- Gst-typefind
- GStreamer overview
- GStreamer troubleshooting grid
- GTK demo launcher
H
- HandsOnTraining
- Hardware
- Hardware random overview
- Hardware Unique Key overview
- HASH device tree configuration
- HASH internal peripheral
- HDP device tree configuration
- HDP internal peripheral
- HDP Linux driver
- How to
- How to accelerate JPEG compression and decompression
- How to access information in sysfs
- How to activate HSE monitoring
- How to activate HSI and CSI oscillators calibration
- How to add a customer application
- How to adjust USBPHYC settings using USB Eye Diagram
- How to assign an internal peripheral to an execution context
- How to avoid proxy issues
- How to boot the kernel via TFTP from U-Boot
- How to build an example using libcoral API
- How to build and use an SDK for QT
- How to build Linux kernel user space tools
- How to build LVGL applications using STM32CubeIDE
- How to calibrate the touchscreen
- How to change the CPU frequency
- How to check that a device tree resource is correctly set
- How to check the CVE status in OpenSTLinux
- How to classify images with AI
- How to compile model and run inference on Coral Edge TPU using STM32MP1
- How to compile the device tree with the Distribution Package
- How to configure a 256MB DDR mapping from STM32 MPU Distribution Package
- How to configure a WLAN gateway
- How to configure a WLAN interface on client mode
- How to configure a WLAN interface on hotspot mode
- How to configure ethernet interface
- How to configure flash memory for TF-A BL2
- How to configure OP-TEE
- How to configure PWR Wake-up pins
- How to configure TF-A BL2
- How to configure TF-A FIP
- How to configure TF-A FW CONFIG
- How to configure the Weston keyboard layout
- How to configure U-Boot for your board
- How to configure U-Boot to support Fastboot mode
- How to configure UEFI boot with the Distribution Package
- How to configure Weston screen resolution
- How to control a GPIO in kernel space
- How to control a GPIO in userspace
- How to control a RNG in userspace
- How to convert a Tensorflow™ Lite model to ONNX using tf2onnx
- How to copy and paste in the STM32CubeIDE console
- How to create a new open embedded layer
- How to create an SDK for OpenSTLinux distribution
- How to create Signed FIT image from Distribution package
- How to create your own distribution
- How to create your own image
- How to create your own machine
- How to create your product from design to manufacturing
- How to cross-compile with the Developer Package
- How to cross-compile with the Distribution Package
- How to customize the Linux kernel
- How to debug a user space application with STM32CubeIDE
- How to debug a user space application with STM32CubeIDE/User space CDT project
- How to debug a user space application with STM32CubeIDE/User space GTK library project
- How to debug a user space application with STM32CubeIDE/User space project
- How to debug a user space application with STM32CubeIDE/User space shared library project
- How to debug a user space application with STM32CubeIDE/User space static library project
- How to debug OP-TEE
- How to debug TF-A BL2
- How to debug Weston
- How to define your low-power strategy
- How to deploy SSP: a step-by-step approach
- How to detect memory leaks
- How to detect objects with AI
- How to develop an OP-TEE Trusted Application
- How to develop an OP-TEE Trusted Application with STM32CubeIDE
- How to develop an X-Linux Expansion Package
- How to diagnose a boot failure
- How to display an image using Weston
- How to display on HDMI
- How to enable earlyprintk for Linux kernel
- How to encrypt a disk with dm-crypt
- How to ensure data coherency when cache and MMU used in STM32CubeMP13
- How to find Linux kernel driver associated to a device
- How to get DRM KMS logs
- How to get name and current status of a DRM connector
- How to get started with STM32CubeIDE from scratch
- How to get Terminal
- How to get video details
- How to install JAVA JDK
- How to install OPC UA
- How to install the Yocto Project SDK in STM32CubeIDE
- How to integrate an external software package
- How to load and start STM32CubeMP13 applications via eMMC storage
- How to load and start STM32CubeMP13 applications via microSD card
- How to load and start STM32CubeMP13 applications via SNOR flash
- How to load U-Boot with dfu-util
- How to load U-Boot with STM32CubeProgrammer
- How to make a camera preview
- How to make a screen capture in Weston
- How to make a video capture of Weston desktop
- How to manage OpenSTLinux projects in STM32CubeIDE
- How to manage OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure acceleration and orientation
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure performance of your NN models using the Coral Edge TPU
- How to measure temperature and humidity
- How to measure the DDR throughput
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to optimize the boot time
- How to perform digital signature with TPM
- How to perform ping test
- How to perform Secure Boot from Distribution package
- How to perform ssh connection
- How to play a video
- How to play audio
- How to populate the SD card with dd command
- How to prevent the year 2038 bug
- How to profile video framerate
- How to read or write peripheral registers
- How to record audio
- How to reproduce an example using PyCoral API
- How to run Coral Edge TPU inference using Python TensorFlow Lite API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to secure STM32 MPU
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to set up proxy and P2P Ethernet connection with STM32CubeIDE
- How to setup a WLAN connection
- How to setup target password in STM32CubeIDE
- How to stop and start Weston
- How to stream camera over network