Applicable for STM32MP13x lines, STM32MP15x lines, STM32MP21x lines, STM32MP23x lines, STM32MP25x lines

This article explains how to create, build and debug a shared library, dynamically linked with a Linux® user space application on STM32 MPU.

Important
This article is based onto STM32MP15x lines  but it is also applicable to any STM32 MPU device.

1. Prerequisites[edit | edit source]

You should have followed instructions given in this article How to develop an OpenSTLinux user space application with STM32CubeIDE before jumping in the current one.

2. Create a user space shared library project[edit | edit source]

In the Cortex®-A7 sub-project context, named here MP157C-DK2_CA7, right-click and select Create a userspace Project...

User space project wizard shortcut


A Shared Library project type, in C language, is selected.

Note that the user space project uses by default the SDK version associated to the Cortex®-A7 sub-project.


User space shared library creation

3. Build[edit | edit source]

  • Select your project, right-click and then Build Project.
Shared library build

4. Update myExe project sources & properties, in order to use mySharedLib[edit | edit source]

Hereafter is an updated code for main() to call mySharedLib function say_hello().
You must also reference mySharedLib project inside myExe properties: C/C++ General > Paths and Symbols > References, as depicted below.

Executable source & properties update

5. Prepare Debug Configuration[edit | edit source]

You can check boot messages via Linux® console opened with butterfly icon (shown below), but remember this console cannot be shared outside STM32CubeIDE (minicom,...).

In order to debug user space application, your target must be Linux® booted and network connected.


In order to check network connection, start the Target Status widget in the bottom right corner of the window.

Target Status - green


Check How to set up proxy and P2P Ethernet connection with STM32CubeIDE if you are in that case.


6. Set Linux® deployment configuration[edit | edit source]

To run or debug the executable myExe and its shared library mySharedLib, it is required to download the shared library object (.so) to the STM32MP15x lines .

Select the shared library project, right-click Run as... > Run Configurations, then select STM32 Cortex-A Linux Deployment'.

Run configuration shortcut


Linux deployment configuration

7. Set Debug Configuration[edit | edit source]

Select your project, right-click Debug as... > Debug Configurations, then select STM32 Cortex-A Remote Application'.

The default connection proposed is "MPU SSH", corresponding to the target IP address discovered by the Target Status widget. The default destination directory is /home/root.

For the executable myExe to load the mySharedLib dynamic library, a setup of LD_LIBRARY_PATH with the path to mySharedLib is needed before starting debug.

Debug configuration setup


64-bit SDK set-up

Warning
For STM32MP23x lines  and STM32MP25x lines  absolute path to 64-bit SDK (MP2) GDB client is needed.

/local/home/<username>/SDK_6.2.1_mp2/sysroots/x86_64-ostl_sdk-linux/usr/bin/aarch64-ostl-linux/aarch64-ostl-linux-gdb

User space debug configuration - main tab Debugger


8. Debug: stepping into mySharedLib[edit | edit source]

Click Debug :

  1. Executable is downloaded to the target,
  2. GDBServer is launched on the target,
  3. GDBClient is launched on the workstation and can exchange via the network with GDBServer.
User space shared library debug
Information
In case of error; stop any GDBServer running on the target before launching a new debug session.