This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This category groups together all articles that are applicable for the STM32MP13x lines
Subcategories
This category has the following 9 subcategories, out of 9 total.
A
M
P
S
U
Pages in category "STM32MP13x"
The following 200 pages are in this category, out of 568 total.
(previous page) (next page)H
- How to develop an OP-TEE Trusted Application with STM32CubeIDE
- How to develop an X-Linux Expansion Package
- How to diagnose a boot failure
- How to display an image using Weston
- How to display on HDMI
- How to enable earlyprintk for Linux kernel
- How to encrypt a disk with dm-crypt
- How to ensure data coherency when cache and MMU used in STM32CubeMP13
- How to find Linux kernel driver associated to a device
- How to get DRM KMS logs
- How to get name and current status of a DRM connector
- How to get started with STM32CubeIDE from scratch
- How to get Terminal
- How to get video details
- How to install JAVA JDK
- How to install OPC UA
- How to install the Yocto Project SDK in STM32CubeIDE
- How to integrate an external software package
- How to load and start STM32CubeMP13 applications via eMMC storage
- How to load and start STM32CubeMP13 applications via microSD card
- How to load and start STM32CubeMP13 applications via SNOR flash
- How to load U-Boot with dfu-util
- How to load U-Boot with STM32CubeProgrammer
- How to make a camera preview
- How to make a screen capture in Weston
- How to make a video capture of Weston desktop
- How to manage OpenSTLinux projects in STM32CubeIDE
- How to manage OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure acceleration and orientation
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure performance of your NN models using the Coral Edge TPU
- How to measure temperature and humidity
- How to measure the DDR throughput
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to optimize the boot time
- How to perform digital signature with TPM
- How to perform ping test
- How to perform Secure Boot from Distribution package
- How to perform ssh connection
- How to play a video
- How to play audio
- How to populate the SD card with dd command
- How to prevent the year 2038 bug
- How to profile video framerate
- How to read or write peripheral registers
- How to record audio
- How to reproduce an example using PyCoral API
- How to run Coral Edge TPU inference using Python TensorFlow Lite API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to secure STM32 MPU
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to set up proxy and P2P Ethernet connection with STM32CubeIDE
- How to setup a WLAN connection
- How to setup target password in STM32CubeIDE
- How to stop and start Weston
- How to stream camera over network
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to transfer a file over network
- How to transfer a file over serial console
- How to update OTP with U-Boot
- How to use SPI from Linux userland with spidev
- How to use STM32CubeProgrammer to populate a board
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- How to use the RTC
- How to use the Target Status widget in STM32CubeIDE
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
I
- I-LINUX-INFINEON-WLAN OpenSTLinux Expansion Package
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S device tree configuration
- I2S Linux driver
- Ifconfig
- IIO libiio
- IIO Linux kernel tools
- IIO overview
- Interrupt overview
- Introduction to Azure RTOS with STM32
- Introduction to FILEX
- Introduction to LEVELX
- Introduction to NETXDUO
- Introduction to THREADX
- Introduction to USBX
- IO expander hardware components
- IP Linux command line
- ISSI
- IWave Systems
- IWDG device tree configuration
- IWDG internal peripheral
L
M
N
O
- Octavo Systems
- Online Linux trainings
- ONNX Cpp object detection
- ONNX Python image classification
- ONNX Python object detection
- OP-TEE Calibration PTA overview
- OP-TEE OTP overview
- OP-TEE overview
- OPC UA overview
- OpenEmbedded
- OpenEmbedded - devtool
- OpenSTLinux architecture overview
- OpenSTLinux BSP architecture overview
- OpenSTLinux directory structure
- OpenSTLinux distribution
- OpenSTLinux filesystem
- OpenSTLinux licenses
- LegalInformation:OpenSTLinux licenses - v4.0.0
- LegalInformation:OpenSTLinux licenses - v4.1.0
- LegalInformation:OpenSTLinux licenses - v5.0.0
- OTG device tree configuration
- OTG internal peripheral
- Overview of GPIO pins
P
- Package repository for OpenSTLinux distribution
- PC prerequisites
- Pengutronix
- Perf
- PHY overview
- PHYTEC
- Pinctrl device tree configuration
- Pinctrl overview
- PKA device tree configuration
- PKA internal peripheral
- PMIC hardware components
- Power overview
- Prevas
- PRG-TOOLBOX-DFU
- PRG-TOOLBOX-DFU release note
- PRG-TOOLBOX-FB
- PRG-TOOLBOX-FB release note
- ProvenRun
- Pseudo filesystem
- PWM overview
- PWR internal peripheral