1. Release information[edit source]
This article aims to describe the content of the software release included in the STM32CubeMP1 Package, version v1.3.0
2. Delivery scope and purpose[edit source]
The STM32CubeMP1 Package is a software package running on Arm® Cortex® M4 processors and is a fundamental part of the STM32MPU Embedded Software distribution.
This release includes:
- The STM32Cube HAL, STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
- Low-layer APIs (LL APIs) offering a fast lightweight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
- A consistent set of middleware components such as FreeRTOS and OpenAMP.
- All embedded software utilities delivered with a full set of examples.
It also includes:
- BSP for the STM32MP157x-EV1 Evaluation board
and the STM32MP157x-DK2 Discovery kit
(button and LEDs only)
- Multi-core components
- OpenAMP
- ResourceManager
- CoproSync
- Projects : several projects ( examples, applications and demonstration firmware) are implemented in different IDEs:
- STM32CubeIDE : IDE delivered by ST
- EWARM (version 8.32.3 and laters)
- MDK-ARM(Pack Keil.STM32MP1xx_DFP.1.1.0.pack + MDK-ARM 5.27 and laters)
- System Workbench for STM32 toolchain (SW4STM32): now deprecated
- BSP for the STM32MP157x-EV1 Evaluation board
3. Supported devices[edit source]
The drivers provided within this package support the following devices :
- STM32MP157Cxx, STM32MP157Axx, STM32MP157Dxx, STM32MP157Fxx
- STM32MP153Cxx, STM32MP153Axx, STM32MP153Dxx, STM32MP153Fxx
- STM32MP151Cxx, STM32MP151Axx, STM32MP151Dxx, STM32MP151Fxx
4. Supported hardware[edit source]
This software delivery is applicable to the following boards:
- STM32MP157C-EV1 Evaluation board
. For information about this board, read the article STM32MP157x-EV1 - hardware description.
- STM32MP157C-DK2 Discovery kit
. For information about this board, read the article STM32MP157x-DKx - hardware description.
5. Known issues and limitations[edit source]
- OpenAMP compilation issue with MDK-ARM when code generated through CubeMx :
- To avoid compiling errors in OpenAMP when compiling in MDK-ARM IDE, you have to disable the « Use MicroLIB » in « Target » tab.
- To avoid compiling errors in OpenAMP when compiling in MDK-ARM IDE, you have to disable the « Use MicroLIB » in « Target » tab.
- Deprecated IDE:
- For projects examples still in SW4STM32 format ( deprecated), you can easily import them in STM32CubeIDE.
- For projects examples still in SW4STM32 format ( deprecated), you can easily import them in STM32CubeIDE.
6. Contents[edit source]
6.1. Main Changes[edit source]
- SMARTCARD:
- HAL driver implemented in this STM32CubeMP1 Package .
- This peripheral has been tested on the STM32MP157C-EV1 Evaluation board
through IO expander (MFXSTM32L152) from MB1262 motherboard
- RCC and CMSIS:
- Several RCC bits definition renamed to be compliant with the RCC specification.
- ADC_SingleConversion_TriggerTimer_DMA Project:
- Fix ADC resolution ( clock speed range was not aligned with ADC specification)
6.2. Released projects[edit source]
The STM32CubeMP1 Package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects. The main supported toolchain is STM32CubeIDE ( System Workbench for STM32 is no more promoted by ST).
- Most of STM32MP157C-DK2
projects are available with 4 IDEs ( STM32CubeIDE, SW4STM32, IAR, KEIL)
- All STM32MP157C-EV1
projects are still available on SW4STM32 (not yet ported on STM32CubeIDE) but these projects can be imported inside STM32CubeIDE.
The exhaustive list of projects is provided in the table List of Projects.
IDE ready projects :
STM32MP157C-DK2 | STM32MP157C-EV1 | |
---|---|---|
Number of projects | 28 | 29 |
6.3. Released components[edit source]
- Drivers
Component | Version | Notes |
---|---|---|
Cortex-M CMSIS | V5.4.0 | |
STM32MP1xx CMSIS | V1.3.0 | |
STM32MP1xx HAL | V1.3.0 | |
BSP STM32MP15xx_EVAL | V1.3.0 | |
BSP STM32MP15xx_DISCO | V1.3.0 |
- Middleware
Component | Version | Notes |
---|---|---|
FreeRTOS | V10.0.1 ST modified 20190719 | |
OpenAMP | v2018.10 ST modified 20200110 and ST interface 20200110 |
- Utilities
Component | Version | Notes |
---|---|---|
Resourcemanager | V1.11.0 |
6.4. Available drivers[edit source]
Please find below the list of available HAL and LL drivers :
6.4.1. HAL drivers[edit source]
Legend : HAL drivers added since ecosystem release ≥ v2.1.0
STM32CubeMP1 HAL Driver items | Description |
---|---|
ADC |
ADC) * peripheral: * + Initialization and de-initialization functions * ++ Initialization and Configuration of ADC * + Operation functions * ++ Start, stop, get result of conversions of regular * group, using 3 possible modes: polling, interruption or DMA. * + Control functions * ++ Channels configuration on regular group * ++ Analog Watchdog configuration * + State functions * ++ ADC state machine management * ++ Interrupts and flags management * + Operation functions * ++ Start, stop, get result of conversions of ADC group injected, * using 2 possible modes: polling, interruption. * ++ Calibration * +++ ADC automatic self-calibration * +++ Calibration factors get or set * ++ Multimode feature when available * + Control functions * ++ Channels configuration on ADC group injected * + State functions * ++ ADC group injected contexts queue management* This driver provides firmware functions to manage the following * functionalities of the Analog to Digital Convertor ( |
CEC |
CEC). * + Initialization and de-initialization function * + IO operation function * + Peripheral Control function* This driver provides firmware functions to manage the following * functionalities of the High Definition Multimedia Interface * Consumer Electronics Control Peripheral ( |
CRC |
CRC) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral State functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Cyclic Redundancy Check ( |
CORTEX |
MPU, Cache, …): * + Initialization and de-initialization functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the CORTEX ( |
CRYP |
CRYP) peripheral: * + Initialization and de-initialization functions * + AES processing functions * + DES processing functions * + TDES processing functions * + DMA callback functions * + CRYP IRQ handler management * + Peripheral State functions * + Extended AES processing functions* This driver provides firmware functions to manage the following * functionalities of the Cryptography ( |
DAC |
DAC) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Digital to Analog Converter ( |
DCMI |
DCMI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions* This driver provides firmware functions to manage the following * functionalities of the Digital Camera Interface ( |
DFSDM |
DFSDM) peripherals: * + Initialization and configuration of channels and filters * + Regular channels configuration * + Injected channels configuration * + Regular/Injected Channels DMA Configuration * + Interrupts and flags management * + Analog watchdog feature * + Short-circuit detector feature * + Extremes detector feature * + Clock absence detector feature * + Break generation on analog watchdog or short-circuit event * + Set and get pulses skipping on channel.* This driver provides firmware functions to manage the following * functionalities of the Digital Filter for Sigma-Delta Modulators * ( |
DMA |
DMA) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and errors functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access ( |
EXTI |
EXTI) peripheral: * + Initialization and de-initialization functions * + IO operation functions* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output ( |
FDCAN |
IO operation functions * + Peripheral Configuration and Control functions * + Peripheral State and Error functions* This driver provides firmware functions to manage the following * functionalities of the Flexible DataRate Controller Area Network * (FDCAN) peripheral: * + Initialization and de-initialization functions * + |
FMC |
* This driver provides a generic firmware to drive SRAM memories
* mounted as external device.
|
GPIO |
GPIO) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Extended Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output ( |
HAL |
HAL, Tick, SYSCFG, DBGMCU: * + Initialization and de-initialization functions * + HAL Initialization and de-initialization functions * + Configure the source of the time base * + HAL Control functions * + Tick management (get/set/inc/priority/suspend/resume) * + Get HAL revision, the device revision identifier, the device identifier * + Enable/Disable DBG wake up on AIEC * + Enable/Disable the Debug Module during Domain1 SLEEP mode * + Enable/Disable the Debug Module during Domain1 STOP mode * + Enable/Disable the Debug Module during Domain1 STANDBY mode * + Configure the internal voltage reference buffer voltage scale * + Configure the internal voltage reference buffer high impedance mode * + Tune the Internal Voltage Reference buffer (VREFBUF) * + Enable/Disable the Internal Voltage Reference buffer (VREFBUF) * + Ethernet PHY Interface Selection either MII or RMII * + Analog Switch control for dual analog pads * + Enable/Disable the booster to reduce the total harmonic distortion of the analog * + Enable/Power-down the I/O Compensation Cell * + To Enable/Disable optimize the I/O speed when the product voltage is low * + Code selection for the I/O Compensation cell* This driver provides firmware functions to manage the following * functionalities of |
HASH |
HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * + Peripheral State methods * + HASH or HMAC processing suspension/resumption * Additionally, this driver provides functions to manage HMAC * multi-buffer DMA-based processing for MD-5, SHA-1, SHA-224 * and SHA-256.* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral: * + Initialization and de-initialization methods * + HASH or |
HSEM |
* This driver provides firmware functions to manage the following
* functionalities of the semaphore peripheral:
* + Semaphore Take function (2-Step Procedure) , non blocking
* + Semaphore FastTake function (1-Step Procedure) , non blocking
* + Semaphore Status check
* + Semaphore Clear Key Set and Get
* + Release and release all functions
* + Semaphore notification enabling and disabling and callnack functions
* + IRQ handler management
|
I2C |
I2C) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Inter Integrated Circuit ( |
IPCC |
IPCC). * + Initialization and de-initialization functions * + Configuration, notification and interrupts handling * + Peripheral State and Error functions* This driver provides firmware functions to manage the following * functionalities of the Inter-Processor communication controller * peripherals ( |
LPTIM |
LPTIM) peripheral: * + Initialization and de-initialization functions. * + Start/Stop operation functions in polling mode. * + Start/Stop operation functions in interrupt mode. * + Reading operation functions. * + Peripheral State functions.* This driver provides firmware functions to manage the following * functionalities of the Low Power Timer ( |
MDIOS |
IO operation functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the MDIOS Peripheral. * + Initialization and de-initialization functions * + |
MDMA |
* This driver provides firmware functions to manage the following
* functionalities of the Master Direct Memory Access (MDMA) peripheral:
* + Initialization/de-initialization functions
* + I/O operation functions
* + Peripheral State and errors functions
|
PWR |
* This driver provides firmware functions to manage the following
* functionalities of the Power Controller (PWR) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Peripheral Extended features functions
|
QUADSPI |
* This driver provides firmware functions to manage the following
* functionalities of the QuadSPI interface (QSPI).
* + Initialization and de-initialization functions
* + Indirect functional mode management
* + Memory-mapped functional mode management
* + Auto-polling functional mode management
* + Interrupts and flags management
* + MDMA channel configuration for indirect functional mode
* + Errors management and abort functionality
|
RCC |
RCC) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Extended Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the Reset and Clock Control ( |
RNG |
RNG) peripheral: * + Initialization and configuration functions * + Peripheral Control functions * + Peripheral State functions* This driver provides firmware functions to manage the following * functionalities of the Random Number Generator ( |
RTC |
RTC) peripheral: * + Initialization/de-initialization functions * + Calendar (Time and Date) configuration * + Alarms (Alarm A and Alarm B) configuration * + WakeUp Timer configuration * + TimeStamp configuration * + Tampers configuration * + Backup Data Registers configuration * + RTC Tamper and TimeStamp Pins Selection * + Interrupts and flags management* This driver provides firmware functions to manage the following * functionalities of the Real-Time Clock ( |
SAI |
SAI) peripheral: * + Initialization/de-initialization functions * + I/O operation functions * + Peripheral Control functions * + Peripheral State functions * + Modify PDM microphone delays.* This driver provides firmware functions to manage the following * functionalities of the Serial Audio Interface ( |
SD |
SD) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the Secure Digital ( |
SMARTCARD |
IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Extended features functions* This driver provides firmware functions to manage the following * functionalities of the SMARTCARD peripheral: * + Initialization and de-initialization functions * + |
SMBUS |
SMBus) peripheral, * based on I2C principles of operation : * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions* This driver provides firmware functions to manage the following * functionalities of the System Management Bus ( |
SPDIFRX |
DMA transfers management * + Interrupts and flags management* This driver provides firmware functions to manage the following * functionalities of the SPDIFRX audio interface: * + Initialization and Configuration * + Data transfers functions * + |
SPI |
SPI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + IO operation functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the Serial Peripheral Interface ( |
TIMER |
DMA * + Time Output Compare/PWM Initialization * + Time Output Compare/PWM Channel Configuration * + Time Output Compare/PWM Start * + Time Output Compare/PWM Start Interruption * + Time Output Compare/PWM Start DMA * + Time Input Capture Initialization * + Time Input Capture Channel Configuration * + Time Input Capture Start * + Time Input Capture Start Interruption * + Time Input Capture Start DMA * + Time One Pulse Initialization * + Time One Pulse Channel Configuration * + Time One Pulse Start * + Time Encoder Interface Initialization * + Time Encoder Interface Start * + Time Encoder Interface Start Interruption * + Time Encoder Interface Start DMA * + Commutation Event configuration with Interruption and DMA * + Time OCRef clear configuration * + Time External Clock configuration * + Time Hall Sensor Interface Initialization * + Time Hall Sensor Interface Start * + Time Complementary signal bread and dead time configuration * + Time Master and Slave synchronization configuration * + Time Output Compare/PWM Channel Configuration (for channels 5 and 6) * + Time OCRef clear configuration * + Timer remapping capabilities configuration* This driver provides firmware functions to manage the following * functionalities of the Timer (TIM) peripheral: * + Time Base Initialization * + Time Base Start * + Time Base Start Interruption * + Time Base Start |
U(S)ART |
ART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Peripheral Control functions* This driver provides firmware functions to manage the following * functionalities of the Universal (Synchronous) Asynchronous Receiver Transmitter * Peripheral (U(S) |
WWDG |
IO operation functions* This driver provides firmware functions to manage the following * functionalities of the Window Watchdog (WWDG) peripheral: * + Initialization and Configuration functions * + |
6.4.2. LL drivers[edit source]
STM32CubeMP1 LL Driver items | Description |
---|---|
ADC |
ADC peripheral: * + Initialization/de-initialization functions * + Configuration functions (ADC instance, group regular, group injected, * channels, analog watchdog, oversampling, multimode) * + IT/FLAGS management functions* This driver provides firmware functions to manage the following * functionalities of the |
BUS |
* This driver provides firmware functions to manage the following
* functionalities of the BUS peripheral:
* + Enable/disable/reset clocks for all system BUS (AHB2, AHB3, AHB4, AHB5, AHB6,
* AXI, MLAHB, APB1, APB2, APB3, APB4, APB5)
|
CORTEX |
SYSTICK configuration used by @ref LL_mDelay and @ref LL_Init1msTick functions * + Low power mode configuration (SCB register of Cortex-MCU) * + API to access to MCU info (CPUID register)* This driver contains a set of generic APIs that can be used by user: * + |
DMA |
DMA peripheral: * + Initialization/de-initialization functions * + Configuration functions * + IT/FLAGS management functions* This driver provides firmware functions to manage the following * functionalities of the |
DMAMUX |
* This driver provides firmware functions to manage the following
* functionalities of the DMAMUX peripheral:
* + Initialization/de-initialization functions
* + IT/FLAGS management functions
|
EXTI |
EXTI peripheral: * + Initialization/de-initialization functions * + IT/FLAGS/Trigger management functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
FMC |
* This driver provides firmware functions to manage the following
* functionalities of the PSRAM peripheral:
* + Initialization/de-initialization functions
* + Timing management functions
* + Configuration functions
|
GPIO |
GPIO peripheral: * + Initialization/de-initialization functions * + Data access functions * + Port configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
HSEM |
HSEM peripheral: * + IT/FLAGS management functions * +Data management functions* This driver provides firmware functions to manage the following * functionalities of the |
I2C |
I2C peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * +Data management functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
IPCC |
IPCC peripheral: * + IT/FLAGS management functions * + Enable/disable transmit and receive channels functions* This driver provides firmware functions to manage the following * functionalities of the |
LPTIM |
LPTIM peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Configuration (Trigger / Clock / Encoder / LPTIM) functions* This driver provides firmware functions to manage the following * functionalities of the |
PWR |
* This driver provides firmware functions to manage the following
* functionalities of the PWR peripheral:
* + Initialization/de-initialization functions
* + FLAGS management functions
* + Configuration functions
|
RCC |
RCC peripheral: * + Clocks management functions (HSE/HSI/CSI/LSE/LSI/MCO/PLL) * + RTC/TIMERS functions * + IT/FLAGS management functions * + De-initialization functions * + Get system and peripherals clocks frequency functions* This driver provides firmware functions to manage the following * functionalities of the |
RTC |
RTC peripheral: * + Initialization/de-initialization functions * + TIME/DATE/ALM functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
SPI |
SPI peripheral: * + Initialization/de-initialization functions * + IT/FLAGS management functions * + Data / DMA management functions * + Configuration functions* This driver provides firmware functions to manage the following * functionalities of the |
SYSTEM |
SYSCFG and DBGMCU functions* This driver provides firmware functions to manage the following * functionalities of the SYSTEM peripheral: * + |
TIM |
DMA Burst Mode ) * + Counter clock selection functions * + Timer input remapping functions * + IT/FLAGS management functions * + DMA management functions * + Event management functions* This driver provides firmware functions to manage the following * functionalities of the TIM peripheral: * + Initialization/de-initialization functions * + Configuration functions (Time base, Capture Compare, Output and Input Channel, * Timer Synchro, Break, |
USART |
USART peripheral: * + Initialization/de-initialization functions * + Configuration functions (Irda, Smartcard, Half duplex, * SPI Slave, LIN, Driver enable) * + Advanced configurations services functions * + IT/FLAGS management functions * + DMA management functions * + Data management functions * + Execution functions* This driver provides firmware functions to manage the following * functionalities of the |
UTILS |
* This driver provides firmware functions to manage the following
* functionalities of the UTILS peripheral:
* + Device Electronic Signature functions
* + DELAY functions
* + SYSTEM functions
|
WWDG |
* This driver provides firmware functions to manage the following
* functionalities of the WWDG peripheral:
* + Enable / Disable functions
* + Configuration functions
* + IT/FLAGS management functions
|
6.5. Available projects[edit source]
Please find below the list of projects available for STM32MP157C-EV1 Evaluation board and STM32MP157C-DK2 Discovery kit
:
The preferred supported toolchain for STM32MP15 is now STM32CubeIDE (All-in-one multi-OS development tool).
All the projects are available with System Workbench for STM32 (inherited from first release), but the projects can be imported inside STM32CubeIDE.
Moreover, other toolchains are now compliant with STM32CubeMP1 Package :
- IAR Embedded Workbench for ARM (EWARM) toolchain,
- RealView Microcontroller Development Kit (MDK-ARM) toolchain,
By default, all the examples are available with SW4STM32. The migration on other toolchain is not yet finished, but some of them are available :
- Legend:
- (**) : List of STM32MP157C-DK2
examples available with 4 IDEs ( SW4STM32, STM32CubeIDE, IAR, KEIL), the others are only available with SW4STM32 for the moment.
- (*) : List of STM32MP157C-EV1
examples available with 4 IDEs ( SW4STM32, STM32CubeIDE, IAR, KEIL), the others are only available with SW4STM32 for the moment.
- (**) : List of STM32MP157C-DK2
7. Minor release updates[edit source]
STMicroelectronics regularly delivers corrections through github® components. You can decide to incorporate them into your developer package or distribution package.
- Please refer to STM32MP1 Developer Package or How to switch to github® mode in distribution package.
8. How to get started with STM32CubeMP1 Package[edit source]
- Please refer to How to get software and start with this release
9. Associated tools[edit source]
- Please refer to Referenced tools release notes to obtain more information on all available tools.
10. References[edit source]