Last edited 4 years ago

Arm CoreSight overview

1. Article purpose[edit source]

The purpose of this article is to provide information on the Arm® CoreSight hardware subsystem.
It explains what are the principle peripherals of this subsystem.

2. Peripheral overview[edit source]

Arm® CoreSight products include a wide range of trace macrocells for Arm® processors, system and software instrumentation and a comprehensive set of IP blocks to enable the debug and trace of the most complex, multi-core SoCs. Arm® has defined an open CoreSight architecture to allow SoC designers to add "debug and trace" capabilities for other IP cores in to the CoreSight infrastructure.

Alternate text
CoreSight overview

2.1. Components description[edit source]

The debug features are based on Arm® CoreSight™ components:
• SWJ-DP: JTAG/Serial-wire debug port
• AXI-AP: AXI access port
AHB-AP: AHB access port
APB-AP: APB access port
ITM: Instrumentation Trace Macrocell
• DWT: Data Watchpoint and Trace
ETM: Embedded Trace Macrocell
• ETF: Embedded Trace FIFO
• TPIU: Trace Port Interface Unit
• SWO: Serial Wire Output
• CTI: Cross Trigger Interface
• CTM: Cross Trigger Matrix
• TSGEN: Timestamp Generator
STM: System Trace Macrocell
More information about these components can be found in the Arm® website [1]

2.2. Features[edit source]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

3. References[edit source]