- Last edited 2 years ago ago
How to setup wifi connection
Contents
Even if the example is related to the RTL8723BU chip (this chip calls for a WiFi (minimally 802.11g/n) and Bluetooth 4.0 LE), most of the commands are generic ones and can be applied to any platform.
1 ifconfig[edit]
Verify the wlan0 interface is present (that means drivers have been started and the WiFi firmware loaded):
1.1 Check WLAN interface[edit]
ifconfig -a lo Link encap:Local Loopback LOOPBACK MTU:65536 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:1 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:10 (10.0 B)
1.2 Initialize WLAN interface[edit]
ifconfig wlan0 192.168.43.135 broadcast 192.168.43.255 netmask 255.255.255.0
ifconfig wlan0 up
ifconfig wlan0 wlan0 Link encap:Ethernet HWaddr 60:F1:89:3F:F6:0E inet addr:192.168.43.135 Bcast:192.168.43.255 Mask:255.255.255.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 /* UP indicate that your interface is UP */ RX packets:19 errors:0 dropped:0 overruns:0 frame:0 TX packets:19 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:1774 (1.7 KiB) TX bytes:2326 (2.2 KiB)
2 iw[edit]
The next phase is to scan for any wireless access points with the command:
2.1 Scan available SSID (AP)[edit]
- Get only SSID name
iw dev wlan0 scan |grep SSID SSID: NETWORK1 SSID: NETWORK2
- List full SSID information
iw dev wlan0 scan BSS 00:23:5e:4a:28:f9(on wlan0) TSF: 0 usec (0d, 00:00:00) freq: 2412 beacon interval: 100 TUs capability: ESS ShortPreamble ShortSlotTime (0x0421) signal: -72.00 dBm last seen: 0 ms ago SSID: NETWORK1 Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0 DS Parameter set: channel 1 TIM: DTIM Count 0 DTIM Period 1 Bitmap Control 0x0 Bitmap[0] 0x2 Country: FR Environment: Indoor/Outdoor Channels [1 - 13] @ 20 dBm BSS Load: * station count: 1 * channel utilisation: 30/255 * available admission capacity: 23437 [*32us] ERP: <no flags> Extended supported rates: 24.0 36.0 48.0 54.0 WMM: * Parameter version 1 * u-APSD * BE: CW 15-1023, AIFSN 3 * BK: CW 15-1023, AIFSN 7 * VI: CW 7-15, AIFSN 2, TXOP 3008 usec * VO: CW 3-7, AIFSN 2, TXOP 1504 usec BSS 00:23:5e:96:57:20(on wlan0) TSF: 0 usec (0d, 00:00:00) freq: 2412 beacon interval: 100 TUs capability: ESS Privacy ShortPreamble ShortSlotTime (0x0431) signal: -66.00 dBm last seen: 0 ms ago SSID: NETWORK2 Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0 DS Parameter set: channel 1 Country: FR Environment: Indoor/Outdoor Channels [1 - 13] @ 20 dBm BSS Load: * station count: 8 * channel utilisation: 48/255 * available admission capacity: 23437 [*32us] ERP: <no flags> RSN: * Version: 1 * Group cipher: CCMP * Pairwise ciphers: CCMP * Authentication suites: IEEE 802.1X 00-40-96:0 * Capabilities: 4-PTKSA-RC 4-GTKSA-RC (0x0028) Extended supported rates: 24.0 36.0 48.0 54.0 WMM: * Parameter version 1 * u-APSD * BE: CW 15-1023, AIFSN 3 * BK: CW 15-1023, AIFSN 7 * VI: CW 7-15, AIFSN 2, TXOP 3008 usec * VO: CW 3-7, AIFSN 2, TXOP 1504 usec
3 Wlan Network attachment (without system which manage systemd-networkd configuration)[edit]
3.1 Configure your WiFi connection[edit]
Configure WiFi connection by using wpa_supplicant tool
- Check current configuration
cat /etc/wpa_supplicant.conf ctrl_interface=/var/run/wpa_supplicant ctrl_interface_group=0 update_config=1 network={ key_mgmt=NONE }
- Set the WiFi network name and password
wpa_passphrase <your_ssid_name> <your_ssid_key> >> /etc/wpa_supplicant.conf
- Check new configuration
cat /etc/wpa_supplicant.conf
ctrl_interface=/var/run/wpa_supplicant
ctrl_interface_group=0
update_config=1
network={
ssid="your_ssid_name"
psk="your_ssid_key"
}
3.1.1 Connect to SSID[edit]
wpa_supplicant -B -iwlan0 -c /etc/wpa_supplicant.conf Successfully initialized wpa_supplicant
3.1.2 link to SSID[edit]
iw wlan0 link SSID: NETWORK1 freq: 2462 RX: 501 bytes (3 packets) TX: 4056 bytes (22 packets) signal: -75 dBm tx bitrate: 12.0 MBit/s bss flags: short-preamble short-slot-time dtim period: 1 beacon int: 100
3.1.3 Assign IP address to WLAN interface[edit]
Use the DHCP client to obtain an address (assuming wireless network (associated to) has a DHCP server):
dhclient wlan0
Use the ip command to verify the IP address assigned by the DHCP. The IP address is 192.168.43.135 from below.
ip addr show wlan0
3: wlan0: mtu 1500 qdisc mq state UP qlen 1000
link/ether 74:e5:43:a1:ce:65 brd ff:ff:ff:ff:ff:ff
inet 192.168.43.135/24 brd 192.168.1.255 scope global wlan0
inet6 fe80::76e5:43ff:fea1:ce65/64 scope link
valid_lft forever preferred_lft forever
3.1.4 Check connectivity[edit]
The most basic connectivity test is to use the “ping” command. In this example, the wireless router (associated to) has an IP address of 192.168.43.1:
ping 192.168.43.1 PING 192.168.43.1 (192.168.43.1): 56 data bytes 64 bytes from 192.168.43.1: seq=0 ttl=64 time=14.905 ms 64 bytes from 192.168.43.1: seq=1 ttl=64 time=30.387 ms 64 bytes from 192.168.43.1: seq=2 ttl=64 time=20.462 ms
- Note : Enter <CTRL+C> to terminate the ping session.
4 Automatic WiFi configuration at start up[edit]
4.1 networkctl[edit]
Systemd has a specific service for the network named systemd-networkd, this service comes with the tool networkctl which allows to show the status of each network interface.
networkctl --no-pager IDX LINK TYPE OPERATIONAL SETUP 1 lo loopback carrier unmanaged 2 eth0 ether routable configured 3 sit0 sit no-carrier unmanaged 4 ip6tnl0 tunnel6 no-carrier unmanaged 5 wlan0 wlan no-carrier unmanaged 6 wlan1 wlan no-carrier unmanaged
6 links listed.
We can see that the eth0 interface is managed by networked via the information configured and the interface is used (routable).
4.2 How to set a wireless configuration with networkd[edit]
The goal is to configure an wlan network interface via systemd-networkd configuration.
All the network configurations are stored on /lib/systemd/network or /etc/systemd/network
Create the file dedicated to wireless interface "/lib/systemd/network/51-wireless.network" :
echo "[Match]" > /lib/systemd/network/51-wireless.network
echo "Name=wlan0" >> /lib/systemd/network/51-wireless.network
echo "[Network]" >> /lib/systemd/network/51-wireless.network
echo "DHCP=ipv4" >> /lib/systemd/network/51-wireless.network
Check content is as follow
cat /lib/systemd/network/51-wireless.network
[Match]
Name=wlan0
[Network]
DHCP=ipv4
For attaching this wireless interface to a specific network, we need to have some information like SSID of network and password.
To see the list of wireless network available:
ifconfig wlan0 up iw dev wlan0 scan |grep SSID SSID: NETWORK1 SSID: NETWORK2
Associate the wireless network to wireless interface, here wlan0:
mkdir -p /etc/wpa_supplicant/ echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf wpa_passphrase SSID_OF_NETWORK PASSWORD_OF_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
Where SSID_OF_NETWORK PASSWORD_OF_NETWORK correspond to the SSID and password of wireless network.
To enable and start the wireless configuration:
systemctl enable wpa_supplicant@wlan0.service systemctl restart systemd-networkd.service systemctl restart wpa_supplicant@wlan0.service