This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Overview
gst-typefind (gst-typefind-1.0) is a GStreamer command line utility.
This utility parses a file with multimedia content in order to provide the type of media.
2. Usage
gst-typefind accepts the following options:
gst-typefind-1.0 --help
gst-typefind-1.0 --help
Usage:
gst-typefind-1.0 [OPTION?] FILES
Help Options:
-h, --help Show help options
--help-all Show all help options
--help-gst Show GStreamer Options
Application Options:
--version Print version information and exit
By default a short level of information is given such as mimetype and other key characteristics like with or height of an image file. Example:
gst-typefind-1.0 rose-flower-blossom-bloom-39517.jpeg
rose-flower-blossom-bloom-39517.jpeg - image/jpeg, width=(int)3482, height=(int)2321, sof-marker=(int)0
See gst-typefind man page for more details and additional options.