Approved version. Approved on: 08:01, 7 October 2019
- Last edited 3 years ago ago
DRM KMS troubleshooting grid
Some typical issues related to the DRM/KMS framework are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try also looking in the articles in the DRM/KMS or troubleshooting grids categories.
Symptom | Resolution |
---|---|
./myQtApplication Could not queue DRM page flip! (Permission denied) Could not queue DRM page flip! (Permission denied) |
The psplash-drm userland splash screen is running and is then the DRM master, avoiding other DRM applications to access to DRM/KMS. Please stop this psplash-drm application with the command below before running your use case: psplash-drm-quit Note: You may need to enter "export QT_QPA_EGLFS_ALWAYS_SET_MODE=1" before running your Qt application, please refer to the Qt documentation. |