Difference between revisions of "X-LINUX-AI - object detection using Coral Edge TPU TensorFlow Lite C++ API"

[unchecked revision] [quality revision]
m
m
 

This article explains how to experiment with Coral Edge TPU[1] applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.

1 Description[edit]

The object detection[2] neural network model allows identification and localization of a known object within an image.

C/C++ Coral Edge TPU object detection application

The application demonstrate demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model executed on the Coral Edge TPU[1] using the TensorFlow Lite C++ API.
A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute a neural network inference (using appsink).
The result of the inference is displayed on the preview. The overlay is done using GTK widget GtkWidget with cairo.
This combination is quite simple and efficient in term terms of CPU consumptionoverhead.

The model used with this application is the COCO SSD MobileNet v1 downloaded from the object detection overview[2] and converted for the Coral Edge TPU.

2 Installation[edit]

2.1 Install from the OpenSTLinux AI package repository[edit]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package you can install X-LINUX-AI components for this application:

Board $> apt-get install tflite-cv-apps-edgetpu-object-detection-c++

And Then restart the demo launcher:

Board $> systemctl restart weston@root

2.2 Source code location[edit]

  • in the Openembedded OpenSTLinux distributionDistribution:
<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src
  • on GitHub:
https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfell/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src

2.3 Re-generate the package from OpenSTLinux distribution Distribution (optional)[edit]

Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.

Info white.png Information
If not already installed, the X-LINUX-AI OpenSTLinux distribution Distribution need to be installed by following this link


  • Set up the build environment:
PC $> cd <Distribution Package installation directory>
PC $> source layers/meta-st/scripts/envsetup.sh
  • Rebuild the application:
PC $> bitbake tflite-cv-apps-edgetpu-object-detection-c++ -c compile

The generated binary is available here:

<Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-edgetpu-object-detection-c++/1.0-r0/tflite-cv-apps-edgetpu-object-detection-c++-1.0/object-detection/src

3 How to use itthe application[edit]

3.1 Launch application Launching via the demo launcher[edit]

Launch cpp tfl edgetpu object detection.png

3.2 Or execute Execute with the command line[edit]

The objdetect_tfl_edgetpu_gst_gtk C/C++ application is located in the userfs partition:

/usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/objdetect_tfl_edgetpu_gst_gtk

It accepts the following input parameters:

Usage: ./objdetect_tfl_edgetpu_gst_gtk -m <model .tflite> -l <label .txt file>                                                        
                                                                                                                                      
-m --model_file <.tflite file path>:  .tflite model to be executed                                                                    
-l --label_file <label file path>:    name of file containing labels                                                                  
-i --image <directory path>:          image directory with image to be classified                                                     
-v --video_device <n>:                video device (default /dev/video0)                                                              
--crop:                               if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized, 
                                      else the nn imput image is only resized to the nn input size (could cause picture deformation). 
--frame_width  <val>:                 width of the camera frame (default is 640)                                                      
--frame_height <val>:                 height of the camera frame (default is 480)                                                     
--framerate <val>:                    framerate of the camera (default is 15fps)                                                      
--input_mean <val>:                   model input mean (default is 127.5)                                                             
--input_std  <val>:                   model input standard deviation (default is 127.5)                                               
--help:                               show this help   

3.3 Testing with COCO SSD MobileNet V1[edit]

The model used for test is the detect_edgetpu.tflite downloaded from the object detection overview[2] and converted for the Coral Edge TPU. If you are interested, please take a look on at how this model has been converted.

Info white.png Information
The different objects the neural network is able to detect are listed in the labels.txt file located in the target:

/usr/local/demo-ai/computer-vision/models/coco_ssd_mobilenet/labels.txt


To ease launching of the application, two shell scripts are available:

  • launch object detection based on camera frame inputs
Board $>/usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/launch_bin_objdetect_tfl_edgetpu_coco_ssd_mobilenet.sh
  • launch object detection based on the pictures located in /usr/local/demo-ai/computer-vision/models/mobilenet/testdata directory
Board $> /usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/launch_bin_objdetect_tfl_edgetpu_coco_ssd_mobilenet.sh
Info white.png Information
Note that you need to populate the testdata directory with your own data sets.

The pictures are then randomly read from the testdata directory

4 References[edit]


This article explains how to experiment with {{Highlight|'''Coral Edge TPU'''<ref name=edgetpu_url>[https://coral.ai/ Coral Edge TPU]</ref>}} applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.

==Description==
The '''object detection'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref> neural network model allows identification and localization of a known object within an image.

[[File: cpp_tfl_edgetpu_object_detection_application_screenshot.png|thumb|upright=2|center|link=|C/C++ Coral Edge TPU object detection application]]

The application demonstratedemonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model executed on the {{Highlight|'''Coral Edge TPU'''<ref name=edgetpu_url></ref>}} using the TensorFlow Lite C++ API.<br>
A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute a neural network inference (using appsink).<br>

The result of the inference is displayed on the preview. The overlay is done using GTK widget GtkWidget with cairo.<br>

This combination is quite simple and efficient in termterms of CPU consumptionoverhead.<br>


The model used with this application is the {{Highlight|COCO SSD MobileNet v1}} downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref> and converted for the Coral Edge TPU.

==Installation==
===Install from the OpenSTLinux AI package repository===
{{Warning|{{SoftwareLicenseAgreement | distribution=X-LINUX-AI}}}}
After having [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure the AI OpenSTLinux package repository|configured the AI OpenSTLinux package]] you can install X-LINUX-AI components for this application:
 {{Board$}} apt-get install tflite-cv-apps-edgetpu-object-detection-c++AndThen restart the demo launcher:
 {{Board$}} systemctl restart weston@root

===Source code location===
* in the Openembedded OpenSTLinux distributionDistribution:
:'''<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src'''
* on GitHub:
:https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfell/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src

===Re-generate the package from OpenSTLinux distributionDistribution (optional)===
Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.

{{Info|If not already installed, the X-LINUX-AI OpenSTLinux distributionDistribution need to be installed by following this [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Re-generate_X-LINUX-AI_OpenSTLinux_distribution|link]]}}

* Set up the build environment:
 {{PC$}} cd <Distribution Package installation directory>

 {{PC$}} source layers/meta-st/scripts/envsetup.sh
* Rebuild the application:
 {{PC$}} bitbake tflite-cv-apps-edgetpu-object-detection-c++ -c compile
The generated binary is available here:<Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-edgetpu-object-detection-c++/1.0-r0/tflite-cv-apps-edgetpu-object-detection-c++-1.0/object-detection/src

==How to use it==
===Launch application the application==
===Launching via the demo launcher===
[[File: launch_cpp_tfl_edgetpu_object_detection.png|thumb|upright=2|center|link=]]

===Or execute Execute with the command line===
The '''objdetect_tfl_edgetpu_gst_gtk''' C/C++ application is located in the userfs partition:
 /usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/objdetect_tfl_edgetpu_gst_gtk
It accepts the following input parameters:
<pre>

Usage: ./objdetect_tfl_edgetpu_gst_gtk -m <model .tflite> -l <label .txt file>                                                        


-m --model_file <.tflite file path>:  .tflite model to be executed                                                                    
-l --label_file <label file path>:    name of file containing labels                                                                  
-i --image <directory path>:          image directory with image to be classified                                                     
-v --video_device <n>:                video device (default /dev/video0)                                                              
--crop:                               if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized, 
                                      else the nn imput image is only resized to the nn input size (could cause picture deformation). 
--frame_width  <val>:                 width of the camera frame (default is 640)                                                      
--frame_height <val>:                 height of the camera frame (default is 480)                                                     
--framerate <val>:                    framerate of the camera (default is 15fps)                                                      
--input_mean <val>:                   model input mean (default is 127.5)                                                             
--input_std  <val>:                   model input standard deviation (default is 127.5)                                               
--help:                               show this help   </pre>


===Testing with COCO SSD MobileNet V1===
The model used for test is the {{Highlight|detect_edgetpu.tflite}} downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url></ref> and converted for the Coral Edge TPU. If you are interested, please take a look onat [[How to compile model and run inference on Coral Edge TPU using STM32MP1#Example: compile an object detection model|how this model has been converted.]]

{{Info|The different objects the neural network is able to detect are listed in the labels.txt file located in the target:
/usr/local/demo-ai/computer-vision/models/coco_ssd_mobilenet/labels.txt}}

To ease launching of the application, two shell scripts are available:
* launch object detection based on camera frame inputs
 {{Board$}}/usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/launch_bin_objdetect_tfl_edgetpu_coco_ssd_mobilenet.sh

*launch object detection based on the pictures located in '''/usr/local/demo-ai/computer-vision/models/mobilenet/testdata''' directory
 {{Board$}} /usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/launch_bin_objdetect_tfl_edgetpu_coco_ssd_mobilenet.sh

{{Info|Note that you need to populate the testdata directory with your own data sets.<br>

The pictures are then randomly read from the testdata directory}}

==References==<references />

<noinclude>

[[Category:Artificial intelligence sample apps|25]]
{{PublicationRequestId | 16541 | 24Jun'20}}</noinclude>
Line 1: Line 1:
This article explains how to experiment{{Highlight|'''Coral Edge TPU'''<ref name=edgetpu_url>[https://coral.ai/ Coral Edge TPU]</ref>}} applications for object detection based on COCO SSD MobileNet v1 model using TensorFlow Lite C++ API.
+
This article explains how to experiment with {{Highlight|'''Coral Edge TPU'''<ref name=edgetpu_url>[https://coral.ai/ Coral Edge TPU]</ref>}} applications for object detection based on the COCO SSD MobileNet v1 model using the TensorFlow Lite C++ API.
   
 
==Description==
 
==Description==
Line 6: Line 6:
 
[[File: cpp_tfl_edgetpu_object_detection_application_screenshot.png|thumb|upright=2|center|link=|C/C++ Coral Edge TPU object detection application]]
 
[[File: cpp_tfl_edgetpu_object_detection_application_screenshot.png|thumb|upright=2|center|link=|C/C++ Coral Edge TPU object detection application]]
   
The application demonstrate a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model executed on the {{Highlight|'''Coral Edge TPU'''<ref name=edgetpu_url></ref>}} using the TensorFlow Lite C++ API.<br>
+
The application demonstrates a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model executed on the {{Highlight|'''Coral Edge TPU'''<ref name=edgetpu_url></ref>}} using the TensorFlow Lite C++ API.<br>
Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute neural network inference (using appsink).<br>
+
A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute a neural network inference (using appsink).<br>
The result of the inference is displayed on the preview. The overlay is done using GTK widget with cairo.<br>
+
The result of the inference is displayed on the preview. The overlay is done using GtkWidget with cairo.<br>
This combination is quite simple and efficient in term of CPU consumption.<br>
+
This combination is quite simple and efficient in terms of CPU overhead.<br>
   
 
The model used with this application is the {{Highlight|COCO SSD MobileNet v1}} downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref> and converted for the Coral Edge TPU.
 
The model used with this application is the {{Highlight|COCO SSD MobileNet v1}} downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url>[https://www.tensorflow.org/lite/models/object_detection/overview TFLite object detection overview]</ref> and converted for the Coral Edge TPU.
Line 18: Line 18:
 
After having [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure the AI OpenSTLinux package repository|configured the AI OpenSTLinux package]] you can install X-LINUX-AI components for this application:
 
After having [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure the AI OpenSTLinux package repository|configured the AI OpenSTLinux package]] you can install X-LINUX-AI components for this application:
 
  {{Board$}} apt-get install tflite-cv-apps-edgetpu-object-detection-c++
 
  {{Board$}} apt-get install tflite-cv-apps-edgetpu-object-detection-c++
And restart the demo launcher:
+
Then restart the demo launcher:
 
  {{Board$}} systemctl restart weston@root
 
  {{Board$}} systemctl restart weston@root
   
 
===Source code location===
 
===Source code location===
* in the Openembedded OpenSTLinux distribution:
+
* in the Openembedded OpenSTLinux Distribution:
 
:'''<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src'''
 
:'''<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src'''
 
* on GitHub:
 
* on GitHub:
 
:https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfell/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src
 
:https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfell/recipes-samples/tflite-cv-apps-edgetpu/files/object-detection/src
   
===Re-generate the package from OpenSTLinux distribution (optional)===
+
===Re-generate the package from OpenSTLinux Distribution (optional)===
 
Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.
 
Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.
   
{{Info|If not already installed, the X-LINUX-AI OpenSTLinux distribution need to be installed by following this [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Re-generate_X-LINUX-AI_OpenSTLinux_distribution|link]]}}
+
{{Info|If not already installed, the X-LINUX-AI OpenSTLinux Distribution need to be installed by following this [[X-LINUX-AI_OpenSTLinux_Expansion_Package#Re-generate_X-LINUX-AI_OpenSTLinux_distribution|link]]}}
   
   
Line 41: Line 41:
 
  <Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-edgetpu-object-detection-c++/1.0-r0/tflite-cv-apps-edgetpu-object-detection-c++-1.0/object-detection/src
 
  <Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-edgetpu-object-detection-c++/1.0-r0/tflite-cv-apps-edgetpu-object-detection-c++-1.0/object-detection/src
   
==How to use it==
+
==How to use the application==
===Launch application via the demo launcher===
+
===Launching via the demo launcher===
 
[[File: launch_cpp_tfl_edgetpu_object_detection.png|thumb|upright=2|center|link=]]
 
[[File: launch_cpp_tfl_edgetpu_object_detection.png|thumb|upright=2|center|link=]]
   
===Or execute with command line===
+
===Execute with the command line===
 
The '''objdetect_tfl_edgetpu_gst_gtk''' C/C++ application is located in the userfs partition:
 
The '''objdetect_tfl_edgetpu_gst_gtk''' C/C++ application is located in the userfs partition:
 
  /usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/objdetect_tfl_edgetpu_gst_gtk
 
  /usr/local/demo-ai/computer-vision/tflite-object-detection-edgetpu/bin/objdetect_tfl_edgetpu_gst_gtk
Line 68: Line 68:
   
 
===Testing with COCO SSD MobileNet V1===
 
===Testing with COCO SSD MobileNet V1===
The model used for test is the {{Highlight|detect_edgetpu.tflite}} downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url></ref> and converted for the Coral Edge TPU. If you are interested, please take a look on [[How to compile model and run inference on Coral Edge TPU using STM32MP1#Example: compile an object detection model|how this model has been converted.]]
+
The model used for test is the {{Highlight|detect_edgetpu.tflite}} downloaded from the '''object detection overview'''<ref name=tflite_obj_detect_url></ref> and converted for the Coral Edge TPU. If you are interested, please take a look at [[How to compile model and run inference on Coral Edge TPU using STM32MP1#Example: compile an object detection model|how this model has been converted.]]
   
 
{{Info|The different objects the neural network is able to detect are listed in the labels.txt file located in the target:
 
{{Info|The different objects the neural network is able to detect are listed in the labels.txt file located in the target: